MCUXpresso SDK API Reference Manual  Rev 2.16.100
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Clock Driver

Overview

The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.

The clock driver supports:

Files

file  fsl_clock.h
 

Data Structures

struct  firc_trim_config_t
 firc trim configuration. More...
 
struct  sirc_trim_config_t
 sirc trim configuration. More...
 

Macros

#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0U
 Configure whether driver controls clock. More...
 
#define CLK_GATE_REG_OFFSET(value)   (((uint32_t)(value)) >> 16U)
 Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More...
 
#define AOI_CLOCKS
 Clock ip name array for AOI. More...
 
#define CRC_CLOCKS
 Clock ip name array for CRC. More...
 
#define CTIMER_CLOCKS
 Clock ip name array for CTIMER. More...
 
#define DMA_CLOCKS
 Clock ip name array for DMA. More...
 
#define EDMA_CLOCKS
 Clock gate name array for EDMA. More...
 
#define ERM_CLOCKS
 Clock ip name array for ERM. More...
 
#define EIM_CLOCKS
 Clock ip name array for EIM. More...
 
#define FREQME_CLOCKS
 Clock ip name array for FREQME. More...
 
#define GPIO_CLOCKS
 Clock ip name array for GPIO. More...
 
#define I3C_CLOCKS
 Clock ip name array for I3C.
 
#define INPUTMUX_CLOCKS
 Clock ip name array for INPUTMUX. More...
 
#define LPCMP_CLOCKS
 Clock ip name array for GPIO. More...
 
#define LPADC_CLOCKS
 Clock ip name array for LPADC. More...
 
#define LPUART_CLOCKS
 Clock ip name array for LPUART. More...
 
#define LPI2C_CLOCKS
 Clock ip name array for LPI2C. More...
 
#define LPSPI_CLOCKS
 Clock ip name array for LSPI. More...
 
#define MTR_CLOCKS
 Clock ip name array for MTR. More...
 
#define OSTIMER_CLOCKS
 Clock ip name array for OSTIMER. More...
 
#define PWM_CLOCKS
 Clock ip name array for PWM. More...
 
#define QDC_CLOCKS
 Clock ip name array for QDC. More...
 
#define UTICK_CLOCKS
 Clock ip name array for UTICK. More...
 
#define WWDT_CLOCKS
 Clock ip name array for WWDT. More...
 
#define BUS_CLK   kCLOCK_BusClk
 Peripherals clock source definition. More...
 
#define CLK_ATTACH_REG_OFFSET(value)   (((uint32_t)(value)) >> 16U)
 Clock Mux Switches The encoding is as follows each connection identified is 32bits wide while 24bits are valuable starting from LSB upwards. More...
 

Enumerations

enum  clock_ip_name_t {
  kCLOCK_GateINPUTMUX0 = (0x00000U | (0U)),
  kCLOCK_InputMux = (0x00000U | (0U)),
  kCLOCK_GateI3C0 = (0x00000U | (1U)),
  kCLOCK_GateCTIMER0 = (0x00000U | (2U)),
  kCLOCK_GateCTIMER1 = (0x00000U | (3U)),
  kCLOCK_GateCTIMER2 = (0x00000U | (4U)),
  kCLOCK_GateFREQME = (0x00000U | (5U)),
  kCLOCK_GateUTICK0 = (0x00000U | (6U)),
  kCLOCK_GateWWDT0 = (0x00000U | (7U)),
  kCLOCK_GateDMA = (0x00000U | (8U)),
  kCLOCK_GateAOI0 = (0x00000U | (9U)),
  kCLOCK_GateCRC = (0x00000U | (10U)),
  kCLOCK_Crc0 = (0x00000U | (10U)),
  kCLOCK_GateEIM = (0x00000U | (11U)),
  kCLOCK_GateERM = (0x00000U | (12U)),
  kCLOCK_GateLPI2C0 = (0x00000U | (16U)),
  kCLOCK_GateLPSPI0 = (0x00000U | (17U)),
  kCLOCK_GateLPSPI1 = (0x00000U | (18U)),
  kCLOCK_GateLPUART0 = (0x00000U | (19U)),
  kCLOCK_GateLPUART1 = (0x00000U | (20U)),
  kCLOCK_GateLPUART2 = (0x00000U | (21U)),
  kCLOCK_GateUSB0 = (0x00000U | (22U)),
  kCLOCK_GateQDC0 = (0x00000U | (23U)),
  kCLOCK_GateFLEXPWM0 = (0x00000U | (24U)),
  kCLOCK_GateOSTIMER0 = (0x00000U | (25U)),
  kCLOCK_GateADC0 = (0x00000U | (26U)),
  kCLOCK_GateCMP0 = (0x00000U | (27U)),
  kCLOCK_GateCMP1 = (0x00000U | (28U)),
  kCLOCK_GatePORT0 = (0x00000U | (29U)),
  kCLOCK_GatePORT1 = (0x00000U | (30U)),
  kCLOCK_GatePORT2 = (0x00000U | (31U)),
  kCLOCK_GatePORT3 = ((0x10U << 16U) | (0U)),
  kCLOCK_GateATX0 = ((0x10U << 16U) | (1U)),
  kCLOCK_GateMTR = ((0x10U << 16U) | (2U)),
  kCLOCK_GateTCU = ((0x10U << 16U) | (3U)),
  kCLOCK_GateEZRAMC_RAMA = ((0x10U << 16U) | (4U)),
  kCLOCK_GateGPIO0 = ((0x10U << 16U) | (5U)),
  kCLOCK_GateGPIO1 = ((0x10U << 16U) | (6U)),
  kCLOCK_GateGPIO2 = ((0x10U << 16U) | (7U)),
  kCLOCK_GateGPIO3 = ((0x10U << 16U) | (8U)),
  kCLOCK_GateROMCP = ((0x10U << 16U) | (9U)),
  kCLOCK_GatePWMSM0 = ((REG_PWM0SUBCTL << 16U) | (0U)),
  kCLOCK_GatePWMSM1 = ((REG_PWM0SUBCTL << 16U) | (1U)),
  kCLOCK_GatePWMSM2 = ((REG_PWM0SUBCTL << 16U) | (2U)),
  kCLOCK_GateNotAvail = (0xFFFFFFFFU)
}
 Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More...
 
enum  clock_name_t {
  kCLOCK_MainClk,
  kCLOCK_CoreSysClk,
  kCLOCK_SYSTEM_CLK,
  kCLOCK_BusClk,
  kCLOCK_ExtClk,
  kCLOCK_FroHf,
  kCLOCK_FroHfDiv,
  kCLOCK_Clk48M,
  kCLOCK_Fro12M,
  kCLOCK_Clk1M,
  kCLOCK_Fro16K,
  kCLOCK_Clk16K0,
  kCLOCK_Clk16K1,
  kCLOCK_SLOW_CLK
}
 Clock name used to get clock frequency. More...
 
enum  clock_select_name_t {
  kCLOCK_SelI3C0_FCLK = (0x0A0U),
  kCLOCK_SelCTIMER0 = (0x0A8U),
  kCLOCK_SelCTIMER1 = (0x0B0U),
  kCLOCK_SelCTIMER2 = (0x0B8U),
  kCLOCK_SelLPI2C0 = (0x0C8U),
  kCLOCK_SelLPSPI0 = (0x0D0U),
  kCLOCK_SelLPSPI1 = (0x0D8U),
  kCLOCK_SelLPUART0 = (0x0E0U),
  kCLOCK_SelLPUART1 = (0x0E8U),
  kCLOCK_SelLPUART2 = (0x0F0U),
  kCLOCK_SelUSB0 = (0x0F8U),
  kCLOCK_SelLPTMR0 = (0x100U),
  kCLOCK_SelOSTIMER0 = (0x108U),
  kCLOCK_SelADC0 = (0x110U),
  kCLOCK_SelCMP0_RR = (0x120U),
  kCLOCK_SelCMP1_RR = (0x130U),
  kCLOCK_SelTRACE = (0x138U),
  kCLOCK_SelCLKOUT = (0x140U),
  kCLOCK_SelSYSTICK = (0x148U),
  kCLOCK_SelSCGSCS = (0x200U),
  kCLOCK_SelMax = (0x200U)
}
 Clock name used to get clock frequency. More...
 
enum  clock_attach_id_t {
  kCLK_IN_to_MAIN_CLK = CLK_ATTACH_MUX(kCLOCK_SelSCGSCS, 1U),
  kFRO12M_to_MAIN_CLK = CLK_ATTACH_MUX(kCLOCK_SelSCGSCS, 2U),
  kFRO_HF_to_MAIN_CLK = CLK_ATTACH_MUX(kCLOCK_SelSCGSCS, 3U),
  kCLK_16K_to_MAIN_CLK = CLK_ATTACH_MUX(kCLOCK_SelSCGSCS, 4U),
  kNONE_to_MAIN_CLK = CLK_ATTACH_MUX(kCLOCK_SelSCGSCS, 7U),
  kFRO12M_to_I3C0FCLK = CLK_ATTACH_MUX(kCLOCK_SelI3C0_FCLK, 0U),
  kFRO_HF_DIV_to_I3C0FCLK = CLK_ATTACH_MUX(kCLOCK_SelI3C0_FCLK, 2U),
  kCLK_IN_to_I3C0FCLK = CLK_ATTACH_MUX(kCLOCK_SelI3C0_FCLK, 3U),
  kCLK_1M_to_I3C0FCLK = CLK_ATTACH_MUX(kCLOCK_SelI3C0_FCLK, 5U),
  kNONE_to_I3C0FCLK = CLK_ATTACH_MUX(kCLOCK_SelI3C0_FCLK, 7U),
  kFRO12M_to_CTIMER0 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER0, 0U),
  kFRO_HF_to_CTIMER0 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER0, 1U),
  kCLK_IN_to_CTIMER0 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER0, 3U),
  kCLK_16K_to_CTIMER0 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER0, 4U),
  kCLK_1M_to_CTIMER0 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER0, 5U),
  kNONE_to_CTIMER0 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER0, 7U),
  kFRO12M_to_CTIMER1 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER1, 0U),
  kFRO_HF_to_CTIMER1 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER1, 1U),
  kCLK_IN_to_CTIMER1 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER1, 3U),
  kCLK_16K_to_CTIMER1 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER1, 4U),
  kCLK_1M_to_CTIMER1 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER1, 5U),
  kNONE_to_CTIMER1 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER1, 7U),
  kFRO12M_to_CTIMER2 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER2, 0U),
  kFRO_HF_to_CTIMER2 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER2, 1U),
  kCLK_IN_to_CTIMER2 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER2, 3U),
  kCLK_16K_to_CTIMER2 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER2, 4U),
  kCLK_1M_to_CTIMER2 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER2, 5U),
  kNONE_to_CTIMER2 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER2, 7U),
  kFRO12M_to_LPI2C0 = CLK_ATTACH_MUX(kCLOCK_SelLPI2C0, 0U),
  kFRO_HF_DIV_to_LPI2C0 = CLK_ATTACH_MUX(kCLOCK_SelLPI2C0, 2U),
  kCLK_IN_to_LPI2C0 = CLK_ATTACH_MUX(kCLOCK_SelLPI2C0, 3U),
  kCLK_1M_to_LPI2C0 = CLK_ATTACH_MUX(kCLOCK_SelLPI2C0, 5U),
  kNONE_to_LPI2C0 = CLK_ATTACH_MUX(kCLOCK_SelLPI2C0, 7U),
  kFRO12M_to_LPSPI0 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI0, 0U),
  kFRO_HF_DIV_to_LPSPI0 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI0, 2U),
  kCLK_IN_to_LPSPI0 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI0, 3U),
  kCLK_1M_to_LPSPI0 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI0, 5U),
  kNONE_to_LPSPI0 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI0, 7U),
  kFRO12M_to_LPSPI1 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI1, 0U),
  kFRO_HF_DIV_to_LPSPI1 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI1, 2U),
  kCLK_IN_to_LPSPI1 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI1, 3U),
  kCLK_1M_to_LPSPI1 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI1, 5U),
  kNONE_to_LPSPI1 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI1, 7U),
  kFRO12M_to_LPUART0 = CLK_ATTACH_MUX(kCLOCK_SelLPUART0, 0U),
  kFRO_HF_DIV_to_LPUART0 = CLK_ATTACH_MUX(kCLOCK_SelLPUART0, 2U),
  kCLK_IN_to_LPUART0 = CLK_ATTACH_MUX(kCLOCK_SelLPUART0, 3U),
  kCLK_16K_to_LPUART0 = CLK_ATTACH_MUX(kCLOCK_SelLPUART0, 4U),
  kCLK_1M_to_LPUART0 = CLK_ATTACH_MUX(kCLOCK_SelLPUART0, 5U),
  kNONE_to_LPUART0 = CLK_ATTACH_MUX(kCLOCK_SelLPUART0, 7U),
  kFRO12M_to_LPUART1 = CLK_ATTACH_MUX(kCLOCK_SelLPUART1, 0U),
  kFRO_HF_DIV_to_LPUART1 = CLK_ATTACH_MUX(kCLOCK_SelLPUART1, 2U),
  kCLK_IN_to_LPUART1 = CLK_ATTACH_MUX(kCLOCK_SelLPUART1, 3U),
  kCLK_16K_to_LPUART1 = CLK_ATTACH_MUX(kCLOCK_SelLPUART1, 4U),
  kCLK_1M_to_LPUART1 = CLK_ATTACH_MUX(kCLOCK_SelLPUART1, 5U),
  kNONE_to_LPUART1 = CLK_ATTACH_MUX(kCLOCK_SelLPUART1, 7U),
  kFRO12M_to_LPUART2 = CLK_ATTACH_MUX(kCLOCK_SelLPUART2, 0U),
  kFRO_HF_DIV_to_LPUART2 = CLK_ATTACH_MUX(kCLOCK_SelLPUART2, 2U),
  kCLK_IN_to_LPUART2 = CLK_ATTACH_MUX(kCLOCK_SelLPUART2, 3U),
  kCLK_16K_to_LPUART2 = CLK_ATTACH_MUX(kCLOCK_SelLPUART2, 4U),
  kCLK_1M_to_LPUART2 = CLK_ATTACH_MUX(kCLOCK_SelLPUART2, 5U),
  kNONE_to_LPUART2 = CLK_ATTACH_MUX(kCLOCK_SelLPUART2, 7U),
  kCLK_48M_to_USB0 = CLK_ATTACH_MUX(kCLOCK_SelUSB0, 1U),
  kCLK_IN_to_USB0 = CLK_ATTACH_MUX(kCLOCK_SelUSB0, 2U),
  kNONE_to_USB0 = CLK_ATTACH_MUX(kCLOCK_SelUSB0, 3U),
  kFRO12M_to_LPTMR0 = CLK_ATTACH_MUX(kCLOCK_SelLPTMR0, 0U),
  kFRO_HF_DIV_to_LPTMR0 = CLK_ATTACH_MUX(kCLOCK_SelLPTMR0, 2U),
  kCLK_IN_to_LPTMR0 = CLK_ATTACH_MUX(kCLOCK_SelLPTMR0, 3U),
  kCLK_1M_to_LPTMR0 = CLK_ATTACH_MUX(kCLOCK_SelLPTMR0, 5U),
  kNONE_to_LPTMR0 = CLK_ATTACH_MUX(kCLOCK_SelLPTMR0, 7U),
  kCLK_16K_to_OSTIMER = CLK_ATTACH_MUX(kCLOCK_SelOSTIMER0, 0U),
  kCLK_1M_to_OSTIMER = CLK_ATTACH_MUX(kCLOCK_SelOSTIMER0, 2U),
  kNONE_to_OSTIMER = CLK_ATTACH_MUX(kCLOCK_SelOSTIMER0, 3U),
  kFRO12M_to_ADC0 = CLK_ATTACH_MUX(kCLOCK_SelADC0, 0U),
  kFRO_HF_to_ADC0 = CLK_ATTACH_MUX(kCLOCK_SelADC0, 1U),
  kCLK_IN_to_ADC0 = CLK_ATTACH_MUX(kCLOCK_SelADC0, 3U),
  kCLK_1M_to_ADC0 = CLK_ATTACH_MUX(kCLOCK_SelADC0, 5U),
  kNONE_to_ADC0 = CLK_ATTACH_MUX(kCLOCK_SelADC0, 7U),
  kFRO12M_to_CMP0 = CLK_ATTACH_MUX(kCLOCK_SelCMP0_RR, 0U),
  kFRO_HF_DIV_to_CMP0 = CLK_ATTACH_MUX(kCLOCK_SelCMP0_RR, 2U),
  kCLK_IN_to_CMP0 = CLK_ATTACH_MUX(kCLOCK_SelCMP0_RR, 3U),
  kCLK_1M_to_CMP0 = CLK_ATTACH_MUX(kCLOCK_SelCMP0_RR, 5U),
  kNONE_to_CMP0 = CLK_ATTACH_MUX(kCLOCK_SelCMP0_RR, 7U),
  kFRO12M_to_CMP1 = CLK_ATTACH_MUX(kCLOCK_SelCMP1_RR, 0U),
  kFRO_HF_DIV_to_CMP1 = CLK_ATTACH_MUX(kCLOCK_SelCMP1_RR, 2U),
  kCLK_IN_to_CMP1 = CLK_ATTACH_MUX(kCLOCK_SelCMP1_RR, 3U),
  kCLK_1M_to_CMP1 = CLK_ATTACH_MUX(kCLOCK_SelCMP1_RR, 5U),
  kNONE_to_CMP1 = CLK_ATTACH_MUX(kCLOCK_SelCMP1_RR, 7U),
  kCPU_CLK_to_TRACE = CLK_ATTACH_MUX(kCLOCK_SelTRACE, 0U),
  kCLK_1M_to_TRACE = CLK_ATTACH_MUX(kCLOCK_SelTRACE, 1U),
  kCLK_16K_to_TRACE = CLK_ATTACH_MUX(kCLOCK_SelTRACE, 2U),
  kNONE_to_TRACE = CLK_ATTACH_MUX(kCLOCK_SelTRACE, 3U),
  kFRO12M_to_CLKOUT = CLK_ATTACH_MUX(kCLOCK_SelCLKOUT, 0U),
  kFRO_HF_DIV_to_CLKOUT = CLK_ATTACH_MUX(kCLOCK_SelCLKOUT, 1U),
  kCLK_IN_to_CLKOUT = CLK_ATTACH_MUX(kCLOCK_SelCLKOUT, 2U),
  kCLK_16K_to_CLKOUT = CLK_ATTACH_MUX(kCLOCK_SelCLKOUT, 3U),
  kSLOW_CLK_to_CLKOUT = CLK_ATTACH_MUX(kCLOCK_SelCLKOUT, 6U),
  kNONE_to_CLKOUT = CLK_ATTACH_MUX(kCLOCK_SelCLKOUT, 7U),
  kCPU_CLK_to_SYSTICK = CLK_ATTACH_MUX(kCLOCK_SelSYSTICK, 0U),
  kCLK_1M_to_SYSTICK = CLK_ATTACH_MUX(kCLOCK_SelSYSTICK, 1U),
  kCLK_16K_to_SYSTICK = CLK_ATTACH_MUX(kCLOCK_SelSYSTICK, 2U),
  kNONE_to_SYSTICK = CLK_ATTACH_MUX(kCLOCK_SelSYSTICK, 3U),
  kNONE_to_NONE = (0xFFFFFFFFU)
}
 The enumerator of clock attach Id. More...
 
enum  clock_div_name_t {
  kCLOCK_DivI3C0_FCLK = (0x0A4U),
  kCLOCK_DivCTIMER0 = (0x0ACU),
  kCLOCK_DivCTIMER1 = (0x0B4U),
  kCLOCK_DivCTIMER2 = (0x0BCU),
  kCLOCK_DivWWDT0 = (0x0C4U),
  kCLOCK_DivLPI2C0 = (0x0CCU),
  kCLOCK_DivLPSPI0 = (0x0D4U),
  kCLOCK_DivLPSPI1 = (0x0DCU),
  kCLOCK_DivLPUART0 = (0x0E4U),
  kCLOCK_DivLPUART1 = (0x0ECU),
  kCLOCK_DivLPUART2 = (0x0F4U),
  kCLOCK_DivLPTMR0 = (0x104U),
  kCLOCK_DivADC0 = (0x114U),
  kCLOCK_DivCMP0_FUNC = (0x11CU),
  kCLOCK_DivCMP0_RR = (0x124U),
  kCLOCK_DivCMP1_FUNC = (0x12CU),
  kCLOCK_DivCMP1_RR = (0x134U),
  kCLOCK_DivTRACE = (0x13CU),
  kCLOCK_DivCLKOUT = (0x144U),
  kCLOCK_DivSYSTICK = (0x14CU),
  kCLOCK_DivFRO_HF_DIV = (0x154U),
  kCLOCK_DivSLOWCLK = (0x378U),
  kCLOCK_DivAHBCLK = (0x380U),
  kCLOCK_DivMax = (0x380U)
}
 Clock dividers. More...
 
enum  firc_trim_mode_t {
  kSCG_FircTrimNonUpdate = SCG_FIRCCSR_FIRCTREN_MASK,
  kSCG_FircTrimUpdate = SCG_FIRCCSR_FIRCTREN_MASK | SCG_FIRCCSR_FIRCTRUP_MASK
}
 firc trim mode. More...
 
enum  firc_trim_src_t {
  kSCG_FircTrimSrcUsb0 = 0U,
  kSCG_FircTrimSrcSysOsc = 2U
}
 firc trim source. More...
 
enum  sirc_trim_mode_t {
  kSCG_SircTrimNonUpdate = SCG_SIRCCSR_SIRCTREN_MASK,
  kSCG_SircTrimUpdate = SCG_SIRCCSR_SIRCTREN_MASK | SCG_SIRCCSR_SIRCTRUP_MASK
}
 sirc trim mode. More...
 
enum  sirc_trim_src_t {
  kNoTrimSrc = 0,
  kSCG_SircTrimSrcSysOsc = 2U
}
 sirc trim source. More...
 
enum  scg_sosc_monitor_mode_t {
  kSCG_SysOscMonitorDisable = 0U,
  kSCG_SysOscMonitorInt = SCG_SOSCCSR_SOSCCM_MASK,
  kSCG_SysOscMonitorReset
}
 SCG system OSC monitor mode. More...
 
enum  clke_16k_t {
  kCLKE_16K_SYSTEM = VBAT_FROCLKE_CLKE(1U),
  kCLKE_16K_COREMAIN = VBAT_FROCLKE_CLKE(2U)
}
 firc trim source. More...
 

Functions

static void CLOCK_EnableClock (clock_ip_name_t clk)
 Enable the clock for specific IP. More...
 
static void CLOCK_DisableClock (clock_ip_name_t clk)
 Disable the clock for specific IP. More...
 
void CLOCK_AttachClk (clock_attach_id_t connection)
 Configure the clock selection muxes. More...
 
clock_attach_id_t CLOCK_GetClockAttachId (clock_attach_id_t connection)
 Get the actual clock attach id. This fuction uses the offset in input attach id, then it reads the actual source value in the register and combine the offset to obtain an actual attach id. More...
 
void CLOCK_SetClockSelect (clock_select_name_t sel_name, uint32_t value)
 Set the clock select value. This fuction set the peripheral clock select value. More...
 
uint32_t CLOCK_GetClockSelect (clock_select_name_t sel_name)
 Get the clock select value. This fuction get the peripheral clock select value. More...
 
void CLOCK_SetClockDiv (clock_div_name_t div_name, uint32_t value)
 Setup peripheral clock dividers. More...
 
uint32_t CLOCK_GetClockDiv (clock_div_name_t div_name)
 Get peripheral clock dividers. More...
 
void CLOCK_HaltClockDiv (clock_div_name_t div_name)
 Halt peripheral clock dividers. More...
 
status_t CLOCK_SetupFROHFClocking (uint32_t iFreq)
 Initialize the FROHF to given frequency (48,64,96,192). This function turns on FIRC and select the given frequency as the source of fro_hf. More...
 
status_t CLOCK_SetupFRO12MClocking (void)
 Initialize the FRO12M. This function turns on FRO12M. More...
 
status_t CLOCK_SetupFRO16KClocking (uint8_t clk_16k_enable_mask)
 Initialize the FRO16K. This function turns on FRO16K. More...
 
status_t CLOCK_SetupExtClocking (uint32_t iFreq)
 Initialize the external osc clock to given frequency. More...
 
status_t CLOCK_SetupExtRefClocking (uint32_t iFreq)
 Initialize the external reference clock to given frequency. More...
 
uint32_t CLOCK_GetFreq (clock_name_t clockName)
 Return Frequency of selected clock. More...
 
uint32_t CLOCK_GetCoreSysClkFreq (void)
 Return Frequency of core. More...
 
uint32_t CLOCK_GetI3CFClkFreq (void)
 Return Frequency of I3C FCLK. More...
 
uint32_t CLOCK_GetCTimerClkFreq (uint32_t id)
 Return Frequency of CTimer functional Clock. More...
 
uint32_t CLOCK_GetLpi2cClkFreq (void)
 Return Frequency of LPI2C0 functional Clock. More...
 
uint32_t CLOCK_GetLpspiClkFreq (uint32_t id)
 Return Frequency of LPSPI functional Clock. More...
 
uint32_t CLOCK_GetLpuartClkFreq (uint32_t id)
 Return Frequency of LPUART functional Clock. More...
 
uint32_t CLOCK_GetLptmrClkFreq (void)
 Return Frequency of LPTMR functional Clock. More...
 
uint32_t CLOCK_GetOstimerClkFreq (void)
 Return Frequency of OSTIMER. More...
 
uint32_t CLOCK_GetAdcClkFreq (void)
 Return Frequency of Adc Clock. More...
 
uint32_t CLOCK_GetCmpFClkFreq (uint32_t id)
 Return Frequency of CMP Function Clock. More...
 
uint32_t CLOCK_GetCmpRRClkFreq (uint32_t id)
 Return Frequency of CMP Round Robin Clock. More...
 
uint32_t CLOCK_GetTraceClkFreq (void)
 Return Frequency of Trace Clock. More...
 
uint32_t CLOCK_GetClkoutClkFreq (void)
 Return Frequency of CLKOUT Clock. More...
 
uint32_t CLOCK_GetSystickClkFreq (void)
 Return Frequency of Systick Clock. More...
 
uint32_t CLOCK_GetWwdtClkFreq (void)
 brief Return Frequency of Systick Clock return Frequency of Systick.
 
status_t CLOCK_FROHFTrimConfig (firc_trim_config_t config)
 Setup FROHF trim. More...
 
status_t CLOCK_FRO12MTrimConfig (sirc_trim_config_t config)
 Setup FRO 12M trim. More...
 
void CLOCK_SetSysOscMonitorMode (scg_sosc_monitor_mode_t mode)
 Sets the system OSC monitor mode. More...
 
bool CLOCK_EnableUsbfsClock (void)
 brief Enable USB FS clock. More...
 

Driver version

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(1, 0, 0))
 CLOCK driver version 1.0.0. More...
 

Data Structure Documentation

struct firc_trim_config_t

Data Fields

firc_trim_mode_t trimMode
 Trim mode. More...
 
firc_trim_src_t trimSrc
 Trim source. More...
 
uint16_t trimDiv
 Divider of SOSC. More...
 
uint8_t trimCoar
 Trim coarse value; Irrelevant if trimMode is kSCG_TrimUpdate. More...
 
uint8_t trimFine
 Trim fine value; Irrelevant if trimMode is kSCG_TrimUpdate. More...
 

Field Documentation

firc_trim_mode_t firc_trim_config_t::trimMode
firc_trim_src_t firc_trim_config_t::trimSrc
uint16_t firc_trim_config_t::trimDiv
uint8_t firc_trim_config_t::trimCoar
uint8_t firc_trim_config_t::trimFine
struct sirc_trim_config_t

Data Fields

sirc_trim_mode_t trimMode
 Trim mode. More...
 
sirc_trim_src_t trimSrc
 Trim source. More...
 
uint16_t trimDiv
 Divider of SOSC. More...
 
uint8_t cltrim
 Trim coarse value; Irrelevant if trimMode is kSCG_TrimUpdate. More...
 
uint8_t ccotrim
 Trim fine value; Irrelevant if trimMode is kSCG_TrimUpdate. More...
 

Field Documentation

sirc_trim_mode_t sirc_trim_config_t::trimMode
sirc_trim_src_t sirc_trim_config_t::trimSrc
uint16_t sirc_trim_config_t::trimDiv
uint8_t sirc_trim_config_t::cltrim
uint8_t sirc_trim_config_t::ccotrim

Macro Definition Documentation

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(1, 0, 0))
#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0U

When set to 0, peripheral drivers will enable clock in initialize function and disable clock in de-initialize function. When set to 1, peripheral driver will not control the clock, application could control the clock out of the driver.

Note
All drivers share this feature switcher. If it is set to 1, application should handle clock enable and disable for all drivers.
#define CLK_GATE_REG_OFFSET (   value)    (((uint32_t)(value)) >> 16U)
#define AOI_CLOCKS
Value:
{ \
}
Clock gate name: AOI0.
Definition: fsl_clock.h:69
#define CRC_CLOCKS
Value:
{ \
}
Clock gate name: CRC.
Definition: fsl_clock.h:70
#define CTIMER_CLOCKS
Value:
{ \
}
Clock gate name: CTIMER2.
Definition: fsl_clock.h:64
Clock gate name: CTIMER0.
Definition: fsl_clock.h:62
Clock gate name: CTIMER1.
Definition: fsl_clock.h:63
#define DMA_CLOCKS
Value:
{ \
}
Clock gate name: DMA.
Definition: fsl_clock.h:68
#define EDMA_CLOCKS
Value:
{ \
}
Clock gate name: DMA.
Definition: fsl_clock.h:68
#define ERM_CLOCKS
Value:
{ \
}
Clock gate name: ERM.
Definition: fsl_clock.h:73
#define EIM_CLOCKS
Value:
{ \
}
Clock gate name: EIM.
Definition: fsl_clock.h:72
#define FREQME_CLOCKS
Value:
{ \
}
Clock gate name: FREQME.
Definition: fsl_clock.h:65
#define GPIO_CLOCKS
Value:
{ \
}
Clock gate name: GPIO2.
Definition: fsl_clock.h:97
Clock gate name: GPIO1.
Definition: fsl_clock.h:96
Clock gate name: GPIO0.
Definition: fsl_clock.h:95
Clock gate name: GPIO3.
Definition: fsl_clock.h:98
#define INPUTMUX_CLOCKS
Value:
{ \
}
Clock gate name: INPUTMUX0.
Definition: fsl_clock.h:59
#define LPCMP_CLOCKS
Value:
{ \
}
Clock gate name: CMP0.
Definition: fsl_clock.h:85
Clock gate name: CMP1.
Definition: fsl_clock.h:86
#define LPADC_CLOCKS
Value:
{ \
}
Clock gate name: ADC0.
Definition: fsl_clock.h:84
#define LPUART_CLOCKS
Value:
{ \
}
Clock gate name: LPUART0.
Definition: fsl_clock.h:77
Clock gate name: LPUART2.
Definition: fsl_clock.h:79
Clock gate name: LPUART1.
Definition: fsl_clock.h:78
#define LPI2C_CLOCKS
Value:
{ \
}
Clock gate name: LPI2C0.
Definition: fsl_clock.h:74
#define LPSPI_CLOCKS
Value:
{ \
}
Clock gate name: LPSPI1.
Definition: fsl_clock.h:76
Clock gate name: LPSPI0.
Definition: fsl_clock.h:75
#define MTR_CLOCKS
Value:
{ \
}
Clock gate name: MTR.
Definition: fsl_clock.h:92
#define OSTIMER_CLOCKS
Value:
{ \
}
Clock gate name: OSTIMER0.
Definition: fsl_clock.h:83
#define PWM_CLOCKS
Value:
{ \
{ \
} \
}
Clock gate name: FlexPWM SM1.
Definition: fsl_clock.h:101
Clock gate name: FlexPWM SM2.
Definition: fsl_clock.h:102
Clock gate name: FlexPWM SM0.
Definition: fsl_clock.h:100
#define QDC_CLOCKS
Value:
{ \
}
Clock gate name: QDC0.
Definition: fsl_clock.h:81
#define UTICK_CLOCKS
Value:
{ \
}
Clock gate name: UTICK0.
Definition: fsl_clock.h:66
#define WWDT_CLOCKS
Value:
{ \
}
Clock gate name: WWDT0.
Definition: fsl_clock.h:67
#define BUS_CLK   kCLOCK_BusClk
#define CLK_ATTACH_REG_OFFSET (   value)    (((uint32_t)(value)) >> 16U)

[4 bits for choice, 0 means invalid choice] [8 bits mux ID]*

Enumeration Type Documentation

Enumerator
kCLOCK_GateINPUTMUX0 

Clock gate name: INPUTMUX0.

kCLOCK_InputMux 

Clock gate name: INPUTMUX0.

kCLOCK_GateI3C0 

Clock gate name: I3C0.

kCLOCK_GateCTIMER0 

Clock gate name: CTIMER0.

kCLOCK_GateCTIMER1 

Clock gate name: CTIMER1.

kCLOCK_GateCTIMER2 

Clock gate name: CTIMER2.

kCLOCK_GateFREQME 

Clock gate name: FREQME.

kCLOCK_GateUTICK0 

Clock gate name: UTICK0.

kCLOCK_GateWWDT0 

Clock gate name: WWDT0.

kCLOCK_GateDMA 

Clock gate name: DMA.

kCLOCK_GateAOI0 

Clock gate name: AOI0.

kCLOCK_GateCRC 

Clock gate name: CRC.

kCLOCK_Crc0 

Clock gate name: CRC.

kCLOCK_GateEIM 

Clock gate name: EIM.

kCLOCK_GateERM 

Clock gate name: ERM.

kCLOCK_GateLPI2C0 

Clock gate name: LPI2C0.

kCLOCK_GateLPSPI0 

Clock gate name: LPSPI0.

kCLOCK_GateLPSPI1 

Clock gate name: LPSPI1.

kCLOCK_GateLPUART0 

Clock gate name: LPUART0.

kCLOCK_GateLPUART1 

Clock gate name: LPUART1.

kCLOCK_GateLPUART2 

Clock gate name: LPUART2.

kCLOCK_GateUSB0 

Clock gate name: USB0.

kCLOCK_GateQDC0 

Clock gate name: QDC0.

kCLOCK_GateFLEXPWM0 

Clock gate name: FLEXPWM0.

kCLOCK_GateOSTIMER0 

Clock gate name: OSTIMER0.

kCLOCK_GateADC0 

Clock gate name: ADC0.

kCLOCK_GateCMP0 

Clock gate name: CMP0.

kCLOCK_GateCMP1 

Clock gate name: CMP1.

kCLOCK_GatePORT0 

Clock gate name: PORT0.

kCLOCK_GatePORT1 

Clock gate name: PORT1.

kCLOCK_GatePORT2 

Clock gate name: PORT2.

kCLOCK_GatePORT3 

Clock gate name: PORT3.

kCLOCK_GateATX0 

Clock gate name: ATX0.

kCLOCK_GateMTR 

Clock gate name: MTR.

kCLOCK_GateTCU 

Clock gate name: TCU.

kCLOCK_GateEZRAMC_RAMA 

Clock gate name: EZRAMC_RAMA.

kCLOCK_GateGPIO0 

Clock gate name: GPIO0.

kCLOCK_GateGPIO1 

Clock gate name: GPIO1.

kCLOCK_GateGPIO2 

Clock gate name: GPIO2.

kCLOCK_GateGPIO3 

Clock gate name: GPIO3.

kCLOCK_GateROMCP 

Clock gate name: ROMCP.

kCLOCK_GatePWMSM0 

Clock gate name: FlexPWM SM0.

kCLOCK_GatePWMSM1 

Clock gate name: FlexPWM SM1.

kCLOCK_GatePWMSM2 

Clock gate name: FlexPWM SM2.

kCLOCK_GateNotAvail 

Clock gate name: None

Enumerator
kCLOCK_MainClk 

MAIN_CLK.

kCLOCK_CoreSysClk 

Core/system clock(CPU_CLK)

kCLOCK_SYSTEM_CLK 

AHB clock.

kCLOCK_BusClk 

Bus clock (AHB clock)

kCLOCK_ExtClk 

External Clock.

kCLOCK_FroHf 

FRO192.

kCLOCK_FroHfDiv 

Divided by FRO192.

kCLOCK_Clk48M 

CLK48M.

kCLOCK_Fro12M 

FRO12M.

kCLOCK_Clk1M 

CLK1M.

kCLOCK_Fro16K 

FRO16K.

kCLOCK_Clk16K0 

CLK16K[0].

kCLOCK_Clk16K1 

CLK16K[1].

kCLOCK_SLOW_CLK 

SYSTEM_CLK divided by 4.

Enumerator
kCLOCK_SelI3C0_FCLK 

I3C0_FCLK clock selection.

kCLOCK_SelCTIMER0 

CTIMER0 clock selection.

kCLOCK_SelCTIMER1 

CTIMER1 clock selection.

kCLOCK_SelCTIMER2 

CTIMER2 clock selection.

kCLOCK_SelLPI2C0 

LPI2C0 clock selection.

kCLOCK_SelLPSPI0 

LPSPI0 clock selection.

kCLOCK_SelLPSPI1 

LPSPI1 clock selection.

kCLOCK_SelLPUART0 

LPUART0 clock selection.

kCLOCK_SelLPUART1 

LPUART1 clock selection.

kCLOCK_SelLPUART2 

LPUART2 clock selection.

kCLOCK_SelUSB0 

USB0 clock selection.

kCLOCK_SelLPTMR0 

LPTMR0 clock selection.

kCLOCK_SelOSTIMER0 

OSTIMER0 clock selection.

kCLOCK_SelADC0 

ADC0 clock selection.

kCLOCK_SelCMP0_RR 

CMP0_RR clock selection.

kCLOCK_SelCMP1_RR 

CMP1_RR clock selection.

kCLOCK_SelTRACE 

TRACE clock selection.

kCLOCK_SelCLKOUT 

CLKOUT clock selection.

kCLOCK_SelSYSTICK 

SYSTICK clock selection.

kCLOCK_SelSCGSCS 

SCG SCS clock selection.

kCLOCK_SelMax 

MAX clock selection.

Enumerator
kCLK_IN_to_MAIN_CLK 

Attach clk_in to MAIN_CLK.

kFRO12M_to_MAIN_CLK 

Attach FRO_12M to MAIN_CLK.

kFRO_HF_to_MAIN_CLK 

Attach FRO_HF to MAIN_CLK.

kCLK_16K_to_MAIN_CLK 

Attach CLK_16K[1] to MAIN_CLK.

kNONE_to_MAIN_CLK 

Attach NONE to MAIN_CLK.

kFRO12M_to_I3C0FCLK 

Attach FRO12M to I3C0FCLK.

kFRO_HF_DIV_to_I3C0FCLK 

Attach FRO_HF_DIV to I3C0FCLK.

kCLK_IN_to_I3C0FCLK 

Attach CLK_IN to I3C0FCLK.

kCLK_1M_to_I3C0FCLK 

Attach CLK_1M to I3C0FCLK.

kNONE_to_I3C0FCLK 

Attach NONE to I3C0FCLK.

kFRO12M_to_CTIMER0 

Attach FRO12M to CTIMER0.

kFRO_HF_to_CTIMER0 

Attach FRO_HF to CTIMER0.

kCLK_IN_to_CTIMER0 

Attach CLK_IN to CTIMER0.

kCLK_16K_to_CTIMER0 

Attach CLK_16K to CTIMER0.

kCLK_1M_to_CTIMER0 

Attach CLK_1M to CTIMER0.

kNONE_to_CTIMER0 

Attach NONE to CTIMER0.

kFRO12M_to_CTIMER1 

Attach FRO12M to CTIMER1.

kFRO_HF_to_CTIMER1 

Attach FRO_HF to CTIMER1.

kCLK_IN_to_CTIMER1 

Attach CLK_IN to CTIMER1.

kCLK_16K_to_CTIMER1 

Attach CLK_16K to CTIMER1.

kCLK_1M_to_CTIMER1 

Attach CLK_1M to CTIMER1.

kNONE_to_CTIMER1 

Attach NONE to CTIMER1.

kFRO12M_to_CTIMER2 

Attach FRO12M to CTIMER2.

kFRO_HF_to_CTIMER2 

Attach FRO_HF to CTIMER2.

kCLK_IN_to_CTIMER2 

Attach CLK_IN to CTIMER2.

kCLK_16K_to_CTIMER2 

Attach CLK_16K to CTIMER2.

kCLK_1M_to_CTIMER2 

Attach CLK_1M to CTIMER2.

kNONE_to_CTIMER2 

Attach NONE to CTIMER2.

kFRO12M_to_LPI2C0 

Attach FRO12M to LPI2C0.

kFRO_HF_DIV_to_LPI2C0 

Attach FRO_HF_DIV to LPI2C0.

kCLK_IN_to_LPI2C0 

Attach CLK_IN to LPI2C0.

kCLK_1M_to_LPI2C0 

Attach CLK_1M to LPI2C0.

kNONE_to_LPI2C0 

Attach NONE to LPI2C0.

kFRO12M_to_LPSPI0 

Attach FRO12M to LPSPI0.

kFRO_HF_DIV_to_LPSPI0 

Attach FRO_HF_DIV to LPSPI0.

kCLK_IN_to_LPSPI0 

Attach CLK_IN to LPSPI0.

kCLK_1M_to_LPSPI0 

Attach CLK_1M to LPSPI0.

kNONE_to_LPSPI0 

Attach NONE to LPSPI0.

kFRO12M_to_LPSPI1 

Attach FRO12M to LPSPI1.

kFRO_HF_DIV_to_LPSPI1 

Attach FRO_HF_DIV to LPSPI1.

kCLK_IN_to_LPSPI1 

Attach CLK_IN to LPSPI1.

kCLK_1M_to_LPSPI1 

Attach CLK_1M to LPSPI1.

kNONE_to_LPSPI1 

Attach NONE to LPSPI1.

kFRO12M_to_LPUART0 

Attach FRO12M to LPUART0.

kFRO_HF_DIV_to_LPUART0 

Attach FRO_HF_DIV to LPUART0.

kCLK_IN_to_LPUART0 

Attach CLK_IN to LPUART0.

kCLK_16K_to_LPUART0 

Attach CLK_16K to LPUART0.

kCLK_1M_to_LPUART0 

Attach CLK_1M to LPUART0.

kNONE_to_LPUART0 

Attach NONE to LPUART0.

kFRO12M_to_LPUART1 

Attach FRO12M to LPUART1.

kFRO_HF_DIV_to_LPUART1 

Attach FRO_HF_DIV to LPUART1.

kCLK_IN_to_LPUART1 

Attach CLK_IN to LPUART1.

kCLK_16K_to_LPUART1 

Attach CLK_16K to LPUART1.

kCLK_1M_to_LPUART1 

Attach CLK_1M to LPUART1.

kNONE_to_LPUART1 

Attach NONE to LPUART1.

kFRO12M_to_LPUART2 

Attach FRO12M to LPUART2.

kFRO_HF_DIV_to_LPUART2 

Attach FRO_HF_DIV to LPUART2.

kCLK_IN_to_LPUART2 

Attach CLK_IN to LPUART2.

kCLK_16K_to_LPUART2 

Attach CLK_16K to LPUART2.

kCLK_1M_to_LPUART2 

Attach CLK_1M to LPUART2.

kNONE_to_LPUART2 

Attach NONE to LPUART2.

kCLK_48M_to_USB0 

Attach FRO12M to USB0.

kCLK_IN_to_USB0 

Attach CLK_IN to USB0.

kNONE_to_USB0 

Attach NONE to USB0.

kFRO12M_to_LPTMR0 

Attach FRO12M to LPTMR0.

kFRO_HF_DIV_to_LPTMR0 

Attach FRO_HF_DIV to LPTMR0.

kCLK_IN_to_LPTMR0 

Attach CLK_IN to LPTMR0.

kCLK_1M_to_LPTMR0 

Attach CLK_1M to LPTMR0.

kNONE_to_LPTMR0 

Attach NONE to LPTMR0.

kCLK_16K_to_OSTIMER 

Attach FRO16K to OSTIMER0.

kCLK_1M_to_OSTIMER 

Attach CLK_1M to OSTIMER0.

kNONE_to_OSTIMER 

Attach NONE to OSTIMER0.

kFRO12M_to_ADC0 

Attach FRO12M to ADC0.

kFRO_HF_to_ADC0 

Attach FRO_HF to ADC0.

kCLK_IN_to_ADC0 

Attach CLK_IN to ADC0.

kCLK_1M_to_ADC0 

Attach CLK_1M to ADC0.

kNONE_to_ADC0 

Attach NONE to ADC0.

kFRO12M_to_CMP0 

Attach FRO12M to CMP0.

kFRO_HF_DIV_to_CMP0 

Attach FRO_HF_DIV to CMP0.

kCLK_IN_to_CMP0 

Attach CLK_IN to CMP0.

kCLK_1M_to_CMP0 

Attach CLK_1M to CMP0.

kNONE_to_CMP0 

Attach NONE to CMP0.

kFRO12M_to_CMP1 

Attach FRO12M to CMP1.

kFRO_HF_DIV_to_CMP1 

Attach FRO_HF_DIV to CMP1.

kCLK_IN_to_CMP1 

Attach CLK_IN to CMP1.

kCLK_1M_to_CMP1 

Attach CLK_1M to CMP1.

kNONE_to_CMP1 

Attach NONE to CMP1.

kCPU_CLK_to_TRACE 

Attach CPU_CLK to TRACE.

kCLK_1M_to_TRACE 

Attach CLK_1M to TRACE.

kCLK_16K_to_TRACE 

Attach CLK_16K to TRACE.

kNONE_to_TRACE 

Attach NONE to TRACE.

kFRO12M_to_CLKOUT 

Attach FRO12M to CLKOUT.

kFRO_HF_DIV_to_CLKOUT 

Attach FRO_HF_DIV to CLKOUT.

kCLK_IN_to_CLKOUT 

Attach CLK_IN to CLKOUT.

kCLK_16K_to_CLKOUT 

Attach CLK_16K to CLKOUT.

kSLOW_CLK_to_CLKOUT 

Attach SLOW_CLK to CLKOUT.

kNONE_to_CLKOUT 

Attach NONE to CLKOUT.

kCPU_CLK_to_SYSTICK 

Attach CPU_CLK to SYSTICK.

kCLK_1M_to_SYSTICK 

Attach CLK_1M to SYSTICK.

kCLK_16K_to_SYSTICK 

Attach CLK_16K to SYSTICK.

kNONE_to_SYSTICK 

Attach NONE to SYSTICK.

kNONE_to_NONE 

Attach NONE to NONE.

Enumerator
kCLOCK_DivI3C0_FCLK 

I3C0_FCLK clock divider.

kCLOCK_DivCTIMER0 

CTIMER0 clock divider.

kCLOCK_DivCTIMER1 

CTIMER1 clock divider.

kCLOCK_DivCTIMER2 

CTIMER2 clock divider.

kCLOCK_DivWWDT0 

WWDT0 clock divider.

kCLOCK_DivLPI2C0 

LPI2C0 clock divider.

kCLOCK_DivLPSPI0 

LPSPI0 clock divider.

kCLOCK_DivLPSPI1 

LPSPI1 clock divider.

kCLOCK_DivLPUART0 

LPUART0 clock divider.

kCLOCK_DivLPUART1 

LPUART1 clock divider.

kCLOCK_DivLPUART2 

LPUART2 clock divider.

kCLOCK_DivLPTMR0 

LPTMR0 clock divider.

kCLOCK_DivADC0 

ADC0 clock divider.

kCLOCK_DivCMP0_FUNC 

CMP0_FUNC clock divider.

kCLOCK_DivCMP0_RR 

CMP0_RR clock divider.

kCLOCK_DivCMP1_FUNC 

CMP1_FUNC clock divider.

kCLOCK_DivCMP1_RR 

CMP1_RR clock divider.

kCLOCK_DivTRACE 

TRACE clock divider.

kCLOCK_DivCLKOUT 

CLKOUT clock divider.

kCLOCK_DivSYSTICK 

SYSTICK clock divider.

kCLOCK_DivFRO_HF_DIV 

FRO_HF_DIV clock divider.

kCLOCK_DivSLOWCLK 

SLOWCLK clock divider.

kCLOCK_DivAHBCLK 

System clock divider.

kCLOCK_DivMax 

MAX clock divider.

Enumerator
kSCG_FircTrimNonUpdate 

Trim enable but not enable trim value update.

In this mode, the trim value is fixed to the initialized value which is defined by trimCoar and trimFine in configure structure firc_trim_config_t.

kSCG_FircTrimUpdate 

Trim enable and trim value update enable.

In this mode, the trim value is auto update.

Enumerator
kSCG_FircTrimSrcUsb0 

USB0 start of frame (1kHz).

kSCG_FircTrimSrcSysOsc 

System OSC.

Enumerator
kSCG_SircTrimNonUpdate 

Trim enable but not enable trim value update.

In this mode, the trim value is fixed to the initialized value which is defined by trimCoar and trimFine in configure structure sirc_trim_config_t.

kSCG_SircTrimUpdate 

Trim enable and trim value update enable.

In this mode, the trim value is auto update.

Enumerator
kNoTrimSrc 

No external tirm source.

kSCG_SircTrimSrcSysOsc 

System OSC.

Enumerator
kSCG_SysOscMonitorDisable 

Monitor disabled.

kSCG_SysOscMonitorInt 

Interrupt when the SOSC error is detected.

kSCG_SysOscMonitorReset 

Reset when the SOSC error is detected.

enum clke_16k_t
Enumerator
kCLKE_16K_SYSTEM 

To VSYS domain.

kCLKE_16K_COREMAIN 

To VDD_CORE domain.

Function Documentation

static void CLOCK_EnableClock ( clock_ip_name_t  clk)
inlinestatic
Parameters
clk: Clock to be enabled.
Returns
Nothing
static void CLOCK_DisableClock ( clock_ip_name_t  clk)
inlinestatic
Parameters
clk: Clock to be Disabled.
Returns
Nothing
void CLOCK_AttachClk ( clock_attach_id_t  connection)
Parameters
connection: Clock to be configured.
Returns
Nothing
clock_attach_id_t CLOCK_GetClockAttachId ( clock_attach_id_t  connection)
Parameters
connection: Clock attach id to get.
Returns
Clock source value.
void CLOCK_SetClockSelect ( clock_select_name_t  sel_name,
uint32_t  value 
)
Parameters
sel_name: Clock select.
value: value to be set.
uint32_t CLOCK_GetClockSelect ( clock_select_name_t  sel_name)
Parameters
sel_name: Clock select.
Returns
Clock source value.
void CLOCK_SetClockDiv ( clock_div_name_t  div_name,
uint32_t  value 
)
Parameters
div_name: Clock divider name
value: Value to be divided
Returns
Nothing
uint32_t CLOCK_GetClockDiv ( clock_div_name_t  div_name)
Parameters
div_name: Clock divider name
Returns
peripheral clock dividers
void CLOCK_HaltClockDiv ( clock_div_name_t  div_name)
Parameters
div_name: Clock divider name
Returns
Nothing
status_t CLOCK_SetupFROHFClocking ( uint32_t  iFreq)
Parameters
iFreq: Desired frequency.
Returns
returns success or fail status.
status_t CLOCK_SetupFRO12MClocking ( void  )
Returns
returns success or fail status.
status_t CLOCK_SetupFRO16KClocking ( uint8_t  clk_16k_enable_mask)
Parameters
clk_16k_enable_mask,:0-3 0b00: disable both clk_16k0 and clk_16k1 0b01: only enable clk_16k0 0b10: only enable clk_16k1 0b11: enable both clk_16k0 and clk_16k1
Returns
returns success or fail status.
status_t CLOCK_SetupExtClocking ( uint32_t  iFreq)
Parameters
iFreq: Desired frequency (must be equal to exact rate in Hz)
Returns
returns success or fail status.
status_t CLOCK_SetupExtRefClocking ( uint32_t  iFreq)
Parameters
iFreq: Desired frequency (must be equal to exact rate in Hz)
Returns
returns success or fail status.
uint32_t CLOCK_GetFreq ( clock_name_t  clockName)
Returns
Frequency of selected clock
uint32_t CLOCK_GetCoreSysClkFreq ( void  )
Returns
Frequency of the core
uint32_t CLOCK_GetI3CFClkFreq ( void  )
Returns
Frequency of I3C FCLK.
uint32_t CLOCK_GetCTimerClkFreq ( uint32_t  id)
Returns
Frequency of CTimer functional Clock
uint32_t CLOCK_GetLpi2cClkFreq ( void  )
Returns
Frequency of LPI2C0 functional Clock
uint32_t CLOCK_GetLpspiClkFreq ( uint32_t  id)
Returns
Frequency of LPSPI functional Clock
uint32_t CLOCK_GetLpuartClkFreq ( uint32_t  id)
Returns
Frequency of LPUART functional Clock
uint32_t CLOCK_GetLptmrClkFreq ( void  )
Returns
Frequency of LPTMR functional Clock
uint32_t CLOCK_GetOstimerClkFreq ( void  )
Returns
Frequency of OSTIMER Clock
uint32_t CLOCK_GetAdcClkFreq ( void  )
Returns
Frequency of Adc.
uint32_t CLOCK_GetCmpFClkFreq ( uint32_t  id)
Returns
Frequency of CMP Function.
uint32_t CLOCK_GetCmpRRClkFreq ( uint32_t  id)
Returns
Frequency of CMP Round Robin.
uint32_t CLOCK_GetTraceClkFreq ( void  )
Returns
Frequency of Trace.
uint32_t CLOCK_GetClkoutClkFreq ( void  )
Returns
Frequency of CLKOUT.
uint32_t CLOCK_GetSystickClkFreq ( void  )
Returns
Frequency of Systick.
status_t CLOCK_FROHFTrimConfig ( firc_trim_config_t  config)
Parameters
config: FROHF trim value
Returns
returns success or fail status.
status_t CLOCK_FRO12MTrimConfig ( sirc_trim_config_t  config)
Parameters
config: FRO 12M trim value
Returns
returns success or fail status.
void CLOCK_SetSysOscMonitorMode ( scg_sosc_monitor_mode_t  mode)

This function sets the system OSC monitor mode. The mode can be disabled, it can generate an interrupt when the error is disabled, or reset when the error is detected.

Parameters
modeMonitor mode to set.
bool CLOCK_EnableUsbfsClock ( void  )

Enable USB Full Speed clock.