MCUXpresso SDK API Reference Manual  Rev 2.16.100
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
MECC: internal error correction code

Overview

The MCUXpresso SDK provides a driver for the MECC module of MCUXpresso SDK devices.

The MECC64 module supports Single Error Correction and Double Error Detection(SECDED) ECC function to provide reliability for 4 banks On-Chip RAM(OCRAM) access.

This example code shows how to correct single error and detect multiple error using the MECC driver.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mecc

Data Structures

struct  _mecc_config
 MECC user configuration. More...
 
struct  _mecc_single_error_info
 MECC ocram single error information, including single error address, ECC code, error data and error bit position. More...
 
struct  _mecc_multi_error_info
 MECC ocram multiple error information, including multiple error address, ECC code, error data. More...
 

Typedefs

typedef struct _mecc_config mecc_config_t
 MECC user configuration. More...
 
typedef struct
_mecc_single_error_info 
mecc_single_error_info_t
 MECC ocram single error information, including single error address, ECC code, error data and error bit position.
 
typedef struct
_mecc_multi_error_info 
mecc_multi_error_info_t
 MECC ocram multiple error information, including multiple error address, ECC code, error data.
 

Enumerations

enum  { kStatus_MECC_BankMiss = MAKE_STATUS(kStatusGroup_MECC, 0) }
 Error codes for the MECC driver. More...
 
enum  {
  kMECC_SingleError0InterruptEnable = MECC_ERR_SIG_EN_SINGLE_ERR0_SIG_EN_MASK,
  kMECC_SingleError1InterruptEnable = MECC_ERR_SIG_EN_SINGLE_ERR1_SIG_EN_MASK,
  kMECC_SingleError2InterruptEnable = MECC_ERR_SIG_EN_SINGLE_ERR2_SIG_EN_MASK,
  kMECC_SingleError3InterruptEnable = MECC_ERR_SIG_EN_SINGLE_ERR3_SIG_EN_MASK,
  kMECC_MultiError0InterruptEnable = MECC_ERR_SIG_EN_MULTI_ERR0_SIG_EN_MASK,
  kMECC_MultiError1InterruptEnable = MECC_ERR_SIG_EN_MULTI_ERR1_SIG_EN_MASK,
  kMECC_MultiError2InterruptEnable = MECC_ERR_SIG_EN_MULTI_ERR2_SIG_EN_MASK,
  kMECC_MultiError3InterruptEnable = MECC_ERR_SIG_EN_MULTI_ERR3_SIG_EN_MASK,
  kMECC_StrobeError0InterruptEnable = MECC_ERR_SIG_EN_STRB_ERR0_SIG_EN_MASK,
  kMECC_StrobeError1InterruptEnable = MECC_ERR_SIG_EN_STRB_ERR1_SIG_EN_MASK,
  kMECC_StrobeError2InterruptEnable = MECC_ERR_SIG_EN_STRB_ERR2_SIG_EN_MASK,
  kMECC_StrobeError3InterruptEnable = MECC_ERR_SIG_EN_STRB_ERR3_SIG_EN_MASK,
  kMECC_AccessError0InterruptEnable = MECC_ERR_SIG_EN_ADDR_ERR0_SIG_EN_MASK,
  kMECC_AccessError1InterruptEnable = MECC_ERR_SIG_EN_ADDR_ERR1_SIG_EN_MASK,
  kMECC_AccessError2InterruptEnable = MECC_ERR_SIG_EN_ADDR_ERR2_SIG_EN_MASK,
  kMECC_AccessError3InterruptEnable = MECC_ERR_SIG_EN_ADDR_ERR3_SIG_EN_MASK,
  kMECC_AllInterruptsEnable = 0xFFFF
}
 MECC interrupt configuration structure, default settings all disabled. More...
 
enum  {
  kMECC_SingleError0InterruptStatusEnable = MECC_ERR_STAT_EN_SINGLE_ERR0_STAT_EN_MASK,
  kMECC_SingleError1InterruptStatusEnable = MECC_ERR_STAT_EN_SINGLE_ERR1_STAT_EN_MASK,
  kMECC_SingleError2InterruptStatusEnable = MECC_ERR_STAT_EN_SINGLE_ERR2_STAT_EN_MASK,
  kMECC_SingleError3InterruptStatusEnable = MECC_ERR_STAT_EN_SINGLE_ERR3_STAT_EN_MASK,
  kMECC_MultiError0InterruptStatusEnable = MECC_ERR_STAT_EN_MULTI_ERR0_STAT_EN_MASK,
  kMECC_MultiError1InterruptStatusEnable = MECC_ERR_STAT_EN_MULTI_ERR1_STAT_EN_MASK,
  kMECC_MultiError2InterruptStatusEnable = MECC_ERR_STAT_EN_MULTI_ERR2_STAT_EN_MASK,
  kMECC_MultiError3InterruptStatusEnable = MECC_ERR_STAT_EN_MULTI_ERR3_STAT_EN_MASK,
  kMECC_StrobeError0InterruptStatusEnable = MECC_ERR_STAT_EN_STRB_ERR0_STAT_EN_MASK,
  kMECC_StrobeError1InterruptStatusEnable = MECC_ERR_STAT_EN_STRB_ERR1_STAT_EN_MASK,
  kMECC_StrobeError2InterruptStatusEnable = MECC_ERR_STAT_EN_STRB_ERR2_STAT_EN_MASK,
  kMECC_StrobeError3InterruptStatusEnable = MECC_ERR_STAT_EN_STRB_ERR3_STAT_EN_MASK,
  kMECC_AccessError0InterruptStatusEnable = MECC_ERR_STAT_EN_ADDR_ERR0_STAT_EN_MASK,
  kMECC_AccessError1InterruptStatusEnable = MECC_ERR_STAT_EN_ADDR_ERR1_STAT_EN_MASK,
  kMECC_AccessError2InterruptStatusEnable = MECC_ERR_STAT_EN_ADDR_ERR2_STAT_EN_MASK,
  kMECC_AccessError3InterruptStatusEnable = MECC_ERR_STAT_EN_ADDR_ERR3_STAT_EN_MASK,
  kMECC_AllInterruptsStatusEnable = 0xFFFF
}
 MECC interrupt status configuration structure, default settings all disabled. More...
 
enum  {
  kMECC_SingleError0InterruptFlag = MECC_ERR_STATUS_SINGLE_ERR0_MASK,
  kMECC_SingleError1InterruptFlag = MECC_ERR_STATUS_SINGLE_ERR1_MASK,
  kMECC_SingleError2InterruptFlag = MECC_ERR_STATUS_SINGLE_ERR2_MASK,
  kMECC_SingleError3InterruptFlag = MECC_ERR_STATUS_SINGLE_ERR3_MASK,
  kMECC_MultiError0InterruptFlag = MECC_ERR_STATUS_MULTI_ERR0_MASK,
  kMECC_MultiError1InterruptFlag = MECC_ERR_STATUS_MULTI_ERR1_MASK,
  kMECC_MultiError2InterruptFlag = MECC_ERR_STATUS_MULTI_ERR2_MASK,
  kMECC_MultiError3InterruptFlag = MECC_ERR_STATUS_MULTI_ERR3_MASK,
  kMECC_StrobeError0InterruptFlag = MECC_ERR_STATUS_STRB_ERR0_MASK,
  kMECC_StrobeError1InterruptFlag = MECC_ERR_STATUS_STRB_ERR1_MASK,
  kMECC_StrobeError2InterruptFlag = MECC_ERR_STATUS_STRB_ERR2_MASK,
  kMECC_StrobeError3InterruptFlag = MECC_ERR_STATUS_STRB_ERR3_MASK,
  kMECC_AccessError0InterruptFlag = MECC_ERR_STATUS_ADDR_ERR0_MASK,
  kMECC_AccessError1InterruptFlag = MECC_ERR_STATUS_ADDR_ERR1_MASK,
  kMECC_AccessError2InterruptFlag = MECC_ERR_STATUS_ADDR_ERR2_MASK,
  kMECC_AccessError3InterruptFlag = MECC_ERR_STATUS_ADDR_ERR3_MASK,
  kMECC_AllInterruptsFlag = 0xFFFF
}
 MECC status flags. More...
 
enum  {
  kMECC_OcramBank0 = 0U,
  kMECC_OcramBank1 = 1U,
  kMECC_OcramBank2 = 2U,
  kMECC_OcramBank3 = 3U
}
 MECC ocram bank number. More...
 
enum  _mecc_pending_flag {
  kMECC_ReadDataWaitPendingFlag = 0x1U,
  kMECC_ReadAddrPipelinePendingFlag = 0x2U,
  kMECC_WriteDataPipelinePendingFlag = 0x4U,
  kMECC_WriteAddrPipelinePendingFlag = 0x8U,
  kMECC_AllPendingFlags = 0xFU
}
 Pending flags for OCRAM wait and pipeline enable. More...
 

Driver version

#define FSL_MECC_DRIVER_VERSION   (MAKE_VERSION(2U, 1U, 0U))
 Driver version 2.1.0. More...
 

Initialization and deinitialization

void MECC_Init (MECC_Type *base, mecc_config_t *config)
 MECC module initialization function. More...
 
void MECC_Deinit (MECC_Type *base)
 Deinitializes the MECC. More...
 
void MECC_GetDefaultConfig (mecc_config_t *config)
 Sets the MECC configuration structure to default values. More...
 

Status

static uint32_t MECC_GetStatusFlags (MECC_Type *base)
 Gets MECC status flags. More...
 
static void MECC_ClearStatusFlags (MECC_Type *base, uint32_t mask)
 MECC module clear interrupt status. More...
 
static void MECC_EnableInterruptStatus (MECC_Type *base, uint32_t mask)
 MECC module enable interrupt status. More...
 
static void MECC_DisableInterruptStatus (MECC_Type *base, uint32_t mask)
 MECC module disable interrupt status. More...
 

Interrupts

static void MECC_EnableInterrupts (MECC_Type *base, uint32_t mask)
 MECC module enable interrupt. More...
 
static void MECC_DisableInterrupts (MECC_Type *base, uint32_t mask)
 MECC module disable interrupt. More...
 

functional

status_t MECC_ErrorInjection (MECC_Type *base, uint32_t lowerrordata, uint32_t higherrordata, uint8_t eccdata, uint8_t banknumber)
 MECC module error injection. More...
 
status_t MECC_GetSingleErrorInfo (MECC_Type *base, mecc_single_error_info_t *info, uint8_t banknumber)
 MECC module get single error information. More...
 
status_t MECC_GetMultiErrorInfo (MECC_Type *base, mecc_multi_error_info_t *info, uint8_t banknumber)
 MECC module get multiple error information. More...
 
static uint32_t MECC_GetPendingFlags (MECC_Type *base)
 Get pending flags for OCRAM wait and pipeline enable. More...
 

Data Structure Documentation

struct _mecc_config
Note
Ocram1StartAddress, Ocram1EndAddress, Ocram2StartAddress, Ocram2EndAddress are removed since 2.1.0 version; This changes will cause compile error for applications which use MECC driver before 2.1.0 version; To resolve compile error please use startAddress and endAddress as instead.

Data Fields

bool enableMecc
 Enable the MECC function. More...
 
uint32_t startAddress
 Start address of corresponding OCRAM memory region to enable ECC. More...
 
uint32_t endAddress
 end address of corresponding OCRAM memory region to enable ECC. More...
 
bool enableReadDataWait
 uint32_t Ocram1StartAddress; Ocram 1 start address, deprecated since 2.1.0 More...
 
bool enableReadAddrPipeline
 If enabled, the read address will be registered before can be applied to memory cell: More...
 
bool enableWriteDataPipeline
 If enabled, the write data will be registered before can be applied to memory cell: More...
 
bool enableWriteAddrPipeline
 If enabled, write address will be registered before can be applied to memory cell: More...
 

Field Documentation

bool _mecc_config::enableMecc
uint32_t _mecc_config::startAddress
uint32_t _mecc_config::endAddress
bool _mecc_config::enableReadDataWait

uint32_t Ocram1EndAddress; Ocram 1 end address, deprecated since 2.1.0

uint32_t Ocram2StartAddress; Ocram 2 start address, deprecated since 2.1.0.

uint32_t Ocram2EndAddress; Ocram 2 end address, deprecated since 2.1.0 If enabled, 1-cycle wait state will be inserted into each read access:

  • true Enable read data wait;
  • false Disable read data wait.
bool _mecc_config::enableReadAddrPipeline
  • true Enable Read address pipeline;
  • false Disable Read address pipeline.
bool _mecc_config::enableWriteDataPipeline
  • true Enable write data pipeline;
  • false Disable write data pipeline.
bool _mecc_config::enableWriteAddrPipeline
  • true Enable write address pipeline;
  • false Disable write address pipeline.
struct _mecc_single_error_info

Data Fields

uint32_t singleErrorAddress
 Single error address on Ocram bank n.
 
uint32_t singleErrorDataLow
 Single error low 32 bits uncorrected read data on Ocram bank n.
 
uint32_t singleErrorDataHigh
 Single error high 32 bits uncorrected read data on Ocram bank n.
 
uint32_t singleErrorPosLow
 Single error bit postion of low 32 bits read data on Ocram bank n.
 
uint32_t singleErrorPosHigh
 Single error bit postion of high 32 bits read data on Ocram bank n.
 
uint8_t singleErrorEccCode
 Single error ECC code on Ocram bank n.
 
struct _mecc_multi_error_info

Data Fields

uint32_t multiErrorAddress
 Multiple error address on Ocram bank n.
 
uint32_t multiErrorDataLow
 Multiple error low 32 bits read data on Ocram bank n.
 
uint32_t multiErrorDataHigh
 Multiple error high 32 bits read data on Ocram bank n.
 
uint8_t multiErrorEccCode
 Multiple error ECC code on Ocram bank n.
 

Macro Definition Documentation

#define FSL_MECC_DRIVER_VERSION   (MAKE_VERSION(2U, 1U, 0U))

Typedef Documentation

typedef struct _mecc_config mecc_config_t
Note
Ocram1StartAddress, Ocram1EndAddress, Ocram2StartAddress, Ocram2EndAddress are removed since 2.1.0 version; This changes will cause compile error for applications which use MECC driver before 2.1.0 version; To resolve compile error please use startAddress and endAddress as instead.

Enumeration Type Documentation

anonymous enum
Enumerator
kStatus_MECC_BankMiss 

Ocram bank miss.

anonymous enum

This structure contains the settings for all of the MECC interrupt configurations.

Enumerator
kMECC_SingleError0InterruptEnable 

Single Bit Error On Ocram Bank0 interrupt enable.

kMECC_SingleError1InterruptEnable 

Single Bit Error On Ocram Bank1 interrupt enable.

kMECC_SingleError2InterruptEnable 

Single Bit Error On Ocram Bank2 interrupt enable.

kMECC_SingleError3InterruptEnable 

Single Bit Error On Ocram Bank3 interrupt enable.

kMECC_MultiError0InterruptEnable 

Multiple Bits Error On Ocram Bank0 interrupt enable.

kMECC_MultiError1InterruptEnable 

Multiple Bits Error On Ocram Bank1 interrupt enable.

kMECC_MultiError2InterruptEnable 

Multiple Bits Error On Ocram Bank2 interrupt enable.

kMECC_MultiError3InterruptEnable 

Multiple Bits Error On Ocram Bank3 interrupt enable.

kMECC_StrobeError0InterruptEnable 

AXI Strobe Error On Ocram Bank0 interrupt enable.

kMECC_StrobeError1InterruptEnable 

AXI Strobe Error On Ocram Bank1 interrupt enable.

kMECC_StrobeError2InterruptEnable 

AXI Strobe Error On Ocram Bank2 interrupt enable.

kMECC_StrobeError3InterruptEnable 

AXI Strobe Error On Ocram Bank3 interrupt enable.

kMECC_AccessError0InterruptEnable 

Ocram Access Error On Bank0 interrupt enable.

kMECC_AccessError1InterruptEnable 

Ocram Access Error On Bank1 interrupt enable.

kMECC_AccessError2InterruptEnable 

Ocram Access Error On Bank2 interrupt enable.

kMECC_AccessError3InterruptEnable 

Ocram Access Error On Bank3 interrupt enable.

kMECC_AllInterruptsEnable 

all interrupts enable

anonymous enum

This structure contains the settings for all of the MECC interrupt status configurations.

Enumerator
kMECC_SingleError0InterruptStatusEnable 

Single Bit Error On Ocram Bank0 interrupt status enable.

kMECC_SingleError1InterruptStatusEnable 

Single Bit Error On Ocram Bank1 interrupt status enable.

kMECC_SingleError2InterruptStatusEnable 

Single Bit Error On Ocram Bank2 interrupt status enable.

kMECC_SingleError3InterruptStatusEnable 

Single Bit Error On Ocram Bank3 interrupt status enable.

kMECC_MultiError0InterruptStatusEnable 

Multiple Bits Error On Ocram Bank0 interrupt status enable.

kMECC_MultiError1InterruptStatusEnable 

Multiple Bits Error On Ocram Bank1 interrupt status enable.

kMECC_MultiError2InterruptStatusEnable 

Multiple Bits Error On Ocram Bank2 interrupt status enable.

kMECC_MultiError3InterruptStatusEnable 

Multiple Bits Error On Ocram Bank3 interrupt status enable.

kMECC_StrobeError0InterruptStatusEnable 

AXI Strobe Error On Ocram Bank0 interrupt status enable.

kMECC_StrobeError1InterruptStatusEnable 

AXI Strobe Error On Ocram Bank1 interrupt status enable.

kMECC_StrobeError2InterruptStatusEnable 

AXI Strobe Error On Ocram Bank2 interrupt status enable.

kMECC_StrobeError3InterruptStatusEnable 

AXI Strobe Error On Ocram Bank3 interrupt status enable.

kMECC_AccessError0InterruptStatusEnable 

Ocram Access Error On Bank0 interrupt status enable.

kMECC_AccessError1InterruptStatusEnable 

Ocram Access Error On Bank1 interrupt status enable.

kMECC_AccessError2InterruptStatusEnable 

Ocram Access Error On Bank2 interrupt status enable.

kMECC_AccessError3InterruptStatusEnable 

Ocram Access Error On Bank3 interrupt status enable.

kMECC_AllInterruptsStatusEnable 

all interrupts enable

anonymous enum

This provides constants for the MECC status flags for use in the MECC functions.

Enumerator
kMECC_SingleError0InterruptFlag 

Single Bit Error On Ocram Bank0 interrupt flag.

kMECC_SingleError1InterruptFlag 

Single Bit Error On Ocram Bank1 interrupt flag.

kMECC_SingleError2InterruptFlag 

Single Bit Error On Ocram Bank2 interrupt flag.

kMECC_SingleError3InterruptFlag 

Single Bit Error On Ocram Bank3 interrupt flag.

kMECC_MultiError0InterruptFlag 

Multiple Bits Error On Ocram Bank0 interrupt flag.

kMECC_MultiError1InterruptFlag 

Multiple Bits Error On Ocram Bank1 interrupt flag.

kMECC_MultiError2InterruptFlag 

Multiple Bits Error On Ocram Bank2 interrupt flag.

kMECC_MultiError3InterruptFlag 

Multiple Bits Error On Ocram Bank3 interrupt flag.

kMECC_StrobeError0InterruptFlag 

AXI Strobe Error On Ocram Bank0 interrupt flag.

kMECC_StrobeError1InterruptFlag 

AXI Strobe Error On Ocram Bank1 interrupt flag.

kMECC_StrobeError2InterruptFlag 

AXI Strobe Error On Ocram Bank2 interrupt flag.

kMECC_StrobeError3InterruptFlag 

AXI Strobe Error On Ocram Bank3 interrupt flag.

kMECC_AccessError0InterruptFlag 

Ocram Access Error On Bank0 interrupt flag.

kMECC_AccessError1InterruptFlag 

Ocram Access Error On Bank1 interrupt flag.

kMECC_AccessError2InterruptFlag 

Ocram Access Error On Bank2 interrupt flag.

kMECC_AccessError3InterruptFlag 

Ocram Access Error On Bank3 interrupt flag.

kMECC_AllInterruptsFlag 

all interrupts interrupt flag

anonymous enum
Enumerator
kMECC_OcramBank0 

ocram bank number 0: ocram_base_address+0x20*i

kMECC_OcramBank1 

ocram bank number 1: ocram_base_address+0x20*i+0x8

kMECC_OcramBank2 

ocram bank number 2: ocram_base_address+0x20*i+0x10

kMECC_OcramBank3 

ocram bank number 3: ocram_base_address+0x20*i+0x18

.

Enumerator
kMECC_ReadDataWaitPendingFlag 

Indicate an update pending status for read data wait.

kMECC_ReadAddrPipelinePendingFlag 

Indicate an update pending status for read address pipeline.

kMECC_WriteDataPipelinePendingFlag 

Indicate an update pending status for write data pipeline.

kMECC_WriteAddrPipelinePendingFlag 

Indicate an update pending status for write address pipeline.

kMECC_AllPendingFlags 

Indicate all pending status flags.

Function Documentation

void MECC_Init ( MECC_Type *  base,
mecc_config_t *  config 
)
Parameters
baseMECC base address.
configpointer to the MECC configuration structure.
void MECC_Deinit ( MECC_Type *  base)
Parameters
baseMECC base address.
void MECC_GetDefaultConfig ( mecc_config_t *  config)
Parameters
configpointer to the MECC configuration structure.
static uint32_t MECC_GetStatusFlags ( MECC_Type *  base)
inlinestatic
Parameters
baseMECC peripheral base address.
Returns
MECC status flags.
static void MECC_ClearStatusFlags ( MECC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseMECC base address.
maskstatus to clear.
static void MECC_EnableInterruptStatus ( MECC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseMECC base address.
maskstatus to enable.
static void MECC_DisableInterruptStatus ( MECC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseMECC base address.
maskstatus to disable.
static void MECC_EnableInterrupts ( MECC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseMECC base address.
maskThe interrupts to enable.
static void MECC_DisableInterrupts ( MECC_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseMECC base address.
maskThe interrupts to disable.
status_t MECC_ErrorInjection ( MECC_Type *  base,
uint32_t  lowerrordata,
uint32_t  higherrordata,
uint8_t  eccdata,
uint8_t  banknumber 
)
Parameters
baseMECC base address.
lowerrordatalow 32 bits data.
higherrordatahigh 32 bits data.
eccdataecc code.
banknumberocram bank number.
Return values
kStatus_Success.Bank0: ocram_base_address+0x20*i Bank1: ocram_base_address+0x20*i+0x8 Bank2: ocram_base_address+0x20*i+0x10 Bank3: ocram_base_address+0x20*i+0x18 i = 0,1,2,3,4.....
status_t MECC_GetSingleErrorInfo ( MECC_Type *  base,
mecc_single_error_info_t *  info,
uint8_t  banknumber 
)
Parameters
baseMECC base address.
infosingle error information.
banknumberocram bank number.
Return values
kStatus_Success.
kStatus_MECC_BankMiss.Bank0: ocram_base_address+0x20*i Bank1: ocram_base_address+0x20*i+0x8 Bank2: ocram_base_address+0x20*i+0x10 Bank3: ocram_base_address+0x20*i+0x18 i = 0,1,2,3,4.....
status_t MECC_GetMultiErrorInfo ( MECC_Type *  base,
mecc_multi_error_info_t *  info,
uint8_t  banknumber 
)
Parameters
baseMECC base address.
infomultiple error information.
banknumberocram bank number.
Return values
kStatus_Success.
kStatus_MECC_BankMiss.Bank0: ocram_base_address+0x20*i Bank1: ocram_base_address+0x20*i+0x8 Bank2: ocram_base_address+0x20*i+0x10 Bank3: ocram_base_address+0x20*i+0x18 i = 0,1,2,3,4.....
static uint32_t MECC_GetPendingFlags ( MECC_Type *  base)
inlinestatic
Parameters
baseMECC base address.
Returns
Pending flags, should be the OR'ed value of mecc_pending_flag_t.