MCUXpresso SDK API Reference Manual  Rev 2.16.100
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
ADC: Analog Digital Converter

Overview

The MCUXpresso SDK provides a driver for the Analog Digital converter (ADC) module of MCUXpresso SDK devices.

Function Groups

The ADC driver can be divided into 7 function groups.

ADC Basic Control Interfaces

The functions in this group can be used to configure the whole ADC module. To initialize the ADC module, the ADC_Init() is provided. Before invoking ADC_Init() function, user can use ADC_GetDefaultConfig() function to get default configurations.

ADC Calibration Control Interfaces

The ADC module supports both automatic calibration and user defined calibration. To do auto calibration, the function ADC_DoAutoCalibration() is provided, to do user defined calibration, the function ADC_DoUserCalibration() is provided.

ADC Temperature Sensor Control Interfaces

The functions in this group can be used to control temperature sensor, including enableing temperature sensor and setting temperature sensor mode.

ADC Audio Control Interfaces

This function group contains 3 functions to control audio. ADC_EnableAudio() can be used to enable/disable audio PGA and decimation rate select. ADC_SetAudioPGAVoltageGain() can be used to set audio PGA voltage gain. ADC_ConfigAudioVoiceLevel() can be used to configure audio voice level.

ADC Conversion Related Interfaces

Conversion related function are placed in this function group. If the trigger mode is set as software trigger, invoking ADC_DoSoftwareTrigger() to trigger the scan. ADC_SetScanChannel() function can be used to set each channel's mux source. After conversion completed, ADC_GetConversionResult() can be used to get 32-bit width packed ADC conversion result.

ADC Interrupt Control Interfaces

The functions in this group can be used to enable/disable interrupts.

ADC Status Control Interfaces

The ACOMP_GetStatusFlags() function in this group can return all status flags. The ACOMP_ClearStatusFlags() can be used to clear status flags, but please note that no all status flags can be cleared by software.

Data Structures

struct  adc_config_t
 The structure of adc options, including clock divider, power mode, and so on. More...
 

Macros

#define FSL_ADC_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))
 ADC driver version. More...
 

Enumerations

enum  _adc_interrupt_enable {
  kADC_DataReadyInterruptEnable = ADC_ADC_REG_IMR_RDY_MASK_MASK,
  kADC_GainSaturationInterruptEnable = ADC_ADC_REG_IMR_GAINSAT_MASK_MASK,
  kADC_OffsetSaturationInterruptEnable = ADC_ADC_REG_IMR_OFFSAT_MASK_MASK,
  kADC_NegativeSaturationInterruptEnable = ADC_ADC_REG_IMR_DATASAT_NEG_MASK_MASK,
  kADC_PositiveSaturationInterruptEnable = ADC_ADC_REG_IMR_DATASAT_POS_MASK_MASK,
  kADC_FifoOverrunInterruptEnable = ADC_ADC_REG_IMR_FIFO_OVERRUN_MASK_MASK,
  kADC_FifoUnderrunInterruptEnable = ADC_ADC_REG_IMR_FIFO_UNDERRUN_MASK_MASK
}
 The enumeration of interrupts, this enumeration can be used to enable/disable interrupts. More...
 
enum  _adc_status_flags {
  kADC_DataReadyInterruptFlag = 1UL << 0UL,
  kADC_GainSaturationInterruptFlag = 1UL << 1UL,
  kADC_OffsetSaturationInterruptFlag = 1UL << 2UL,
  kADC_NegativeSaturationInterruptFlag = 1UL << 3UL,
  kADC_PositiveSaturationInterruptFlag = 1UL << 4UL,
  kADC_FifoOverrunInterruptFlag = 1UL << 5UL,
  kADC_FifoUnderrunInterruptFlag = 1UL << 6UL,
  kADC_DataReadyRawFlag = 1UL << 7UL,
  kADC_GainSaturationRawFlag = 1UL << 8UL,
  kADC_OffsetSaturationRawFlag = 1UL << 9UL,
  kADC_NegativeSaturationRawFlag = 1UL << 10UL,
  kADC_PositiveSaturationRawFlag = 1UL << 11UL,
  kADC_FifoOverrunRawFlag = 1UL << 12UL,
  kADC_FifoUnderrunRawFlag = 1UL << 13UL,
  kADC_ActiveStatusFlag = 1UL << 14UL,
  kADC_FIFONotEmptyStatusFlag = 1UL << 15UL,
  kADC_FifoFullStatusFlag = 1UL << 16UL
}
 The enumeration of adc status flags, including interrupt flags, raw flags, and so on. More...
 
enum  adc_clock_divider_t {
  kADC_ClockDivider1 = 0U,
  kADC_ClockDivider2 = 1U,
  kADC_ClockDivider3 = 2U,
  kADC_ClockDivider4 = 3U,
  kADC_ClockDivider5 = 4U,
  kADC_ClockDivider6 = 5U,
  kADC_ClockDivider7 = 6U,
  kADC_ClockDivider8 = 7U,
  kADC_ClockDivider9 = 8U,
  kADC_ClockDivider10 = 9U,
  kADC_ClockDivider11 = 10U,
  kADC_ClockDivider12 = 11U,
  kADC_ClockDivider13 = 12U,
  kADC_ClockDivider14 = 13U,
  kADC_ClockDivider15 = 14U,
  kADC_ClockDivider16 = 15U,
  kADC_ClockDivider17 = 16U,
  kADC_ClockDivider18 = 17U,
  kADC_ClockDivider19 = 18U,
  kADC_ClockDivider20 = 19U,
  kADC_ClockDivider21 = 20U,
  kADC_ClockDivider22 = 21U,
  kADC_ClockDivider23 = 22U,
  kADC_ClockDivider24 = 23U,
  kADC_ClockDivider25 = 24U,
  kADC_ClockDivider26 = 25U,
  kADC_ClockDivider27 = 26U,
  kADC_ClockDivider28 = 27U,
  kADC_ClockDivider29 = 28U,
  kADC_ClockDivider30 = 29U,
  kADC_ClockDivider31 = 30U,
  kADC_ClockDivider32 = 31U
}
 ADC clock divider ratio type. More...
 
enum  adc_analog_portion_power_mode_t {
  kADC_PowerModeFullBiasingCurrent = 0U,
  kADC_PowerModeHalfBiasingCurrent
}
 ADC analog portion low-power mode selection. More...
 
enum  adc_resolution_t {
  kADC_Resolution12Bit = 0U,
  kADC_Resolution14Bit = 1U,
  kADC_Resolution16Bit = 2U,
  kADC_Resolution16BitAudio = 3U
}
 ADC resolution type. More...
 
enum  adc_warm_up_time_t {
  kADC_WarmUpTime1us = 0U,
  kADC_WarmUpTime2us,
  kADC_WarmUpTime3us,
  kADC_WarmUpTime4us,
  kADC_WarmUpTime5us,
  kADC_WarmUpTime6us,
  kADC_WarmUpTime7us,
  kADC_WarmUpTime8us,
  kADC_WarmUpTime9us,
  kADC_WarmUpTime10us,
  kADC_WarmUpTime11us,
  kADC_WarmUpTime12us,
  kADC_WarmUpTime13us,
  kADC_WarmUpTime14us,
  kADC_WarmUpTime15us,
  kADC_WarmUpTime16us,
  kADC_WarmUpTime17us,
  kADC_WarmUpTime18us,
  kADC_WarmUpTime19us,
  kADC_WarmUpTime20us,
  kADC_WarmUpTime21us,
  kADC_WarmUpTime22us,
  kADC_WarmUpTime23us,
  kADC_WarmUpTime24us,
  kADC_WarmUpTime25us,
  kADC_WarmUpTime26us,
  kADC_WarmUpTime27us,
  kADC_WarmUpTime28us,
  kADC_WarmUpTime29us,
  kADC_WarmUpTime30us,
  kADC_WarmUpTime31us,
  kADC_WarmUpTime32us,
  kADC_WarmUpStateBypass = 0x20U
}
 The enumeration of adc warm up time, the ADC warm-up state can also bypassed. More...
 
enum  adc_vref_source_t {
  kADC_Vref1P8V = 0U,
  kADC_Vref1P2V = 1U,
  kADC_VrefExternal = 2U,
  kADC_VrefInternal1P2V = 3U
}
 ADC voltage reference source type. More...
 
enum  adc_input_mode_t {
  kADC_InputSingleEnded = 0U,
  kADC_InputDifferential = 1U
}
 ADC input mode type. More...
 
enum  adc_conversion_mode_t {
  kADC_ConversionOneShot = 0U,
  kADC_ConversionContinuous = 1U
}
 ADC conversion mode type. More...
 
enum  adc_scan_length_t {
  kADC_ScanLength_1 = 0U,
  kADC_ScanLength_2 = 1U,
  kADC_ScanLength_3 = 2U,
  kADC_ScanLength_4 = 3U,
  kADC_ScanLength_5 = 4U,
  kADC_ScanLength_6 = 5U,
  kADC_ScanLength_7 = 6U,
  kADC_ScanLength_8 = 7U,
  kADC_ScanLength_9 = 8U,
  kADC_ScanLength_10 = 9U,
  kADC_ScanLength_11 = 10U,
  kADC_ScanLength_12 = 11U,
  kADC_ScanLength_13 = 12U,
  kADC_ScanLength_14 = 13U,
  kADC_ScanLength_15 = 14U,
  kADC_ScanLength_16 = 15U
}
 ADC scan length type. More...
 
enum  adc_average_length_t {
  kADC_AverageNone = 0U,
  kADC_Average2 = 1U,
  kADC_Average4 = 2U,
  kADC_Average8 = 3U,
  kADC_Average16 = 4U
}
 ADC average length type. More...
 
enum  adc_input_gain_t {
  kADC_InputGain0P5 = 0U,
  kADC_InputGain1 = 1U,
  kADC_InputGain2 = 2U
}
 ADC input buffer gain type. More...
 
enum  adc_result_width_t {
  kADC_ResultWidth16 = 0U,
  kADC_ResultWidth32 = 1U
}
 ADC result width type. More...
 
enum  adc_fifo_threshold_t {
  kADC_FifoThresholdData1 = 0U,
  kADC_FifoThresholdData4,
  kADC_FifoThresholdData8,
  kADC_FifoThresholdData16
}
 The threshold of FIFO. More...
 
enum  adc_calibration_ref_t {
  kADC_CalibrationVrefInternal = 0,
  kADC_CalibrationVrefExternal = 1
}
 ADC calibration voltage reference type. More...
 
enum  adc_scan_channel_t {
  kADC_ScanChannel0 = 0U,
  kADC_ScanChannel1 = 1U,
  kADC_ScanChannel2 = 2U,
  kADC_ScanChannel3 = 3U,
  kADC_ScanChannel4 = 4U,
  kADC_ScanChannel5 = 5U,
  kADC_ScanChannel6 = 6U,
  kADC_ScanChannel7 = 7U,
  kADC_ScanChannel8 = 8U,
  kADC_ScanChannel9 = 9U,
  kADC_ScanChannel10 = 10U,
  kADC_ScanChannel11 = 11U,
  kADC_ScanChannel12 = 12U,
  kADC_ScanChannel13 = 13U,
  kADC_ScanChannel14 = 14U,
  kADC_ScanChannel15 = 15U
}
 ADC scan channel type. More...
 
enum  adc_channel_source_t {
  kADC_CH0 = 0U,
  kADC_CH1 = 1U,
  kADC_CH2 = 2U,
  kADC_CH3 = 3U,
  kADC_CH4 = 4U,
  kADC_CH5 = 5U,
  kADC_CH6 = 6U,
  kADC_CH7 = 7U,
  kADC_VBATS = 8U,
  kADC_VREF = 9U,
  kADC_DACA = 10U,
  kADC_DACB = 11U,
  kADC_VSSA = 12U,
  kADC_CH0_CH1 = 0U,
  kADC_CH2_CH3 = 1U,
  kADC_CH4_CH5 = 2U,
  kADC_CH6_CH7 = 3U,
  kADC_DACA_DACB = 4U
}
 ADC channel source type. More...
 
enum  adc_temperature_sensor_mode_t { kADC_TSensorExternal }
 Temperature sensor mode, including internal diode mode and external diode mode. More...
 
enum  adc_audio_pga_voltage_gain_t {
  kADC_AudioGain4 = 0U,
  kADC_AudioGain8 = 1U,
  kADC_AudioGain16 = 2U,
  kADC_AudioGain32 = 3U
}
 ADC audio pga gain type. More...
 
enum  adc_audio_voice_level_t {
  kADC_VoiceLevel0 = 0U,
  kADC_VoiceLevel1 = 1U,
  kADC_VoiceLevel2 = 2U,
  kADC_VoiceLevel3 = 3U
}
 ADC audio voice level selection. More...
 

ADC Basic Control Interfaces

void ADC_Init (ADC_Type *base, const adc_config_t *config)
 Initialize ADC module, including clock divider, power mode, and so on. More...
 
void ADC_GetDefaultConfig (adc_config_t *config)
 Get default configuration. More...
 
void ADC_Deinit (ADC_Type *base)
 De-initialize the ADC module. More...
 
static void ADC_DoSoftwareReset (ADC_Type *base)
 Reset the whole ADC block. More...
 
static void ADC_SelectAnalogPortionPowerMode (ADC_Type *base, adc_analog_portion_power_mode_t powerMode)
 Select ADC analog portion power mode. More...
 

ADC Calibration Control Interfaces

status_t ADC_DoAutoCalibration (ADC_Type *base, adc_calibration_ref_t calVref)
 Do automatic calibration measurement. More...
 
static void ADC_GetAutoCalibrationData (ADC_Type *base, uint16_t *offsetCal, uint16_t *gainCal)
 Get the ADC automatic calibration data. More...
 
static void ADC_ResetAutoCalibrationData (ADC_Type *base)
 Reset the automatic calibration data. More...
 
static void ADC_DoUserCalibration (ADC_Type *base, uint16_t offsetCal, uint16_t gainCal)
 Do user defined calibration. More...
 

ADC Temperature Sensor Control Interfaces

static void ADC_EnableTemperatureSensor (ADC_Type *base, bool enable)
 Enable/disable temperature sensor. More...
 
static void ADC_SetTemperatureSensorMode (ADC_Type *base, adc_temperature_sensor_mode_t tSensorMode)
 Set temperature sensor mode, available selections are internal diode mode and external diode mode. More...
 

ADC Audio Control Interfaces

static void ADC_EnableAudio (ADC_Type *base, bool enable)
 Enable/disable audio PGA and decimation rate select. More...
 
static void ADC_SetAudioPGAVoltageGain (ADC_Type *base, adc_audio_pga_voltage_gain_t voltageGain)
 Set audio PGA voltage gain. More...
 
void ADC_ConfigAudioVoiceLevel (ADC_Type *base, bool enableDetect, adc_audio_voice_level_t voiceLevel)
 Configure audio voice level. More...
 

ADC Conversion Related Interfaces

void ADC_SetScanChannel (ADC_Type *base, adc_scan_channel_t scanChannel, adc_channel_source_t channelSource)
 Set scan channel mux source. More...
 
static void ADC_DoSoftwareTrigger (ADC_Type *base)
 If trigger mode is selected as software trigger, invoking this function to start conversion. More...
 
static void ADC_StopConversion (ADC_Type *base)
 Invoke this function to stop conversion. More...
 
static uint32_t ADC_GetConversionResult (ADC_Type *base)
 Get the 32-bit width packed ADC conversion result. More...
 
static uint8_t ADC_GetFifoDataCount (ADC_Type *base)
 Get the ADC FIFO data count. More...
 

ADC Interrupt Control Interfaces

static void ADC_EnableInterrupts (ADC_Type *base, uint32_t interruptMask)
 Enable interrupts, such as conversion data ready interrupt, gain correction saturation interrupt, FIFO under run interrupt, and so on. More...
 
static void ADC_DisableInterrupts (ADC_Type *base, uint32_t interruptMask)
 Disable interrupts, such as conversion data ready interrupt, gain correction saturation interrupt, FIFO under run interrupt, and so on. More...
 

ADC Status Control Interfaces

uint32_t ADC_GetStatusFlags (ADC_Type *base)
 Get status flags, including interrupt flags, raw flags, and so on. More...
 
static void ADC_ClearStatusFlags (ADC_Type *base, uint32_t statusFlagsMask)
 Clear status flags. More...
 

Data Structure Documentation

struct adc_config_t

Data Fields

adc_clock_divider_t clockDivider: 5U
 Analog 64M clock division ratio, please refer to adc_clock_divider_t. More...
 
adc_resolution_t resolution: 2U
 Configure ADC resolution, please refer to adc_resolution_t. More...
 
adc_warm_up_time_t warmupTime: 6U
 Configure warm-up time. More...
 
adc_vref_source_t vrefSource: 2U
 Configure voltage reference source, please refer to adc_vref_source_t. More...
 
adc_input_mode_t inputMode: 1U
 Configure input mode, such as kADC_InputSingleEnded or kADC_InputDifferential. More...
 
adc_conversion_mode_t conversionMode: 1U
 Configure convrsion mode, such as kADC_ConversionOneShot or kADC_ConversionContinuous. More...
 
adc_scan_length_t scanLength: 4U
 Configure the length of scan, please refer to adc_scan_length_t. More...
 
adc_average_length_t averageLength: 3U
 Configure hardware average number, please refer to adc_average_length_t.
 
adc_trigger_source_t triggerSource: 3U
 Configure trigger source, the trigger source can be divided into hardware trigger and software trigger, please refer to adc_trigger_source_t for details. More...
 
adc_input_gain_t inputGain: 2U
 Configure ADC input buffer gain, please refer to adc_input_gain_t. More...
 
bool enableInputGainBuffer: 1U
 Enable/Disable input gain buffer. More...
 
bool enableInputBufferChop: 1U
 Enable/Disable input buffer chopper: More...
 
bool enableChop: 1U
 Enable/Disable the ADC chopper: More...
 
adc_result_width_t resultWidth: 1U
 Select result FIFO data packed format, please refer to adc_result_width_t. More...
 
adc_fifo_threshold_t fifoThreshold: 2U
 Configure FIFO threshold, please refer to adc_fifo_threshold_t. More...
 
bool enableDMA: 1U
 Enable/Disable DMA reqeust. More...
 
bool enableADC: 1U
 Enable/Disable ADC module. More...
 

Field Documentation

adc_clock_divider_t adc_config_t::clockDivider
adc_resolution_t adc_config_t::resolution
adc_warm_up_time_t adc_config_t::warmupTime
adc_vref_source_t adc_config_t::vrefSource
adc_input_mode_t adc_config_t::inputMode
adc_conversion_mode_t adc_config_t::conversionMode
adc_scan_length_t adc_config_t::scanLength
adc_trigger_source_t adc_config_t::triggerSource
adc_input_gain_t adc_config_t::inputGain
bool adc_config_t::enableInputGainBuffer
  • true Enable input gain buffer.
  • false Disable input gain buffer.
bool adc_config_t::enableInputBufferChop
  • true Enable input buffer chopper;
  • false Disable input buffer chopper.
bool adc_config_t::enableChop
  • true Enable the chopper;
  • false Disable the chopper.
adc_result_width_t adc_config_t::resultWidth
adc_fifo_threshold_t adc_config_t::fifoThreshold
bool adc_config_t::enableDMA
  • true Enable DMA request.
  • false Disable DMA request.
bool adc_config_t::enableADC
  • true Enable ADC module.
  • false Disable ADC module.

Macro Definition Documentation

#define FSL_ADC_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))

Version 2.2.0.

Enumeration Type Documentation

Enumerator
kADC_DataReadyInterruptEnable 

Conversion data ready interrupt.

kADC_GainSaturationInterruptEnable 

Gain correction saturation interrupt.

kADC_OffsetSaturationInterruptEnable 

Offset correction saturation interupt enable.

kADC_NegativeSaturationInterruptEnable 

ADC data negative side saturation interrupt enable.

kADC_PositiveSaturationInterruptEnable 

ADC data positive side saturation interrupt enable.

kADC_FifoOverrunInterruptEnable 

FIFO overrun interrupt enable.

kADC_FifoUnderrunInterruptEnable 

FIFO underrun interrupt enable.

Note
The raw flags will be captured regardless the interrupt mask. Both interrupt flags and raw flags can be cleared.
Enumerator
kADC_DataReadyInterruptFlag 

Conversion Data Ready interrupt flag.

kADC_GainSaturationInterruptFlag 

Gain correction saturation interrupt flag.

kADC_OffsetSaturationInterruptFlag 

Offset correction saturation interupt flag.

kADC_NegativeSaturationInterruptFlag 

ADC data negative side saturation interrupt flag.

kADC_PositiveSaturationInterruptFlag 

ADC data positive side saturation interrupt flag.

kADC_FifoOverrunInterruptFlag 

FIFO overrun interrupt flag.

kADC_FifoUnderrunInterruptFlag 

FIFO underrun interrupt flag.

kADC_DataReadyRawFlag 

Conversion data ready raw flag, this flag will be captured regardless the interrupt mask.

kADC_GainSaturationRawFlag 

Gain correction saturation raw flag, this flag will be captured regardless the interrupt mask.

kADC_OffsetSaturationRawFlag 

Offset correction saturation raw flag, this flag will be captured regardless the interrupt mask.

kADC_NegativeSaturationRawFlag 

ADC data negative side saturation raw flag, this flag will be captured regardless the interrupt mask.

kADC_PositiveSaturationRawFlag 

ADC data positive side saturation raw flag, this flag will be captured regardless the interrupt mask.

kADC_FifoOverrunRawFlag 

FIFO overrun raw flag, this flag will be captured regardless the interrupt mask.

kADC_FifoUnderrunRawFlag 

FIFO underrun interrupt mask, this flag will be captured regardless the interrupt mask.

kADC_ActiveStatusFlag 

ADC conversion active status flag.

kADC_FIFONotEmptyStatusFlag 

FIFO not empty status flag.

kADC_FifoFullStatusFlag 

FIFO full status flag.

Enumerator
kADC_ClockDivider1 

Clock divider ratio is 1.

kADC_ClockDivider2 

Clock divider ratio is 2.

kADC_ClockDivider3 

Clock divider ratio is 3.

kADC_ClockDivider4 

Clock divider ratio is 4.

kADC_ClockDivider5 

Clock divider ratio is 5.

kADC_ClockDivider6 

Clock divider ratio is 6.

kADC_ClockDivider7 

Clock divider ratio is 7.

kADC_ClockDivider8 

Clock divider ratio is 8.

kADC_ClockDivider9 

Clock divider ratio is 9.

kADC_ClockDivider10 

Clock divider ratio is 10.

kADC_ClockDivider11 

Clock divider ratio is 11.

kADC_ClockDivider12 

Clock divider ratio is 12.

kADC_ClockDivider13 

Clock divider ratio is 13.

kADC_ClockDivider14 

Clock divider ratio is 14.

kADC_ClockDivider15 

Clock divider ratio is 15.

kADC_ClockDivider16 

Clock divider ratio is 16.

kADC_ClockDivider17 

Clock divider ratio is 17.

kADC_ClockDivider18 

Clock divider ratio is 18.

kADC_ClockDivider19 

Clock divider ratio is 19.

kADC_ClockDivider20 

Clock divider ratio is 20.

kADC_ClockDivider21 

Clock divider ratio is 21.

kADC_ClockDivider22 

Clock divider ratio is 22.

kADC_ClockDivider23 

Clock divider ratio is 23.

kADC_ClockDivider24 

Clock divider ratio is 24.

kADC_ClockDivider25 

Clock divider ratio is 25.

kADC_ClockDivider26 

Clock divider ratio is 26.

kADC_ClockDivider27 

Clock divider ratio is 27.

kADC_ClockDivider28 

Clock divider ratio is 28.

kADC_ClockDivider29 

Clock divider ratio is 29.

kADC_ClockDivider30 

Clock divider ratio is 30.

kADC_ClockDivider31 

Clock divider ratio is 31.

kADC_ClockDivider32 

Clock divider ratio is 32.

Enumerator
kADC_PowerModeFullBiasingCurrent 

Full biasing current.

kADC_PowerModeHalfBiasingCurrent 

Half biasing current.

Enumerator
kADC_Resolution12Bit 

12-bit resolution

kADC_Resolution14Bit 

14-bit resolution

kADC_Resolution16Bit 

16-bit resolution

kADC_Resolution16BitAudio 

16-bit resolution for audio application

Enumerator
kADC_WarmUpTime1us 

ADC warm-up time is 1 us.

kADC_WarmUpTime2us 

ADC warm-up time is 2 us.

kADC_WarmUpTime3us 

ADC warm-up time is 3 us.

kADC_WarmUpTime4us 

ADC warm-up time is 4 us.

kADC_WarmUpTime5us 

ADC warm-up time is 5 us.

kADC_WarmUpTime6us 

ADC warm-up time is 6 us.

kADC_WarmUpTime7us 

ADC warm-up time is 7 us.

kADC_WarmUpTime8us 

ADC warm-up time is 8 us.

kADC_WarmUpTime9us 

ADC warm-up time is 9 us.

kADC_WarmUpTime10us 

ADC warm-up time is 10 us.

kADC_WarmUpTime11us 

ADC warm-up time is 11 us.

kADC_WarmUpTime12us 

ADC warm-up time is 12 us.

kADC_WarmUpTime13us 

ADC warm-up time is 13 us.

kADC_WarmUpTime14us 

ADC warm-up time is 14 us.

kADC_WarmUpTime15us 

ADC warm-up time is 15 us.

kADC_WarmUpTime16us 

ADC warm-up time is 16 us.

kADC_WarmUpTime17us 

ADC warm-up time is 17 us.

kADC_WarmUpTime18us 

ADC warm-up time is 18 us.

kADC_WarmUpTime19us 

ADC warm-up time is 19 us.

kADC_WarmUpTime20us 

ADC warm-up time is 20 us.

kADC_WarmUpTime21us 

ADC warm-up time is 21 us.

kADC_WarmUpTime22us 

ADC warm-up time is 22 us.

kADC_WarmUpTime23us 

ADC warm-up time is 23 us.

kADC_WarmUpTime24us 

ADC warm-up time is 24 us.

kADC_WarmUpTime25us 

ADC warm-up time is 25 us.

kADC_WarmUpTime26us 

ADC warm-up time is 26 us.

kADC_WarmUpTime27us 

ADC warm-up time is 27 us.

kADC_WarmUpTime28us 

ADC warm-up time is 28 us.

kADC_WarmUpTime29us 

ADC warm-up time is 29 us.

kADC_WarmUpTime30us 

ADC warm-up time is 30 us.

kADC_WarmUpTime31us 

ADC warm-up time is 31 us.

kADC_WarmUpTime32us 

ADC warm-up time is 32 us.

kADC_WarmUpStateBypass 

ADC warm-up state bypassed.

Enumerator
kADC_Vref1P8V 

Internal 1.8V reference.

kADC_Vref1P2V 

Internal 1.2V reference.

kADC_VrefExternal 

External single-ended reference though ADC_CH3.

kADC_VrefInternal1P2V 

Internal 1.2V reference with cap filter though ADC_CH3.

Enumerator
kADC_InputSingleEnded 

Single-ended mode.

kADC_InputDifferential 

Differential mode.

Enumerator
kADC_ConversionOneShot 

One shot mode.

kADC_ConversionContinuous 

Continuous mode.

Enumerator
kADC_ScanLength_1 

Scan length is 1.

kADC_ScanLength_2 

Scan length is 2.

kADC_ScanLength_3 

Scan length is 3.

kADC_ScanLength_4 

Scan length is 4.

kADC_ScanLength_5 

Scan length is 5.

kADC_ScanLength_6 

Scan length is 6.

kADC_ScanLength_7 

Scan length is 7.

kADC_ScanLength_8 

Scan length is 8.

kADC_ScanLength_9 

Scan length is 9.

kADC_ScanLength_10 

Scan length is 10.

kADC_ScanLength_11 

Scan length is 11.

kADC_ScanLength_12 

Scan length is 12.

kADC_ScanLength_13 

Scan length is 13.

kADC_ScanLength_14 

Scan length is 14.

kADC_ScanLength_15 

Scan length is 15.

kADC_ScanLength_16 

Scan length is 16.

Enumerator
kADC_AverageNone 

Average length: no average.

kADC_Average2 

Average length: 2.

kADC_Average4 

Average length: 4.

kADC_Average8 

Average length: 8.

kADC_Average16 

Average length: 16.

Enumerator
kADC_InputGain0P5 

Input buffer gain is 0.5.

kADC_InputGain1 

Input buffer gain is 1.

kADC_InputGain2 

Input buffer gain is 2.

Enumerator
kADC_ResultWidth16 

16-bit final result buffer width

kADC_ResultWidth32 

32-bit final result buffer width

Enumerator
kADC_FifoThresholdData1 

FIFO Threshold is 1 data.

kADC_FifoThresholdData4 

FIFO Threshold is 4 data.

kADC_FifoThresholdData8 

FIFO Threshold is 8 data.

kADC_FifoThresholdData16 

FIFO Threshold is 16 data.

Enumerator
kADC_CalibrationVrefInternal 

Internal vref as input for calibration.

kADC_CalibrationVrefExternal 

External vref as input for calibration.

Enumerator
kADC_ScanChannel0 

Scan channel 0.

kADC_ScanChannel1 

Scan channel 1.

kADC_ScanChannel2 

Scan channel 2.

kADC_ScanChannel3 

Scan channel 3.

kADC_ScanChannel4 

Scan channel 4.

kADC_ScanChannel5 

Scan channel 5.

kADC_ScanChannel6 

Scan channel 6.

kADC_ScanChannel7 

Scan channel 7.

kADC_ScanChannel8 

Scan channel 8.

kADC_ScanChannel9 

Scan channel 9.

kADC_ScanChannel10 

Scan channel 10.

kADC_ScanChannel11 

Scan channel 11.

kADC_ScanChannel12 

Scan channel 12.

kADC_ScanChannel13 

Scan channel 13.

kADC_ScanChannel14 

Scan channel 14.

kADC_ScanChannel15 

Scan channel 15.

Enumerator
kADC_CH0 

Single-ended mode, channel[0] and vssa.

kADC_CH1 

Single-ended mode, channel[1] and vssa.

kADC_CH2 

Single-ended mode, channel[2] and vssa.

kADC_CH3 

Single-ended mode, channel[3] and vssa.

kADC_CH4 

Single-ended mode, channel[4] and vssa.

kADC_CH5 

Single-ended mode, channel[5] and vssa.

kADC_CH6 

Single-ended mode, channel[6] and vssa.

kADC_CH7 

Single-ended mode, channel[7] and vssa.

kADC_VBATS 

Single-ended mode, vbat_s and vssa.

kADC_VREF 

Single-ended mode, vref_12 and vssa.

kADC_DACA 

Single-ended mode, daca and vssa.

kADC_DACB 

Single-ended mode, dacb and vssa.

kADC_VSSA 

Single-ended mode, vssa and vssa.

kADC_CH0_CH1 

Differential mode, channel[0] and channel[1].

kADC_CH2_CH3 

Differential mode, channel[2] and channel[3].

kADC_CH4_CH5 

Differential mode, channel[4] and channel[5].

kADC_CH6_CH7 

Differential mode, channel[6] and channel[7].

kADC_DACA_DACB 

Differential mode, daca and dacb.

Enumerator
kADC_TSensorExternal 

External diode mode.

Enumerator
kADC_AudioGain4 

Audio pga gain is 4.

kADC_AudioGain8 

Audio pga gain is 8.

kADC_AudioGain16 

Audio pga gain is 16.

kADC_AudioGain32 

Audio pga gain is 32.

Enumerator
kADC_VoiceLevel0 

Input voice level >+255LSB or <-256LSB.

kADC_VoiceLevel1 

Input voice level >+511LSB or <-512LSB.

kADC_VoiceLevel2 

Input voice level >+1023LSB or <-1024LSB.

kADC_VoiceLevel3 

Input voice level >+2047LSB or <-2048LSB.

Function Documentation

void ADC_Init ( ADC_Type *  base,
const adc_config_t config 
)
Parameters
baseADC peripheral base address.
configThe pointer to the structure adc_config_t.
void ADC_GetDefaultConfig ( adc_config_t config)
* config->clockDivider = kADC_ClockDivider1;
* config->powerMode = kADC_PowerModeFullBiasingCurrent;
* config->resolution = kADC_Resolution12Bit;
* config->warmupTime = kADC_WarmUpTime16us;
* config->vrefSource = kADC_Vref1P2V;
* config->inputMode = kADC_InputSingleEnded;
* config->conversionMode = kADC_ConversionContinuous;
* config->scanLength = kADC_ScanLength_1;
* config->averageLength = kADC_AverageNone;
* config->triggerSource = kADC_TriggerSourceSoftware;
* config->inputGain = kADC_InputGain1;
* config->enableInputGainBuffer = false;
* config->resultWidth = kADC_ResultWidth16;
* config->fifoThreshold = kADC_FifoThresholdData1;
* config->enableDMA = false;
* config->enableADC = false;
*
Parameters
configThe Pointer to the structure adc_config_t.
void ADC_Deinit ( ADC_Type *  base)
Parameters
baseADC peripheral base address.
static void ADC_DoSoftwareReset ( ADC_Type *  base)
inlinestatic
Parameters
baseADC peripheral base address.
static void ADC_SelectAnalogPortionPowerMode ( ADC_Type *  base,
adc_analog_portion_power_mode_t  powerMode 
)
inlinestatic
Parameters
baseADC peripheral base address.
powerModeThe power mode to be set, please refer to adc_analog_portion_power_mode_t.
status_t ADC_DoAutoCalibration ( ADC_Type *  base,
adc_calibration_ref_t  calVref 
)
Note
After auto calibrate successful, user can invoke ADC_GetAutoCalibrationData() to get self offset calibration value and self gain calibration value.
Parameters
baseADC peripheral base address.
calVrefThe inpul reference channel for gain calibration, please refer to adc_calibration_ref_t for details.
Return values
kStatus_SuccessAuto calibrate successfully.
kStatus_FailAuto calibrate failure.
static void ADC_GetAutoCalibrationData ( ADC_Type *  base,
uint16_t *  offsetCal,
uint16_t *  gainCal 
)
inlinestatic
Parameters
baseADC peripheral base address.
offsetCalSelf offset calibration data pointer, evaluate NULL if not requried.
gainCalSelf gain calibration data pointer, evaluate NULL if not requried.
static void ADC_ResetAutoCalibrationData ( ADC_Type *  base)
inlinestatic
Parameters
baseADC peripheral base address.
static void ADC_DoUserCalibration ( ADC_Type *  base,
uint16_t  offsetCal,
uint16_t  gainCal 
)
inlinestatic
Parameters
baseADC peripheral base address.
offsetCalUser defined offset calibration data.
gainCalUser defined gain calibration date.
static void ADC_EnableTemperatureSensor ( ADC_Type *  base,
bool  enable 
)
inlinestatic
Note
This function is useful only when the channel source is temperature sensor.
Parameters
baseADC peripheral base address.
enableUsed to enable/disable temperature sensor.
  • true Enable temperature sensor.
  • false Disable temperature sensor.
static void ADC_SetTemperatureSensorMode ( ADC_Type *  base,
adc_temperature_sensor_mode_t  tSensorMode 
)
inlinestatic
Parameters
baseADC peripheral base address.
tSensorModeThe temperature sensor mode to be set, please refer to adc_temperature_sensor_mode_t.
static void ADC_EnableAudio ( ADC_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseADC peripheral base address.
enableUsed to enable/disable audio PGA and decimation rate select.
  • true Enable audio PGA and decimation rate select.
  • false Disable audio PGA and decimation rate select.
static void ADC_SetAudioPGAVoltageGain ( ADC_Type *  base,
adc_audio_pga_voltage_gain_t  voltageGain 
)
inlinestatic
Parameters
baseADC peripheral base address.
voltageGainThe selected audio PGA voltage gain, please refer to adc_audio_pga_voltage_gain_t.
void ADC_ConfigAudioVoiceLevel ( ADC_Type *  base,
bool  enableDetect,
adc_audio_voice_level_t  voiceLevel 
)
Parameters
baseADC peripheral base address.
enableDetectUsed to enable/disable voice level detection.
  • true Enable voice level detection.
  • false Disable voice level detection.
voiceLevelSelected voice level, please refer to adc_audio_voice_level_t.
void ADC_SetScanChannel ( ADC_Type *  base,
adc_scan_channel_t  scanChannel,
adc_channel_source_t  channelSource 
)
Parameters
baseADC peripheral base address.
scanChannelThe selected channel, please refer to adc_scan_channel_t for details.
channelSourceThe mux source to be set to the selected channel, please refer to adc_channel_source_t for details.
static void ADC_DoSoftwareTrigger ( ADC_Type *  base)
inlinestatic
Note
This API will also clear the FIFO.
Parameters
baseADC peripheral base address.
static void ADC_StopConversion ( ADC_Type *  base)
inlinestatic
Parameters
baseADC peripheral base address.
static uint32_t ADC_GetConversionResult ( ADC_Type *  base)
inlinestatic
Parameters
baseADC peripheral base address.
Returns
32-bit width packed ADC conversion result.
static uint8_t ADC_GetFifoDataCount ( ADC_Type *  base)
inlinestatic
Parameters
baseADC peripheral base address.
Returns
ADC FIFO data count.
static void ADC_EnableInterrupts ( ADC_Type *  base,
uint32_t  interruptMask 
)
inlinestatic
Parameters
baseADC peripheral base address.
interruptMaskThe interrupts to be enabled, should be the OR'ed value of _adc_interrupt_enable.
static void ADC_DisableInterrupts ( ADC_Type *  base,
uint32_t  interruptMask 
)
inlinestatic
Parameters
baseADC peripheral base address.
interruptMaskThe interrupts to be disabled, should be the OR'ed value of _adc_interrupt_enable.
uint32_t ADC_GetStatusFlags ( ADC_Type *  base)
Parameters
baseADC peripheral base address.
Returns
The OR'ed value of ADC status flags, please refer to _adc_status_flags for details.
static void ADC_ClearStatusFlags ( ADC_Type *  base,
uint32_t  statusFlagsMask 
)
inlinestatic
Note
Only interrupt flags and raw flags can be cleared.
Parameters
baseADC peripheral base address.
statusFlagsMaskThe OR'ed value of status flags to be cleared, please refer to _adc_status_flags for details.