![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.100
NXP Semiconductors
|
Data Structures | |
| struct | _domain_slot_config |
| Key Manager slot configuration structure. More... | |
Typedefs | |
| typedef struct _domain_slot_config | domain_slot_config_t |
| Key Manager slot configuration structure. More... | |
Functions | |
| status_t | KEYMGR_MasterKeyControll (KEY_MANAGER_Type *base, keymgr_select_t select, keymgr_lock_t lock) |
| Configures Master key settings. More... | |
| status_t | KEYMGR_OTFAD1KeyControll (KEY_MANAGER_Type *base, keymgr_select_t select, keymgr_lock_t lock) |
| Configures OTFAD1 key settings. More... | |
| status_t | KEYMGR_OTFAD2KeyControll (KEY_MANAGER_Type *base, keymgr_select_t select, keymgr_lock_t lock) |
| Configures OTFAD2 key settings. More... | |
| void | KEYMGR_IEEKeyReload (KEY_MANAGER_Type *base) |
| Restart load key signal for IEE. More... | |
| void | KEYMGR_PUFKeyLock (KEY_MANAGER_Type *base, keymgr_lock_t lock) |
| Lock the key select from PUF. More... | |
| status_t | KEYMGR_SlotControl (KEY_MANAGER_Type *base, domain_slot_config_t *config, keymgr_slot_t slot) |
| Configures Slot Domain control. More... | |
| void | KEYMGR_Init (KEY_MANAGER_Type *base) |
| Resets Key Manager module to factory default values. More... | |
| status_t | KEYMGR_GetDefaultConfig (domain_slot_config_t *config) |
| Sets the default configuration of Key manager slot. More... | |
Driver version | |
| #define | FSL_KEYMGR_DRIVER_VERSION (MAKE_VERSION(2, 0, 2)) |
| Key Manager driver version. More... | |
| struct _domain_slot_config |
Data Fields | |
| keymgr_lock_t | lockControl |
| Lock control register of slot. More... | |
| keymgr_allow_t | allowUser |
| Allow user write access to domain control register or domain register. More... | |
| keymgr_allow_t | allowNonSecure |
| Allow non-secure write access to domain control register or domain register. More... | |
| keymgr_lock_t | lockList |
| Lock whitelist. More... | |
| uint8_t | whiteList |
| Domains that on the Whitelist can change given slot. More... | |
| keymgr_lock_t _domain_slot_config::lockControl |
| keymgr_allow_t _domain_slot_config::allowUser |
| keymgr_allow_t _domain_slot_config::allowNonSecure |
| keymgr_lock_t _domain_slot_config::lockList |
SLOTx_CTRL[WHITE_LIST] cannot be changed.
| uint8_t _domain_slot_config::whiteList |
Each field represents one domain. Bit0~Bit3 represent DOMAIN0~DOMAIN3 respectively.
| #define FSL_KEYMGR_DRIVER_VERSION (MAKE_VERSION(2, 0, 2)) |
Version 2.0.2.
Current version: 2.0.2
Change log:
| typedef struct _domain_slot_config domain_slot_config_t |
| status_t KEYMGR_MasterKeyControll | ( | KEY_MANAGER_Type * | base, |
| keymgr_select_t | select, | ||
| keymgr_lock_t | lock | ||
| ) |
This function configures Key Manager's setting for Master key.
| base | Key Manager peripheral address. |
| select | select source for Master key. |
| lock | setting for lock Master key. |
| status_t KEYMGR_OTFAD1KeyControll | ( | KEY_MANAGER_Type * | base, |
| keymgr_select_t | select, | ||
| keymgr_lock_t | lock | ||
| ) |
This function configures Key Manager's setting for OTFAD1 key.
| base | Key Manager peripheral address. |
| select | select source for OTFAD1 key. |
| lock | setting for lock OTFAD1 key. |
| status_t KEYMGR_OTFAD2KeyControll | ( | KEY_MANAGER_Type * | base, |
| keymgr_select_t | select, | ||
| keymgr_lock_t | lock | ||
| ) |
This function configures Key Manager's setting for OTFAD2 key.
| base | Key Manager peripheral address. |
| select | select source for OTFAD2 key. |
| lock | setting for lock OTFAD2 key. |
| void KEYMGR_IEEKeyReload | ( | KEY_MANAGER_Type * | base | ) |
This function genrates Key Manager's restart signal for IEE key.
| base | Key Manager peripheral address. |
| void KEYMGR_PUFKeyLock | ( | KEY_MANAGER_Type * | base, |
| keymgr_lock_t | lock | ||
| ) |
This function locks selection of key for PUF.
| base | Key Manager peripheral address. |
| lock | Setting for selection of key for PUF. |
| status_t KEYMGR_SlotControl | ( | KEY_MANAGER_Type * | base, |
| domain_slot_config_t * | config, | ||
| keymgr_slot_t | slot | ||
| ) |
This function configures domain slot control which locks and allows writes.
| base | Key Manager peripheral address. |
| config | Pointer to slot configuration structure. |
| slot | Select slot to be configured. |
| void KEYMGR_Init | ( | KEY_MANAGER_Type * | base | ) |
This function performs hardware reset of Key Manager module.
| base | Key Manager peripheral address. |
| status_t KEYMGR_GetDefaultConfig | ( | domain_slot_config_t * | config | ) |
This function initialize Key Manager slot config structure to default values.
| config | Pointer to slot configuration structure. |