![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.100
NXP Semiconductors
|
The MCUXpresso SDK provides a Peripheral driver for the Secure Non-Volatile Storage High-Power(SNVS-HP) module.
The SNVS_HP is in the chip's power-supply domain and thus receives the power along with the rest of the chip. The SNVS_HP provides an interface between the SNVS_LP and the rest of the system; there is no way to access the SNVS_LP registers except through the SNVS_HP. For access to the SNVS_LP registers, the SNVS_HP must be powered up. It uses a register access permission policy to determine whether the access to the particular registers is permitted.
Data Structures | |
| struct | _snvs_hp_rtc_datetime |
| Structure is used to hold the date and time. More... | |
| struct | _snvs_hp_rtc_config |
| SNVS config structure. More... | |
Macros | |
| #define | SNVS_MAKE_HP_SV_FLAG(x) (1U << (SNVS_HPSVSR_SV0_SHIFT + (x))) |
| Macro to make security violation flag. More... | |
Typedefs | |
| typedef enum _snvs_hp_interrupts | snvs_hp_interrupts_t |
| List of SNVS interrupts. | |
| typedef enum _snvs_hp_status_flags | snvs_hp_status_flags_t |
| List of SNVS flags. | |
|
typedef enum _snvs_hp_sv_status_flags | snvs_hp_sv_status_flags_t |
| List of SNVS security violation flags. | |
|
typedef struct _snvs_hp_rtc_datetime | snvs_hp_rtc_datetime_t |
| Structure is used to hold the date and time. | |
| typedef struct _snvs_hp_rtc_config | snvs_hp_rtc_config_t |
| SNVS config structure. More... | |
| typedef enum _snvs_hp_ssm_state | snvs_hp_ssm_state_t |
| List of SNVS Security State Machine State. | |
Enumerations | |
| enum | _snvs_hp_interrupts { kSNVS_RTC_AlarmInterrupt = SNVS_HPCR_HPTA_EN_MASK, kSNVS_RTC_PeriodicInterrupt = SNVS_HPCR_PI_EN_MASK } |
| List of SNVS interrupts. More... | |
| enum | _snvs_hp_status_flags { kSNVS_RTC_AlarmInterruptFlag = SNVS_HPSR_HPTA_MASK, kSNVS_RTC_PeriodicInterruptFlag = SNVS_HPSR_PI_MASK, kSNVS_ZMK_ZeroFlag = (int)SNVS_HPSR_ZMK_ZERO_MASK, kSNVS_OTPMK_ZeroFlag = SNVS_HPSR_OTPMK_ZERO_MASK } |
| List of SNVS flags. More... | |
| enum | _snvs_hp_sv_status_flags { kSNVS_LP_ViolationFlag = SNVS_HPSVSR_SW_LPSV_MASK, kSNVS_ZMK_EccFailFlag = SNVS_HPSVSR_ZMK_ECC_FAIL_MASK, kSNVS_LP_SoftwareViolationFlag = SNVS_HPSVSR_SW_LPSV_MASK, kSNVS_FatalSoftwareViolationFlag = SNVS_HPSVSR_SW_FSV_MASK, kSNVS_SoftwareViolationFlag = SNVS_HPSVSR_SW_SV_MASK, kSNVS_Violation0Flag = SNVS_HPSVSR_SV0_MASK, kSNVS_Violation1Flag = SNVS_HPSVSR_SV1_MASK, kSNVS_Violation2Flag = SNVS_HPSVSR_SV2_MASK, kSNVS_Violation4Flag = SNVS_HPSVSR_SV4_MASK, kSNVS_Violation5Flag = SNVS_HPSVSR_SV5_MASK } |
| List of SNVS security violation flags. More... | |
| enum | _snvs_hp_ssm_state { kSNVS_SSMInit = 0x00, kSNVS_SSMHardFail = 0x01, kSNVS_SSMSoftFail = 0x03, kSNVS_SSMInitInter = 0x08, kSNVS_SSMCheck = 0x09, kSNVS_SSMNonSecure = 0x0B, kSNVS_SSMTrusted = 0x0D, kSNVS_SSMSecure = 0x0F } |
| List of SNVS Security State Machine State. More... | |
Functions | |
| static void | SNVS_HP_EnableMasterKeySelection (SNVS_Type *base, bool enable) |
| Enable or disable master key selection. More... | |
| static void | SNVS_HP_ProgramZeroizableMasterKey (SNVS_Type *base) |
| Trigger to program Zeroizable Master Key. More... | |
| static void | SNVS_HP_ChangeSSMState (SNVS_Type *base) |
| Trigger SSM State Transition. More... | |
| static void | SNVS_HP_SetSoftwareFatalSecurityViolation (SNVS_Type *base) |
| Trigger Software Fatal Security Violation. More... | |
| static void | SNVS_HP_SetSoftwareSecurityViolation (SNVS_Type *base) |
| Trigger Software Security Violation. More... | |
| static snvs_hp_ssm_state_t | SNVS_HP_GetSSMState (SNVS_Type *base) |
| Get current SSM State. More... | |
| static void | SNVS_HP_ResetLP (SNVS_Type *base) |
| Reset the SNVS LP section. More... | |
| static uint32_t | SNVS_HP_GetStatusFlags (SNVS_Type *base) |
| Get the SNVS HP status flags. More... | |
| static void | SNVS_HP_ClearStatusFlags (SNVS_Type *base, uint32_t mask) |
| Clear the SNVS HP status flags. More... | |
| static uint32_t | SNVS_HP_GetSecurityViolationStatusFlags (SNVS_Type *base) |
| Get the SNVS HP security violation status flags. More... | |
| static void | SNVS_HP_ClearSecurityViolationStatusFlags (SNVS_Type *base, uint32_t mask) |
| Clear the SNVS HP security violation status flags. More... | |
Driver version | |
| #define | FSL_SNVS_HP_DRIVER_VERSION (MAKE_VERSION(2, 3, 2)) |
| Version 2.3.2. | |
Initialization and deinitialization | |
| void | SNVS_HP_Init (SNVS_Type *base) |
| Initialize the SNVS. More... | |
| void | SNVS_HP_Deinit (SNVS_Type *base) |
| Deinitialize the SNVS. More... | |
| void | SNVS_HP_RTC_Init (SNVS_Type *base, const snvs_hp_rtc_config_t *config) |
| Ungates the SNVS clock and configures the peripheral for basic operation. More... | |
| void | SNVS_HP_RTC_Deinit (SNVS_Type *base) |
| Stops the RTC and SRTC timers. More... | |
| void | SNVS_HP_RTC_GetDefaultConfig (snvs_hp_rtc_config_t *config) |
| Fills in the SNVS config struct with the default settings. More... | |
Non secure RTC current Time & Alarm | |
| status_t | SNVS_HP_RTC_SetDatetime (SNVS_Type *base, const snvs_hp_rtc_datetime_t *datetime) |
| Sets the SNVS RTC date and time according to the given time structure. More... | |
| void | SNVS_HP_RTC_GetDatetime (SNVS_Type *base, snvs_hp_rtc_datetime_t *datetime) |
| Gets the SNVS RTC time and stores it in the given time structure. More... | |
| status_t | SNVS_HP_RTC_SetAlarm (SNVS_Type *base, const snvs_hp_rtc_datetime_t *alarmTime) |
| Sets the SNVS RTC alarm time. More... | |
| void | SNVS_HP_RTC_GetAlarm (SNVS_Type *base, snvs_hp_rtc_datetime_t *datetime) |
| Returns the SNVS RTC alarm time. More... | |
| void | SNVS_HP_RTC_TimeSynchronize (SNVS_Type *base) |
| The function synchronizes RTC counter value with SRTC. More... | |
Interrupt Interface | |
| static void | SNVS_HP_RTC_EnableInterrupts (SNVS_Type *base, uint32_t mask) |
| Enables the selected SNVS interrupts. More... | |
| static void | SNVS_HP_RTC_DisableInterrupts (SNVS_Type *base, uint32_t mask) |
| Disables the selected SNVS interrupts. More... | |
| uint32_t | SNVS_HP_RTC_GetEnabledInterrupts (SNVS_Type *base) |
| Gets the enabled SNVS interrupts. More... | |
Status Interface | |
| uint32_t | SNVS_HP_RTC_GetStatusFlags (SNVS_Type *base) |
| Gets the SNVS status flags. More... | |
| static void | SNVS_HP_RTC_ClearStatusFlags (SNVS_Type *base, uint32_t mask) |
| Clears the SNVS status flags. More... | |
Timer Start and Stop | |
| static void | SNVS_HP_RTC_StartTimer (SNVS_Type *base) |
| Starts the SNVS RTC time counter. More... | |
| static void | SNVS_HP_RTC_StopTimer (SNVS_Type *base) |
| Stops the SNVS RTC time counter. More... | |
High Assurance Counter (HAC) | |
| static void | SNVS_HP_EnableHighAssuranceCounter (SNVS_Type *base, bool enable) |
| Enable or disable the High Assurance Counter (HAC) More... | |
| static void | SNVS_HP_StartHighAssuranceCounter (SNVS_Type *base, bool start) |
| Start or stop the High Assurance Counter (HAC) More... | |
| static void | SNVS_HP_SetHighAssuranceCounterInitialValue (SNVS_Type *base, uint32_t value) |
| Set the High Assurance Counter (HAC) initialize value. More... | |
| static void | SNVS_HP_LoadHighAssuranceCounter (SNVS_Type *base) |
| Load the High Assurance Counter (HAC) More... | |
| static uint32_t | SNVS_HP_GetHighAssuranceCounter (SNVS_Type *base) |
| Get the current High Assurance Counter (HAC) value. More... | |
| static void | SNVS_HP_ClearHighAssuranceCounter (SNVS_Type *base) |
| Clear the High Assurance Counter (HAC) More... | |
| static void | SNVS_HP_LockHighAssuranceCounter (SNVS_Type *base) |
| Lock the High Assurance Counter (HAC) More... | |
| struct _snvs_hp_rtc_datetime |
Data Fields | |
| uint16_t | year |
| Range from 1970 to 2099. More... | |
| uint8_t | month |
| Range from 1 to 12. More... | |
| uint8_t | day |
| Range from 1 to 31 (depending on month). More... | |
| uint8_t | hour |
| Range from 0 to 23. More... | |
| uint8_t | minute |
| Range from 0 to 59. More... | |
| uint8_t | second |
| Range from 0 to 59. More... | |
| uint16_t _snvs_hp_rtc_datetime::year |
| uint8_t _snvs_hp_rtc_datetime::month |
| uint8_t _snvs_hp_rtc_datetime::day |
| uint8_t _snvs_hp_rtc_datetime::hour |
| uint8_t _snvs_hp_rtc_datetime::minute |
| uint8_t _snvs_hp_rtc_datetime::second |
| struct _snvs_hp_rtc_config |
This structure holds the configuration settings for the SNVS peripheral. To initialize this structure to reasonable defaults, call the SNVS_GetDefaultConfig() function and pass a pointer to your config structure instance.
The config struct can be made const so it resides in flash
Data Fields | |
| bool | rtcCalEnable |
| true: RTC calibration mechanism is enabled; false:No calibration is used | |
| uint32_t | rtcCalValue |
| Defines signed calibration value for nonsecure RTC; This is a 5-bit 2's complement value, range from -16 to +15. | |
| uint32_t | periodicInterruptFreq |
| Defines frequency of the periodic interrupt; Range from 0 to 15. | |
| #define SNVS_MAKE_HP_SV_FLAG | ( | x | ) | (1U << (SNVS_HPSVSR_SV0_SHIFT + (x))) |
Macro help to make security violation flag kSNVS_Violation0Flag to kSNVS_Violation5Flag, For example, SNVS_MAKE_HP_SV_FLAG(0) is kSNVS_Violation0Flag.
| typedef struct _snvs_hp_rtc_config snvs_hp_rtc_config_t |
This structure holds the configuration settings for the SNVS peripheral. To initialize this structure to reasonable defaults, call the SNVS_GetDefaultConfig() function and pass a pointer to your config structure instance.
The config struct can be made const so it resides in flash
| enum _snvs_hp_interrupts |
| enum _snvs_hp_ssm_state |
| void SNVS_HP_Init | ( | SNVS_Type * | base | ) |
| base | SNVS peripheral base address |
| void SNVS_HP_Deinit | ( | SNVS_Type * | base | ) |
| base | SNVS peripheral base address |
| void SNVS_HP_RTC_Init | ( | SNVS_Type * | base, |
| const snvs_hp_rtc_config_t * | config | ||
| ) |
| base | SNVS peripheral base address |
| config | Pointer to the user's SNVS configuration structure. |
| void SNVS_HP_RTC_Deinit | ( | SNVS_Type * | base | ) |
| base | SNVS peripheral base address |
| void SNVS_HP_RTC_GetDefaultConfig | ( | snvs_hp_rtc_config_t * | config | ) |
The default values are as follows.
| config | Pointer to the user's SNVS configuration structure. |
| status_t SNVS_HP_RTC_SetDatetime | ( | SNVS_Type * | base, |
| const snvs_hp_rtc_datetime_t * | datetime | ||
| ) |
| base | SNVS peripheral base address |
| datetime | Pointer to the structure where the date and time details are stored. |
| void SNVS_HP_RTC_GetDatetime | ( | SNVS_Type * | base, |
| snvs_hp_rtc_datetime_t * | datetime | ||
| ) |
| base | SNVS peripheral base address |
| datetime | Pointer to the structure where the date and time details are stored. |
| status_t SNVS_HP_RTC_SetAlarm | ( | SNVS_Type * | base, |
| const snvs_hp_rtc_datetime_t * | alarmTime | ||
| ) |
The function sets the RTC alarm. It also checks whether the specified alarm time is greater than the present time. If not, the function does not set the alarm and returns an error.
| base | SNVS peripheral base address |
| alarmTime | Pointer to the structure where the alarm time is stored. |
| void SNVS_HP_RTC_GetAlarm | ( | SNVS_Type * | base, |
| snvs_hp_rtc_datetime_t * | datetime | ||
| ) |
| base | SNVS peripheral base address |
| datetime | Pointer to the structure where the alarm date and time details are stored. |
| void SNVS_HP_RTC_TimeSynchronize | ( | SNVS_Type * | base | ) |
| base | SNVS peripheral base address |
|
inlinestatic |
| base | SNVS peripheral base address |
| mask | The interrupts to enable. This is a logical OR of members of the enumeration :: _snvs_hp_interrupts_t |
|
inlinestatic |
| base | SNVS peripheral base address |
| mask | The interrupts to disable. This is a logical OR of members of the enumeration :: _snvs_hp_interrupts_t |
| uint32_t SNVS_HP_RTC_GetEnabledInterrupts | ( | SNVS_Type * | base | ) |
| base | SNVS peripheral base address |
| uint32_t SNVS_HP_RTC_GetStatusFlags | ( | SNVS_Type * | base | ) |
| base | SNVS peripheral base address |
|
inlinestatic |
| base | SNVS peripheral base address |
| mask | The status flags to clear. This is a logical OR of members of the enumeration :: _snvs_hp_status_flags_t |
|
inlinestatic |
| base | SNVS peripheral base address |
|
inlinestatic |
| base | SNVS peripheral base address |
|
inlinestatic |
| base | SNVS peripheral base address |
| enable | Pass true to enable, false to disable. |
|
inlinestatic |
| base | SNVS peripheral base address |
|
inlinestatic |
Trigger state transition of the system security monitor (SSM). It results only the following transitions of the SSM:
| base | SNVS peripheral base address |
|
inlinestatic |
The result SSM state transition is:
| base | SNVS peripheral base address |
|
inlinestatic |
The result SSM state transition is:
| base | SNVS peripheral base address |
|
inlinestatic |
| base | SNVS peripheral base address |
|
inlinestatic |
Reset the LP section except SRTC and Time alarm.
| base | SNVS peripheral base address |
|
inlinestatic |
| base | SNVS peripheral base address |
| enable | Pass true to enable, false to disable. |
|
inlinestatic |
| base | SNVS peripheral base address |
| start | Pass true to start, false to stop. |
|
inlinestatic |
| base | SNVS peripheral base address |
| value | The initial value to set. |
|
inlinestatic |
This function loads the HAC initialize value to counter register.
| base | SNVS peripheral base address |
|
inlinestatic |
| base | SNVS peripheral base address |
|
inlinestatic |
This function can be called in a functional or soft fail state. When the HAC is enabled:
| base | SNVS peripheral base address |
|
inlinestatic |
Once locked, the HAC initialize value could not be changed, the HAC enable status could not be changed. This could only be unlocked by system reset.
| base | SNVS peripheral base address |
|
inlinestatic |
The flags are returned as the OR'ed value f the enumeration :: _snvs_hp_status_flags_t.
| base | SNVS peripheral base address |
|
inlinestatic |
The flags to clear are passed in as the OR'ed value of the enumeration :: _snvs_hp_status_flags_t. Only these flags could be cleared using this API.
| base | SNVS peripheral base address |
| mask | OR'ed value of the flags to clear. |
|
inlinestatic |
The flags are returned as the OR'ed value of the enumeration :: _snvs_hp_sv_status_flags_t.
| base | SNVS peripheral base address |
|
inlinestatic |
The flags to clear are passed in as the OR'ed value of the enumeration :: _snvs_hp_sv_status_flags_t. Only these flags could be cleared using this API.
| base | SNVS peripheral base address |
| mask | OR'ed value of the flags to clear. |