![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.100
NXP Semiconductors
|
Files | |
| file | fsl_soc_mipi_csi2rx.h |
Macros | |
| #define | FSL_SOC_MIPI_CSI2RX_DRIVER_VERSION (MAKE_VERSION(2, 0, 2)) |
| Driver version. More... | |
Functions | |
| void | MIPI_CSI2RX_SoftwareReset (MIPI_CSI2RX_Type *base, bool reset) |
| Assert or deassert CSI2RX reset in system level. More... | |
| void | MIPI_CSI2RX_InitInterface (MIPI_CSI2RX_Type *base, uint8_t tHsSettle_EscClk) |
| Initialize the CSI2RX interface. More... | |
| void | MIPI_CSI2RX_DeinitInterface (MIPI_CSI2RX_Type *base) |
| Deinitialize the CSI2RX interface. More... | |
| #define FSL_SOC_MIPI_CSI2RX_DRIVER_VERSION (MAKE_VERSION(2, 0, 2)) |
| void MIPI_CSI2RX_SoftwareReset | ( | MIPI_CSI2RX_Type * | base, |
| bool | reset | ||
| ) |
| base | The CSI2RX peripheral base address. |
| reset | Pass in true to set to reset state, false to release reset. |
| void MIPI_CSI2RX_InitInterface | ( | MIPI_CSI2RX_Type * | base, |
| uint8_t | tHsSettle_EscClk | ||
| ) |
| base | The CSI2RX peripheral base address. |
| tHsSettle_EscClk | t-HS_SETTLE in esc clock period. |
| void MIPI_CSI2RX_DeinitInterface | ( | MIPI_CSI2RX_Type * | base | ) |
| base | The CSI2RX peripheral base address. |