MCUXpresso SDK API Reference Manual  Rev 2.16.100
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Clock Driver

Overview

The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.

The clock driver supports:

The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.

Modules

 System Clock Generator (SCG)
 

Files

file  fsl_clock.h
 

Data Structures

struct  scg_sys_clk_config_t
 SCG system clock configuration. More...
 
struct  scg_sosc_config_t
 SCG system OSC configuration. More...
 
struct  scg_rosc_config_t
 SCG ROSC configuration. More...
 
struct  scg_sirc_config_t
 SCG slow IRC clock configuration. More...
 
struct  scg_firc_trim_config_t
 SCG fast IRC clock trim configuration. More...
 
struct  scg_firc_config_t
 SCG fast IRC clock configuration. More...
 
struct  fro192m_rf_clk_config_t
 FRO192M RF clock configuration. More...
 

Macros

#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0
 Configure whether driver controls clock. More...
 
#define EDMA_CLOCKS
 Clock ip name array for EDMA. More...
 
#define SYSPM_CLOCKS
 Clock ip name array for SYSPM. More...
 
#define SFA_CLOCKS
 Clock ip name array for SFA. More...
 
#define CRC_CLOCKS
 Clock ip name array for CRC. More...
 
#define TPM_CLOCKS
 Clock ip name array for TPM. More...
 
#define LPI2C_CLOCKS
 Clock ip name array for LPI2C. More...
 
#define I3C_CLOCKS
 Clock ip name array for I3C. More...
 
#define LPSPI_CLOCKS
 Clock ip name array for LPSPI. More...
 
#define LPUART_CLOCKS
 Clock ip name array for LPUART. More...
 
#define PORT_CLOCKS
 Clock ip name array for PORT. More...
 
#define LPADC_CLOCKS
 Clock ip name array for LPADC. More...
 
#define LPCMP_CLOCKS
 Clock ip name array for LPCMP. More...
 
#define VREF_CLOCKS
 Clock ip name array for VREF. More...
 
#define GPIO_CLOCKS
 Clock ip name array for GPIO. More...
 
#define LPIT_CLOCKS
 Clock ip name array for LPIT. More...
 
#define RF_CLOCKS
 Clock ip name array for RF. More...
 
#define WDOG_CLOCKS
 Clock ip name array for WDOG. More...
 
#define FLEXCAN_CLOCKS
 Clock ip name array for FLEXCAN. More...
 
#define FLEXIO_CLOCKS
 Clock ip name array for FLEXIO. More...
 
#define TSTMR_CLOCKS
 Clock ip name array for TSTMR. More...
 
#define EWM_CLOCKS
 Clock ip name array for EWM. More...
 
#define SEMA42_CLOCKS
 Clock ip name array for SEMA42. More...
 
#define MAKE_MRCC_REGADDR(base, offset)   ((base) + (offset))
 "IP Connector name difinition used for clock gate, clock source and clock divider setting. More...
 

Enumerations

enum  clock_name_t {
  kCLOCK_CoreSysClk,
  kCLOCK_SlowClk,
  kCLOCK_PlatClk,
  kCLOCK_SysClk,
  kCLOCK_BusClk,
  kCLOCK_ScgSysOscClk,
  kCLOCK_ScgSircClk,
  kCLOCK_ScgFircClk,
  kCLOCK_RtcOscClk
}
 Clock name used to get clock frequency. More...
 
enum  clock_ip_control_t {
  kCLOCK_IpClkControl_fun0 = 0U,
  kCLOCK_IpClkControl_fun1 = 1U,
  kCLOCK_IpClkControl_fun2 = 2U,
  kCLOCK_IpClkControl_fun3
}
 Clock source for peripherals that support various clock selections. More...
 
enum  clock_ip_src_t {
  kCLOCK_IpSrcFro6M = 2U,
  kCLOCK_IpSrcFro192M = 3U,
  kCLOCK_IpSrcSoscClk = 4U,
  kCLOCK_IpSrc32kClk = 5U
}
 Clock source for peripherals that support various clock selections. More...
 
enum  clock_ip_name_t {
  kCLOCK_NOGATE = 0U,
  kCLOCK_Ewm0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x4C),
  kCLOCK_Syspm0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x5C),
  kCLOCK_Wdog0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x68),
  kCLOCK_Wdog1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x6C),
  kCLOCK_Sfa0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x74),
  kCLOCK_Crc0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x8C),
  kCLOCK_Secsubsys = MAKE_MRCC_REGADDR(MRCC_BASE, 0x90),
  kCLOCK_Lpit0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xBC),
  kCLOCK_Tstmr0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xC0),
  kCLOCK_Tpm0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xC4),
  kCLOCK_Tpm1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xC8),
  kCLOCK_Lpi2c0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xCC),
  kCLOCK_Lpi2c1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xD0),
  kCLOCK_I3c0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xD4),
  kCLOCK_Lpspi0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xD8),
  kCLOCK_Lpspi1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xDC),
  kCLOCK_Lpuart0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xE0),
  kCLOCK_Lpuart1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xE4),
  kCLOCK_Flexio0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xE8),
  kCLOCK_Can0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xEC),
  kCLOCK_Sema0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xFC),
  kCLOCK_Data_stream_2p4 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x104),
  kCLOCK_PortA = MAKE_MRCC_REGADDR(MRCC_BASE, 0x108),
  kCLOCK_PortB = MAKE_MRCC_REGADDR(MRCC_BASE, 0x10C),
  kCLOCK_PortC = MAKE_MRCC_REGADDR(MRCC_BASE, 0x110),
  kCLOCK_Lpadc0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x11C),
  kCLOCK_Lpcmp0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x120),
  kCLOCK_Lpcmp1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x124),
  kCLOCK_Vref0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x128),
  kCLOCK_Mtr_master = MAKE_MRCC_REGADDR(MRCC_BASE, 0x134),
  kCLOCK_GpioA = MAKE_MRCC_REGADDR(MRCC_BASE, 0x404),
  kCLOCK_GpioB = MAKE_MRCC_REGADDR(MRCC_BASE, 0x408),
  kCLOCK_GpioC = MAKE_MRCC_REGADDR(MRCC_BASE, 0x40C),
  kCLOCK_Dma0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x410),
  kCLOCK_Pflexnvm = MAKE_MRCC_REGADDR(MRCC_BASE, 0x414),
  kCLOCK_Sram0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x41C),
  kCLOCK_Sram1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x420),
  kCLOCK_Sram2 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x424),
  kCLOCK_Sram3 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x428),
  kCLOCK_Rf_2p4ghz_bist = MAKE_MRCC_REGADDR(MRCC_BASE, 0x42C)
}
 Clock IP name. More...
 
enum  _scg_status {
  kStatus_SCG_Busy = MAKE_STATUS(kStatusGroup_SCG, 1),
  kStatus_SCG_InvalidSrc = MAKE_STATUS(kStatusGroup_SCG, 2)
}
 SCG status return codes. More...
 
enum  scg_sys_clk_t {
  kSCG_SysClkSlow,
  kSCG_SysClkBus,
  kSCG_SysClkPlatform,
  kSCG_SysClkCore
}
 SCG system clock type. More...
 
enum  scg_sys_clk_src_t {
  kSCG_SysClkSrcSysOsc = 1U,
  kSCG_SysClkSrcSirc = 2U,
  kSCG_SysClkSrcFirc = 3U,
  kSCG_SysClkSrcRosc = 4U
}
 SCG system clock source. More...
 
enum  scg_sys_clk_div_t {
  kSCG_SysClkDivBy1 = 0U,
  kSCG_SysClkDivBy2 = 1U,
  kSCG_SysClkDivBy3 = 2U,
  kSCG_SysClkDivBy4 = 3U,
  kSCG_SysClkDivBy5 = 4U,
  kSCG_SysClkDivBy6 = 5U,
  kSCG_SysClkDivBy7 = 6U,
  kSCG_SysClkDivBy8 = 7U,
  kSCG_SysClkDivBy9 = 8U,
  kSCG_SysClkDivBy10 = 9U,
  kSCG_SysClkDivBy11 = 10U,
  kSCG_SysClkDivBy12 = 11U,
  kSCG_SysClkDivBy13 = 12U,
  kSCG_SysClkDivBy14 = 13U,
  kSCG_SysClkDivBy15 = 14U,
  kSCG_SysClkDivBy16 = 15U
}
 SCG system clock divider value. More...
 
enum  clock_clkout_src_t {
  kClockClkoutSelScgSlow = 0U,
  kClockClkoutSelSosc = 1U,
  kClockClkoutSelSirc = 2U,
  kClockClkoutSelFirc = 3U,
  kClockClkoutSelScgRtcOsc = 4U
}
 SCG clock out configuration (CLKOUTSEL). More...
 
enum  scg_sosc_monitor_mode_t {
  kSCG_SysOscMonitorDisable = 0U,
  kSCG_SysOscMonitorInt = SCG_SOSCCSR_SOSCCM_MASK,
  kSCG_SysOscMonitorReset
}
 SCG system OSC monitor mode. More...
 
enum  {
  kSCG_SoscDisable = 0,
  kSCG_SoscEnable = SCG_SOSCCSR_SOSCEN_MASK,
  kSCG_SoscEnableInSleep = SCG_SOSCCSR_SOSCSTEN_MASK
}
 SOSC enable mode. More...
 
enum  scg_rosc_monitor_mode_t {
  kSCG_RoscMonitorDisable = 0U,
  kSCG_RoscMonitorInt = SCG_ROSCCSR_ROSCCM_MASK,
  kSCG_RoscMonitorReset
}
 SCG ROSC monitor mode. More...
 
enum  scg_sirc_enable_mode_t {
  kSCG_SircDisableInSleep = 0,
  kSCG_SircEnableInSleep = SCG_SIRCCSR_SIRCSTEN_MASK
}
 SIRC enable mode. More...
 
enum  scg_firc_trim_mode_t {
  kSCG_FircTrimNonUpdate = SCG_FIRCCSR_FIRCTREN_MASK,
  kSCG_FircTrimUpdate = SCG_FIRCCSR_FIRCTREN_MASK | SCG_FIRCCSR_FIRCTRUP_MASK
}
 SCG fast IRC trim mode. More...
 
enum  scg_firc_trim_src_t {
  kSCG_FircTrimSrcSysOsc = 2U,
  kSCG_FircTrimSrcRtcOsc = 3U
}
 SCG fast IRC trim source. More...
 
enum  {
  kSCG_FircDisable = 0,
  kSCG_FircEnable = SCG_FIRCCSR_FIRCEN_MASK,
  kSCG_FircEnableInSleep = SCG_FIRCCSR_FIRCSTEN_MASK
}
 FIRC enable mode. More...
 
enum  scg_firc_range_t {
  kSCG_FircRange48M,
  kSCG_FircRange64M,
  kSCG_FircRange96M,
  kSCG_FircRange192M
}
 SCG fast IRC clock frequency range. More...
 
enum  fro192m_rf_range_t {
  kFro192M_Range16M,
  kFro192M_Range24M,
  kFro192M_Range32M,
  kFro192M_Range48M,
  kFro192M_Range64M
}
 FRO192M RF clock frequency range. More...
 
enum  fro192m_rf_clk_div_t {
  kFro192M_ClkDivBy1 = 0U,
  kFro192M_ClkDivBy2 = 1U,
  kFro192M_ClkDivBy4 = 2U,
  kFro192M_ClkDivBy8 = 3U
}
 RF Flash APB and RF_CMC clock divide. More...
 

Functions

static void CLOCK_EnableClock (clock_ip_name_t name)
 Enable the clock for specific IP. More...
 
static void CLOCK_EnableClockLPMode (clock_ip_name_t name, clock_ip_control_t control)
 Enable the clock for specific IP in low power mode. More...
 
static void CLOCK_DisableClock (clock_ip_name_t name)
 Disable the clock for specific IP. More...
 
static void CLOCK_SetIpSrc (clock_ip_name_t name, clock_ip_src_t src)
 Set the clock source for specific IP module. More...
 
static void CLOCK_SetIpSrcDiv (clock_ip_name_t name, uint8_t divValue)
 Set the clock source and divider for specific IP module. More...
 
uint32_t CLOCK_GetFreq (clock_name_t clockName)
 Gets the clock frequency for a specific clock name. More...
 
uint32_t CLOCK_GetCoreSysClkFreq (void)
 Get the core clock or system clock frequency. More...
 
uint32_t CLOCK_GetPlatClkFreq (void)
 Get the platform clock frequency. More...
 
uint32_t CLOCK_GetBusClkFreq (void)
 Get the bus clock frequency. More...
 
uint32_t CLOCK_GetFlashClkFreq (void)
 Get the flash clock frequency. More...
 
uint32_t CLOCK_GetIpFreq (clock_ip_name_t name)
 Gets the functional clock frequency for a specific IP module. More...
 

Variables

volatile uint32_t g_xtal0Freq
 External XTAL0 (OSC0/SYSOSC) clock frequency. More...
 
volatile uint32_t g_xtal32Freq
 External XTAL32/EXTAL32 clock frequency. More...
 

Driver version

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(1, 0, 0))
 CLOCK driver version 1.0.0. More...
 

MCU System Clock.

uint32_t CLOCK_GetSysClkFreq (scg_sys_clk_t type)
 Gets the SCG system clock frequency. More...
 
static void CLOCK_SetRunModeSysClkConfig (const scg_sys_clk_config_t *config)
 Sets the system clock configuration for RUN mode. More...
 
static void CLOCK_GetCurSysClkConfig (scg_sys_clk_config_t *config)
 Gets the system clock configuration in the current power mode. More...
 
static void CLOCK_SetClkOutSel (clock_clkout_src_t setting)
 Sets the clock out selection. More...
 

SCG System OSC Clock.

status_t CLOCK_InitSysOsc (const scg_sosc_config_t *config)
 Initializes the SCG system OSC. More...
 
status_t CLOCK_DeinitSysOsc (void)
 De-initializes the SCG system OSC. More...
 
uint32_t CLOCK_GetSysOscFreq (void)
 Gets the SCG system OSC clock frequency (SYSOSC). More...
 
static bool CLOCK_IsSysOscErr (void)
 Checks whether the system OSC clock error occurs. More...
 
static void CLOCK_ClearSysOscErr (void)
 Clears the system OSC clock error.
 
static void CLOCK_SetSysOscMonitorMode (scg_sosc_monitor_mode_t mode)
 Sets the system OSC monitor mode. More...
 
static bool CLOCK_IsSysOscValid (void)
 Checks whether the system OSC clock is valid. More...
 
static void CLOCK_UnlockSysOscControlStatusReg (void)
 Unlock the SOSCCSR control status register.
 
static void CLOCK_LockSysOscControlStatusReg (void)
 Lock the SOSCCSR control status register.
 

SCG Slow IRC Clock.

status_t CLOCK_InitSirc (const scg_sirc_config_t *config)
 Initializes the SCG slow IRC clock. More...
 
status_t CLOCK_DeinitSirc (void)
 De-initializes the SCG slow IRC. More...
 
uint32_t CLOCK_GetSircFreq (void)
 Gets the SCG SIRC clock frequency. More...
 
static bool CLOCK_IsSircValid (void)
 Checks whether the SIRC clock is valid. More...
 
static void CLOCK_UnlockSircControlStatusReg (void)
 Unlock the SIRCCSR control status register.
 
static void CLOCK_LockSircControlStatusReg (void)
 Lock the SIRCCSR control status register.
 

SCG Fast IRC Clock.

status_t CLOCK_InitFirc (const scg_firc_config_t *config)
 Initializes the SCG fast IRC clock. More...
 
status_t CLOCK_DeinitFirc (void)
 De-initializes the SCG fast IRC. More...
 
uint32_t CLOCK_GetFircFreq (void)
 Gets the SCG FIRC clock frequency. More...
 
static bool CLOCK_IsFircErr (void)
 Checks whether the FIRC clock error occurs. More...
 
static void CLOCK_ClearFircErr (void)
 Clears the FIRC clock error.
 
static bool CLOCK_IsFircValid (void)
 Checks whether the FIRC clock is valid. More...
 
static void CLOCK_UnlockFircControlStatusReg (void)
 Unlock the FIRCCSR control status register.
 
static void CLOCK_LockFircControlStatusReg (void)
 Lock the FIRCCSR control status register.
 
status_t CLOCK_InitRosc (const scg_rosc_config_t *config)
 brief Initializes the SCG ROSC. More...
 
status_t CLOCK_DeinitRosc (void)
 brief De-initializes the SCG ROSC. More...
 
uint32_t CLOCK_GetRtcOscFreq (void)
 Gets the SCG RTC OSC clock frequency. More...
 
status_t CLOCK_InitRfFro192M (const fro192m_rf_clk_config_t *config)
 Initializes the FRO192M clock for the Radio Mode Controller. More...
 
uint32_t CLOCK_GetRfFro192MFreq (void)
 Gets the FRO192M clock frequency. More...
 
static bool CLOCK_IsRoscErr (void)
 Checks whether the ROSC clock error occurs. More...
 
static void CLOCK_ClearRoscErr (void)
 Clears the ROSC clock error.
 
static void CLOCK_SetRoscMonitorMode (scg_rosc_monitor_mode_t mode)
 Sets the ROSC monitor mode. More...
 
static bool CLOCK_IsRoscValid (void)
 Checks whether the ROSC clock is valid. More...
 
static void CLOCK_UnlockRoscControlStatusReg (void)
 Unlock the ROSCCSR control status register.
 
static void CLOCK_LockRoscControlStatusReg (void)
 Lock the ROSCCSR control status register.
 

External clock frequency

static void CLOCK_SetXtal0Freq (uint32_t freq)
 Sets the XTAL0 frequency based on board settings. More...
 
static void CLOCK_SetXtal32Freq (uint32_t freq)
 Sets the XTAL32 frequency based on board settings. More...
 

Data Structure Documentation

struct scg_sys_clk_config_t

Data Fields

uint32_t divSlow: 4
 Slow clock divider, see scg_sys_clk_div_t. More...
 
uint32_t divBus: 4
 Bus clock divider, see scg_sys_clk_div_t. More...
 
uint32_t __pad0__: 8
 Reserved. More...
 
uint32_t divCore: 4
 Core clock divider, see scg_sys_clk_div_t. More...
 
uint32_t __pad1__: 4
 Reserved. More...
 
uint32_t src: 3
 System clock source, see scg_sys_clk_src_t. More...
 
uint32_t __pad2__: 5
 reserved. More...
 

Field Documentation

uint32_t scg_sys_clk_config_t::divSlow
uint32_t scg_sys_clk_config_t::divBus
uint32_t scg_sys_clk_config_t::__pad0__
uint32_t scg_sys_clk_config_t::divCore
uint32_t scg_sys_clk_config_t::__pad1__
uint32_t scg_sys_clk_config_t::src
uint32_t scg_sys_clk_config_t::__pad2__
struct scg_sosc_config_t

Data Fields

uint32_t freq
 System OSC frequency. More...
 
uint32_t enableMode
 Enable mode, OR'ed value of _scg_sosc_enable_mode. More...
 
scg_sosc_monitor_mode_t monitorMode
 Clock monitor mode selected. More...
 

Field Documentation

uint32_t scg_sosc_config_t::freq
uint32_t scg_sosc_config_t::enableMode
scg_sosc_monitor_mode_t scg_sosc_config_t::monitorMode
struct scg_rosc_config_t

Data Fields

scg_rosc_monitor_mode_t monitorMode
 Clock monitor mode selected. More...
 

Field Documentation

scg_rosc_monitor_mode_t scg_rosc_config_t::monitorMode
struct scg_sirc_config_t

Data Fields

scg_sirc_enable_mode_t enableMode
 Enable mode, OR'ed value of _scg_sirc_enable_mode. More...
 

Field Documentation

scg_sirc_enable_mode_t scg_sirc_config_t::enableMode
struct scg_firc_trim_config_t

Data Fields

scg_firc_trim_mode_t trimMode
 FIRC trim mode. More...
 
scg_firc_trim_src_t trimSrc
 Trim source. More...
 
uint16_t trimDiv
 Divider of SOSC for FIRC. More...
 
uint8_t trimCoar
 Trim coarse value; Irrelevant if trimMode is kSCG_FircTrimUpdate. More...
 
uint8_t trimFine
 Trim fine value; Irrelevant if trimMode is kSCG_FircTrimUpdate. More...
 

Field Documentation

scg_firc_trim_mode_t scg_firc_trim_config_t::trimMode
scg_firc_trim_src_t scg_firc_trim_config_t::trimSrc
uint16_t scg_firc_trim_config_t::trimDiv
uint8_t scg_firc_trim_config_t::trimCoar
uint8_t scg_firc_trim_config_t::trimFine
struct scg_firc_config_t

Data Fields

uint32_t enableMode
 Enable mode. More...
 
scg_firc_range_t range
 Fast IRC frequency range. More...
 
const scg_firc_trim_config_t * trimConfig
 Pointer to the FIRC trim configuration; set NULL to disable trim. More...
 

Field Documentation

uint32_t scg_firc_config_t::enableMode
scg_firc_range_t scg_firc_config_t::range
const scg_firc_trim_config_t* scg_firc_config_t::trimConfig
struct fro192m_rf_clk_config_t

Data Fields

fro192m_rf_range_t range
 FRO192M RF clock frequency range. More...
 
fro192m_rf_clk_div_t apb_rfcmc_div
 RF Flash APB and RF_CMC clock divide. More...
 

Field Documentation

fro192m_rf_range_t fro192m_rf_clk_config_t::range
fro192m_rf_clk_div_t fro192m_rf_clk_config_t::apb_rfcmc_div

Macro Definition Documentation

#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0

When set to 0, peripheral drivers will enable clock in initialize function and disable clock in de-initialize function. When set to 1, peripheral driver will not control the clock, application could control the clock out of the driver.

Note
All drivers share this feature switcher. If it is set to 1, application should handle clock enable and disable for all drivers.
#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(1, 0, 0))
#define EDMA_CLOCKS
Value:
{ \
}
Clock dma0.
Definition: fsl_clock.h:311
#define SYSPM_CLOCKS
Value:
{ \
}
Clock syspm0.
Definition: fsl_clock.h:279
#define SFA_CLOCKS
Value:
{ \
}
Clock sfa0.
Definition: fsl_clock.h:282
No clock gate for the IP in MRCC.
Definition: fsl_clock.h:277
#define CRC_CLOCKS
Value:
{ \
}
Clock crc0.
Definition: fsl_clock.h:283
#define TPM_CLOCKS
Value:
{ \
}
Clock tpm1.
Definition: fsl_clock.h:288
Clock tpm0.
Definition: fsl_clock.h:287
No clock gate for the IP in MRCC.
Definition: fsl_clock.h:277
#define LPI2C_CLOCKS
Value:
{ \
}
Clock lpi2c1.
Definition: fsl_clock.h:290
Clock lpi2c0.
Definition: fsl_clock.h:289
#define I3C_CLOCKS
Value:
{ \
}
Clock i3c.
Definition: fsl_clock.h:291
#define LPSPI_CLOCKS
Value:
{ \
}
Clock lpspi0.
Definition: fsl_clock.h:292
Clock lpspi1.
Definition: fsl_clock.h:293
#define LPUART_CLOCKS
Value:
{ \
}
Clock lpuart0.
Definition: fsl_clock.h:294
Clock lpuart1.
Definition: fsl_clock.h:295
#define PORT_CLOCKS
Value:
{ \
}
Clock portB.
Definition: fsl_clock.h:301
Clock portA.
Definition: fsl_clock.h:300
Clock portC.
Definition: fsl_clock.h:302
#define LPADC_CLOCKS
Value:
{ \
}
Clock lpadc0.
Definition: fsl_clock.h:303
#define LPCMP_CLOCKS
Value:
{ \
}
Clock lpcmp0.
Definition: fsl_clock.h:304
Clock lpcmp1.
Definition: fsl_clock.h:305
#define VREF_CLOCKS
Value:
{ \
}
Clock verf0.
Definition: fsl_clock.h:306
#define GPIO_CLOCKS
Value:
{ \
}
Clock gpioB.
Definition: fsl_clock.h:309
Clock gpioA.
Definition: fsl_clock.h:308
Clock gpioC.
Definition: fsl_clock.h:310
#define LPIT_CLOCKS
Value:
{ \
}
Clock lpit0.
Definition: fsl_clock.h:285
#define RF_CLOCKS
Value:
{ \
}
Clock rf_2p4ghz_bist.
Definition: fsl_clock.h:317
#define WDOG_CLOCKS
Value:
{ \
}
Clock wdog1.
Definition: fsl_clock.h:281
Clock wdog0.
Definition: fsl_clock.h:280
#define FLEXCAN_CLOCKS
Value:
{ \
}
Clock Can0.
Definition: fsl_clock.h:297
#define FLEXIO_CLOCKS
Value:
{ \
}
Clock Flexio0.
Definition: fsl_clock.h:296
#define TSTMR_CLOCKS
Value:
{ \
}
Clock tstmr0.
Definition: fsl_clock.h:286
#define EWM_CLOCKS
Value:
{ \
}
Clock ewm0.
Definition: fsl_clock.h:278
#define SEMA42_CLOCKS
Value:
{ \
}
Clock Sema0.
Definition: fsl_clock.h:298
#define MAKE_MRCC_REGADDR (   base,
  offset 
)    ((base) + (offset))

It is defined as the corresponding register address.

Enumeration Type Documentation

These clocks source would be generated from SCG module.

Enumerator
kCLOCK_CoreSysClk 

Cortex M33 clock.

kCLOCK_SlowClk 

SLOW_CLK with DIVSLOW.

kCLOCK_PlatClk 

PLAT_CLK.

kCLOCK_SysClk 

SYS_CLK.

kCLOCK_BusClk 

BUS_CLK with DIVBUS.

kCLOCK_ScgSysOscClk 

SCG system OSC clock.

kCLOCK_ScgSircClk 

SCG SIRC clock.

kCLOCK_ScgFircClk 

SCG FIRC clock.

kCLOCK_RtcOscClk 

RTC OSC clock.

These options are for MRCC->XX[CC]

Enumerator
kCLOCK_IpClkControl_fun0 

Peripheral clocks are disabled, module does not stall low power mode entry.

kCLOCK_IpClkControl_fun1 

Peripheral clocks are enabled, module does not stall low power mode entry.

kCLOCK_IpClkControl_fun2 

Peripherals clocks are enabled unless peripheral is idle, low power mode entry will stall until peripheral is idle.

kCLOCK_IpClkControl_fun3 

Peripheral clocks are enabled unless in SLEEP mode (or lower), low power mode entry will stall until peripheral is idle Peripheral functional clocks that remain enabled in SLEEP mode are enabled and do not stall low power mode entry unless entering DEEPSLEEP mode (or lower)

These options are for MRCC->XX[MUX].

Enumerator
kCLOCK_IpSrcFro6M 

FRO 6M clock.

kCLOCK_IpSrcFro192M 

FRO 192M clock.

kCLOCK_IpSrcSoscClk 

OSC RF clock.

kCLOCK_IpSrc32kClk 

32k Clk clock.

Enumerator
kCLOCK_NOGATE 

No clock gate for the IP in MRCC.

kCLOCK_Ewm0 

Clock ewm0.

kCLOCK_Syspm0 

Clock syspm0.

kCLOCK_Wdog0 

Clock wdog0.

kCLOCK_Wdog1 

Clock wdog1.

kCLOCK_Sfa0 

Clock sfa0.

kCLOCK_Crc0 

Clock crc0.

kCLOCK_Secsubsys 

Clock secsubsys.

kCLOCK_Lpit0 

Clock lpit0.

kCLOCK_Tstmr0 

Clock tstmr0.

kCLOCK_Tpm0 

Clock tpm0.

kCLOCK_Tpm1 

Clock tpm1.

kCLOCK_Lpi2c0 

Clock lpi2c0.

kCLOCK_Lpi2c1 

Clock lpi2c1.

kCLOCK_I3c0 

Clock i3c.

kCLOCK_Lpspi0 

Clock lpspi0.

kCLOCK_Lpspi1 

Clock lpspi1.

kCLOCK_Lpuart0 

Clock lpuart0.

kCLOCK_Lpuart1 

Clock lpuart1.

kCLOCK_Flexio0 

Clock Flexio0.

kCLOCK_Can0 

Clock Can0.

kCLOCK_Sema0 

Clock Sema0.

kCLOCK_Data_stream_2p4 

Clock data_stream_2p4.

kCLOCK_PortA 

Clock portA.

kCLOCK_PortB 

Clock portB.

kCLOCK_PortC 

Clock portC.

kCLOCK_Lpadc0 

Clock lpadc0.

kCLOCK_Lpcmp0 

Clock lpcmp0.

kCLOCK_Lpcmp1 

Clock lpcmp1.

kCLOCK_Vref0 

Clock verf0.

kCLOCK_Mtr_master 

Clock mtr_master.

kCLOCK_GpioA 

Clock gpioA.

kCLOCK_GpioB 

Clock gpioB.

kCLOCK_GpioC 

Clock gpioC.

kCLOCK_Dma0 

Clock dma0.

kCLOCK_Pflexnvm 

Clock pflexnvm.

kCLOCK_Sram0 

Clock Sram0.

kCLOCK_Sram1 

Clock Sram1.

kCLOCK_Sram2 

Clock Sram2.

kCLOCK_Sram3 

Clock Sram3.

kCLOCK_Rf_2p4ghz_bist 

Clock rf_2p4ghz_bist.

Enumerator
kStatus_SCG_Busy 

Clock is busy.

kStatus_SCG_InvalidSrc 

Invalid source.

Enumerator
kSCG_SysClkSlow 

System slow clock.

kSCG_SysClkBus 

Bus clock.

kSCG_SysClkPlatform 

Platform clock.

kSCG_SysClkCore 

Core clock.

Enumerator
kSCG_SysClkSrcSysOsc 

System OSC.

kSCG_SysClkSrcSirc 

Slow IRC.

kSCG_SysClkSrcFirc 

Fast IRC.

kSCG_SysClkSrcRosc 

RTC OSC.

Enumerator
kSCG_SysClkDivBy1 

Divided by 1.

kSCG_SysClkDivBy2 

Divided by 2.

kSCG_SysClkDivBy3 

Divided by 3.

kSCG_SysClkDivBy4 

Divided by 4.

kSCG_SysClkDivBy5 

Divided by 5.

kSCG_SysClkDivBy6 

Divided by 6.

kSCG_SysClkDivBy7 

Divided by 7.

kSCG_SysClkDivBy8 

Divided by 8.

kSCG_SysClkDivBy9 

Divided by 9.

kSCG_SysClkDivBy10 

Divided by 10.

kSCG_SysClkDivBy11 

Divided by 11.

kSCG_SysClkDivBy12 

Divided by 12.

kSCG_SysClkDivBy13 

Divided by 13.

kSCG_SysClkDivBy14 

Divided by 14.

kSCG_SysClkDivBy15 

Divided by 15.

kSCG_SysClkDivBy16 

Divided by 16.

Enumerator
kClockClkoutSelScgSlow 

SCG Slow clock.

kClockClkoutSelSosc 

System OSC.

kClockClkoutSelSirc 

Slow IRC.

kClockClkoutSelFirc 

Fast IRC.

kClockClkoutSelScgRtcOsc 

SCG RTC OSC clock.

Enumerator
kSCG_SysOscMonitorDisable 

Monitor disabled.

kSCG_SysOscMonitorInt 

Interrupt when the SOSC error is detected.

kSCG_SysOscMonitorReset 

Reset when the SOSC error is detected.

anonymous enum
Enumerator
kSCG_SoscDisable 

Disable SOSC clock.

kSCG_SoscEnable 

Enable SOSC clock.

kSCG_SoscEnableInSleep 

Enable SOSC in sleep mode.

Enumerator
kSCG_RoscMonitorDisable 

Monitor disabled.

kSCG_RoscMonitorInt 

Interrupt when the RTC OSC error is detected.

kSCG_RoscMonitorReset 

Reset when the RTC OSC error is detected.

Enumerator
kSCG_SircDisableInSleep 

Disable SIRC clock.

kSCG_SircEnableInSleep 

Enable SIRC in sleep mode.

Enumerator
kSCG_FircTrimNonUpdate 

FIRC trim enable but not enable trim value update.

In this mode, the trim value is fixed to the initialized value which is defined by trimCoar and trimFine in configure structure scg_firc_trim_config_t.

kSCG_FircTrimUpdate 

FIRC trim enable and trim value update enable.

In this mode, the trim value is auto update.

Enumerator
kSCG_FircTrimSrcSysOsc 

System OSC.

kSCG_FircTrimSrcRtcOsc 

RTC OSC (32.768 kHz).

anonymous enum
Enumerator
kSCG_FircDisable 

Disable FIRC clock.

kSCG_FircEnable 

Enable FIRC clock.

kSCG_FircEnableInSleep 

Enable FIRC in sleep mode.

Enumerator
kSCG_FircRange48M 

Fast IRC is trimmed to 48 MHz.

kSCG_FircRange64M 

Fast IRC is trimmed to 64 MHz.

kSCG_FircRange96M 

Fast IRC is trimmed to 96 MHz.

kSCG_FircRange192M 

Fast IRC is trimmed to 192 MHz.

Enumerator
kFro192M_Range16M 

FRO192M output frequenc 16 MHz.

kFro192M_Range24M 

FRO192M output frequenc 24 MHz.

kFro192M_Range32M 

FRO192M output frequenc 32 MHz.

kFro192M_Range48M 

FRO192M output frequenc 48 MHz.

kFro192M_Range64M 

FRO192M output frequenc 64 MHz.

Enumerator
kFro192M_ClkDivBy1 

Divided by 1.

kFro192M_ClkDivBy2 

Divided by 2.

kFro192M_ClkDivBy4 

Divided by 4.

kFro192M_ClkDivBy8 

Divided by 8.

Function Documentation

static void CLOCK_EnableClock ( clock_ip_name_t  name)
inlinestatic
Parameters
nameWhich clock to enable, see clock_ip_name_t.
static void CLOCK_EnableClockLPMode ( clock_ip_name_t  name,
clock_ip_control_t  control 
)
inlinestatic
Parameters
nameWhich clock to enable, see clock_ip_name_t.
controlClock Config, see clock_ip_control_t.
static void CLOCK_DisableClock ( clock_ip_name_t  name)
inlinestatic
Parameters
nameWhich clock to disable, see clock_ip_name_t.
static void CLOCK_SetIpSrc ( clock_ip_name_t  name,
clock_ip_src_t  src 
)
inlinestatic

Set the clock source for specific IP, not all modules need to set the clock source, should only use this function for the modules need source setting.

Parameters
nameWhich peripheral to check, see clock_ip_name_t.
srcClock source to set.
static void CLOCK_SetIpSrcDiv ( clock_ip_name_t  name,
uint8_t  divValue 
)
inlinestatic

Set the clock source and divider for specific IP, not all modules need to set the clock source and divider, should only use this function for the modules need source and divider setting.

Divider output clock = Divider input clock / (divValue+1)]).

Parameters
nameWhich peripheral to check, see clock_ip_name_t.
divValueThe divider value.
uint32_t CLOCK_GetFreq ( clock_name_t  clockName)

This function checks the current clock configurations and then calculates the clock frequency for a specific clock name defined in clock_name_t.

Parameters
clockNameClock names defined in clock_name_t
Returns
Clock frequency value in hertz
uint32_t CLOCK_GetCoreSysClkFreq ( void  )
Returns
Clock frequency in Hz.
uint32_t CLOCK_GetPlatClkFreq ( void  )
Returns
Clock frequency in Hz.
uint32_t CLOCK_GetBusClkFreq ( void  )
Returns
Clock frequency in Hz.
uint32_t CLOCK_GetFlashClkFreq ( void  )
Returns
Clock frequency in Hz.
uint32_t CLOCK_GetIpFreq ( clock_ip_name_t  name)

This function gets the IP module's functional clock frequency based on MRCC registers. It is only used for the IP modules which could select clock source by MRCC[PCS].

Parameters
nameWhich peripheral to get, see clock_ip_name_t.
Returns
Clock frequency value in Hz
uint32_t CLOCK_GetSysClkFreq ( scg_sys_clk_t  type)

This function gets the SCG system clock frequency. These clocks are used for core, platform, external, and bus clock domains.

Parameters
typeWhich type of clock to get, core clock or slow clock.
Returns
Clock frequency.
static void CLOCK_SetRunModeSysClkConfig ( const scg_sys_clk_config_t *  config)
inlinestatic

This function sets the system clock configuration for RUN mode.

Parameters
configPointer to the configuration.
static void CLOCK_GetCurSysClkConfig ( scg_sys_clk_config_t *  config)
inlinestatic

This function gets the system configuration in the current power mode.

Parameters
configPointer to the configuration.
static void CLOCK_SetClkOutSel ( clock_clkout_src_t  setting)
inlinestatic

This function sets the clock out selection (CLKOUTSEL).

Parameters
settingThe selection to set.
status_t CLOCK_InitSysOsc ( const scg_sosc_config_t *  config)

This function enables the SCG system OSC clock according to the configuration.

Parameters
configPointer to the configuration structure.
Return values
kStatus_SuccessSystem OSC is initialized.
kStatus_SCG_BusySystem OSC has been enabled and is used by the system clock.
kStatus_ReadOnlySystem OSC control register is locked.
Note
This function can't detect whether the system OSC has been enabled and used by an IP.
status_t CLOCK_DeinitSysOsc ( void  )

This function disables the SCG system OSC clock.

Return values
kStatus_SuccessSystem OSC is deinitialized.
kStatus_SCG_BusySystem OSC is used by the system clock.
kStatus_ReadOnlySystem OSC control register is locked.
Note
This function can't detect whether the system OSC is used by an IP.
uint32_t CLOCK_GetSysOscFreq ( void  )
Returns
Clock frequency; If the clock is invalid, returns 0.
static bool CLOCK_IsSysOscErr ( void  )
inlinestatic
Returns
True if the error occurs, false if not.
static void CLOCK_SetSysOscMonitorMode ( scg_sosc_monitor_mode_t  mode)
inlinestatic

This function sets the system OSC monitor mode. The mode can be disabled, it can generate an interrupt when the error is disabled, or reset when the error is detected.

Parameters
modeMonitor mode to set.
static bool CLOCK_IsSysOscValid ( void  )
inlinestatic
Returns
True if clock is valid, false if not.
status_t CLOCK_InitSirc ( const scg_sirc_config_t *  config)

This function enables the SCG slow IRC clock according to the configuration.

Parameters
configPointer to the configuration structure.
Return values
kStatus_SuccessSIRC is initialized.
kStatus_SCG_BusySIRC has been enabled and is used by system clock.
kStatus_ReadOnlySIRC control register is locked.
Note
This function can't detect whether the system OSC has been enabled and used by an IP.
status_t CLOCK_DeinitSirc ( void  )

This function disables the SCG slow IRC.

Return values
kStatus_SuccessSIRC is deinitialized.
kStatus_SCG_BusySIRC is used by system clock.
kStatus_ReadOnlySIRC control register is locked.
Note
This function can't detect whether the SIRC is used by an IP.
uint32_t CLOCK_GetSircFreq ( void  )
Returns
Clock frequency; If the clock is invalid, returns 0.
static bool CLOCK_IsSircValid ( void  )
inlinestatic
Returns
True if clock is valid, false if not.
status_t CLOCK_InitFirc ( const scg_firc_config_t *  config)

This function enables the SCG fast IRC clock according to the configuration.

Parameters
configPointer to the configuration structure.
Return values
kStatus_SuccessFIRC is initialized.
kStatus_SCG_BusyFIRC has been enabled and is used by the system clock.
kStatus_ReadOnlyFIRC control register is locked.
Note
This function can't detect whether the FIRC has been enabled and used by an IP.
status_t CLOCK_DeinitFirc ( void  )

This function disables the SCG fast IRC.

Return values
kStatus_SuccessFIRC is deinitialized.
kStatus_SCG_BusyFIRC is used by the system clock.
kStatus_ReadOnlyFIRC control register is locked.
Note
This function can't detect whether the FIRC is used by an IP.
uint32_t CLOCK_GetFircFreq ( void  )
Returns
Clock frequency; If the clock is invalid, returns 0.
static bool CLOCK_IsFircErr ( void  )
inlinestatic
Returns
True if the error occurs, false if not.
static bool CLOCK_IsFircValid ( void  )
inlinestatic
Returns
True if clock is valid, false if not.
status_t CLOCK_InitRosc ( const scg_rosc_config_t *  config)

This function enables the SCG ROSC clock according to the configuration.

param config Pointer to the configuration structure. retval kStatus_Success ROSC is initialized. retval kStatus_SCG_Busy ROSC has been enabled and is used by the system clock. retval kStatus_ReadOnly ROSC control register is locked.

note This function can't detect whether the system OSC has been enabled and used by an IP.

status_t CLOCK_DeinitRosc ( void  )

This function disables the SCG ROSC clock.

retval kStatus_Success System OSC is deinitialized. retval kStatus_SCG_Busy System OSC is used by the system clock. retval kStatus_ReadOnly System OSC control register is locked.

note This function can't detect whether the ROSC is used by an IP.

uint32_t CLOCK_GetRtcOscFreq ( void  )
Returns
Clock frequency; If the clock is invalid, returns 0.
status_t CLOCK_InitRfFro192M ( const fro192m_rf_clk_config_t *  config)

This function configure the RF FRO192M clock according to the configuration.

Parameters
configPointer to the configuration structure.
Return values
kStatus_SuccessRF FRO192M is configured.
uint32_t CLOCK_GetRfFro192MFreq ( void  )
Returns
Clock frequency; If the clock is invalid, returns 0.
static bool CLOCK_IsRoscErr ( void  )
inlinestatic
Returns
True if the error occurs, false if not.
static void CLOCK_SetRoscMonitorMode ( scg_rosc_monitor_mode_t  mode)
inlinestatic

This function sets the ROSC monitor mode. The mode can be disabled, it can generate an interrupt when the error is disabled, or reset when the error is detected.

Parameters
modeMonitor mode to set.
static bool CLOCK_IsRoscValid ( void  )
inlinestatic
Returns
True if clock is valid, false if not.
static void CLOCK_SetXtal0Freq ( uint32_t  freq)
inlinestatic
Parameters
freqThe XTAL0/EXTAL0 input clock frequency in Hz.
static void CLOCK_SetXtal32Freq ( uint32_t  freq)
inlinestatic
Parameters
freqThe XTAL32/EXTAL32 input clock frequency in Hz.

Variable Documentation

volatile uint32_t g_xtal0Freq

The XTAL0/EXTAL0 (OSC0/SYSOSC) clock frequency in Hz. When the clock is set up, use the function CLOCK_SetXtal0Freq to set the value in the clock driver. For example, if XTAL0 is 8 MHz:

* CLOCK_SetXtal0Freq(80000000);
*

This is important for the multicore platforms where only one core needs to set up the OSC0/SYSOSC using CLOCK_InitSysOsc. All other cores need to call the CLOCK_SetXtal0Freq to get a valid clock frequency.

volatile uint32_t g_xtal32Freq

The XTAL32/EXTAL32 clock frequency in Hz. When the clock is set up, use the function CLOCK_SetXtal32Freq to set the value in the clock driver.

This is important for the multicore platforms where only one core needs to set up the clock. All other cores need to call the CLOCK_SetXtal32Freq to get a valid clock frequency.