MCUXpresso SDK API Reference Manual  Rev 2.16.100
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
I3C Master Driver

Overview

Data Structures

struct  i3c_register_ibi_addr_t
 Structure with setting master IBI rules and slave registry. More...
 
struct  i3c_baudrate_hz_t
 Structure with I3C baudrate settings. More...
 
struct  i3c_master_daa_baudrate_t
 I3C DAA baud rate configuration. More...
 
struct  i3c_master_config_t
 Structure with settings to initialize the I3C master module. More...
 
struct  i3c_master_transfer_callback_t
 i3c master callback functions. More...
 
struct  i3c_master_transfer_t
 Non-blocking transfer descriptor structure. More...
 
struct  i3c_master_handle_t
 Driver handle for master non-blocking APIs. More...
 

Typedefs

typedef void(* i3c_master_isr_t )(I3C_Type *base, void *handle)
 Typedef for master interrupt handler. More...
 

Enumerations

enum  _i3c_master_flags {
  kI3C_MasterBetweenFlag = I3C_MSTATUS_BETWEEN_MASK,
  kI3C_MasterNackDetectFlag = I3C_MSTATUS_NACKED_MASK,
  kI3C_MasterSlaveStartFlag = I3C_MSTATUS_SLVSTART_MASK,
  kI3C_MasterControlDoneFlag = I3C_MSTATUS_MCTRLDONE_MASK,
  kI3C_MasterCompleteFlag = I3C_MSTATUS_COMPLETE_MASK,
  kI3C_MasterRxReadyFlag = I3C_MSTATUS_RXPEND_MASK,
  kI3C_MasterTxReadyFlag = I3C_MSTATUS_TXNOTFULL_MASK,
  kI3C_MasterArbitrationWonFlag = I3C_MSTATUS_IBIWON_MASK,
  kI3C_MasterErrorFlag = I3C_MSTATUS_ERRWARN_MASK,
  kI3C_MasterSlave2MasterFlag = I3C_MSTATUS_NOWMASTER_MASK
}
 I3C master peripheral flags. More...
 
enum  _i3c_master_error_flags {
  kI3C_MasterErrorNackFlag = I3C_MERRWARN_NACK_MASK,
  kI3C_MasterErrorWriteAbortFlag = I3C_MERRWARN_WRABT_MASK,
  kI3C_MasterErrorTermFlag = I3C_MERRWARN_TERM_MASK,
  kI3C_MasterErrorParityFlag = I3C_MERRWARN_HPAR_MASK,
  kI3C_MasterErrorCrcFlag = I3C_MERRWARN_HCRC_MASK,
  kI3C_MasterErrorReadFlag = I3C_MERRWARN_OREAD_MASK,
  kI3C_MasterErrorWriteFlag = I3C_MERRWARN_OWRITE_MASK,
  kI3C_MasterErrorMsgFlag = I3C_MERRWARN_MSGERR_MASK,
  kI3C_MasterErrorInvalidReqFlag = I3C_MERRWARN_INVREQ_MASK,
  kI3C_MasterErrorTimeoutFlag = I3C_MERRWARN_TIMEOUT_MASK,
  kI3C_MasterAllErrorFlags
}
 I3C master error flags to indicate the causes. More...
 
enum  i3c_master_state_t {
  kI3C_MasterStateIdle = 0U,
  kI3C_MasterStateSlvReq = 1U,
  kI3C_MasterStateMsgSdr = 2U,
  kI3C_MasterStateNormAct = 3U,
  kI3C_MasterStateDdr = 4U,
  kI3C_MasterStateDaa = 5U,
  kI3C_MasterStateIbiAck = 6U,
  kI3C_MasterStateIbiRcv = 7U
}
 I3C working master state. More...
 
enum  i3c_master_enable_t {
  kI3C_MasterOff = 0U,
  kI3C_MasterOn = 1U,
  kI3C_MasterCapable = 2U
}
 I3C master enable configuration. More...
 
enum  i3c_master_hkeep_t {
  kI3C_MasterHighKeeperNone = 0U,
  kI3C_MasterHighKeeperWiredIn = 1U,
  kI3C_MasterPassiveSDA = 2U,
  kI3C_MasterPassiveSDASCL = 3U
}
 I3C high keeper configuration. More...
 
enum  i3c_bus_request_t {
  kI3C_RequestNone = 0U,
  kI3C_RequestEmitStartAddr = 1U,
  kI3C_RequestEmitStop = 2U,
  kI3C_RequestIbiAckNack = 3U,
  kI3C_RequestProcessDAA = 4U,
  kI3C_RequestForceExit = 6U,
  kI3C_RequestAutoIbi = 7U
}
 Emits the requested operation when doing in pieces vs. More...
 
enum  i3c_bus_type_t {
  kI3C_TypeI3CSdr = 0U,
  kI3C_TypeI2C = 1U,
  kI3C_TypeI3CDdr = 2U
}
 Bus type with EmitStartAddr. More...
 
enum  i3c_ibi_response_t {
  kI3C_IbiRespAck = 0U,
  kI3C_IbiRespNack = 1U,
  kI3C_IbiRespAckMandatory = 2U,
  kI3C_IbiRespManual = 3U
}
 IBI response. More...
 
enum  i3c_ibi_type_t {
  kI3C_IbiNormal = 0U,
  kI3C_IbiHotJoin = 1U,
  kI3C_IbiMasterRequest = 2U
}
 IBI type. More...
 
enum  i3c_ibi_state_t {
  kI3C_IbiReady = 0U,
  kI3C_IbiDataBuffNeed = 1U,
  kI3C_IbiAckNackPending = 2U
}
 IBI state. More...
 
enum  i3c_direction_t {
  kI3C_Write = 0U,
  kI3C_Read = 1U
}
 Direction of master and slave transfers. More...
 
enum  i3c_tx_trigger_level_t {
  kI3C_TxTriggerOnEmpty = 0U,
  kI3C_TxTriggerUntilOneQuarterOrLess = 1U,
  kI3C_TxTriggerUntilOneHalfOrLess = 2U,
  kI3C_TxTriggerUntilOneLessThanFull = 3U
}
 Watermark of TX int/dma trigger level. More...
 
enum  i3c_rx_trigger_level_t {
  kI3C_RxTriggerOnNotEmpty = 0U,
  kI3C_RxTriggerUntilOneQuarterOrMore = 1U,
  kI3C_RxTriggerUntilOneHalfOrMore = 2U,
  kI3C_RxTriggerUntilThreeQuarterOrMore = 3U
}
 Watermark of RX int/dma trigger level. More...
 
enum  i3c_rx_term_ops_t {
  kI3C_RxTermDisable = 0U,
  kI3C_RxAutoTerm = 1U,
  kI3C_RxTermLastByte = 2U
}
 I3C master read termination operations. More...
 
enum  i3c_start_scl_delay_t {
  kI3C_NoDelay = 0U,
  kI3C_IncreaseSclHalfPeriod = 1U,
  kI3C_IncreaseSclOnePeriod = 2U,
  kI3C_IncreaseSclOneAndHalfPeriod = 3U
}
 I3C start SCL delay options. More...
 
enum  _i3c_master_transfer_flags {
  kI3C_TransferDefaultFlag = 0x00U,
  kI3C_TransferNoStartFlag = 0x01U,
  kI3C_TransferRepeatedStartFlag = 0x02U,
  kI3C_TransferNoStopFlag = 0x04U,
  kI3C_TransferWordsFlag = 0x08U,
  kI3C_TransferDisableRxTermFlag = 0x10U,
  kI3C_TransferRxAutoTermFlag,
  kI3C_TransferStartWithBroadcastAddr = 0x40U
}
 Transfer option flags. More...
 

Initialization and deinitialization

void I3C_MasterGetDefaultConfig (i3c_master_config_t *masterConfig)
 Provides a default configuration for the I3C master peripheral. More...
 
void I3C_MasterInit (I3C_Type *base, const i3c_master_config_t *masterConfig, uint32_t sourceClock_Hz)
 Initializes the I3C master peripheral. More...
 
void I3C_MasterDeinit (I3C_Type *base)
 Deinitializes the I3C master peripheral. More...
 
status_t I3C_MasterCheckAndClearError (I3C_Type *base, uint32_t status)
 
status_t I3C_MasterWaitForCtrlDone (I3C_Type *base, bool waitIdle)
 
status_t I3C_CheckForBusyBus (I3C_Type *base)
 
static void I3C_MasterEnable (I3C_Type *base, i3c_master_enable_t enable)
 Set I3C module master mode. More...
 
void I3C_SlaveGetDefaultConfig (i3c_slave_config_t *slaveConfig)
 Provides a default configuration for the I3C slave peripheral. More...
 
void I3C_SlaveInit (I3C_Type *base, const i3c_slave_config_t *slaveConfig, uint32_t slowClock_Hz)
 Initializes the I3C slave peripheral. More...
 
void I3C_SlaveDeinit (I3C_Type *base)
 Deinitializes the I3C slave peripheral. More...
 
static void I3C_SlaveEnable (I3C_Type *base, bool isEnable)
 Enable/Disable Slave. More...
 

Status

static uint32_t I3C_MasterGetStatusFlags (I3C_Type *base)
 Gets the I3C master status flags. More...
 
static void I3C_MasterClearStatusFlags (I3C_Type *base, uint32_t statusMask)
 Clears the I3C master status flag state. More...
 
static uint32_t I3C_MasterGetErrorStatusFlags (I3C_Type *base)
 Gets the I3C master error status flags. More...
 
static void I3C_MasterClearErrorStatusFlags (I3C_Type *base, uint32_t statusMask)
 Clears the I3C master error status flag state. More...
 
i3c_master_state_t I3C_MasterGetState (I3C_Type *base)
 Gets the I3C master state. More...
 
static uint32_t I3C_SlaveGetStatusFlags (I3C_Type *base)
 Gets the I3C slave status flags. More...
 
static void I3C_SlaveClearStatusFlags (I3C_Type *base, uint32_t statusMask)
 Clears the I3C slave status flag state. More...
 
static uint32_t I3C_SlaveGetErrorStatusFlags (I3C_Type *base)
 Gets the I3C slave error status flags. More...
 
static void I3C_SlaveClearErrorStatusFlags (I3C_Type *base, uint32_t statusMask)
 Clears the I3C slave error status flag state. More...
 
i3c_slave_activity_state_t I3C_SlaveGetActivityState (I3C_Type *base)
 Gets the I3C slave state. More...
 
status_t I3C_SlaveCheckAndClearError (I3C_Type *base, uint32_t status)
 

Interrupts

static void I3C_MasterEnableInterrupts (I3C_Type *base, uint32_t interruptMask)
 Enables the I3C master interrupt requests. More...
 
static void I3C_MasterDisableInterrupts (I3C_Type *base, uint32_t interruptMask)
 Disables the I3C master interrupt requests. More...
 
static uint32_t I3C_MasterGetEnabledInterrupts (I3C_Type *base)
 Returns the set of currently enabled I3C master interrupt requests. More...
 
static uint32_t I3C_MasterGetPendingInterrupts (I3C_Type *base)
 Returns the set of pending I3C master interrupt requests. More...
 
static void I3C_SlaveEnableInterrupts (I3C_Type *base, uint32_t interruptMask)
 Enables the I3C slave interrupt requests. More...
 
static void I3C_SlaveDisableInterrupts (I3C_Type *base, uint32_t interruptMask)
 Disables the I3C slave interrupt requests. More...
 
static uint32_t I3C_SlaveGetEnabledInterrupts (I3C_Type *base)
 Returns the set of currently enabled I3C slave interrupt requests. More...
 
static uint32_t I3C_SlaveGetPendingInterrupts (I3C_Type *base)
 Returns the set of pending I3C slave interrupt requests. More...
 

DMA control

static void I3C_MasterEnableDMA (I3C_Type *base, bool enableTx, bool enableRx, uint32_t width)
 Enables or disables I3C master DMA requests. More...
 
static uint32_t I3C_MasterGetTxFifoAddress (I3C_Type *base, uint32_t width)
 Gets I3C master transmit data register address for DMA transfer. More...
 
static uint32_t I3C_MasterGetRxFifoAddress (I3C_Type *base, uint32_t width)
 Gets I3C master receive data register address for DMA transfer. More...
 
static void I3C_SlaveEnableDMA (I3C_Type *base, bool enableTx, bool enableRx, uint32_t width)
 Enables or disables I3C slave DMA requests. More...
 
static uint32_t I3C_SlaveGetTxFifoAddress (I3C_Type *base, uint32_t width)
 Gets I3C slave transmit data register address for DMA transfer. More...
 
static uint32_t I3C_SlaveGetRxFifoAddress (I3C_Type *base, uint32_t width)
 Gets I3C slave receive data register address for DMA transfer. More...
 

FIFO control

static void I3C_MasterSetWatermarks (I3C_Type *base, i3c_tx_trigger_level_t txLvl, i3c_rx_trigger_level_t rxLvl, bool flushTx, bool flushRx)
 Sets the watermarks for I3C master FIFOs. More...
 
static void I3C_MasterGetFifoCounts (I3C_Type *base, size_t *rxCount, size_t *txCount)
 Gets the current number of bytes in the I3C master FIFOs. More...
 
static void I3C_SlaveSetWatermarks (I3C_Type *base, i3c_tx_trigger_level_t txLvl, i3c_rx_trigger_level_t rxLvl, bool flushTx, bool flushRx)
 Sets the watermarks for I3C slave FIFOs. More...
 
static void I3C_SlaveGetFifoCounts (I3C_Type *base, size_t *rxCount, size_t *txCount)
 Gets the current number of bytes in the I3C slave FIFOs. More...
 

Bus operations

void I3C_MasterSetBaudRate (I3C_Type *base, const i3c_baudrate_hz_t *baudRate_Hz, uint32_t sourceClock_Hz)
 Sets the I3C bus frequency for master transactions. More...
 
static bool I3C_MasterGetBusIdleState (I3C_Type *base)
 Returns whether the bus is idle. More...
 
status_t I3C_MasterStartWithRxSize (I3C_Type *base, i3c_bus_type_t type, uint8_t address, i3c_direction_t dir, uint8_t rxSize)
 Sends a START signal and slave address on the I2C/I3C bus, receive size is also specified in the call. More...
 
status_t I3C_MasterStart (I3C_Type *base, i3c_bus_type_t type, uint8_t address, i3c_direction_t dir)
 Sends a START signal and slave address on the I2C/I3C bus. More...
 
status_t I3C_MasterRepeatedStartWithRxSize (I3C_Type *base, i3c_bus_type_t type, uint8_t address, i3c_direction_t dir, uint8_t rxSize)
 Sends a repeated START signal and slave address on the I2C/I3C bus, receive size is also specified in the call. More...
 
static status_t I3C_MasterRepeatedStart (I3C_Type *base, i3c_bus_type_t type, uint8_t address, i3c_direction_t dir)
 Sends a repeated START signal and slave address on the I2C/I3C bus. More...
 
status_t I3C_MasterSend (I3C_Type *base, const void *txBuff, size_t txSize, uint32_t flags)
 Performs a polling send transfer on the I2C/I3C bus. More...
 
status_t I3C_MasterReceive (I3C_Type *base, void *rxBuff, size_t rxSize, uint32_t flags)
 Performs a polling receive transfer on the I2C/I3C bus. More...
 
status_t I3C_MasterStop (I3C_Type *base)
 Sends a STOP signal on the I2C/I3C bus. More...
 
void I3C_MasterEmitRequest (I3C_Type *base, i3c_bus_request_t masterReq)
 I3C master emit request. More...
 
static void I3C_MasterEmitIBIResponse (I3C_Type *base, i3c_ibi_response_t ibiResponse)
 I3C master emit request. More...
 
void I3C_MasterRegisterIBI (I3C_Type *base, i3c_register_ibi_addr_t *ibiRule)
 I3C master register IBI rule. More...
 
void I3C_MasterGetIBIRules (I3C_Type *base, i3c_register_ibi_addr_t *ibiRule)
 I3C master get IBI rule. More...
 
i3c_ibi_type_t I3C_GetIBIType (I3C_Type *base)
 I3C master get IBI Type. More...
 
static uint8_t I3C_GetIBIAddress (I3C_Type *base)
 I3C master get IBI Address. More...
 
status_t I3C_MasterProcessDAASpecifiedBaudrate (I3C_Type *base, uint8_t *addressList, uint32_t count, i3c_master_daa_baudrate_t *daaBaudRate)
 Performs a DAA in the i3c bus with specified temporary baud rate. More...
 
static status_t I3C_MasterProcessDAA (I3C_Type *base, uint8_t *addressList, uint32_t count)
 Performs a DAA in the i3c bus. More...
 
i3c_device_info_t * I3C_MasterGetDeviceListAfterDAA (I3C_Type *base, uint8_t *count)
 Get device information list after DAA process is done. More...
 
status_t I3C_MasterTransferBlocking (I3C_Type *base, i3c_master_transfer_t *transfer)
 Performs a master polling transfer on the I2C/I3C bus. More...
 
void I3C_SlaveRequestEvent (I3C_Type *base, i3c_slave_event_t event)
 I3C slave request event. More...
 
status_t I3C_SlaveSend (I3C_Type *base, const void *txBuff, size_t txSize)
 Performs a polling send transfer on the I3C bus. More...
 
status_t I3C_SlaveReceive (I3C_Type *base, void *rxBuff, size_t rxSize)
 Performs a polling receive transfer on the I3C bus. More...
 

Non-blocking

void I3C_MasterTransferCreateHandle (I3C_Type *base, i3c_master_handle_t *handle, const i3c_master_transfer_callback_t *callback, void *userData)
 Creates a new handle for the I3C master non-blocking APIs. More...
 
status_t I3C_MasterTransferNonBlocking (I3C_Type *base, i3c_master_handle_t *handle, i3c_master_transfer_t *transfer)
 Performs a non-blocking transaction on the I2C/I3C bus. More...
 
status_t I3C_MasterTransferGetCount (I3C_Type *base, i3c_master_handle_t *handle, size_t *count)
 Returns number of bytes transferred so far. More...
 
void I3C_MasterTransferAbort (I3C_Type *base, i3c_master_handle_t *handle)
 Terminates a non-blocking I3C master transmission early. More...
 

IRQ handler

void I3C_MasterTransferHandleIRQ (I3C_Type *base, void *intHandle)
 Reusable routine to handle master interrupts. More...
 

Data Structure Documentation

struct i3c_register_ibi_addr_t

Data Fields

uint8_t address [5]
 Address array for registry. More...
 
bool ibiHasPayload
 Whether the address array has mandatory IBI byte. More...
 

Field Documentation

uint8_t i3c_register_ibi_addr_t::address[5]
bool i3c_register_ibi_addr_t::ibiHasPayload
struct i3c_baudrate_hz_t

Data Fields

uint32_t i2cBaud
 Desired I2C baud rate in Hertz. More...
 
uint32_t i3cPushPullBaud
 Desired I3C push-pull baud rate in Hertz. More...
 
uint32_t i3cOpenDrainBaud
 Desired I3C open-drain baud rate in Hertz. More...
 

Field Documentation

uint32_t i3c_baudrate_hz_t::i2cBaud
uint32_t i3c_baudrate_hz_t::i3cPushPullBaud
uint32_t i3c_baudrate_hz_t::i3cOpenDrainBaud
struct i3c_master_daa_baudrate_t

Data Fields

uint32_t sourceClock_Hz
 FCLK, function clock in Hertz. More...
 
uint32_t i3cPushPullBaud
 Desired I3C push-pull baud rate in Hertz. More...
 
uint32_t i3cOpenDrainBaud
 Desired I3C open-drain baud rate in Hertz. More...
 

Field Documentation

uint32_t i3c_master_daa_baudrate_t::sourceClock_Hz
uint32_t i3c_master_daa_baudrate_t::i3cPushPullBaud
uint32_t i3c_master_daa_baudrate_t::i3cOpenDrainBaud
struct i3c_master_config_t

This structure holds configuration settings for the I3C peripheral. To initialize this structure to reasonable defaults, call the I3C_MasterGetDefaultConfig() function and pass a pointer to your configuration structure instance.

The configuration structure can be made constant so it resides in flash.

Data Fields

i3c_master_enable_t enableMaster
 Enable master mode. More...
 
bool disableTimeout
 Whether to disable timeout to prevent the ERRWARN. More...
 
i3c_master_hkeep_t hKeep
 High keeper mode setting. More...
 
bool enableOpenDrainStop
 Whether to emit open-drain speed STOP. More...
 
bool enableOpenDrainHigh
 Enable Open-Drain High to be 1 PPBAUD count for i3c messages, or 1 ODBAUD. More...
 
i3c_baudrate_hz_t baudRate_Hz
 Desired baud rate settings. More...
 
uint32_t slowClock_Hz
 Slow clock frequency. More...
 

Field Documentation

i3c_master_enable_t i3c_master_config_t::enableMaster
bool i3c_master_config_t::disableTimeout
i3c_master_hkeep_t i3c_master_config_t::hKeep
bool i3c_master_config_t::enableOpenDrainStop
bool i3c_master_config_t::enableOpenDrainHigh
i3c_baudrate_hz_t i3c_master_config_t::baudRate_Hz
uint32_t i3c_master_config_t::slowClock_Hz
struct i3c_master_transfer_callback_t

Data Fields

void(* slave2Master )(I3C_Type *base, void *userData)
 Transfer complete callback.
 
void(* ibiCallback )(I3C_Type *base, i3c_master_handle_t *handle, i3c_ibi_type_t ibiType, i3c_ibi_state_t ibiState)
 IBI event callback.
 
void(* transferComplete )(I3C_Type *base, i3c_master_handle_t *handle, status_t completionStatus, void *userData)
 Transfer complete callback.
 
struct _i3c_master_transfer

This structure is used to pass transaction parameters to the I3C_MasterTransferNonBlocking() API.

Data Fields

uint32_t flags
 Bit mask of options for the transfer. More...
 
uint8_t slaveAddress
 The 7-bit slave address. More...
 
i3c_direction_t direction
 Either kI3C_Read or kI3C_Write. More...
 
uint32_t subaddress
 Sub address. More...
 
size_t subaddressSize
 Length of sub address to send in bytes. More...
 
void * data
 Pointer to data to transfer. More...
 
size_t dataSize
 Number of bytes to transfer. More...
 
i3c_bus_type_t busType
 bus type. More...
 
i3c_ibi_response_t ibiResponse
 ibi response during transfer. More...
 

Field Documentation

uint32_t i3c_master_transfer_t::flags

See enumeration _i3c_master_transfer_flags for available options. Set to 0 or kI3C_TransferDefaultFlag for normal transfers.

uint8_t i3c_master_transfer_t::slaveAddress
i3c_direction_t i3c_master_transfer_t::direction
uint32_t i3c_master_transfer_t::subaddress

Transferred MSB first.

size_t i3c_master_transfer_t::subaddressSize

Maximum size is 4 bytes.

void* i3c_master_transfer_t::data
size_t i3c_master_transfer_t::dataSize
i3c_bus_type_t i3c_master_transfer_t::busType
i3c_ibi_response_t i3c_master_transfer_t::ibiResponse
struct _i3c_master_handle
Note
The contents of this structure are private and subject to change.

Data Fields

uint8_t state
 Transfer state machine current state. More...
 
uint32_t remainingBytes
 Remaining byte count in current state. More...
 
i3c_rx_term_ops_t rxTermOps
 Read termination operation. More...
 
i3c_master_transfer_t transfer
 Copy of the current transfer info. More...
 
uint8_t ibiAddress
 Slave address which request IBI. More...
 
uint8_t * ibiBuff
 Pointer to IBI buffer to keep ibi bytes. More...
 
size_t ibiPayloadSize
 IBI payload size. More...
 
i3c_ibi_type_t ibiType
 IBI type. More...
 
i3c_master_transfer_callback_t callback
 Callback functions pointer. More...
 
void * userData
 Application data passed to callback. More...
 

Field Documentation

uint8_t i3c_master_handle_t::state
uint32_t i3c_master_handle_t::remainingBytes
i3c_rx_term_ops_t i3c_master_handle_t::rxTermOps
i3c_master_transfer_t i3c_master_handle_t::transfer
uint8_t i3c_master_handle_t::ibiAddress
uint8_t* i3c_master_handle_t::ibiBuff
size_t i3c_master_handle_t::ibiPayloadSize
i3c_ibi_type_t i3c_master_handle_t::ibiType
i3c_master_transfer_callback_t i3c_master_handle_t::callback
void* i3c_master_handle_t::userData

Typedef Documentation

typedef void(* i3c_master_isr_t)(I3C_Type *base, void *handle)

Enumeration Type Documentation

The following status register flags can be cleared:

All flags except kI3C_MasterBetweenFlag and kI3C_MasterNackDetectFlag can be enabled as interrupts.

Note
These enums are meant to be OR'd together to form a bit mask.
Enumerator
kI3C_MasterBetweenFlag 

Between messages/DAAs flag.

kI3C_MasterNackDetectFlag 

NACK detected flag.

kI3C_MasterSlaveStartFlag 

Slave request start flag.

kI3C_MasterControlDoneFlag 

Master request complete flag.

kI3C_MasterCompleteFlag 

Transfer complete flag.

kI3C_MasterRxReadyFlag 

Rx data ready in Rx buffer flag.

kI3C_MasterTxReadyFlag 

Tx buffer ready for Tx data flag.

kI3C_MasterArbitrationWonFlag 

Header address won arbitration flag.

kI3C_MasterErrorFlag 

Error occurred flag.

kI3C_MasterSlave2MasterFlag 

Switch from slave to master flag.

Note
These enums are meant to be OR'd together to form a bit mask.
Enumerator
kI3C_MasterErrorNackFlag 

Slave NACKed the last address.

kI3C_MasterErrorWriteAbortFlag 

Slave NACKed the write data.

kI3C_MasterErrorTermFlag 

Master terminates slave read.

kI3C_MasterErrorParityFlag 

Parity error from DDR read.

kI3C_MasterErrorCrcFlag 

CRC error from DDR read.

kI3C_MasterErrorReadFlag 

Read from MRDATAB register when FIFO empty.

kI3C_MasterErrorWriteFlag 

Write to MWDATAB register when FIFO full.

kI3C_MasterErrorMsgFlag 

Message SDR/DDR mismatch or read/write message in wrong state.

kI3C_MasterErrorInvalidReqFlag 

Invalid use of request.

kI3C_MasterErrorTimeoutFlag 

The module has stalled too long in a frame.

kI3C_MasterAllErrorFlags 

All error flags.

Enumerator
kI3C_MasterStateIdle 

Bus stopped.

kI3C_MasterStateSlvReq 

Bus stopped but slave holding SDA low.

kI3C_MasterStateMsgSdr 

In SDR Message mode from using MWMSG_SDR.

kI3C_MasterStateNormAct 

In normal active SDR mode.

kI3C_MasterStateDdr 

In DDR Message mode.

kI3C_MasterStateDaa 

In ENTDAA mode.

kI3C_MasterStateIbiAck 

Waiting on IBI ACK/NACK decision.

kI3C_MasterStateIbiRcv 

receiving IBI.

Enumerator
kI3C_MasterOff 

Master off.

kI3C_MasterOn 

Master on.

kI3C_MasterCapable 

Master capable.

Enumerator
kI3C_MasterHighKeeperNone 

Use PUR to hold SCL high.

kI3C_MasterHighKeeperWiredIn 

Use pin_HK controls.

kI3C_MasterPassiveSDA 

Hi-Z for Bus Free and hold SDA.

kI3C_MasterPassiveSDASCL 

Hi-Z both for Bus Free, and can Hi-Z SDA for hold.

by message.

Enumerator
kI3C_RequestNone 

No request.

kI3C_RequestEmitStartAddr 

Request to emit start and address on bus.

kI3C_RequestEmitStop 

Request to emit stop on bus.

kI3C_RequestIbiAckNack 

Manual IBI ACK or NACK.

kI3C_RequestProcessDAA 

Process DAA.

kI3C_RequestForceExit 

Request to force exit.

kI3C_RequestAutoIbi 

Hold in stopped state, but Auto-emit START,7E.

Enumerator
kI3C_TypeI3CSdr 

SDR mode of I3C.

kI3C_TypeI2C 

Standard i2c protocol.

kI3C_TypeI3CDdr 

HDR-DDR mode of I3C.

Enumerator
kI3C_IbiRespAck 

ACK with no mandatory byte.

kI3C_IbiRespNack 

NACK.

kI3C_IbiRespAckMandatory 

ACK with mandatory byte.

kI3C_IbiRespManual 

Reserved.

Enumerator
kI3C_IbiNormal 

In-band interrupt.

kI3C_IbiHotJoin 

slave hot join.

kI3C_IbiMasterRequest 

slave master ship request.

Enumerator
kI3C_IbiReady 

In-band interrupt ready state, ready for user to handle.

kI3C_IbiDataBuffNeed 

In-band interrupt need data buffer for data receive.

kI3C_IbiAckNackPending 

In-band interrupt Ack/Nack pending for decision.

Enumerator
kI3C_Write 

Master transmit.

kI3C_Read 

Master receive.

Enumerator
kI3C_TxTriggerOnEmpty 

Trigger on empty.

kI3C_TxTriggerUntilOneQuarterOrLess 

Trigger on 1/4 full or less.

kI3C_TxTriggerUntilOneHalfOrLess 

Trigger on 1/2 full or less.

kI3C_TxTriggerUntilOneLessThanFull 

Trigger on 1 less than full or less.

Enumerator
kI3C_RxTriggerOnNotEmpty 

Trigger on not empty.

kI3C_RxTriggerUntilOneQuarterOrMore 

Trigger on 1/4 full or more.

kI3C_RxTriggerUntilOneHalfOrMore 

Trigger on 1/2 full or more.

kI3C_RxTriggerUntilThreeQuarterOrMore 

Trigger on 3/4 full or more.

Enumerator
kI3C_RxTermDisable 

Master doesn't terminate read, used for CCC transfer.

kI3C_RxAutoTerm 

Master auto terminate read after receiving specified bytes(<=255).

kI3C_RxTermLastByte 

Master terminates read at any time after START, no length limitation.

Enumerator
kI3C_NoDelay 

No delay.

kI3C_IncreaseSclHalfPeriod 

Increases SCL clock period by 1/2.

kI3C_IncreaseSclOnePeriod 

Increases SCL clock period by 1.

kI3C_IncreaseSclOneAndHalfPeriod 

Increases SCL clock period by 1 1/2.

Note
These enumerations are intended to be OR'd together to form a bit mask of options for the _i3c_master_transfer::flags field.
Enumerator
kI3C_TransferDefaultFlag 

Transfer starts with a start signal, stops with a stop signal.

kI3C_TransferNoStartFlag 

Don't send a start condition, address, and sub address.

kI3C_TransferRepeatedStartFlag 

Send a repeated start condition.

kI3C_TransferNoStopFlag 

Don't send a stop condition.

kI3C_TransferWordsFlag 

Transfer in words, else transfer in bytes.

kI3C_TransferDisableRxTermFlag 

Disable Rx termination.

Note: It's for I3C CCC transfer.

kI3C_TransferRxAutoTermFlag 

Set Rx auto-termination.

Note: It's adaptive based on Rx size(<=255 bytes) except in I3C_MasterReceive.

kI3C_TransferStartWithBroadcastAddr 

Start transfer with 0x7E, then read/write data with device address.

Function Documentation

void I3C_MasterGetDefaultConfig ( i3c_master_config_t *  masterConfig)

This function provides the following default configuration for the I3C master peripheral:

* masterConfig->enableMaster = kI3C_MasterOn;
* masterConfig->disableTimeout = false;
* masterConfig->hKeep = kI3C_MasterHighKeeperNone;
* masterConfig->enableOpenDrainStop = true;
* masterConfig->enableOpenDrainHigh = true;
* masterConfig->baudRate_Hz = 100000U;
* masterConfig->busType = kI3C_TypeI2C;
*

After calling this function, you can override any settings in order to customize the configuration, prior to initializing the master driver with I3C_MasterInit().

Parameters
[out]masterConfigUser provided configuration structure for default values. Refer to i3c_master_config_t.
void I3C_MasterInit ( I3C_Type *  base,
const i3c_master_config_t *  masterConfig,
uint32_t  sourceClock_Hz 
)

This function enables the peripheral clock and initializes the I3C master peripheral as described by the user provided configuration. A software reset is performed prior to configuration.

Parameters
baseThe I3C peripheral base address.
masterConfigUser provided peripheral configuration. Use I3C_MasterGetDefaultConfig() to get a set of defaults that you can override.
sourceClock_HzFrequency in Hertz of the I3C functional clock. Used to calculate the baud rate divisors, filter widths, and timeout periods.
void I3C_MasterDeinit ( I3C_Type *  base)

This function disables the I3C master peripheral and gates the clock. It also performs a software reset to restore the peripheral to reset conditions.

Parameters
baseThe I3C peripheral base address.
static void I3C_MasterEnable ( I3C_Type *  base,
i3c_master_enable_t  enable 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
enableEnable master mode.
static uint32_t I3C_MasterGetStatusFlags ( I3C_Type *  base)
inlinestatic

A bit mask with the state of all I3C master status flags is returned. For each flag, the corresponding bit in the return value is set if the flag is asserted.

Parameters
baseThe I3C peripheral base address.
Returns
State of the status flags:
  • 1: related status flag is set.
  • 0: related status flag is not set.
See Also
_i3c_master_flags
static void I3C_MasterClearStatusFlags ( I3C_Type *  base,
uint32_t  statusMask 
)
inlinestatic

The following status register flags can be cleared:

Attempts to clear other flags has no effect.

Parameters
baseThe I3C peripheral base address.
statusMaskA bitmask of status flags that are to be cleared. The mask is composed of _i3c_master_flags enumerators OR'd together. You may pass the result of a previous call to I3C_MasterGetStatusFlags().
See Also
_i3c_master_flags.
static uint32_t I3C_MasterGetErrorStatusFlags ( I3C_Type *  base)
inlinestatic

A bit mask with the state of all I3C master error status flags is returned. For each flag, the corresponding bit in the return value is set if the flag is asserted.

Parameters
baseThe I3C peripheral base address.
Returns
State of the error status flags:
  • 1: related status flag is set.
  • 0: related status flag is not set.
See Also
_i3c_master_error_flags
static void I3C_MasterClearErrorStatusFlags ( I3C_Type *  base,
uint32_t  statusMask 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
statusMaskA bitmask of error status flags that are to be cleared. The mask is composed of _i3c_master_error_flags enumerators OR'd together. You may pass the result of a previous call to I3C_MasterGetStatusFlags().
See Also
_i3c_master_error_flags.
i3c_master_state_t I3C_MasterGetState ( I3C_Type *  base)
Parameters
baseThe I3C peripheral base address.
Returns
I3C master state.
static void I3C_MasterEnableInterrupts ( I3C_Type *  base,
uint32_t  interruptMask 
)
inlinestatic

All flags except kI3C_MasterBetweenFlag and kI3C_MasterNackDetectFlag can be enabled as interrupts.

Parameters
baseThe I3C peripheral base address.
interruptMaskBit mask of interrupts to enable. See _i3c_master_flags for the set of constants that should be OR'd together to form the bit mask.
static void I3C_MasterDisableInterrupts ( I3C_Type *  base,
uint32_t  interruptMask 
)
inlinestatic

All flags except kI3C_MasterBetweenFlag and kI3C_MasterNackDetectFlag can be enabled as interrupts.

Parameters
baseThe I3C peripheral base address.
interruptMaskBit mask of interrupts to disable. See _i3c_master_flags for the set of constants that should be OR'd together to form the bit mask.
static uint32_t I3C_MasterGetEnabledInterrupts ( I3C_Type *  base)
inlinestatic
Parameters
baseThe I3C peripheral base address.
Returns
A bitmask composed of _i3c_master_flags enumerators OR'd together to indicate the set of enabled interrupts.
static uint32_t I3C_MasterGetPendingInterrupts ( I3C_Type *  base)
inlinestatic
Parameters
baseThe I3C peripheral base address.
Returns
A bitmask composed of _i3c_master_flags enumerators OR'd together to indicate the set of pending interrupts.
static void I3C_MasterEnableDMA ( I3C_Type *  base,
bool  enableTx,
bool  enableRx,
uint32_t  width 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
enableTxEnable flag for transmit DMA request. Pass true for enable, false for disable.
enableRxEnable flag for receive DMA request. Pass true for enable, false for disable.
widthDMA read/write unit in bytes.
static uint32_t I3C_MasterGetTxFifoAddress ( I3C_Type *  base,
uint32_t  width 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
widthDMA read/write unit in bytes.
Returns
The I3C Master Transmit Data Register address.
static uint32_t I3C_MasterGetRxFifoAddress ( I3C_Type *  base,
uint32_t  width 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
widthDMA read/write unit in bytes.
Returns
The I3C Master Receive Data Register address.
static void I3C_MasterSetWatermarks ( I3C_Type *  base,
i3c_tx_trigger_level_t  txLvl,
i3c_rx_trigger_level_t  rxLvl,
bool  flushTx,
bool  flushRx 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
txLvlTransmit FIFO watermark level. The kI3C_MasterTxReadyFlag flag is set whenever the number of words in the transmit FIFO reaches txLvl.
rxLvlReceive FIFO watermark level. The kI3C_MasterRxReadyFlag flag is set whenever the number of words in the receive FIFO reaches rxLvl.
flushTxtrue if TX FIFO is to be cleared, otherwise TX FIFO remains unchanged.
flushRxtrue if RX FIFO is to be cleared, otherwise RX FIFO remains unchanged.
static void I3C_MasterGetFifoCounts ( I3C_Type *  base,
size_t *  rxCount,
size_t *  txCount 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
[out]txCountPointer through which the current number of bytes in the transmit FIFO is returned. Pass NULL if this value is not required.
[out]rxCountPointer through which the current number of bytes in the receive FIFO is returned. Pass NULL if this value is not required.
void I3C_MasterSetBaudRate ( I3C_Type *  base,
const i3c_baudrate_hz_t *  baudRate_Hz,
uint32_t  sourceClock_Hz 
)

The I3C master is automatically disabled and re-enabled as necessary to configure the baud rate. Do not call this function during a transfer, or the transfer is aborted.

Parameters
baseThe I3C peripheral base address.
baudRate_HzPointer to structure of requested bus frequency in Hertz.
sourceClock_HzI3C functional clock frequency in Hertz.
static bool I3C_MasterGetBusIdleState ( I3C_Type *  base)
inlinestatic

Requires the master mode to be enabled.

Parameters
baseThe I3C peripheral base address.
Return values
trueBus is busy.
falseBus is idle.
status_t I3C_MasterStartWithRxSize ( I3C_Type *  base,
i3c_bus_type_t  type,
uint8_t  address,
i3c_direction_t  dir,
uint8_t  rxSize 
)

This function is used to initiate a new master mode transfer. First, the bus state is checked to ensure that another master is not occupying the bus. Then a START signal is transmitted, followed by the 7-bit address specified in the a address parameter. Note that this function does not actually wait until the START and address are successfully sent on the bus before returning.

Parameters
baseThe I3C peripheral base address.
typeThe bus type to use in this transaction.
address7-bit slave device address, in bits [6:0].
dirMaster transfer direction, either kI3C_Read or kI3C_Write. This parameter is used to set the R/w bit (bit 0) in the transmitted slave address.
rxSizeRead terminate size for the followed read transfer, limit to 255 bytes.
Return values
kStatus_SuccessSTART signal and address were successfully enqueued in the transmit FIFO.
kStatus_I3C_BusyAnother master is currently utilizing the bus.
status_t I3C_MasterStart ( I3C_Type *  base,
i3c_bus_type_t  type,
uint8_t  address,
i3c_direction_t  dir 
)

This function is used to initiate a new master mode transfer. First, the bus state is checked to ensure that another master is not occupying the bus. Then a START signal is transmitted, followed by the 7-bit address specified in the address parameter. Note that this function does not actually wait until the START and address are successfully sent on the bus before returning.

Parameters
baseThe I3C peripheral base address.
typeThe bus type to use in this transaction.
address7-bit slave device address, in bits [6:0].
dirMaster transfer direction, either kI3C_Read or kI3C_Write. This parameter is used to set the R/w bit (bit 0) in the transmitted slave address.
Return values
kStatus_SuccessSTART signal and address were successfully enqueued in the transmit FIFO.
kStatus_I3C_BusyAnother master is currently utilizing the bus.
status_t I3C_MasterRepeatedStartWithRxSize ( I3C_Type *  base,
i3c_bus_type_t  type,
uint8_t  address,
i3c_direction_t  dir,
uint8_t  rxSize 
)

This function is used to send a Repeated START signal when a transfer is already in progress. Like I3C_MasterStart(), it also sends the specified 7-bit address. Call this API also configures the read terminate size for the following read transfer. For example, set the rxSize = 2, the following read transfer will be terminated after two bytes of data received. Write transfer will not be affected by the rxSize configuration.

Note
This function exists primarily to maintain compatible APIs between I3C and I2C drivers, as well as to better document the intent of code that uses these APIs.
Parameters
baseThe I3C peripheral base address.
typeThe bus type to use in this transaction.
address7-bit slave device address, in bits [6:0].
dirMaster transfer direction, either kI3C_Read or kI3C_Write. This parameter is used to set the R/w bit (bit 0) in the transmitted slave address.
rxSizeRead terminate size for the followed read transfer, limit to 255 bytes.
Return values
kStatus_SuccessRepeated START signal and address were successfully enqueued in the transmit FIFO.
static status_t I3C_MasterRepeatedStart ( I3C_Type *  base,
i3c_bus_type_t  type,
uint8_t  address,
i3c_direction_t  dir 
)
inlinestatic

This function is used to send a Repeated START signal when a transfer is already in progress. Like I3C_MasterStart(), it also sends the specified 7-bit address.

Note
This function exists primarily to maintain compatible APIs between I3C and I2C drivers, as well as to better document the intent of code that uses these APIs.
Parameters
baseThe I3C peripheral base address.
typeThe bus type to use in this transaction.
address7-bit slave device address, in bits [6:0].
dirMaster transfer direction, either kI3C_Read or kI3C_Write. This parameter is used to set the R/w bit (bit 0) in the transmitted slave address.
Return values
kStatus_SuccessRepeated START signal and address were successfully enqueued in the transmit FIFO.
status_t I3C_MasterSend ( I3C_Type *  base,
const void *  txBuff,
size_t  txSize,
uint32_t  flags 
)

Sends up to txSize number of bytes to the previously addressed slave device. The slave may reply with a NAK to any byte in order to terminate the transfer early. If this happens, this function returns kStatus_I3C_Nak.

Parameters
baseThe I3C peripheral base address.
txBuffThe pointer to the data to be transferred.
txSizeThe length in bytes of the data to be transferred.
flagsBit mask of options for the transfer. See enumeration _i3c_master_transfer_flags for available options.
Return values
kStatus_SuccessData was sent successfully.
kStatus_I3C_BusyAnother master is currently utilizing the bus.
kStatus_I3C_TimeoutThe module has stalled too long in a frame.
kStatus_I3C_NakThe slave device sent a NAK in response to an address.
kStatus_I3C_WriteAbortThe slave device sent a NAK in response to a write.
kStatus_I3C_MsgErrorMessage SDR/DDR mismatch or read/write message in wrong state.
kStatus_I3C_WriteFifoErrorWrite to M/SWDATAB register when FIFO full.
kStatus_I3C_InvalidReqInvalid use of request.
status_t I3C_MasterReceive ( I3C_Type *  base,
void *  rxBuff,
size_t  rxSize,
uint32_t  flags 
)
Parameters
baseThe I3C peripheral base address.
rxBuffThe pointer to the data to be transferred.
rxSizeThe length in bytes of the data to be transferred.
flagsBit mask of options for the transfer. See enumeration _i3c_master_transfer_flags for available options.
Return values
kStatus_SuccessData was received successfully.
kStatus_I3C_BusyAnother master is currently utilizing the bus.
kStatus_I3C_TimeoutThe module has stalled too long in a frame.
kStatus_I3C_TermThe master terminates slave read.
kStatus_I3C_HdrParityErrorParity error from DDR read.
kStatus_I3C_CrcErrorCRC error from DDR read.
kStatus_I3C_MsgErrorMessage SDR/DDR mismatch or read/write message in wrong state.
kStatus_I3C_ReadFifoErrorRead from M/SRDATAB register when FIFO empty.
kStatus_I3C_InvalidReqInvalid use of request.
status_t I3C_MasterStop ( I3C_Type *  base)

This function does not return until the STOP signal is seen on the bus, or an error occurs.

Parameters
baseThe I3C peripheral base address.
Return values
kStatus_SuccessThe STOP signal was successfully sent on the bus and the transaction terminated.
kStatus_I3C_BusyAnother master is currently utilizing the bus.
kStatus_I3C_TimeoutThe module has stalled too long in a frame.
kStatus_I3C_InvalidReqInvalid use of request.
void I3C_MasterEmitRequest ( I3C_Type *  base,
i3c_bus_request_t  masterReq 
)
Parameters
baseThe I3C peripheral base address.
masterReqI3C master request of type i3c_bus_request_t
static void I3C_MasterEmitIBIResponse ( I3C_Type *  base,
i3c_ibi_response_t  ibiResponse 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
ibiResponseI3C master emit IBI response of type i3c_ibi_response_t
void I3C_MasterRegisterIBI ( I3C_Type *  base,
i3c_register_ibi_addr_t *  ibiRule 
)
Parameters
baseThe I3C peripheral base address.
ibiRulePointer to ibi rule description of type i3c_register_ibi_addr_t
void I3C_MasterGetIBIRules ( I3C_Type *  base,
i3c_register_ibi_addr_t *  ibiRule 
)
Parameters
baseThe I3C peripheral base address.
ibiRulePointer to store the read out ibi rule description.
i3c_ibi_type_t I3C_GetIBIType ( I3C_Type *  base)
Parameters
baseThe I3C peripheral base address.
Return values
i3c_ibi_type_tType of i3c_ibi_type_t.
static uint8_t I3C_GetIBIAddress ( I3C_Type *  base)
inlinestatic
Parameters
baseThe I3C peripheral base address.
Return values
The8-bit IBI address.
status_t I3C_MasterProcessDAASpecifiedBaudrate ( I3C_Type *  base,
uint8_t *  addressList,
uint32_t  count,
i3c_master_daa_baudrate_t *  daaBaudRate 
)
Parameters
baseThe I3C peripheral base address.
addressListThe pointer for address list which is used to do DAA.
countThe address count in the address list.
daaBaudRateThe temporary baud rate in DAA process, NULL for using initial setting. The initial setting is set back between the completion of the DAA and the return of this function.
Return values
kStatus_SuccessThe transaction was started successfully.
kStatus_I3C_BusyEither another master is currently utilizing the bus, or a non-blocking transaction is already in progress.
kStatus_I3C_SlaveCountExceedThe I3C slave count has exceed the definition in I3C_MAX_DEVCNT.
static status_t I3C_MasterProcessDAA ( I3C_Type *  base,
uint8_t *  addressList,
uint32_t  count 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
addressListThe pointer for address list which is used to do DAA.
countThe address count in the address list. The initial setting is set back between the completion of the DAA and the return of this function.
Return values
kStatus_SuccessThe transaction was started successfully.
kStatus_I3C_BusyEither another master is currently utilizing the bus, or a non-blocking transaction is already in progress.
kStatus_I3C_SlaveCountExceedThe I3C slave count has exceed the definition in I3C_MAX_DEVCNT.
i3c_device_info_t* I3C_MasterGetDeviceListAfterDAA ( I3C_Type *  base,
uint8_t *  count 
)
Parameters
baseThe I3C peripheral base address.
[out]countThe pointer to store the available device count.
Returns
Pointer to the i3c_device_info_t array.
status_t I3C_MasterTransferBlocking ( I3C_Type *  base,
i3c_master_transfer_t *  transfer 
)
Note
The API does not return until the transfer succeeds or fails due to error happens during transfer.
Parameters
baseThe I3C peripheral base address.
transferPointer to the transfer structure.
Return values
kStatus_SuccessData was received successfully.
kStatus_I3C_BusyAnother master is currently utilizing the bus.
kStatus_I3C_IBIWonThe I3C slave event IBI or MR or HJ won the arbitration on a header address.
kStatus_I3C_TimeoutThe module has stalled too long in a frame.
kStatus_I3C_NakThe slave device sent a NAK in response to an address.
kStatus_I3C_WriteAbortThe slave device sent a NAK in response to a write.
kStatus_I3C_TermThe master terminates slave read.
kStatus_I3C_HdrParityErrorParity error from DDR read.
kStatus_I3C_CrcErrorCRC error from DDR read.
kStatus_I3C_MsgErrorMessage SDR/DDR mismatch or read/write message in wrong state.
kStatus_I3C_ReadFifoErrorRead from M/SRDATAB register when FIFO empty.
kStatus_I3C_WriteFifoErrorWrite to M/SWDATAB register when FIFO full.
kStatus_I3C_InvalidReqInvalid use of request.
void I3C_MasterTransferCreateHandle ( I3C_Type *  base,
i3c_master_handle_t *  handle,
const i3c_master_transfer_callback_t *  callback,
void *  userData 
)

The creation of a handle is for use with the non-blocking APIs. Once a handle is created, there is not a corresponding destroy handle. If the user wants to terminate a transfer, the I3C_MasterTransferAbort() API shall be called.

Note
The function also enables the NVIC IRQ for the input I3C. Need to notice that on some SoCs the I3C IRQ is connected to INTMUX, in this case user needs to enable the associated INTMUX IRQ in application.
Parameters
baseThe I3C peripheral base address.
[out]handlePointer to the I3C master driver handle.
callbackUser provided pointer to the asynchronous callback function.
userDataUser provided pointer to the application callback data.
status_t I3C_MasterTransferNonBlocking ( I3C_Type *  base,
i3c_master_handle_t *  handle,
i3c_master_transfer_t *  transfer 
)
Parameters
baseThe I3C peripheral base address.
handlePointer to the I3C master driver handle.
transferThe pointer to the transfer descriptor.
Return values
kStatus_SuccessThe transaction was started successfully.
kStatus_I3C_BusyEither another master is currently utilizing the bus, or a non-blocking transaction is already in progress.
status_t I3C_MasterTransferGetCount ( I3C_Type *  base,
i3c_master_handle_t *  handle,
size_t *  count 
)
Parameters
baseThe I3C peripheral base address.
handlePointer to the I3C master driver handle.
[out]countNumber of bytes transferred so far by the non-blocking transaction.
Return values
kStatus_Success
kStatus_NoTransferInProgressThere is not a non-blocking transaction currently in progress.
void I3C_MasterTransferAbort ( I3C_Type *  base,
i3c_master_handle_t *  handle 
)
Note
It is not safe to call this function from an IRQ handler that has a higher priority than the I3C peripheral's IRQ priority.
Parameters
baseThe I3C peripheral base address.
handlePointer to the I3C master driver handle.
Return values
kStatus_SuccessA transaction was successfully aborted.
kStatus_I3C_IdleThere is not a non-blocking transaction currently in progress.
void I3C_MasterTransferHandleIRQ ( I3C_Type *  base,
void *  intHandle 
)
Note
This function does not need to be called unless you are reimplementing the nonblocking API's interrupt handler routines to add special functionality.
Parameters
baseThe I3C peripheral base address.
intHandlePointer to the I3C master driver handle.
void I3C_SlaveGetDefaultConfig ( i3c_slave_config_t *  slaveConfig)

This function provides the following default configuration for the I3C slave peripheral:

* slaveConfig->enableslave = true;
*

After calling this function, you can override any settings in order to customize the configuration, prior to initializing the slave driver with I3C_SlaveInit().

Parameters
[out]slaveConfigUser provided configuration structure for default values. Refer to i3c_slave_config_t.
void I3C_SlaveInit ( I3C_Type *  base,
const i3c_slave_config_t *  slaveConfig,
uint32_t  slowClock_Hz 
)

This function enables the peripheral clock and initializes the I3C slave peripheral as described by the user provided configuration.

Parameters
baseThe I3C peripheral base address.
slaveConfigUser provided peripheral configuration. Use I3C_SlaveGetDefaultConfig() to get a set of defaults that you can override.
slowClock_HzFrequency in Hertz of the I3C slow clock. Used to calculate the bus match condition values. If FSL_FEATURE_I3C_HAS_NO_SCONFIG_BAMATCH defines as 1, this parameter is useless.
void I3C_SlaveDeinit ( I3C_Type *  base)

This function disables the I3C slave peripheral and gates the clock.

Parameters
baseThe I3C peripheral base address.
static void I3C_SlaveEnable ( I3C_Type *  base,
bool  isEnable 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
isEnableEnable or disable.
static uint32_t I3C_SlaveGetStatusFlags ( I3C_Type *  base)
inlinestatic

A bit mask with the state of all I3C slave status flags is returned. For each flag, the corresponding bit in the return value is set if the flag is asserted.

Parameters
baseThe I3C peripheral base address.
Returns
State of the status flags:
  • 1: related status flag is set.
  • 0: related status flag is not set.
See Also
_i3c_slave_flags
static void I3C_SlaveClearStatusFlags ( I3C_Type *  base,
uint32_t  statusMask 
)
inlinestatic

The following status register flags can be cleared:

Attempts to clear other flags has no effect.

Parameters
baseThe I3C peripheral base address.
statusMaskA bitmask of status flags that are to be cleared. The mask is composed of _i3c_slave_flags enumerators OR'd together. You may pass the result of a previous call to I3C_SlaveGetStatusFlags().
See Also
_i3c_slave_flags.
static uint32_t I3C_SlaveGetErrorStatusFlags ( I3C_Type *  base)
inlinestatic

A bit mask with the state of all I3C slave error status flags is returned. For each flag, the corresponding bit in the return value is set if the flag is asserted.

Parameters
baseThe I3C peripheral base address.
Returns
State of the error status flags:
  • 1: related status flag is set.
  • 0: related status flag is not set.
See Also
_i3c_slave_error_flags
static void I3C_SlaveClearErrorStatusFlags ( I3C_Type *  base,
uint32_t  statusMask 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
statusMaskA bitmask of error status flags that are to be cleared. The mask is composed of _i3c_slave_error_flags enumerators OR'd together. You may pass the result of a previous call to I3C_SlaveGetErrorStatusFlags().
See Also
_i3c_slave_error_flags.
i3c_slave_activity_state_t I3C_SlaveGetActivityState ( I3C_Type *  base)
Parameters
baseThe I3C peripheral base address.
Returns
I3C slave activity state, refer i3c_slave_activity_state_t.
static void I3C_SlaveEnableInterrupts ( I3C_Type *  base,
uint32_t  interruptMask 
)
inlinestatic

Only below flags can be enabled as interrupts.

Parameters
baseThe I3C peripheral base address.
interruptMaskBit mask of interrupts to enable. See _i3c_slave_flags for the set of constants that should be OR'd together to form the bit mask.
static void I3C_SlaveDisableInterrupts ( I3C_Type *  base,
uint32_t  interruptMask 
)
inlinestatic

Only below flags can be disabled as interrupts.

Parameters
baseThe I3C peripheral base address.
interruptMaskBit mask of interrupts to disable. See _i3c_slave_flags for the set of constants that should be OR'd together to form the bit mask.
static uint32_t I3C_SlaveGetEnabledInterrupts ( I3C_Type *  base)
inlinestatic
Parameters
baseThe I3C peripheral base address.
Returns
A bitmask composed of _i3c_slave_flags enumerators OR'd together to indicate the set of enabled interrupts.
static uint32_t I3C_SlaveGetPendingInterrupts ( I3C_Type *  base)
inlinestatic
Parameters
baseThe I3C peripheral base address.
Returns
A bitmask composed of _i3c_slave_flags enumerators OR'd together to indicate the set of pending interrupts.
static void I3C_SlaveEnableDMA ( I3C_Type *  base,
bool  enableTx,
bool  enableRx,
uint32_t  width 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
enableTxEnable flag for transmit DMA request. Pass true for enable, false for disable.
enableRxEnable flag for receive DMA request. Pass true for enable, false for disable.
widthDMA read/write unit in bytes.
static uint32_t I3C_SlaveGetTxFifoAddress ( I3C_Type *  base,
uint32_t  width 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
widthDMA read/write unit in bytes.
Returns
The I3C Slave Transmit Data Register address.
static uint32_t I3C_SlaveGetRxFifoAddress ( I3C_Type *  base,
uint32_t  width 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
widthDMA read/write unit in bytes.
Returns
The I3C Slave Receive Data Register address.
static void I3C_SlaveSetWatermarks ( I3C_Type *  base,
i3c_tx_trigger_level_t  txLvl,
i3c_rx_trigger_level_t  rxLvl,
bool  flushTx,
bool  flushRx 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
txLvlTransmit FIFO watermark level. The kI3C_SlaveTxReadyFlag flag is set whenever the number of words in the transmit FIFO reaches txLvl.
rxLvlReceive FIFO watermark level. The kI3C_SlaveRxReadyFlag flag is set whenever the number of words in the receive FIFO reaches rxLvl.
flushTxtrue if TX FIFO is to be cleared, otherwise TX FIFO remains unchanged.
flushRxtrue if RX FIFO is to be cleared, otherwise RX FIFO remains unchanged.
static void I3C_SlaveGetFifoCounts ( I3C_Type *  base,
size_t *  rxCount,
size_t *  txCount 
)
inlinestatic
Parameters
baseThe I3C peripheral base address.
[out]txCountPointer through which the current number of bytes in the transmit FIFO is returned. Pass NULL if this value is not required.
[out]rxCountPointer through which the current number of bytes in the receive FIFO is returned. Pass NULL if this value is not required.
void I3C_SlaveRequestEvent ( I3C_Type *  base,
i3c_slave_event_t  event 
)
Parameters
baseThe I3C peripheral base address.
eventI3C slave event of type i3c_slave_event_t
status_t I3C_SlaveSend ( I3C_Type *  base,
const void *  txBuff,
size_t  txSize 
)
Parameters
baseThe I3C peripheral base address.
txBuffThe pointer to the data to be transferred.
txSizeThe length in bytes of the data to be transferred.
Returns
Error or success status returned by API.
status_t I3C_SlaveReceive ( I3C_Type *  base,
void *  rxBuff,
size_t  rxSize 
)
Parameters
baseThe I3C peripheral base address.
rxBuffThe pointer to the data to be transferred.
rxSizeThe length in bytes of the data to be transferred.
Returns
Error or success status returned by API.