MCUXpresso SDK API Reference Manual  Rev 2.16.100
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

Data Structures

struct  sai_dma_handle_t
 SAI DMA transfer handle, users should not touch the content of the handle. More...
 

Typedefs

typedef void(* sai_dma_callback_t )(I2S_Type *base, sai_dma_handle_t *handle, status_t status, void *userData)
 Define SAI DMA callback.
 

Driver version

#define FSL_SAI_DMA_DRIVER_VERSION   (MAKE_VERSION(2, 4, 0))
 Version 2.4.0.
 

DMA Transactional

void SAI_TransferTxCreateHandleDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_dma_callback_t callback, void *userData, dma_handle_t *dmaHandle)
 Initializes the SAI master DMA handle. More...
 
void SAI_TransferRxCreateHandleDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_dma_callback_t callback, void *userData, dma_handle_t *dmaHandle)
 Initializes the SAI slave DMA handle. More...
 
status_t SAI_TransferSendDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transfer_t *xfer)
 Performs a non-blocking SAI transfer using DMA. More...
 
status_t SAI_TransferReceiveDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transfer_t *xfer)
 Performs a non-blocking SAI transfer using DMA. More...
 
void SAI_TransferAbortSendDMA (I2S_Type *base, sai_dma_handle_t *handle)
 Aborts a SAI transfer using DMA. More...
 
void SAI_TransferAbortReceiveDMA (I2S_Type *base, sai_dma_handle_t *handle)
 Aborts a SAI transfer using DMA. More...
 
status_t SAI_TransferGetSendCountDMA (I2S_Type *base, sai_dma_handle_t *handle, size_t *count)
 Gets byte count sent by SAI. More...
 
status_t SAI_TransferGetReceiveCountDMA (I2S_Type *base, sai_dma_handle_t *handle, size_t *count)
 Gets byte count received by SAI. More...
 
void SAI_TransferTxSetConfigDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transceiver_t *saiConfig)
 Configures the SAI Tx. More...
 
void SAI_TransferRxSetConfigDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transceiver_t *saiConfig)
 Configures the SAI Rx. More...
 

Data Structure Documentation

struct _sai_dma_handle

Data Fields

dma_handle_t * dmaHandle
 DMA handler for SAI send.
 
uint8_t bytesPerFrame
 Bytes in a frame.
 
uint8_t channel
 Which Data channel SAI use.
 
uint32_t state
 SAI DMA transfer internal state.
 
sai_dma_callback_t callback
 Callback for users while transfer finish or error occurred.
 
void * userData
 User callback parameter.
 
sai_transfer_t saiQueue [SAI_XFER_QUEUE_SIZE]
 Transfer queue storing queued transfer. More...
 
size_t transferSize [SAI_XFER_QUEUE_SIZE]
 Data bytes need to transfer.
 
volatile uint8_t queueUser
 Index for user to queue transfer. More...
 
volatile uint8_t queueDriver
 Index for driver to get the transfer data and size.
 

Field Documentation

sai_transfer_t sai_dma_handle_t::saiQueue[SAI_XFER_QUEUE_SIZE]
volatile uint8_t sai_dma_handle_t::queueUser

Function Documentation

void SAI_TransferTxCreateHandleDMA ( I2S_Type *  base,
sai_dma_handle_t *  handle,
sai_dma_callback_t  callback,
void *  userData,
dma_handle_t *  dmaHandle 
)

This function initializes the SAI master DMA handle, which can be used for other SAI master transactional APIs. Usually, for a specified SAI instance, call this API once to get the initialized handle.

Parameters
baseSAI base pointer.
handleSAI DMA handle pointer.
baseSAI peripheral base address.
callbackPointer to user callback function.
userDataUser parameter passed to the callback function.
dmaHandleDMA handle pointer, this handle shall be static allocated by users.
void SAI_TransferRxCreateHandleDMA ( I2S_Type *  base,
sai_dma_handle_t *  handle,
sai_dma_callback_t  callback,
void *  userData,
dma_handle_t *  dmaHandle 
)

This function initializes the SAI slave DMA handle, which can be used for other SAI master transactional APIs. Usually, for a specified SAI instance, call this API once to get the initialized handle.

Parameters
baseSAI base pointer.
handleSAI DMA handle pointer.
baseSAI peripheral base address.
callbackPointer to user callback function.
userDataUser parameter passed to the callback function.
dmaHandleDMA handle pointer, this handle shall be static allocated by users.
status_t SAI_TransferSendDMA ( I2S_Type *  base,
sai_dma_handle_t *  handle,
sai_transfer_t *  xfer 
)
Note
This interface returns immediately after the transfer initiates. Call the SAI_GetTransferStatus to poll the transfer status to check whether the SAI transfer finished.
Parameters
baseSAI base pointer.
handleSAI DMA handle pointer.
xferPointer to DMA transfer structure.
Return values
kStatus_SuccessSuccessfully start the data receive.
kStatus_SAI_TxBusyPrevious receive still not finished.
kStatus_InvalidArgumentThe input parameter is invalid.
status_t SAI_TransferReceiveDMA ( I2S_Type *  base,
sai_dma_handle_t *  handle,
sai_transfer_t *  xfer 
)
Note
This interface returns immediately after transfer initiates. Call SAI_GetTransferStatus to poll the transfer status to check whether the SAI transfer is finished.
Parameters
baseSAI base pointer
handleSAI DMA handle pointer.
xferPointer to DMA transfer structure.
Return values
kStatus_SuccessSuccessfully start the data receive.
kStatus_SAI_RxBusyPrevious receive still not finished.
kStatus_InvalidArgumentThe input parameter is invalid.
void SAI_TransferAbortSendDMA ( I2S_Type *  base,
sai_dma_handle_t *  handle 
)
Parameters
baseSAI base pointer.
handleSAI DMA handle pointer.
void SAI_TransferAbortReceiveDMA ( I2S_Type *  base,
sai_dma_handle_t *  handle 
)
Parameters
baseSAI base pointer.
handleSAI DMA handle pointer.
status_t SAI_TransferGetSendCountDMA ( I2S_Type *  base,
sai_dma_handle_t *  handle,
size_t *  count 
)
Parameters
baseSAI base pointer.
handleSAI DMA handle pointer.
countBytes count sent by SAI.
Return values
kStatus_SuccessSucceed get the transfer count.
kStatus_NoTransferInProgressThere is not a non-blocking transaction currently in progress.
status_t SAI_TransferGetReceiveCountDMA ( I2S_Type *  base,
sai_dma_handle_t *  handle,
size_t *  count 
)
Parameters
baseSAI base pointer.
handleSAI DMA handle pointer.
countBytes count received by SAI.
Return values
kStatus_SuccessSucceed get the transfer count.
kStatus_NoTransferInProgressThere is not a non-blocking transaction currently in progress.
void SAI_TransferTxSetConfigDMA ( I2S_Type *  base,
sai_dma_handle_t *  handle,
sai_transceiver_t *  saiConfig 
)
Parameters
baseSAI base pointer.
handleSAI DMA handle pointer.
saiConfigsai configurations.
void SAI_TransferRxSetConfigDMA ( I2S_Type *  base,
sai_dma_handle_t *  handle,
sai_transceiver_t *  saiConfig 
)
Parameters
baseSAI base pointer.
handleSAI DMA handle pointer.
saiConfigsai configurations.