MCUXpresso SDK API Reference Manual  Rev 2.16.100
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
CAAM HASH driver

Overview

This section describes the programming interface of the CAAM HASH driver.

Macros

#define CAAM_SHA_BLOCK_SIZE   128U
 CAAM HASH Context size. More...
 
#define CAAM_HASH_BLOCK_SIZE   CAAM_SHA_BLOCK_SIZE
 CAAM hash block size.
 
#define CAAM_HASH_CTX_SIZE   83
 CAAM HASH Context size. More...
 

Typedefs

typedef enum _caam_hash_algo_t caam_hash_algo_t
 Supported cryptographic block cipher functions for HASH creation.
 
typedef uint32_t caam_hash_ctx_t [CAAM_HASH_CTX_SIZE]
 Storage type used to save hash context. More...
 

Enumerations

enum  _caam_hash_algo_t {
  kCAAM_XcbcMac = 0,
  kCAAM_Cmac,
  kCAAM_Sha1,
  kCAAM_Sha224,
  kCAAM_Sha256,
  kCAAM_Sha384,
  kCAAM_Sha512,
  kCAAM_HmacSha1,
  kCAAM_HmacSha224,
  kCAAM_HmacSha256,
  kCAAM_HmacSha384,
  kCAAM_HmacSha512
}
 Supported cryptographic block cipher functions for HASH creation. More...
 

Functions

status_t CAAM_HASH_Init (CAAM_Type *base, caam_handle_t *handle, caam_hash_ctx_t *ctx, caam_hash_algo_t algo, const uint8_t *key, size_t keySize)
 Initialize HASH context. More...
 
status_t CAAM_HASH_Update (caam_hash_ctx_t *ctx, const uint8_t *input, size_t inputSize)
 Add data to current HASH. More...
 
status_t CAAM_HASH_Finish (caam_hash_ctx_t *ctx, uint8_t *output, size_t *outputSize)
 Finalize hashing. More...
 
status_t CAAM_HASH (CAAM_Type *base, caam_handle_t *handle, caam_hash_algo_t algo, const uint8_t *input, size_t inputSize, const uint8_t *key, size_t keySize, uint8_t *output, size_t *outputSize)
 Create HASH on given data. More...
 

Macro Definition Documentation

#define CAAM_SHA_BLOCK_SIZE   128U

up to SHA-512 block size

#define CAAM_HASH_CTX_SIZE   83

Typedef Documentation

typedef uint32_t caam_hash_ctx_t[CAAM_HASH_CTX_SIZE]

Enumeration Type Documentation

Enumerator
kCAAM_XcbcMac 

XCBC-MAC (AES engine)

kCAAM_Cmac 

CMAC (AES engine)

kCAAM_Sha1 

SHA_1 (MDHA engine)

kCAAM_Sha224 

SHA_224 (MDHA engine)

kCAAM_Sha256 

SHA_256 (MDHA engine)

kCAAM_Sha384 

SHA_384 (MDHA engine)

kCAAM_Sha512 

SHA_512 (MDHA engine)

kCAAM_HmacSha1 

HMAC_SHA_1 (MDHA engine)

kCAAM_HmacSha224 

HMAC_SHA_224 (MDHA engine)

kCAAM_HmacSha256 

HMAC_SHA_256 (MDHA engine)

kCAAM_HmacSha384 

HMAC_SHA_384 (MDHA engine)

kCAAM_HmacSha512 

HMAC_SHA_512 (MDHA engine)

Function Documentation

status_t CAAM_HASH_Init ( CAAM_Type *  base,
caam_handle_t *  handle,
caam_hash_ctx_t *  ctx,
caam_hash_algo_t  algo,
const uint8_t *  key,
size_t  keySize 
)

This function initializes the HASH. Key shall be supplied if the underlaying algoritm is AES XCBC-MAC or CMAC. Key shall be NULL if the underlaying algoritm is SHA.

For XCBC-MAC, the key length must be 16. For CMAC, the key length can be the AES key lengths supported by AES engine. For MDHA the key length argument is ignored.

This functions is used to initialize the context for both blocking and non-blocking CAAM_HASH API. For blocking CAAM HASH API, the HASH context contains all information required for context switch, such as running hash or MAC. For non-blocking CAAM HASH API, the HASH context is used to hold SGT. Therefore, the HASH context cannot be shared between blocking and non-blocking HASH API. With one HASH context, either use only blocking HASH API or only non-blocking HASH API.

Parameters
baseCAAM peripheral base address
handleHandle used for this request.
[out]ctxOutput hash context
algoUnderlaying algorithm to use for hash computation.
keyInput key (NULL if underlaying algorithm is SHA)
keySizeSize of input key in bytes
Returns
Status of initialization
status_t CAAM_HASH_Update ( caam_hash_ctx_t *  ctx,
const uint8_t *  input,
size_t  inputSize 
)

Add data to current HASH. This can be called repeatedly with an arbitrary amount of data to be hashed. The functions blocks. If it returns kStatus_Success, the running hash or mac has been updated (CAAM has processed the input data), so the memory at input pointer can be released back to system. The context is updated with the running hash or mac and with all necessary information to support possible context switch.

Parameters
[in,out]ctxHASH context
inputInput data
inputSizeSize of input data in bytes
Returns
Status of the hash update operation
status_t CAAM_HASH_Finish ( caam_hash_ctx_t *  ctx,
uint8_t *  output,
size_t *  outputSize 
)

Outputs the final hash (computed by CAAM_HASH_Update()) and erases the context.

Parameters
[in,out]ctxInput hash context
[out]outputOutput hash data
[out]outputSizeOutput parameter storing the size of the output hash in bytes
Returns
Status of the hash finish operation
status_t CAAM_HASH ( CAAM_Type *  base,
caam_handle_t *  handle,
caam_hash_algo_t  algo,
const uint8_t *  input,
size_t  inputSize,
const uint8_t *  key,
size_t  keySize,
uint8_t *  output,
size_t *  outputSize 
)

Perform the full keyed XCBC-MAC/CMAC or SHA in one function call.

Key shall be supplied if the underlaying algoritm is AES XCBC-MAC or CMAC. Key shall be NULL if the underlaying algoritm is SHA.

For XCBC-MAC, the key length must be 16. For CMAC, the key length can be the AES key lengths supported by AES engine. For MDHA the key length argument is ignored.

The function is blocking.

Parameters
baseCAAM peripheral base address
handleHandle used for this request.
algoUnderlaying algorithm to use for hash computation.
inputInput data
inputSizeSize of input data in bytes
keyInput key (NULL if underlaying algorithm is SHA)
keySizeSize of input key in bytes
[out]outputOutput hash data
[out]outputSizeOutput parameter storing the size of the output hash in bytes
Returns
Status of the one call hash operation.