MCUXpresso SDK API Reference Manual  Rev 2.16.001
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

The sdmmc osa adapter provide interface of os adapter.

Data Structures

struct  _sdmmc_osa_event
 sdmmc osa event More...
 
struct  _sdmmc_osa_mutex
 sdmmc osa mutex More...
 

Macros

#define SDMMC_OSA_EVENT_TRANSFER_CMD_SUCCESS   (1UL << 0U)
 transfer event
 
#define SDMMC_OSA_EVENT_CARD_INSERTED   (1UL << 8U)
 card detect event, start from index 8
 
#define SDMMC_OSA_POLLING_EVENT_BY_SEMPHORE   1
 enable semphore by default
 

Typedefs

typedef struct _sdmmc_osa_event sdmmc_osa_event_t
 sdmmc osa event
 
typedef struct _sdmmc_osa_mutex sdmmc_osa_mutex_t
 sdmmc osa mutex
 

sdmmc osa Function

void SDMMC_OSAInit (void)
 Initialize OSA.
 
status_t SDMMC_OSAEventCreate (void *eventHandle)
 OSA Create event. More...
 
status_t SDMMC_OSAEventWait (void *eventHandle, uint32_t eventType, uint32_t timeoutMilliseconds, uint32_t *event)
 Wait event. More...
 
status_t SDMMC_OSAEventSet (void *eventHandle, uint32_t eventType)
 set event. More...
 
status_t SDMMC_OSAEventGet (void *eventHandle, uint32_t eventType, uint32_t *flag)
 Get event flag. More...
 
status_t SDMMC_OSAEventClear (void *eventHandle, uint32_t eventType)
 clear event flag. More...
 
status_t SDMMC_OSAEventDestroy (void *eventHandle)
 Delete event. More...
 
status_t SDMMC_OSAMutexCreate (void *mutexHandle)
 Create a mutex. More...
 
status_t SDMMC_OSAMutexLock (void *mutexHandle, uint32_t millisec)
 set event. More...
 
status_t SDMMC_OSAMutexUnlock (void *mutexHandle)
 Get event flag. More...
 
status_t SDMMC_OSAMutexDestroy (void *mutexHandle)
 Delete mutex. More...
 
void SDMMC_OSADelay (uint32_t milliseconds)
 sdmmc delay. More...
 
uint32_t SDMMC_OSADelayUs (uint32_t microseconds)
 sdmmc delay us. More...
 

Data Structure Documentation

struct _sdmmc_osa_event
struct _sdmmc_osa_mutex

Function Documentation

status_t SDMMC_OSAEventCreate ( void *  eventHandle)
Parameters
eventHandleevent handle.
Return values
kStatus_Failor kStatus_Success.
status_t SDMMC_OSAEventWait ( void *  eventHandle,
uint32_t  eventType,
uint32_t  timeoutMilliseconds,
uint32_t *  event 
)
Parameters
eventHandleThe event type
eventTypeTimeout time in milliseconds.
timeoutMillisecondstimeout value in ms.
eventevent flags.
Return values
kStatus_Failor kStatus_Success.
status_t SDMMC_OSAEventSet ( void *  eventHandle,
uint32_t  eventType 
)
Parameters
eventHandleevent handle.
eventTypeThe event type
Return values
kStatus_Failor kStatus_Success.
status_t SDMMC_OSAEventGet ( void *  eventHandle,
uint32_t  eventType,
uint32_t *  flag 
)
Parameters
eventHandleevent handle.
eventTypeevent type.
flagpointer to store event value.
Return values
kStatus_Failor kStatus_Success.
status_t SDMMC_OSAEventClear ( void *  eventHandle,
uint32_t  eventType 
)
Parameters
eventHandleevent handle.
eventTypeThe event type
Return values
kStatus_Failor kStatus_Success.
status_t SDMMC_OSAEventDestroy ( void *  eventHandle)
Parameters
eventHandleThe event handle.
status_t SDMMC_OSAMutexCreate ( void *  mutexHandle)
Parameters
mutexHandlemutex handle.
Return values
kStatus_Failor kStatus_Success.
status_t SDMMC_OSAMutexLock ( void *  mutexHandle,
uint32_t  millisec 
)
Parameters
mutexHandlemutex handle.
millisecThe maximum number of milliseconds to wait for the mutex. If the mutex is locked, Pass the value osaWaitForever_c will wait indefinitely, pass 0 will return KOSA_StatusTimeout immediately.
Return values
kStatus_Failor kStatus_Success.
status_t SDMMC_OSAMutexUnlock ( void *  mutexHandle)
Parameters
mutexHandlemutex handle.
Return values
kStatus_Failor kStatus_Success.
status_t SDMMC_OSAMutexDestroy ( void *  mutexHandle)
Parameters
mutexHandleThe mutex handle.
void SDMMC_OSADelay ( uint32_t  milliseconds)
Parameters
millisecondstime to delay
uint32_t SDMMC_OSADelayUs ( uint32_t  microseconds)
Parameters
microsecondstime to delay
Returns
actual delayed microseconds