MCUXpresso SDK API Reference Manual  Rev 2.14.030
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

Data Structures

struct  flexcan_edma_handle_t
 FlexCAN eDMA handle. More...
 

Typedefs

typedef void(* flexcan_edma_transfer_callback_t )(CAN_Type *base, flexcan_edma_handle_t *handle, status_t status, void *userData)
 FlexCAN transfer callback function. More...
 

Driver version

#define FSL_FLEXCAN_EDMA_DRIVER_VERSION   (MAKE_VERSION(2, 11, 0))
 FlexCAN EDMA driver version. More...
 

eDMA transactional

void FLEXCAN_TransferCreateHandleEDMA (CAN_Type *base, flexcan_edma_handle_t *handle, flexcan_edma_transfer_callback_t callback, void *userData, edma_handle_t *rxFifoEdmaHandle)
 Initializes the FlexCAN handle, which is used in transactional functions. More...
 
void FLEXCAN_PrepareTransfConfiguration (CAN_Type *base, flexcan_fifo_transfer_t *pFifoXfer, edma_transfer_config_t *pEdmaConfig)
 Prepares the eDMA transfer configuration for FLEXCAN Legacy RX FIFO. More...
 
status_t FLEXCAN_StartTransferDatafromRxFIFO (CAN_Type *base, flexcan_edma_handle_t *handle, edma_transfer_config_t *pEdmaConfig)
 Start Transfer Data from the FLEXCAN Legacy Rx FIFO using eDMA. More...
 
status_t FLEXCAN_TransferReceiveFifoEDMA (CAN_Type *base, flexcan_edma_handle_t *handle, flexcan_fifo_transfer_t *pFifoXfer)
 Receives the CAN Message from the Legacy Rx FIFO using eDMA. More...
 
status_t FLEXCAN_TransferGetReceiveFifoCountEMDA (CAN_Type *base, flexcan_edma_handle_t *handle, size_t *count)
 Gets the Legacy Rx Fifo transfer status during a interrupt non-blocking receive. More...
 
void FLEXCAN_TransferAbortReceiveFifoEDMA (CAN_Type *base, flexcan_edma_handle_t *handle)
 Aborts the receive Legacy/Enhanced Rx FIFO process which used eDMA. More...
 

Data Structure Documentation

struct _flexcan_edma_handle

Data Fields

flexcan_edma_transfer_callback_t callback
 Callback function. More...
 
void * userData
 FlexCAN callback function parameter. More...
 
edma_handle_t * rxFifoEdmaHandle
 The EDMA handler for Rx FIFO. More...
 
volatile uint8_t rxFifoState
 Rx FIFO transfer state. More...
 
size_t frameNum
 The number of messages that need to be received. More...
 

Field Documentation

flexcan_edma_transfer_callback_t flexcan_edma_handle_t::callback
void* flexcan_edma_handle_t::userData
edma_handle_t* flexcan_edma_handle_t::rxFifoEdmaHandle
volatile uint8_t flexcan_edma_handle_t::rxFifoState
size_t flexcan_edma_handle_t::frameNum

Macro Definition Documentation

#define FSL_FLEXCAN_EDMA_DRIVER_VERSION   (MAKE_VERSION(2, 11, 0))

Typedef Documentation

typedef void(* flexcan_edma_transfer_callback_t)(CAN_Type *base, flexcan_edma_handle_t *handle, status_t status, void *userData)

Function Documentation

void FLEXCAN_TransferCreateHandleEDMA ( CAN_Type *  base,
flexcan_edma_handle_t *  handle,
flexcan_edma_transfer_callback_t  callback,
void *  userData,
edma_handle_t *  rxFifoEdmaHandle 
)
Parameters
baseFlexCAN peripheral base address.
handlePointer to flexcan_edma_handle_t structure.
callbackThe callback function.
userDataThe parameter of the callback function.
rxFifoEdmaHandleUser-requested DMA handle for Rx FIFO DMA transfer.
void FLEXCAN_PrepareTransfConfiguration ( CAN_Type *  base,
flexcan_fifo_transfer_t *  pFifoXfer,
edma_transfer_config_t *  pEdmaConfig 
)

This function prepares the eDMA transfer configuration structure according to FLEXCAN Legacy RX FIFO.

Parameters
baseFlexCAN peripheral base address.
pFifoXferFlexCAN Rx FIFO EDMA transfer structure, see flexcan_fifo_transfer_t.
pEdmaConfigThe user configuration structure of type edma_transfer_t.
status_t FLEXCAN_StartTransferDatafromRxFIFO ( CAN_Type *  base,
flexcan_edma_handle_t *  handle,
edma_transfer_config_t *  pEdmaConfig 
)

This function to Update edma transfer confiugration and Start eDMA transfer

Parameters
baseFlexCAN peripheral base address.
handlePointer to flexcan_edma_handle_t structure.
pEdmaConfigThe user configuration structure of type edma_transfer_t.
Return values
kStatus_Successif succeed, others failed.
kStatus_FLEXCAN_RxFifoBusyPrevious transfer ongoing.
status_t FLEXCAN_TransferReceiveFifoEDMA ( CAN_Type *  base,
flexcan_edma_handle_t *  handle,
flexcan_fifo_transfer_t *  pFifoXfer 
)

This function receives the CAN Message using eDMA. This is a non-blocking function, which returns right away. After the CAN Message is received, the receive callback function is called.

Parameters
baseFlexCAN peripheral base address.
handlePointer to flexcan_edma_handle_t structure.
pFifoXferFlexCAN Rx FIFO EDMA transfer structure, see flexcan_fifo_transfer_t.
Return values
kStatus_Successif succeed, others failed.
kStatus_FLEXCAN_RxFifoBusyPrevious transfer ongoing.
status_t FLEXCAN_TransferGetReceiveFifoCountEMDA ( CAN_Type *  base,
flexcan_edma_handle_t *  handle,
size_t *  count 
)
Parameters
baseFlexCAN peripheral base address.
handleFlexCAN handle pointer.
countNumber of CAN messages receive so far by the non-blocking transaction.
Return values
kStatus_InvalidArgumentcount is Invalid.
kStatus_SuccessSuccessfully return the count.
void FLEXCAN_TransferAbortReceiveFifoEDMA ( CAN_Type *  base,
flexcan_edma_handle_t *  handle 
)

This function aborts the receive Legacy/Enhanced Rx FIFO process which used eDMA.

Parameters
baseFlexCAN peripheral base address.
handlePointer to flexcan_edma_handle_t structure.