MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
ACOMP: Analog Comparator

Overview

The MCUXpresso SDK provides a driver for the Analog Converter (ACOMP) module of MCUXpreeso SDK devices.

The ACOMP driver can be divided into 4 function groups.

ACOMP Control Interfaces

The functions in this group can be used to control the ACOMP module. User can invoke ACOMP_GetDefaultConfig() function to configure the default setting, then invoking ACOMP_Init() to initialize the module. All ACOMP feature(except software reset comparators and clock divider) can be enabled by invoking ACOMP_Init() function.

ACOMP Result Interface

There is only one function in this function groups, it is ACOMP_GetResult(). User can get the result of comparator by invoking this function.

ACOMP Interrupt Control Interfaces

The functions in this group can be used to enable/disable interrupts.

ACOMP Status Flag Interfaces

The ACOMP_GetStatusFlags() function in this group can return all status flags. The ACOMP_ClearStatusFlags() can be used to clear status flags, but please note that no all status flags can be cleared by software.

Data Structures

struct  acomp_positive_input_config_t
 The configuration of positive input, including channel selection and hysteresis level. More...
 
struct  acomp_negative_input_config_t
 The configuration of negative input, including channel selection and hysteresis level. More...
 
struct  acomp_config_t
 The configure structure of acomp, including warm up time, response mode and so on. More...
 

Macros

#define FSL_ACOMP_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 ACOMP driver version. More...
 
#define ACOMP_REG_ADDR(startAddr, id)   ((uint32_t *)((volatile uint32_t *)(startAddr) + (uint32_t)(id)))
 The macro to get the address based on start address and acomp id.
 
#define ACOMP_GET_REG_VAL(startAddr, id)   (*ACOMP_REG_ADDR((startAddr), (id)))
 The macro to get register value based on start address and acomp id.
 
#define ACOMP_SET_REG_BIT(startAddr, id, val)   (ACOMP_GET_REG_VAL((startAddr), (id)) |= (val))
 Sets register's bit field.
 
#define ACOMP_CLEAR_REG_BIT(startAddr, id, val)   (ACOMP_GET_REG_VAL((startAddr), (id)) &= ~(val))
 Clears register's bit field.
 

Enumerations

enum  _acomp_interrupt_enable {
  kACOMP_Out0InterruptEnable = ACOMP_IMR0_OUT_INT_MASK_MASK,
  kACOMP_OutA0InterruptEnable = ACOMP_IMR0_OUTA_INT_MASK_MASK,
  kACOMP_Out1InterruptEnable = ACOMP_IMR1_OUT_INT_MASK_MASK << 2U,
  kACOMP_OutA1InterruptEnable = ACOMP_IMR1_OUTA_INT_MASK_MASK << 2U
}
 The enumeration of interrupts, including ACOMP0 synchrnized output interrupt, ACOMP0 asynchrnized output interrupt, ACOMP1 synchrnized output interrupt, and ACOMP1 asynchrnized output interrupt. More...
 
enum  _acomp_status_flags {
  kACOMP_Acomp0ActiveFlag = 1UL << 0UL,
  kACOMP_Acomp0OutInterruptFlag = 1UL << 1UL,
  kACOMP_Acomp0OutAInterruptFlag = 1UL << 2UL,
  kACOMP_Acomp0RawOutInterruptFlag = 1UL << 3UL,
  kACOMP_Acomp0RawOutAInterruptFlag = 1UL << 4UL,
  kACOMP_Acomp1ActiveFlag = 1UL << 5UL,
  kACOMP_Acomp1OutInterruptFlag = 1UL << 6UL,
  kACOMP_Acomp1OutAInterruptFlag = 1UL << 7UL,
  kACOMP_Acomp1RawOutInterruptFlag = 1UL << 8UL,
  kACOMP_Acomp1RawOutAInterruptFlag = 1UL << 9U
}
 The enumeration of status flags, including ACOMP0 active staus flag, ACOMP1 active status flag, and so on. More...
 
enum  acomp_result_logic_status_t {
  kACOMP_ResultLogicLow = 0U,
  kACOMP_ResultLogicHigh = 1U
}
 ACOMP result logical status Type definition. More...
 
enum  acomp_comparator_id_t {
  kACOMP_Acomp0,
  kACOMP_Acomp1
}
 ACOMP comparator id. More...
 
enum  acomp_warm_up_time_t {
  kACOMP_WarmUpTime1us = 0U,
  kACOMP_WarmUpTime2us,
  kACOMP_WarmUpTime4us,
  kACOMP_WarmUpTime8us
}
 The enumeration of wave up time. More...
 
enum  acomp_response_mode_t {
  kACOMP_SlowResponseMode = 0U,
  kACOMP_MediumResponseMode,
  kACOMP_FastResponseMode
}
 The enumeration of response mode. More...
 
enum  acomp_interrupt_trigger_type_t {
  kACOMP_LowLevelTrig = 0U,
  kACOMP_HighLevelTrig = 1U,
  kACOMP_FallingEdgeTrig = 2U,
  kACOMP_RisingEdgeTrig = 3U
}
 ACOMP interrupt trigger type definition. More...
 
enum  acomp_edge_pulse_trig_source_t {
  kACOMP_EdgePulseDis = 0U,
  kACOMP_EdgePulseRising,
  kACOMP_EdgePulseFalling,
  kACOMP_EdgePulseBothEdge
}
 ACOMP edge pule trigger source type definition. More...
 
enum  acomp_pin_out_type_t {
  kACOMP_PinOutSyn = 0U,
  kACOMP_PinOutAsyn = 1U,
  kACOMP_PinOutSynInverted = 2U,
  kACOMP_PinOutAsynInverted = 3U,
  kACOMP_PinOutDisable = 4U
}
 ACOMP synchronous/asynchronous output type to pin. More...
 
enum  acomp_positive_channel_t {
  kACOMP_PosChGPIO42,
  kACOMP_PosChGPIO43,
  kACOMP_PosChGPIO44,
  kACOMP_PosChGPIO45,
  kACOMP_PosChGPIO46,
  kACOMP_PosChGPIO47,
  kACOMP_PosChGPIO48,
  kACOMP_PosChGPIO49,
  kACOMP_PosChDACA,
  kACOMP_PosChDACB
}
 ACOMP positive channel enumeration. More...
 
enum  acomp_negative_channel_t {
  kACOMP_NegChGPIO42,
  kACOMP_NegChGPIO43,
  kACOMP_NegChGPIO44,
  kACOMP_NegChGPIO45,
  kACOMP_NegChGPIO46,
  kACOMP_NegChGPIO47,
  kACOMP_NegChGPIO48,
  kACOMP_NegChGPIO49,
  kACOMP_NegChDACA,
  kACOMP_NegChDACB,
  kACOMP_NegChVREF1P2,
  kACOMP_NegChAVSS,
  kACOMP_NegChVIO_0P25,
  kACOMP_NegChVIO_0P50,
  kACOMP_NegChVIO_0P75,
  kACOMP_NegChVIO_1P00
}
 ACOMP negative channel enumeration. More...
 
enum  acomp_input_hysteresis_t {
  kACOMP_Hyster0MV,
  kACOMP_Hyster10MV,
  kACOMP_Hyster20MV,
  kACOMP_Hyster30MV,
  kACOMP_Hyster40MV,
  kACOMP_Hyster50MV,
  kACOMP_Hyster60MV,
  kACOMP_Hyster70MV
}
 ACOMP hysteresis level enumeration. More...
 

ACOMP Control Interfaces

void ACOMP_Init (ACOMP_Type *base, const acomp_config_t *config)
 Initializes the module, including warm up time, response mode, inactive value and so on. More...
 
void ACOMP_GetDefaultConfig (acomp_config_t *config)
 Gets the default configuration of ACOMP module. More...
 
void ACOMP_Deinit (ACOMP_Type *base)
 De-initializes the module. More...
 
void ACOMP_SetInputConfig (ACOMP_Type *base, acomp_comparator_id_t id, const acomp_positive_input_config_t *posInput, const acomp_negative_input_config_t *negInput)
 Configures selected comparator's inputs, inclduing input channel and hysteresis level. More...
 
static void ACOMP_DoSoftwareReset (ACOMP_Type *base, acomp_comparator_id_t id)
 Does software reset to the selected ACOMP module. More...
 
static void ACOMP_Enable (ACOMP_Type *base, acomp_comparator_id_t id, bool enable)
 Enables/Disables ACOMP module. More...
 
static void ACOMP_ResetClockDivider (ACOMP_Type *base)
 Resets clock divider. More...
 

ACOMP Result Interface

static acomp_result_logic_status_t ACOMP_GetResult (ACOMP_Type *base, acomp_comparator_id_t id)
 Gets the selected acomp conversion result. More...
 
static void ACOMP_EnableInterrupts (ACOMP_Type *base, uint32_t interruptMask)
 ACOMP Interrupt Control Interfaces. More...
 
static void ACOMP_DisableInterrupt (ACOMP_Type *base, uint32_t interruptMask)
 Disables interrupts, including acomp0 asynchronized interrupt, acomp0 synchronized interrupt, acomp1 asynchronized interrupt, and acomp1 synchronized interrupt. More...
 
uint32_t ACOMP_GetStatusFlags (ACOMP_Type *base)
 ACOMP Status Flag Interfaces. More...
 
static void ACOMP_ClearStatusFlags (ACOMP_Type *base, uint32_t statusFlagMask)
 Clears status flags that can be cleared by software. More...
 

Data Structure Documentation

struct acomp_positive_input_config_t

Data Fields

acomp_positive_channel_t channel: 4U
 Positive input channel selection, please refer to acomp_positive_channel_t. More...
 
acomp_input_hysteresis_t hysterLevel: 4U
 Positive hysteresis voltage level selection, please refer to acomp_input_hysteresis_t. More...
 

Field Documentation

acomp_positive_channel_t acomp_positive_input_config_t::channel
acomp_input_hysteresis_t acomp_positive_input_config_t::hysterLevel
struct acomp_negative_input_config_t

Data Fields

acomp_negative_channel_t channel: 4U
 Negative input channel selection, please refer to acomp_negative_channel_t. More...
 
acomp_input_hysteresis_t hysterLevel: 4U
 Negative hystersis voltage level selection, please refer to acomp_input_hysteresis_t. More...
 

Field Documentation

acomp_negative_channel_t acomp_negative_input_config_t::channel
acomp_input_hysteresis_t acomp_negative_input_config_t::hysterLevel
struct acomp_config_t

Data Fields

acomp_comparator_id_t id: 1U
 The id of comparator, please refer to acomp_comparator_id_t. More...
 
bool enable: 1U
 Enable/Disable the selected ACOMP. More...
 
acomp_warm_up_time_t warmupTime: 2U
 Configure warm-up time, please refer to acomp_warm_up_time_t. More...
 
acomp_response_mode_t responseMode: 2U
 Configure responde mode(power mode), please refer to acomp_response_mode_t for details. More...
 
acomp_interrupt_trigger_type_t intTrigType: 2U
 Select interrupt trigger type, please refer to acomp_interrupt_trigger_type_t. More...
 
acomp_result_logic_status_t inactiveValue: 1U
 Configure output value for inactive state. More...
 
acomp_edge_pulse_trig_source_t edgeDetectTrigSrc: 2U
 Config edge detect trigger source, please refer to acomp_edge_pulse_trig_source_t. More...
 
acomp_pin_out_type_t outPinMode: 3U
 Config the output pin mode, please refer to acomp_pin_out_type_t for details. More...
 
const
acomp_positive_input_config_t * 
posInput
 
  The pointer to the configuration structure of positive input,

please refer to acomp_positive_input_config_t. More...

 
const
acomp_negative_input_config_t * 
negInput
 
  The pointer to the configuration structure of negative input,

please refer to acomp_positive_input_config_t. More...

 

Field Documentation

acomp_comparator_id_t acomp_config_t::id
bool acomp_config_t::enable
  • true Enable the selected ACOMP.
  • false Disable the selected ACOMP.
acomp_warm_up_time_t acomp_config_t::warmupTime
acomp_response_mode_t acomp_config_t::responseMode
acomp_interrupt_trigger_type_t acomp_config_t::intTrigType
acomp_result_logic_status_t acomp_config_t::inactiveValue
acomp_edge_pulse_trig_source_t acomp_config_t::edgeDetectTrigSrc
acomp_pin_out_type_t acomp_config_t::outPinMode
const acomp_positive_input_config_t* acomp_config_t::posInput
const acomp_negative_input_config_t* acomp_config_t::negInput

Macro Definition Documentation

#define FSL_ACOMP_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))

Version 2.0.0.

Enumeration Type Documentation

Enumerator
kACOMP_Out0InterruptEnable 

ACOMP0 synchrnized output interrupt enable.

kACOMP_OutA0InterruptEnable 

ACOMP0 asynchrnized output interrupt enable.

kACOMP_Out1InterruptEnable 

ACOMP1 synchrnized output interrupt enable.

kACOMP_OutA1InterruptEnable 

ACOMP1 asynchrnized output interrupt enable.

Enumerator
kACOMP_Acomp0ActiveFlag 

ACOMP0 active status flag, if this flag is set it means the ACOMP0 is active.

kACOMP_Acomp0OutInterruptFlag 

ACOMP0 Synchronized output interrupt flags, this flag is set when ACOMP0 synchronized output changes from 0 to 1 and the corresponding interrupt is enabled.

kACOMP_Acomp0OutAInterruptFlag 

ACOMP0 Asynchronized output interrupt flags, this flag is set when ACOMP0 asynchronized output changes from 0 to 1 and the corresponding interrupt is enabled.

kACOMP_Acomp0RawOutInterruptFlag 

ACOMP0 raw synchroized output interrrupt flags.

kACOMP_Acomp0RawOutAInterruptFlag 

ACOMP0 raw asynchroized output interrupt flags.

kACOMP_Acomp1ActiveFlag 

ACOMP1 active status flag, if this flag is set it means the ACOMP0 is active.

kACOMP_Acomp1OutInterruptFlag 

ACOMP1 Synchronized output interrupt flags, this flag is set when ACOMP1 synchronized output changes from 0 to 1 and the corresponding interrupt is enabled.

kACOMP_Acomp1OutAInterruptFlag 

ACOMP1 Asynchronized output interrupt flags, this flag is set when ACOMP1 asynchronized output changes from 0 to 1 and the corresponding interrupt is enabled.

kACOMP_Acomp1RawOutInterruptFlag 

ACOMP1 raw synchroized output interrrupt flags.

kACOMP_Acomp1RawOutAInterruptFlag 

ACOMP1 raw asynchroized output interrupt flags.

Enumerator
kACOMP_ResultLogicLow 

The comparsion result is high logic.

kACOMP_ResultLogicHigh 

The comparsion result is low logic.

Enumerator
kACOMP_Acomp0 

Index for ACOMP0.

kACOMP_Acomp1 

Index for ACOMP1.

Enumerator
kACOMP_WarmUpTime1us 

Set wave-up time as 1us.

kACOMP_WarmUpTime2us 

Set wave-up time as 2us.

kACOMP_WarmUpTime4us 

Set wave-up time as 4us.

kACOMP_WarmUpTime8us 

Set wave-up time as 8us.

The response mode will affect the delay from input to output.

Enumerator
kACOMP_SlowResponseMode 

Slow response mode also called power mode 1.

kACOMP_MediumResponseMode 

Medium response mode also called power mode 2.

kACOMP_FastResponseMode 

Fast response mode also called power mode 3.

Enumerator
kACOMP_LowLevelTrig 

Low level trigger interrupt.

kACOMP_HighLevelTrig 

High level trigger interrupt.

kACOMP_FallingEdgeTrig 

Falling edge trigger interrupt.

kACOMP_RisingEdgeTrig 

Rising edge trigger interrupt.

Enumerator
kACOMP_EdgePulseDis 

edge pulse function is disable

kACOMP_EdgePulseRising 

Rising edge can trigger edge pulse.

kACOMP_EdgePulseFalling 

Falling edge can trigger edge pulse.

kACOMP_EdgePulseBothEdge 

Both edge can trigger edge pulse.

Enumerator
kACOMP_PinOutSyn 

Enable ACOMP synchronous pin output.

kACOMP_PinOutAsyn 

Enable ACOMP asynchronous pin output.

kACOMP_PinOutSynInverted 

Enable ACOMP inverted synchronous pin output.

kACOMP_PinOutAsynInverted 

Enable ACOMP inverted asynchronous pin output.

kACOMP_PinOutDisable 

Diable ACOMP pin output.

Enumerator
kACOMP_PosChGPIO42 

Gpio42 selection.

kACOMP_PosChGPIO43 

Gpio43 selection.

kACOMP_PosChGPIO44 

Gpio44 selection.

kACOMP_PosChGPIO45 

Gpio45 selection.

kACOMP_PosChGPIO46 

Gpio46 selection.

kACOMP_PosChGPIO47 

Gpio47 selection.

kACOMP_PosChGPIO48 

Gpio48 selection.

kACOMP_PosChGPIO49 

Gpio49 selection.

kACOMP_PosChDACA 

DACA selection.

kACOMP_PosChDACB 

DACB selection.

Enumerator
kACOMP_NegChGPIO42 

Gpio42 selection.

kACOMP_NegChGPIO43 

Gpio43 selection.

kACOMP_NegChGPIO44 

Gpio44 selection.

kACOMP_NegChGPIO45 

Gpio45 selection.

kACOMP_NegChGPIO46 

Gpio46 selection.

kACOMP_NegChGPIO47 

Gpio47 selection.

kACOMP_NegChGPIO48 

Gpio48 selection.

kACOMP_NegChGPIO49 

Gpio49 selection.

kACOMP_NegChDACA 

DACA selection.

kACOMP_NegChDACB 

DACB selection.

kACOMP_NegChVREF1P2 

Vref1p2 selection.

kACOMP_NegChAVSS 

AVSS selection.

kACOMP_NegChVIO_0P25 

VIO Scaling factor 0.25.

kACOMP_NegChVIO_0P50 

VIO Scaling factor 0.50.

kACOMP_NegChVIO_0P75 

VIO Scaling factor 0.75.

kACOMP_NegChVIO_1P00 

VIO Scaling factor 1.00.

Enumerator
kACOMP_Hyster0MV 

Hysteresis level = 0mv.

kACOMP_Hyster10MV 

Hysteresis level = 10mv.

kACOMP_Hyster20MV 

Hysteresis level = 20mv.

kACOMP_Hyster30MV 

Hysteresis level = 30mv.

kACOMP_Hyster40MV 

Hysteresis level = 40mv.

kACOMP_Hyster50MV 

Hysteresis level = 50mv.

kACOMP_Hyster60MV 

Hysteresis level = 60mv.

kACOMP_Hyster70MV 

Hysteresis level = 70mv.

Function Documentation

void ACOMP_Init ( ACOMP_Type *  base,
const acomp_config_t *  config 
)
Parameters
baseACOMP peripheral base address.
configThe pointer to the structure acomp_config_t.
void ACOMP_GetDefaultConfig ( acomp_config_t *  config)
* config->id = kACOMP_Acomp0;
* config->enable = false;
* config->warmupTime = kACOMP_WarmUpTime1us;
* config->responseMode = kACOMP_SlowResponseMode;
* config->inactiveValue = kACOMP_ResultLogicLow;
* config->intTrigType = kACOMP_HighLevelTrig;
* config->edgeDetectTrigSrc = kACOMP_EdgePulseDis;
* config->outPinMode = kACOMP_PinOutDisable;
* config->posInput = NULL;
* config->negInput = NULL;
*
Parameters
configThe pointer to the structure acomp_config_t.
void ACOMP_Deinit ( ACOMP_Type *  base)
Parameters
baseACOMP peripheral base address.
void ACOMP_SetInputConfig ( ACOMP_Type *  base,
acomp_comparator_id_t  id,
const acomp_positive_input_config_t *  posInput,
const acomp_negative_input_config_t *  negInput 
)
Parameters
baseACOMP peripheral base address.
idThe selected acomp comparator's id, please refer to acomp_comparator_id_t.
posInputThe configuration of selected comparator's positive input, please refer to acomp_positive_input_config_t.
negInputThe configuration of selected comparator's negative input, please refer to acomp_negative_input_config_t.
static void ACOMP_DoSoftwareReset ( ACOMP_Type *  base,
acomp_comparator_id_t  id 
)
inlinestatic
Parameters
baseACOMP peripheral base address.
idThe selected acomp comparator's id, please refer to acomp_comparator_id_t.
static void ACOMP_Enable ( ACOMP_Type *  base,
acomp_comparator_id_t  id,
bool  enable 
)
inlinestatic
Parameters
baseACOMP peripheral base address.
idThe selected acomp comparator's id, please refer to acomp_comparator_id_t.
enableUsed to enable/disable module.
  • true Enable comparator instance.
  • false Disable comparator instance.
static void ACOMP_ResetClockDivider ( ACOMP_Type *  base)
inlinestatic
Parameters
baseACOMP peripheral base address.
static acomp_result_logic_status_t ACOMP_GetResult ( ACOMP_Type *  base,
acomp_comparator_id_t  id 
)
inlinestatic
Parameters
baseACOMP peripheral base address.
idThe selected acomp comparator's id, please refer to acomp_comparator_id_t.
Returns
The result of the selected acomp instance.
static void ACOMP_EnableInterrupts ( ACOMP_Type *  base,
uint32_t  interruptMask 
)
inlinestatic

Enables interrupts, including acomp0 asynchronized interrupt, acomp0 synchronized interrupt, acomp1 asynchronized interrupt, and acomp1 synchronized interrupt.

Parameters
baseACOMP peripheral base address.
interruptMaskThe OR'ed value of the interrupts to be enabled, please refer to _acomp_interrupt_enable.
static void ACOMP_DisableInterrupt ( ACOMP_Type *  base,
uint32_t  interruptMask 
)
inlinestatic
Parameters
baseACOMP peripheral base address.
interruptMaskThe OR'ed value of the interrupts to be disabled, please refer to _acomp_interrupt_enable.
uint32_t ACOMP_GetStatusFlags ( ACOMP_Type *  base)

Gets status flags, such as ACOMP0 active status flags, ACOMP1 active status flags, and so on.

Parameters
baseACOMP peripheral base address.
Returns
The OR'ed value ACOMP status flags, please refer to _acomp_status_flags for details.
static void ACOMP_ClearStatusFlags ( ACOMP_Type *  base,
uint32_t  statusFlagMask 
)
inlinestatic
Note
Only kACOMP_Acomp0OutInterruptFlag, kACOMP_Acomp0OutAInterruptFlag, kACOMP_Acomp1OutInterruptFlag, and kACOMP_Acomp1OutAInterruptFlag can be cleared by software.
Parameters
baseACOMP peripheral base address.
statusFlagMaskThe OR'ed value of the status flags that can be cleared.