MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Clock Driver

Overview

The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.

The clock driver supports:

Files

file  fsl_clock.h
 

Data Structures

struct  clock_sfll_config_t
 SFLL configuration. More...
 
struct  clock_aupll_config_t
 AUPLL configuration. More...
 

Macros

#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0
 Configure whether driver controls clock. More...
 
#define GPIO_CLOCKS
 Clock ip name array for GPIO. More...
 
#define I2C_CLOCKS
 Clock ip name array for I2C. More...
 
#define QSPI_CLOCKS
 Clock ip name array for QSPI. More...
 
#define UART_CLOCKS
 Clock ip name array for UART. More...
 
#define SSP_CLOCKS
 Clock ip name array for SSP. More...
 
#define GPT_CLOCKS
 Clock ip name array for GPT. More...
 
#define WDT_CLOCKS
 Clock ip name array for WDT. More...
 
#define RTC_CLOCKS
 Clock ip name array for RTC. More...
 
#define ACOMP_CLOCKS
 Clock ip name array for ACOMP. More...
 
#define ADC_CLOCKS
 Clock ip name array for ADC. More...
 
#define DAC_CLOCKS
 Clock ip name array for DAC. More...
 
#define DMAC_CLOCKS
 Clock ip name array for DMAC. More...
 
#define CLK_OP_CODE_DEFINE(regOff, bitPos, bitWid, val)   (((regOff) << 16U) | ((bitPos) << 11U) | ((bitWid) << 8U) | (val))
 Clock operation code. More...
 

Enumerations

enum  clock_ip_name_t
 Peripheral clock name difinition used for clock gate.
 
enum  clock_attach_id_t
 Peripheral clock source selection definition.
 
enum  clock_div_name_t
 Clock divider definition.
 
enum  clock_sys_clk_src_t {
  kCLOCK_SysClkSrcSFll = 0U,
  kCLOCK_SysClkSrcRC32M_1 = 1U,
  kCLOCK_SysClkSrcMainXtal = 2U,
  kCLOCK_SysClkSrcRC32M_3 = 3U
}
 CLOCK system clock source. More...
 
enum  clock_refclk_t {
  kCLOCK_RefClk_SYS = (1U << PMU_WLAN_CTRL_REFCLK_SYS_REQ_SHIFT),
  kCLOCK_RefClk_AUD = (1U << PMU_WLAN_CTRL_REFCLK_AUD_REQ_SHIFT),
  kCLOCK_RefClk_USB = (1U << PMU_WLAN_CTRL_REFCLK_USB_REQ_SHIFT)
}
 System reference clock option. More...
 
enum  clock_osc32k_mode_t {
  kCLOCK_Osc32k_Internal = 0,
  kCLOCK_Osc32k_External = 1
}
 XTAL32K mode option. More...
 
enum  clock_sfll_src_t {
  kCLOCK_SFllSrcRC32M = 0U,
  kCLOCK_SFllSrcMainXtal = 1U
}
 SFLL Reference Input Clock Source. More...
 
enum  clock_aupll_src_t {
  kCLOCK_AuPllSrcRC32M = 0U,
  kCLOCK_AuPllSrcRefClk = 1U
}
 AUPLL Reference Input Clock Source. More...
 

Functions

void CLOCK_EnableClock (clock_ip_name_t name)
 Enable the clock for specific IP. More...
 
void CLOCK_DisableClock (clock_ip_name_t name)
 Disable the clock for specific IP. More...
 
void CLOCK_AttachClk (clock_attach_id_t connection)
 Configure the clock selection muxes. More...
 
void CLOCK_SetClkDiv (clock_div_name_t name, uint32_t divider)
 Setup clock dividers. More...
 
void CLOCK_SetUartClkDiv (clock_div_name_t name, uint32_t nom, uint32_t denom)
 Setup UART clock dividers. More...
 
uint32_t CLOCK_GetSysClkFreq (void)
 Get the system clock frequency. More...
 
void CLOCK_SetSysClkSource (clock_sys_clk_src_t src)
 Set the system clock source. More...
 
void CLOCK_EnableXtal32K (clock_osc32k_mode_t mode)
 Enable the 32K XTAL. More...
 
void CLOCK_DisableXtal32K (void)
 Disable the 32K XTAL output.
 
void CLOCK_EnableRC32M (bool halfDiv)
 Enable the RC32M OSC. More...
 
void CLOCK_DisableRC32M (void)
 Disable the RC32M OSC.
 
int32_t CLOCK_CalibrateRC32M (bool autoCal, uint32_t manCalCode)
 RC32M clock calibration function. More...
 
void CLOCK_EnableRC32K (void)
 Enable the RC32K OSC.
 
void CLOCK_DisableRC32K (void)
 Disable the RC32K OSC.
 
int32_t CLOCK_CalibrateRC32K (bool autoCal, uint32_t manCalCode)
 RC32K clock calibration function. More...
 
void CLOCK_EnableRefClk (uint32_t refclks)
 Enable the REFCLK for SYS/AUD/USB reference. More...
 
void CLOCK_DisableRefClk (uint32_t refclks)
 Disable the REFCLK for SYS/AUD/USB reference. More...
 
void CLOCK_InitSFll (const clock_sfll_config_t *config)
 Initialize the SFLL. More...
 
void CLOCK_DeinitSFll (void)
 Deinit the SFLL.
 
void CLOCK_InitAuPll (const clock_aupll_config_t *config)
 Initialize the AUPLL. More...
 
void CLOCK_DeinitAuPll (void)
 Deinit the AUPLL.
 
void CLOCK_UpdateAupllPostDiv (uint8_t postDivPattern, uint8_t postDivModulo)
 Update the AUPLL post divider.
 
__STATIC_INLINE void CLOCK_SetMainXtalFreq (uint32_t freq)
 Set the MAIN XTAL frequency based on board setting. More...
 
uint32_t CLOCK_GetMainXtalFreq (void)
 Return Frequency of MAIN XTAL Clock. More...
 
uint32_t CLOCK_GetRefClkAudFreq (void)
 Return Frequency of REFCLK_AUD Clock. More...
 
uint32_t CLOCK_GetRC32MFreq (void)
 Return Frequency of RC32M Clock. More...
 
uint32_t CLOCK_GetXtal32KFreq (void)
 Return Frequency of XTAL32K Clock. More...
 
uint32_t CLOCK_GetRC32KFreq (void)
 Return Frequency of RC32K Clock. More...
 
uint32_t CLOCK_GetSFllFreq (void)
 Return Frequency of SFLL Clock. More...
 
uint32_t CLOCK_GetAuPllFreq (void)
 Return Frequency of AUPLL Clock. More...
 
uint32_t CLOCK_GetCoreBusFreq (void)
 Return Frequency of M4/AHB Clock. More...
 
uint32_t CLOCK_GetApbFreq (uint32_t instance)
 Return Frequency of APB Clock. More...
 
uint32_t CLOCK_GetUartClkFreq (uint32_t instance)
 Return Frequency of UART Clock. More...
 
uint32_t CLOCK_GetGptClkFreq (uint32_t instance)
 Return Frequency of GPT Clock. More...
 
uint32_t CLOCK_GetGptSampleClkFreq (void)
 Return Frequency of GPT Sample Clock. More...
 
uint32_t CLOCK_GetSspClkFreq (uint32_t instance)
 Return Frequency of SSP Clock. More...
 
uint32_t CLOCK_GetGauClkFreq (void)
 Return Frequency of GAU Clock. More...
 
uint32_t CLOCK_GetRtcClkFreq (void)
 Return Frequency of RTC Clock. More...
 
uint32_t CLOCK_GetI2cClkFreq (void)
 Return Frequency of I2C Clock. More...
 
uint32_t CLOCK_GetQspiClkFreq (void)
 Return Frequency of QSPI Clock. More...
 
uint32_t CLOCK_GetFlashCClkFreq (void)
 Return Frequency of FlashC Clock. More...
 
uint32_t CLOCK_GetWdtClkFreq (void)
 Return Frequency of WDT Clock. More...
 
uint32_t CLOCK_GetSdioClkFreq (void)
 Return Frequency of SDIO Clock. More...
 

Variables

volatile uint32_t g_mainXtalFreq
 External crystal MAINXTAL clock frequency. More...
 

Driver version

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))
 CLOCK driver version 2.0.1. More...
 

Data Structure Documentation

struct clock_sfll_config_t

Data Fields

clock_sfll_src_t sfllSrc
 Reference Input Clock Source.
 
uint16_t refDiv
 Divider for reference clock, 9-bit. More...
 
uint16_t fbDiv
 Divider for feedback clock, 9-bit.
 
uint8_t kvco
 VCO setting, 2-bit. More...
 
uint8_t postDiv
 Post divider, 2-bit. More...
 

Field Documentation

uint16_t clock_sfll_config_t::refDiv

0.2 MHz <= Fref (frequency of Reference clock / refDiv) <= 0.4 MHz

uint8_t clock_sfll_config_t::kvco

Select KVCO per VCO target frequency

uint8_t clock_sfll_config_t::postDiv

2'b01, Fout = Fvco/2 2'b10, Fout = Fvco/4 2'b11, Fout = Fvco/8

struct clock_aupll_config_t

Data Fields

clock_aupll_src_t aupllSrc
 Reference Input Clock Source.
 
uint8_t refDiv
 Divider for reference clock, 4-bit, range: 3 ~ 10.
 
uint8_t fbDiv
 Divider for feedback clock, 6-bit, range: 27, 29, 31 ~ 36, 38, 39, 42, 46.
 
uint8_t icp
 charge pump current control, 2-bit, reserved now More...
 
uint8_t postDivPattern
 Pattern divider for ouput clock, 2-bit, range: 0 ~ 2. More...
 
uint8_t postDivModulo
 Modulo divider for ouput clock, 3-bit, range: 0 ~ 2, 4, 7. More...
 
bool enaVcoClkX2
 < 1'b0, Integration only More...
 
uint32_t fract
 < 1'b0, Disable VCOCLK_X2 More...
 

Field Documentation

uint8_t clock_aupll_config_t::icp

2'b00, 2.5 uA 2'b01, 5 uA 2'b10, 7.5 uA 2'b11, 10 uA

uint8_t clock_aupll_config_t::postDivPattern

2'b00, pattern = 4.0 2'b01, pattern = 3.0 2'b10, pattern = 4.5

uint8_t clock_aupll_config_t::postDivModulo

3'b000, modulo = 1 3'b001, modulo = 2 3'b010, modulo = 4 3'b100, modulo = 8 3'b111, modulo = 16

bool clock_aupll_config_t::enaVcoClkX2

< 1'b1, Integration + MASH

uint32_t clock_aupll_config_t::fract

< 1'b1, Enable VCOCLK_X2 Fractional PLL feedback divider 20-bits, range: 0 ~ 0x10000

Macro Definition Documentation

#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0

When set to 0, peripheral drivers will enable clock in initialize function and disable clock in de-initialize function. When set to 1, peripheral driver will not control the clock, application could control the clock out of the driver.

Note
All drivers share this feature switcher. If it is set to 1, application should handle clock enable and disable for all drivers.
#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))
#define GPIO_CLOCKS
Value:
{ \
kCLOCK_Gpio \
}
#define I2C_CLOCKS
Value:
{ \
kCLOCK_I2c0, kCLOCK_I2c1 \
}
#define QSPI_CLOCKS
Value:
{ \
kCLOCK_Qspi \
}
#define UART_CLOCKS
Value:
{ \
kCLOCK_Uart0, kCLOCK_Uart1, kCLOCK_Uart2 \
}
#define SSP_CLOCKS
Value:
{ \
kCLOCK_Ssp0, kCLOCK_Ssp1, kCLOCK_Ssp2 \
}
#define GPT_CLOCKS
Value:
{ \
kCLOCK_Gpt0, kCLOCK_Gpt1, kCLOCK_Gpt2, kCLOCK_Gpt3 \
}
#define WDT_CLOCKS
Value:
{ \
kCLOCK_Wdt \
}
#define RTC_CLOCKS
Value:
{ \
kCLOCK_Rtc \
}
#define ACOMP_CLOCKS
Value:
{ \
kCLOCK_AcompMclk \
}
#define ADC_CLOCKS
Value:
{ \
kCLOCK_AdcMclk \
}
#define DAC_CLOCKS
Value:
{ \
kCLOCK_DacMclk \
}
#define DMAC_CLOCKS
Value:
{ \
kCLOCK_Dma \
}
#define CLK_OP_CODE_DEFINE (   regOff,
  bitPos,
  bitWid,
  val 
)    (((regOff) << 16U) | ((bitPos) << 11U) | ((bitWid) << 8U) | (val))

[31:16] Register offset from PMU base. [15:11] Register bit position. [10: 8] Register bits width to operate. [ 7: 0] Value to set to the bits.

Enumeration Type Documentation

Enumerator
kCLOCK_SysClkSrcSFll 

SFLL.

kCLOCK_SysClkSrcRC32M_1 

RC 32MHz clock.

kCLOCK_SysClkSrcMainXtal 

XTAL 38.4MHz clock.

kCLOCK_SysClkSrcRC32M_3 

RC 32MHz clock.

Enumerator
kCLOCK_RefClk_SYS 

REFCLK_SYS.

kCLOCK_RefClk_AUD 

REFCLK_AUD.

kCLOCK_RefClk_USB 

REFCLK_USB.

Enumerator
kCLOCK_Osc32k_Internal 

Internal oscillator mode.

kCLOCK_Osc32k_External 

External oscillator mode.

Enumerator
kCLOCK_SFllSrcRC32M 

RC32M clock.

kCLOCK_SFllSrcMainXtal 

Main XTAL clock.

Enumerator
kCLOCK_AuPllSrcRC32M 

RC32M clock.

kCLOCK_AuPllSrcRefClk 

REFCLK_AUD clock.

Function Documentation

void CLOCK_EnableClock ( clock_ip_name_t  name)
Parameters
nameWhich clock to enable, see clock_ip_name_t.
void CLOCK_DisableClock ( clock_ip_name_t  name)
Parameters
nameWhich clock to disable, see clock_ip_name_t.
void CLOCK_AttachClk ( clock_attach_id_t  connection)
Parameters
connection: Clock to be configured.
void CLOCK_SetClkDiv ( clock_div_name_t  name,
uint32_t  divider 
)
Parameters
name: Clock divider name
divider: Value to be divided.
void CLOCK_SetUartClkDiv ( clock_div_name_t  name,
uint32_t  nom,
uint32_t  denom 
)
Parameters
name: Clock divider name
nom: Nominator for fraction divider.
denom: Denominator for fraction divider.
uint32_t CLOCK_GetSysClkFreq ( void  )
Returns
Clock frequency in Hz.
void CLOCK_SetSysClkSource ( clock_sys_clk_src_t  src)

This function sets the system clock source.

Parameters
srcSystem clock source to set.
void CLOCK_EnableXtal32K ( clock_osc32k_mode_t  mode)
Parameters
modeInternal or external OSC selection.
void CLOCK_EnableRC32M ( bool  halfDiv)
Parameters
halfDivhalf-divided reference clock. True for 16MHz and false for original 32MHz output.
int32_t CLOCK_CalibrateRC32M ( bool  autoCal,
uint32_t  manCalCode 
)
Parameters
autoCalCalibration option, true for auto and false for manual
manCalCodeSelect manual way, need input the calibration code
Returns
return the calibration result -1, calibration failure else, internal calibration code
Note
Clock CLK_AUPLL_CAU must be ready before RC32M calibration
int32_t CLOCK_CalibrateRC32K ( bool  autoCal,
uint32_t  manCalCode 
)
Parameters
autoCalCalibration option, true for auto and false for manual
manCalCodeSelect manual way, need input the calibration code
Returns
return the calibration result -1, calibration failure else, internal calibration code
Note
Clock XTAL32K must be ready before RC32K calibration
void CLOCK_EnableRefClk ( uint32_t  refclks)
Parameters
refclksOr'ed value to select SYS/AUD/USB REFCLK to disable. See clock_refclk_t.
void CLOCK_DisableRefClk ( uint32_t  refclks)
Parameters
refclksOr'ed value to select SYS/AUD/USB REFCLK to disable. See clock_refclk_t.
void CLOCK_InitSFll ( const clock_sfll_config_t *  config)
Parameters
config: Configuration to set to SFLL.
void CLOCK_InitAuPll ( const clock_aupll_config_t *  config)
Parameters
config: Configuration to set to AUPLL.
__STATIC_INLINE void CLOCK_SetMainXtalFreq ( uint32_t  freq)
Parameters
freq: The XTAL input clock frequency in Hz.
uint32_t CLOCK_GetMainXtalFreq ( void  )
Returns
Frequency of MAIN XTAL Clock.
uint32_t CLOCK_GetRefClkAudFreq ( void  )
Returns
Frequency of REFCLK_AUD Clock.
uint32_t CLOCK_GetRC32MFreq ( void  )
Returns
Frequency of RC32M Clock.
uint32_t CLOCK_GetXtal32KFreq ( void  )
Returns
Frequency of XTAL32K Clock.
uint32_t CLOCK_GetRC32KFreq ( void  )
Returns
Frequency of RC32K Clock.
uint32_t CLOCK_GetSFllFreq ( void  )
Returns
Frequency of SFLL Clock.
uint32_t CLOCK_GetAuPllFreq ( void  )
Returns
Frequency of AUPLL Clock.
uint32_t CLOCK_GetCoreBusFreq ( void  )
Returns
Frequency of M4/AHB Clock.
uint32_t CLOCK_GetApbFreq ( uint32_t  instance)
Parameters
instanceAPB instance 0-1.
Returns
Frequency of APB Clock.
uint32_t CLOCK_GetUartClkFreq ( uint32_t  instance)
Parameters
instanceUART instance 0-2.
Returns
Frequency of UART Clock.
uint32_t CLOCK_GetGptClkFreq ( uint32_t  instance)
Parameters
instanceGPT instance 0-3.
Returns
Frequency of GPT Clock.
uint32_t CLOCK_GetGptSampleClkFreq ( void  )
Returns
Frequency of GPT Sample Clock.
uint32_t CLOCK_GetSspClkFreq ( uint32_t  instance)
Parameters
instanceSSP instance 0-2.
Returns
Frequency of SSP Clock.
uint32_t CLOCK_GetGauClkFreq ( void  )
Returns
Frequency of GAU Clock.
uint32_t CLOCK_GetRtcClkFreq ( void  )
Returns
Frequency of RTC Clock.
uint32_t CLOCK_GetI2cClkFreq ( void  )
Returns
Frequency of I2C Clock.
uint32_t CLOCK_GetQspiClkFreq ( void  )
Returns
Frequency of QSPI Clock.
uint32_t CLOCK_GetFlashCClkFreq ( void  )
Returns
Frequency of FlashC Clock.
uint32_t CLOCK_GetWdtClkFreq ( void  )
Returns
Frequency of WDT Clock.
uint32_t CLOCK_GetSdioClkFreq ( void  )
Returns
Frequency of SDIO Clock.

Variable Documentation

volatile uint32_t g_mainXtalFreq

The MAINXTAL clock frequency in Hz. When the clock is set up, use the function CLOCK_SetMainXtalFreq to set the value in the clock driver. For example, if MAINXTAL is 38.4 MHz:

* CLOCK_SetMainXtalFreq(384000000);
*