MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
DAC: Digital Analog Converter

Overview

The MCUXpresso SDK provides a driver for the Digital Analog Converter (DAC) module of MCUXpreeso SDK devices.

Based on the features of the DAC module, the DAC driver is divided into serval function groups.

Module Initialization Interfaces

The functions in this group can be used to initialize or de-initialize the DAC module. To initialize the DAC module, the function DAC_GetDefaultConfig() can be invoked to get the module's default configuration.

Channels Control Interfaces

This function group contains channel control APIs. To configure the channels' all options directly at one time, the function DAC_SetChannelConfig() is provided, this function takes the pointer to structure that in the type of dac_channel_config_t as the parameter. All channel-related options are covered in this structure type. To set some specific options of channels, some low-level APIs also provided in this function group. All APIs in this function group take channelMask as the parameter, it means the mask of channel ID. If both channel A and channel B are aimed to set the same options, then users just need to invoke related APIs once with the channelMask set as the OR'ed value of channel A and channel B.

Triangle Waveform Configuration Interface

There is only one API in this function group, it is DAC_SetTriangleConfig() function. This function is used to configure the triangle waveform when channel A's wave type is selected as the triangle type.

Interrupts Control Interfaces.

The APIs in this function group can be used to enable/disable interrupts.

Status Flags Control Interfaces

The APIs in this function group can be used to get/clear status flags.

Data Structures

struct  dac_config_t
 The structure of dac module basic configuration, including conversion rate, output range, and reference voltage source. More...
 
struct  dac_channel_config_t
 The structure of dac channel configuration, such as trigger type, wave type, timing mode, and so on. More...
 
struct  dac_triangle_config_t
 The structure of triangle waveform, including maximum value, minimum value, step size, and so on. More...
 

Macros

#define FSL_DAC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 DAC driver version. More...
 
#define IS_DAC_CHANNEL_A_WAVE(CH_WAVE)   ((CH_WAVE) <= kDAC_WaveNoiseDifferential)
 DAC channel A wave mode check.
 
#define IS_DAC_CHANNEL_B_WAVE(CH_WAVE)   (((CH_WAVE) == kDAC_WaveNormal) || ((CH_WAVE) == kDAC_WaveNoiseDifferential))
 DAC channel B wave mode check.
 

Enumerations

enum  _dac_interrupt_enable {
  kDAC_ChannelAReadyInterruptEnable = DAC_IMR_A_RDY_INT_MSK_MASK,
  kDAC_ChannelBReadyInterruptEnable = DAC_IMR_B_RDY_INT_MSK_MASK,
  kDAC_ChannelATimeoutInterruptEnable = DAC_IMR_A_TO_INT_MSK_MASK,
  kDAC_ChannelBTimeoutInterruptEnable = DAC_IMR_B_TO_INT_MSK_MASK,
  kDAC_TriangleOverflowInterruptEnable = DAC_IMR_TRIA_OVFL_INT_MSK_MASK
}
 The enumeration of interrupts that DAC support. More...
 
enum  _dac_status_flags {
  kDAC_ChannelADataReadyInterruptFlag = DAC_ISR_A_RDY_INT_MASK,
  kDAC_ChannelBDataReadyInterruptFlag = DAC_ISR_B_RDY_INT_MASK,
  kDAC_ChannelATimeoutInterruptFlag = DAC_ISR_A_TO_INT_MASK,
  kDAC_ChannelBTimeoutInterruptFlag = DAC_ISR_B_TO_INT_MASK,
  kDAC_TriangleOverflowInterruptFlag = DAC_ISR_TRIA_OVFL_INT_MASK,
  kDAC_RawChannelADataReadyFlag = DAC_IRSR_A_RDY_INT_RAW_MASK << 5UL,
  kDAC_RawChannelBDataReadyFlag = DAC_IRSR_B_RDY_INT_RAW_MASK << 5UL,
  kDAC_RawChannelATimeoutFlag = DAC_IRSR_A_TO_INT_RAW_MASK << 5UL,
  kDAC_RawChannelBTimeoutFlag = DAC_IRSR_B_TO_INT_RAW_MASK << 5UL,
  kDAC_RawTriangleOverflowFlag = DAC_IRSR_TRIA_OVFL_INT_RAW_MASK << 5UL,
  kDAC_ChannelAConversionCompleteFlag = DAC_STATUS_A_DV_MASK << 10UL,
  kDAC_ChannelBConversionCompleteFlag = DAC_STATUS_B_DV_MASK << 10UL
}
 The enumeration of DAC status flags, including interrupt status flags, raw status flags, and conversion status flags. More...
 
enum  dac_channel_id_t
 The enumeration of dac channels, including channel A and channel B.
 
enum  dac_conversion_rate_t {
  kDAC_ConversionRate62P5KHZ = 0U,
  kDAC_ConversionRate125KHZ,
  kDAC_ConversionRate250KHZ,
  kDAC_ConversionRate500KHZ
}
 The enumeration of dac converion rate, including 62.5 KHz, 125 KHz, 250 KHz, and 500 KHz. More...
 
enum  dac_reference_voltage_source_t {
  kDAC_ReferenceInternalVoltageSource = 0U,
  kDAC_ReferenceExternalVoltageSource
}
 The enumeration of dac reference voltage source. More...
 
enum  dac_output_voltage_range_t {
  kDAC_RangeSmall = 0U,
  kDAC_RangeMiddle = 1U,
  kDAC_RangeLarge = 3U
}
 The enumeration of dac output voltage range. More...
 
enum  dac_channel_output_t {
  kDAC_ChannelOutputInternal = 0U,
  kDAC_ChannelOutputPAD
}
 The enumeration of dac channel's output mode. More...
 
enum  dac_channel_trigger_type_t {
  kDAC_RisingEdgeTrigger = 1U,
  kDAC_FallingEdgeTrigger = 2U,
  kDAC_BothEdgeTrigger = 3U
}
 The enumeration of dac channel's trigger type, including rising edge trigger, falling edge trigger, and both edge triggers. More...
 
enum  dac_channel_trigger_source_t {
  kDAC_GPT2Trigger = 0U,
  kDAC_GPT3Trigger = 1U,
  kDAC_GPIO45Trigger = 2U,
  kDAC_GPIO44Trigger = 3U
}
 The enumeration of dac channel trigger source. More...
 
enum  dac_channel_timing_mode_t {
  kDAC_NonTimingCorrelated = 0U,
  kDAC_TimingCorrelated
}
 The enumeration of dac channel timing mode. More...
 
enum  dac_channel_wave_type_t {
  kDAC_WaveNormal = 0U,
  kDAC_WaveTriangle = 1U,
  kDAC_WaveSine = 2U,
  kDAC_WaveNoiseDifferential = 3U
}
 The enumerator of channel output wave type, please note that not all wave types are effective to A and B channel. More...
 
enum  dac_triangle_mamp_t {
  kDAC_TriangleAmplitude63 = 0U,
  kDAC_TriangleAmplitude127,
  kDAC_TriangleAmplitude191,
  kDAC_TriangleAmplitude255,
  kDAC_TriangleAmplitude319,
  kDAC_TriangleAmplitude383,
  kDAC_TriangleAmplitude447,
  kDAC_TriangleAmplitude511,
  kDAC_TriangleAmplitude575,
  kDAC_TriangleAmplitude639,
  kDAC_TriangleAmplitude703,
  kDAC_TriangleAmplitude767,
  kDAC_TriangleAmplitude831,
  kDAC_TriangleAmplitude895,
  kDAC_TriangleAmplitude959,
  kDAC_TriangleAmplitude1023
}
 DAC triangle maximum amplitude type. More...
 
enum  dac_triangle_step_size_t {
  kDAC_TriangleStepSize1 = 0U,
  kDAC_TriangleStepSize3,
  kDAC_TriangleStepSize15,
  kDAC_TriangleStepSize511
}
 DAC triangle step size type. More...
 
enum  dac_triangle_waveform_type_t {
  kDAC_TriangleFull = 0U,
  kDAC_TriangleHalf
}
 DAC triangle waveform type. More...
 

Module Initialization Interfaces

void DAC_Init (DAC_Type *base, const dac_config_t *config)
 Initializes DAC module, including set reference voltage source, set conversion range, and set output voltage range. More...
 
void DAC_GetDefaultConfig (dac_config_t *config)
 Gets the default configurations of DAC module. More...
 
void DAC_Deinit (DAC_Type *base)
 De-initializes the DAC module, including reset clock divider, reset each channel, and so on. More...
 

Channels Control Interfaces

void DAC_SetChannelConfig (DAC_Type *base, uint32_t channelMask, const dac_channel_config_t *channelConfig)
 Configures the DAC channels, including enable channel conversion, set wave type, set timing mode, and so on. More...
 
static void DAC_ResetChannel (DAC_Type *base, uint32_t channelMask)
 Does software reset for the selected DAC channels. More...
 
static void DAC_EnableChannelConversion (DAC_Type *base, uint32_t channelMask, bool enable)
 Enables/Disables selected channel conversion. More...
 
static void DAC_SetChannelOutMode (DAC_Type *base, uint32_t channelMask, dac_channel_output_t outMode)
 Sets channels out mode, including kDAC_ChannelOutputInternal and kDAC_ChannelOutputPad. More...
 
static void DAC_EnableChannelTriggerMode (DAC_Type *base, uint32_t channelMask, bool enable)
 Enables/Disables channels trigger mode. More...
 
static void DAC_SetChannelTrigSource (DAC_Type *base, uint32_t channelMask, dac_channel_trigger_source_t trigSource)
 Sets channels trigger source. More...
 
static void DAC_SetChannelTrigType (DAC_Type *base, uint32_t channelMask, dac_channel_trigger_type_t trigType)
 Sets channels trigger type, such as rising edge trigger, falling edge trigger, or both edge trigger. More...
 
static void DAC_SetChannelTimingMode (DAC_Type *base, uint32_t channelMask, dac_channel_timing_mode_t timingMode)
 Sets channels timing mode, including not-timing related or timing related. More...
 
static void DAC_EnableChannelDMA (DAC_Type *base, uint32_t channelMask, bool enable)
 Enables/Disables channels DMA. More...
 
static void DAC_SetChannelWaveType (DAC_Type *base, uint32_t channelMask, dac_channel_wave_type_t waveType)
 Sets channels wave type, such as sine, noise, or triangle. More...
 
static void DAC_SetChannelData (DAC_Type *base, uint32_t channelMask, uint16_t data)
 Sets DAC channels data. More...
 

Triangle Waveform Configuration Interface

void DAC_SetTriangleConfig (DAC_Type *base, const dac_triangle_config_t *triangleConfig)
 Configures the options of triangle waveform. More...
 

Interrupts Control Interfaces.

static void DAC_EnableInterrupts (DAC_Type *base, uint32_t interruptMask)
 Enables interrupts, such as channel A data ready interupt, channel A timeout interrupt, and so on. More...
 
static void DAC_DisableInterrupts (DAC_Type *base, uint32_t interruptMask)
 Disables interrupts, such as channel B data ready interrupt, channel B timeout interrupt, and so on. More...
 

Status Flags Control Interfaces

static uint32_t DAC_GetStatusFlags (DAC_Type *base)
 Gets the status flags, including interrupt status flags, raw status flags, and conversion status flags. More...
 
static void DAC_ClearStatusFlags (DAC_Type *base, uint32_t statusFlagsMask)
 Clears the interrups status flags, such as channel A data ready interrupt flag, channel B data ready interrupt flag, and so on. More...
 

Data Structure Documentation

struct dac_config_t

Data Fields

dac_conversion_rate_t conversionRate
 Configure DAC conversion rate, please refer to dac_conversion_rate_t. More...
 
dac_reference_voltage_source_t refSource
 Configure DAC vref source, please refer to dac_reference_voltage_source_t. More...
 
dac_output_voltage_range_t rangeSelect
 Configure DAC channel output range, please refer to dac_output_voltage_range_t. More...
 

Field Documentation

dac_conversion_rate_t dac_config_t::conversionRate
dac_reference_voltage_source_t dac_config_t::refSource
dac_output_voltage_range_t dac_config_t::rangeSelect
struct dac_channel_config_t

Data Fields

bool enableConversion
 Enable/Disable selected channel's conversion. More...
 
dac_channel_output_t outMode
 Configure channel output mode, please refer to dac_channel_output_t.
 
bool enableDMA
 Enable/Disable channel DAM data transfer. More...
 
bool enableTrigger
 Enable/Disable external event trigger. More...
 
dac_channel_trigger_type_t triggerType
 Configure the channel trigger type, please refer to dac_channel_trigger_type_t. More...
 
dac_channel_trigger_source_t triggerSource
 Configure DAC channel trigger source, please refer to dac_channel_trigger_source_t. More...
 
dac_channel_timing_mode_t timingMode
 Configure channel timing mode, please refer to dac_channel_timing_mode_t. More...
 
dac_channel_wave_type_t waveType
 Configure wave type for the selected channel, please refer to dac_channel_wave_type_t. More...
 

Field Documentation

bool dac_channel_config_t::enableConversion
  • true Enable selected channel's conversion.
  • false Disable selected channel's conversion.
bool dac_channel_config_t::enableDMA
  • true DMA data transfer enabled.
  • false DMA data transfer disabled.
bool dac_channel_config_t::enableTrigger
dac_channel_trigger_type_t dac_channel_config_t::triggerType
dac_channel_trigger_source_t dac_channel_config_t::triggerSource
dac_channel_timing_mode_t dac_channel_config_t::timingMode
dac_channel_wave_type_t dac_channel_config_t::waveType
struct dac_triangle_config_t

Data Fields

dac_triangle_mamp_t triangleMamp
 Configure triangle maximum value. More...
 
dac_triangle_step_size_t triangleStepSize
 Configure triangle step size. More...
 
dac_triangle_waveform_type_t triangleWaveform
 Configure triangle waveform type. More...
 
uint32_t triangleBase
 Configure triangle minimum value. More...
 

Field Documentation

dac_triangle_mamp_t dac_triangle_config_t::triangleMamp
dac_triangle_step_size_t dac_triangle_config_t::triangleStepSize
dac_triangle_waveform_type_t dac_triangle_config_t::triangleWaveform
uint32_t dac_triangle_config_t::triangleBase

Macro Definition Documentation

#define FSL_DAC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))

Version 2.0.0.

Enumeration Type Documentation

Enumerator
kDAC_ChannelAReadyInterruptEnable 

Enable channel A data ready interrupt.

kDAC_ChannelBReadyInterruptEnable 

Enable channel B data ready interrupt.

kDAC_ChannelATimeoutInterruptEnable 

Enable channel A time out interrupt.

kDAC_ChannelBTimeoutInterruptEnable 

Enable channel B time out interrupt.

kDAC_TriangleOverflowInterruptEnable 

Enable triangle overflow interrupt.

Note
The interrupt status flags can only be asserted upon both enabling and happening of related interrupts. Comparatively, the raw status flags will be asserted as long as related events happen regardless of whether related interrupts are enabled or not.
Only interrupt status flags can be cleared mannually.
Enumerator
kDAC_ChannelADataReadyInterruptFlag 

Channel A data ready.

kDAC_ChannelBDataReadyInterruptFlag 

Channel B data ready.

kDAC_ChannelATimeoutInterruptFlag 

Channel A time out.

kDAC_ChannelBTimeoutInterruptFlag 

Channel B time out.

kDAC_TriangleOverflowInterruptFlag 

Triangle overflow.

kDAC_RawChannelADataReadyFlag 

Channel A data ready raw.

kDAC_RawChannelBDataReadyFlag 

Channel B data ready raw.

kDAC_RawChannelATimeoutFlag 

Channel A timeout raw.

kDAC_RawChannelBTimeoutFlag 

Channel B timeout raw.

kDAC_RawTriangleOverflowFlag 

Triangle overflow raw.

kDAC_ChannelAConversionCompleteFlag 

Channel A conversion complete.

kDAC_ChannelBConversionCompleteFlag 

Channel B conversion complete.

Enumerator
kDAC_ConversionRate62P5KHZ 

DAC Conversion Rate selects as 62.5 KHz.

kDAC_ConversionRate125KHZ 

DAC Conversion Rate selects as 125 KHz.

kDAC_ConversionRate250KHZ 

DAC Conversion Rate selects as 250 KHz.

kDAC_ConversionRate500KHZ 

DAC Conversion Rate selects as 500 KHz.

Enumerator
kDAC_ReferenceInternalVoltageSource 

Select internal voltage reference.

kDAC_ReferenceExternalVoltageSource 

Select external voltage reference.

Enumerator
kDAC_RangeSmall 

DAC output small range.

kDAC_RangeMiddle 

DAC output middle range.

kDAC_RangeLarge 

DAC output large range.

Enumerator
kDAC_ChannelOutputInternal 

Enable internal output but disable output to pad.

kDAC_ChannelOutputPAD 

Enable output to pad but disable internal output.

Enumerator
kDAC_RisingEdgeTrigger 

Rising edge trigger.

kDAC_FallingEdgeTrigger 

Failing edge trigger.

kDAC_BothEdgeTrigger 

Rising and Failing edge trigger.

Enumerator
kDAC_GPT2Trigger 

GPT2 trigger source.

kDAC_GPT3Trigger 

GPT3 trigger source.

kDAC_GPIO45Trigger 

GPIO45 trigger source.

kDAC_GPIO44Trigger 

GPIO44 trigger source.

Enumerator
kDAC_NonTimingCorrelated 

DAC non-timing-correlated mode.

kDAC_TimingCorrelated 

DAC timing-correlated mode.

Enumerator
kDAC_WaveNormal 

No predefined waveform, effective to A or B channel.

kDAC_WaveTriangle 

Triangle wave, effective only to A channel.

kDAC_WaveSine 

Sine wave, effective only to A channel.

kDAC_WaveNoiseDifferential 

Noise wave, effective only to A channel; Differential mode, one's complemental code from A data, effective only to B channel.

Enumerator
kDAC_TriangleAmplitude63 

DAC triangle amplitude 63 lsb.

kDAC_TriangleAmplitude127 

DAC triangle amplitude 127 lsb.

kDAC_TriangleAmplitude191 

DAC triangle amplitude 191 lsb.

kDAC_TriangleAmplitude255 

DAC triangle amplitude 255 lsb.

kDAC_TriangleAmplitude319 

DAC triangle amplitude 319 lsb.

kDAC_TriangleAmplitude383 

DAC triangle amplitude 383 lsb.

kDAC_TriangleAmplitude447 

DAC triangle amplitude 447 lsb.

kDAC_TriangleAmplitude511 

DAC triangle amplitude 511 lsb.

kDAC_TriangleAmplitude575 

DAC triangle amplitude 575 lsb.

kDAC_TriangleAmplitude639 

DAC triangle amplitude 639 lsb.

kDAC_TriangleAmplitude703 

DAC triangle amplitude 703 lsb.

kDAC_TriangleAmplitude767 

DAC triangle amplitude 767 lsb.

kDAC_TriangleAmplitude831 

DAC triangle amplitude 831 lsb.

kDAC_TriangleAmplitude895 

DAC triangle amplitude 895 lsb.

kDAC_TriangleAmplitude959 

DAC triangle amplitude 959 lsb.

kDAC_TriangleAmplitude1023 

DAC triangle amplitude 1023 lsb.

Enumerator
kDAC_TriangleStepSize1 

DAC triangle step size 1 lsb.

kDAC_TriangleStepSize3 

DAC triangle step size 3 lsb.

kDAC_TriangleStepSize15 

DAC triangle step size 15 lsb.

kDAC_TriangleStepSize511 

DAC triangle step size 511 lsb.

Enumerator
kDAC_TriangleFull 

DAC full triangle waveform.

kDAC_TriangleHalf 

DAC half triangle waveform.

Function Documentation

void DAC_Init ( DAC_Type *  base,
const dac_config_t *  config 
)
Parameters
baseDAC peripheral base address.
configPointer to the structure which in type of dac_config_t.
void DAC_GetDefaultConfig ( dac_config_t *  config)
* config->conversionRate = kDAC_ConversionRate62P5KHZ;
* config->rangeSelect = kDAC_RangeLarge;
*
Parameters
configPointer to the structure which in the type of dac_config_t.
void DAC_Deinit ( DAC_Type *  base)
Parameters
baseDAC peripheral base address.
void DAC_SetChannelConfig ( DAC_Type *  base,
uint32_t  channelMask,
const dac_channel_config_t *  channelConfig 
)
Parameters
baseDAC peripheral base address.
channelMaskThe mask of channel, can be the OR'ed value of dac_channel_id_t.
channelConfigThe pointer of structure which in the type of dac_channel_config_t.
static void DAC_ResetChannel ( DAC_Type *  base,
uint32_t  channelMask 
)
inlinestatic
Parameters
baseDAC peripheral base address.
channelMaskThe mask of channel to be reset, should be the OR'ed value of dac_channel_id_t.
static void DAC_EnableChannelConversion ( DAC_Type *  base,
uint32_t  channelMask,
bool  enable 
)
inlinestatic
Note
To enable/disable the conversions of both channels, invoking this API with the parameter channelMask set as kDAC_ChannelA|kDAC_ChannelB .
Parameters
baseDAC peripheral base address.
channelMaskThe mask of channel to be reset, can be the OR'ed value of dac_channel_id_t.
enableEnable/Disable channel conversion.
  • true Enable selected channels' conversion.
  • false Disable selected channels' conversion.
static void DAC_SetChannelOutMode ( DAC_Type *  base,
uint32_t  channelMask,
dac_channel_output_t  outMode 
)
inlinestatic
Parameters
baseDAC peripheral base address.
channelMaskThe mask of channel, can be the OR'ed value of dac_channel_id_t.
outModeThe out mode of selected channels, please refer to dac_channel_output_t for details.
static void DAC_EnableChannelTriggerMode ( DAC_Type *  base,
uint32_t  channelMask,
bool  enable 
)
inlinestatic
Note
To enable/disable the trigger mode of both two channels, invoking this API with the parameter channelMask set as kDAC_ChannelA|kDAC_ChannelB .
Parameters
baseDAC peripheral base address.
channelMaskThe mask of channel, can be the OR'ed value of dac_channel_id_t.
enableEnable/Disable channel trigger mode.
  • true Channels' conversion triggered by external event enabled.
  • false Channels' conversion trigged by external event disabled.
static void DAC_SetChannelTrigSource ( DAC_Type *  base,
uint32_t  channelMask,
dac_channel_trigger_source_t  trigSource 
)
inlinestatic
Note
To set the same trigger source to both two channels, invoking this API with the parameter channelMask set as kDAC_ChannelA|kDAC_ChannelB .
Parameters
baseDAC peripheral base address.
channelMaskThe mask of channel, can be the OR'ed value of dac_channel_id_t.
trigSourceThe selected trigger source, please refer to dac_channel_trigger_source_t for details.
static void DAC_SetChannelTrigType ( DAC_Type *  base,
uint32_t  channelMask,
dac_channel_trigger_type_t  trigType 
)
inlinestatic
Note
To set the same trigger type to both two channels, invoking this API with the parameter channelMask set as kDAC_ChannelA|kDAC_ChannelB .
Parameters
baseDAC peripheral base address.
channelMaskThe mask of channel, can be the OR'ed value of dac_channel_id_t;
trigTypeThe selected trigger type, please refer to dac_channel_trigger_type_t;
static void DAC_SetChannelTimingMode ( DAC_Type *  base,
uint32_t  channelMask,
dac_channel_timing_mode_t  timingMode 
)
inlinestatic
Note
To the same timing mode to both two channels, invoking this API with the parameter channelMask set as kDAC_ChannelA|kDAC_ChannelB .
Parameters
baseDAC peripheral base address.
channelMaskThe mask of channel, can be the OR'ed value of dac_channel_id_t.
timingModeThe selected timing mode, please refer to dac_channel_timing_mode_t for details.
static void DAC_EnableChannelDMA ( DAC_Type *  base,
uint32_t  channelMask,
bool  enable 
)
inlinestatic
Parameters
baseDAC peripheral base address.
channelMaskThe mask of channel, can be the OR'ed value of dac_channel_id_t.
enableEnable/Disable channel DMA data transfer.
  • true DMA data transfer enabled.
  • false DMA data transfer disabled.
static void DAC_SetChannelWaveType ( DAC_Type *  base,
uint32_t  channelMask,
dac_channel_wave_type_t  waveType 
)
inlinestatic
Note
To set the same wave type to both channel, invoking this API with the parameter channelMask set as kDAC_ChannelA|kDAC_ChannelB .
Parameters
baseDAC peripheral base address.
channelMaskThe mask of channel, should be the OR'ed value of dac_channel_id_t.
waveTypeThe wave type to set, please refer to dac_channel_wave_type_t.
static void DAC_SetChannelData ( DAC_Type *  base,
uint32_t  channelMask,
uint16_t  data 
)
inlinestatic
Note
To set the same data to both channel, invoking this API with the parameter channelMask set as kDAC_ChannelA|kDAC_ChannelB .
Parameters
baseDAC peripheral base address.
channelMaskThe mask of channel, can be the OR'ed value of dac_channel_id_t.
data
void DAC_SetTriangleConfig ( DAC_Type *  base,
const dac_triangle_config_t *  triangleConfig 
)
Note
This API should be invoked to set the options of triangle waveform when channel A's output wave type is selected as kDAC_WaveTriangle.
Parameters
baseDAC peripheral base address.
triangleConfigThe pointer of structure which in the type of dac_triangle_config_t.
static void DAC_EnableInterrupts ( DAC_Type *  base,
uint32_t  interruptMask 
)
inlinestatic
Parameters
baseDAC peripheral base address.
interruptMaskThe or'ed value of the interrupts to be enabled, please refer to _dac_interrupt_enable.
static void DAC_DisableInterrupts ( DAC_Type *  base,
uint32_t  interruptMask 
)
inlinestatic
Parameters
baseDAC peripheral base address.
interruptMaskThe or'ed value of the interrupts to be disabled, please refer to _dac_interrupt_enable.
static uint32_t DAC_GetStatusFlags ( DAC_Type *  base)
inlinestatic
Parameters
baseDAC peripheral base address.
Returns
The mask of status flags, please refer to _dac_status_flags.
static void DAC_ClearStatusFlags ( DAC_Type *  base,
uint32_t  statusFlagsMask 
)
inlinestatic
Parameters
baseDAC peripheral base address.
statusFlagsMaskThe mask of the status flags to be cleared, please refer to _dac_status_flags.