MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
GPT: General Purpose Timer Driver

Overview

The MCUXpresso SDK provides a driver for the General Purpose Timer Module (GPT) of MCUXpresso SDK devices.

Function groups

The GPT driver supports the generation of one-shot pulse/edge, PWM signals, and input capture modes.

Initialization and deinitialization

The function GPT_Init() initializes the GPT with specified configurations. The function GPT_GetDefaultConfig() gets the default configurations. The initialization function configures the GPT for the requested parameters.

The function GPT_Deinit() disables the GPT counter and turns off the module clock.

Input capture operations

The function GPT_SetupInputCapture() sets up a GPT channel for the input capture. The user can specify the capture edge and a filter value to be used when processing the input signal.

The function GPT_TriggerInputCapture() can be used to trigger the capture by software.

One-shot operations

The function GPT_SetupOneshotPulse() sets up a GPT channel for one-shot pulse generation on the output pin.

The function GPT_SetupOneshotEdge() sets up a GPT channel for one-shot edge toggle on the output pin.

PWM Operations

The function GPT_SetupPwm() sets up GPT channels for the PWM output. The function sets up the PWM signal properties for 1 of 6 channels. Each channel has its own period, duty cycle and polarity specified. However, the same counter is applied to all channels requesting the PWM output. The signal duty cycle is provided as a percentage of the PWM period. Its value should be between 0 and 100 0=inactive signal (0% duty cycle) and 100=always active signal (100% duty cycle).

The function GPT_UpdatePwmDutycycle() updates the PWM signal duty cycle of a particular GPT channel. The update will take effect on the end of PWM period. If it's called again before last update doesn't take effect, error will be returned.

The function GPT_PausePwm() pauses the PWM signal on particular GPT channel. This can be used to disable the PWM output when making changes to the PWM signal. Pause will also take effect on the end of PWM period, so check the return value to see if it's set correctly.

Typical use case

PWM output

Output a PWM signal on two GPT channels with different duty cycles. Periodically update the PWM signal duty cycle. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/gpt

Data Structures

struct  gpt_config_t
 GPT configuration structure. More...
 

Enumerations

enum  gpt_chnl_t {
  kGPT_Chnl_0 = 0U,
  kGPT_Chnl_1,
  kGPT_Chnl_2,
  kGPT_Chnl_3,
  kGPT_Chnl_4,
  kGPT_Chnl_5
}
 List of GPT channels. More...
 
enum  gpt_chnl_pol_t {
  kGPT_ChnlPol_Low = 0U,
  kGPT_ChnlPol_High
}
 GPT channel polarity. More...
 
enum  gpt_pwm_mode_t {
  kGPT_EdgeAlignedPwm = 0U,
  kGPT_CenterAlignedPwm
}
 GPT PWM operation modes. More...
 
enum  gpt_input_capture_edge_t {
  kGPT_RisingEdge = 0U,
  kGPT_FallingEdge
}
 GPT input capture edge. More...
 
enum  gpt_input_capture_filter_t {
  kGPT_InputCapFilter_None = 0U,
  kGPT_InputCapFilter_2Cycles,
  kGPT_InputCapFilter_3Cycles,
  kGPT_InputCapFilter_4Cycles,
  kGPT_InputCapFilter_5Cycles,
  kGPT_InputCapFilter_6Cycles,
  kGPT_InputCapFilter_7Cycles
}
 GPT input capture edge. More...
 
enum  gpt_clock_source_t {
  kGPT_SystemClock = 0U,
  kGPT_ExternalClock
}
 GPT clock source selection. More...
 
enum  gpt_clock_div_t {
  kGPT_ClkDiv_Divide_1 = 0U,
  kGPT_ClkDiv_Divide_2,
  kGPT_ClkDiv_Divide_4,
  kGPT_ClkDiv_Divide_8,
  kGPT_ClkDiv_Divide_16,
  kGPT_ClkDiv_Divide_32,
  kGPT_ClkDiv_Divide_64,
  kGPT_ClkDiv_Divide_128,
  kGPT_ClkDiv_Divide_256,
  kGPT_ClkDiv_Divide_512,
  kGPT_ClkDiv_Divide_1024,
  kGPT_ClkDiv_Divide_2048,
  kGPT_ClkDiv_Divide_4096,
  kGPT_ClkDiv_Divide_8192,
  kGPT_ClkDiv_Divide_16384,
  kGPT_ClkDiv_Divide_32768
}
 GPT clock divider factor selection for the clock source. More...
 
enum  gpt_interrupt_enable_t {
  kGPT_Chnl0InterruptEnable = (1U << 0),
  kGPT_Chnl1InterruptEnable = (1U << 1),
  kGPT_Chnl2InterruptEnable = (1U << 2),
  kGPT_Chnl3InterruptEnable = (1U << 3),
  kGPT_Chnl4InterruptEnable = (1U << 4),
  kGPT_Chnl5InterruptEnable = (1U << 5),
  kGPT_Chnl0ErrInterruptEnable = (1U << 8),
  kGPT_Chnl1ErrInterruptEnable = (1U << 9),
  kGPT_Chnl2ErrInterruptEnable = (1U << 10),
  kGPT_Chnl3ErrInterruptEnable = (1U << 11),
  kGPT_Chnl4ErrInterruptEnable = (1U << 12),
  kGPT_Chnl5ErrInterruptEnable = (1U << 13),
  kGPT_TimeOverflowInterruptEnable = (1U << 16),
  kGPT_Dma0OverflowInterruptEnable = (1U << 24),
  kGPT_Dma1OverflowInterruptEnable = (1U << 25),
  kGPT_AllInterruptsEnable = 0x3013F3FUL
}
 List of GPT interrupts. More...
 
enum  gpt_status_flags_t {
  kGPT_Chnl0Flag = (1U << 0),
  kGPT_Chnl1Flag = (1U << 1),
  kGPT_Chnl2Flag = (1U << 2),
  kGPT_Chnl3Flag = (1U << 3),
  kGPT_Chnl4Flag = (1U << 4),
  kGPT_Chnl5Flag = (1U << 5),
  kGPT_Chnl0ErrFlag = (1U << 8),
  kGPT_Chnl1ErrFlag = (1U << 9),
  kGPT_Chnl2ErrFlag = (1U << 10),
  kGPT_Chnl3ErrFlag = (1U << 11),
  kGPT_Chnl4ErrFlag = (1U << 12),
  kGPT_Chnl5ErrFlag = (1U << 13),
  kGPT_TimeOverflowFlag = (1U << 16),
  kGPT_Dma0OverflowFlag = (1U << 24),
  kGPT_Dma1OverflowFlag = (1U << 25),
  kGPT_AllFlags = 0x3013F3FUL
}
 List of GPT flags. More...
 
enum  gpt_cnt_update_mode_t {
  kGPT_CntUpdateMode_Normal = 0U,
  kGPT_CntUpdateMode_Fast = 1U,
  kGPT_CntUpdateMode_Off = 3U
}
 GPT counter update mode. More...
 
enum  gpt_input_capture_div_t {
  kGPT_SampClkDiv_Divide_1 = 0U,
  kGPT_SampClkDiv_Divide_2,
  kGPT_SampClkDiv_Divide_4,
  kGPT_SampClkDiv_Divide_8,
  kGPT_SampClkDiv_Divide_16,
  kGPT_SampClkDiv_Divide_32,
  kGPT_SampClkDiv_Divide_64,
  kGPT_SampClkDiv_Divide_128
}
 GPT sample clock divider factor selection. More...
 

Driver version

#define FSL_GPT_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 GPT driver version 2.0.0. More...
 

Initialization and deinitialization

status_t GPT_Init (GPT_Type *base, const gpt_config_t *config)
 Ungates the GPT clock and configures the peripheral for basic operation. More...
 
void GPT_Deinit (GPT_Type *base)
 Gates the GPT clock. More...
 
void GPT_GetDefaultConfig (gpt_config_t *config)
 Fills in the GPT configuration structure with the default settings. More...
 

Channel mode operations

void GPT_SetupInputCapture (GPT_Type *base, gpt_chnl_t chnlNumber, gpt_input_capture_edge_t captureMode)
 Enables capturing an input signal on the channel using the function parameters. More...
 
void GPT_TriggerInputCapture (GPT_Type *base, gpt_chnl_t chnlNumber)
 Trigger input capturing by software. More...
 
uint32_t GPT_GetCapturedValue (GPT_Type *base, gpt_chnl_t chnlNumber)
 Get captured value. More...
 
void GPT_SetupOneshotPulse (GPT_Type *base, gpt_chnl_t chnlNumber, gpt_chnl_pol_t pol, uint32_t delayTicks, uint32_t dutyTicks)
 Configures one-shot pulse on the channel. More...
 
void GPT_SetupOneshotEdge (GPT_Type *base, gpt_chnl_t chnlNumber, gpt_chnl_pol_t pol, uint32_t delayTicks)
 Configures one-shot edge on the channel. More...
 
status_t GPT_SetupPwm (GPT_Type *base, gpt_chnl_t chnlNumber, gpt_chnl_pol_t pol, uint32_t dutyPercent, gpt_pwm_mode_t mode, uint32_t pwmFreq_Hz, uint32_t srcClock_Hz)
 Configures the PWM signal parameters. More...
 
status_t GPT_SetupPwmMode (GPT_Type *base, gpt_chnl_t chnlNumber, gpt_chnl_pol_t pol, uint32_t periodTicks, uint32_t dutyTicks, gpt_pwm_mode_t mode)
 Configures the PWM mode parameters. More...
 
status_t GPT_UpdatePwmDutycycle (GPT_Type *base, gpt_chnl_t chnlNumber, uint8_t dutyPercent)
 Updates the duty cycle of an active PWM signal. More...
 
status_t GPT_PausePwm (GPT_Type *base, gpt_chnl_t chnlNumber)
 Pause the PWM signal. More...
 

Interrupt Interface

void GPT_EnableInterrupts (GPT_Type *base, uint32_t mask)
 Enables the selected GPT interrupts. More...
 
void GPT_DisableInterrupts (GPT_Type *base, uint32_t mask)
 Disables the selected GPT interrupts. More...
 
uint32_t GPT_GetEnabledInterrupts (GPT_Type *base)
 Gets the enabled GPT interrupts. More...
 

Status Interface

uint32_t GPT_GetStatusFlags (GPT_Type *base)
 Gets the GPT status flags. More...
 
void GPT_ClearStatusFlags (GPT_Type *base, uint32_t mask)
 Clears the GPT status flags. More...
 

Read and write the timer period

void GPT_SetTimerPeriod (GPT_Type *base, uint32_t ticks)
 Sets the timer period in units of ticks for the GPT instance. More...
 
uint32_t GPT_GetCurrentTimerCount (GPT_Type *base)
 Reads the current timer counting value. More...
 

Timer Start and Stop

void GPT_StartTimer (GPT_Type *base)
 Starts the GPT counter. More...
 
void GPT_StopTimer (GPT_Type *base)
 Stops the GPT counter. More...
 
void GPT_ResetTimer (GPT_Type *base)
 Performs a GPT counter reset. More...
 

Data Structure Documentation

struct gpt_config_t

This structure holds the configuration settings for the GPT peripheral. To initialize this structure to reasonable defaults, call the GPT_GetDefaultConfig() function and pass a pointer to the configuration structure instance.

The configuration structure can be made constant so as to reside in flash.

Data Fields

gpt_clock_source_t src
 GPT clock source selection. More...
 
gpt_clock_div_t div
 GPT clock divider value for counter. More...
 
uint8_t prescale
 GPT clock prescale value for counter, divided by (prescale + 1)
 
gpt_cnt_update_mode_t cntUpdateMode
 Counter value update mode. More...
 
bool stopCntInDebug
 true: In debug mode, stop the counters. More...
 
uint32_t cntUppVal
 If counter reaches this value, the counter will overflow to 0. More...
 
gpt_input_capture_div_t icDiv
 Input capture sample clock divider. More...
 
gpt_input_capture_filter_t icFilter
 Input capture filter cycles in sampling ticks. More...
 

Field Documentation

gpt_clock_source_t gpt_config_t::src
gpt_clock_div_t gpt_config_t::div
gpt_cnt_update_mode_t gpt_config_t::cntUpdateMode
bool gpt_config_t::stopCntInDebug

false: In debug mode, counters are not affected.

uint32_t gpt_config_t::cntUppVal
gpt_input_capture_div_t gpt_config_t::icDiv
gpt_input_capture_filter_t gpt_config_t::icFilter

Macro Definition Documentation

#define FSL_GPT_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))

Enumeration Type Documentation

enum gpt_chnl_t
Note
Actual number of available channels is SoC dependent
Enumerator
kGPT_Chnl_0 

GPT channel number 0.

kGPT_Chnl_1 

GPT channel number 1.

kGPT_Chnl_2 

GPT channel number 2.

kGPT_Chnl_3 

GPT channel number 3.

kGPT_Chnl_4 

GPT channel number 4.

kGPT_Chnl_5 

GPT channel number 5.

Enumerator
kGPT_ChnlPol_Low 

Output state reset to 0.

kGPT_ChnlPol_High 

Output state reset to 1.

Enumerator
kGPT_EdgeAlignedPwm 

Edge-aligned PWM.

kGPT_CenterAlignedPwm 

Center-aligned PWM.

Enumerator
kGPT_RisingEdge 

Capture on rising edge only.

kGPT_FallingEdge 

Capture on falling edge only.

Enumerator
kGPT_InputCapFilter_None 

No filter.

kGPT_InputCapFilter_2Cycles 

Filter 2 consecutive cycles.

kGPT_InputCapFilter_3Cycles 

Filter 3 consecutive cycles.

kGPT_InputCapFilter_4Cycles 

Filter 4 consecutive cycles.

kGPT_InputCapFilter_5Cycles 

Filter 5 consecutive cycles.

kGPT_InputCapFilter_6Cycles 

Filter 6 consecutive cycles.

kGPT_InputCapFilter_7Cycles 

Filter 7 consecutive cycles.

Enumerator
kGPT_SystemClock 

System clock from PMU selected.

kGPT_ExternalClock 

External clock from pad.

Enumerator
kGPT_ClkDiv_Divide_1 

Divide by 1.

kGPT_ClkDiv_Divide_2 

Divide by 2.

kGPT_ClkDiv_Divide_4 

Divide by 4.

kGPT_ClkDiv_Divide_8 

Divide by 8.

kGPT_ClkDiv_Divide_16 

Divide by 16.

kGPT_ClkDiv_Divide_32 

Divide by 32.

kGPT_ClkDiv_Divide_64 

Divide by 64.

kGPT_ClkDiv_Divide_128 

Divide by 128.

kGPT_ClkDiv_Divide_256 

Divide by 256.

kGPT_ClkDiv_Divide_512 

Divide by 512.

kGPT_ClkDiv_Divide_1024 

Divide by 1024.

kGPT_ClkDiv_Divide_2048 

Divide by 2048.

kGPT_ClkDiv_Divide_4096 

Divide by 4096.

kGPT_ClkDiv_Divide_8192 

Divide by 8192.

kGPT_ClkDiv_Divide_16384 

Divide by 16384.

kGPT_ClkDiv_Divide_32768 

Divide by 32768.

Enumerator
kGPT_Chnl0InterruptEnable 

Channel 0 interrupt.

kGPT_Chnl1InterruptEnable 

Channel 1 interrupt.

kGPT_Chnl2InterruptEnable 

Channel 2 interrupt.

kGPT_Chnl3InterruptEnable 

Channel 3 interrupt.

kGPT_Chnl4InterruptEnable 

Channel 4 interrupt.

kGPT_Chnl5InterruptEnable 

Channel 5 interrupt.

kGPT_Chnl0ErrInterruptEnable 

Channel 0 error interrupt.

kGPT_Chnl1ErrInterruptEnable 

Channel 1 error interrupt.

kGPT_Chnl2ErrInterruptEnable 

Channel 2 error interrupt.

kGPT_Chnl3ErrInterruptEnable 

Channel 3 error interrupt.

kGPT_Chnl4ErrInterruptEnable 

Channel 4 error interrupt.

kGPT_Chnl5ErrInterruptEnable 

Channel 5 error interrupt.

kGPT_TimeOverflowInterruptEnable 

Time overflow interrupt.

kGPT_Dma0OverflowInterruptEnable 

DMA0 overflow interrupt.

kGPT_Dma1OverflowInterruptEnable 

DMA1 overflow interrupt.

kGPT_AllInterruptsEnable 

All interrupts.

Enumerator
kGPT_Chnl0Flag 

Channel 0 flag.

kGPT_Chnl1Flag 

Channel 1 flag.

kGPT_Chnl2Flag 

Channel 2 flag.

kGPT_Chnl3Flag 

Channel 3 flag.

kGPT_Chnl4Flag 

Channel 4 flag.

kGPT_Chnl5Flag 

Channel 5 flag.

kGPT_Chnl0ErrFlag 

Channel 0 error flag.

kGPT_Chnl1ErrFlag 

Channel 1 error flag.

kGPT_Chnl2ErrFlag 

Channel 2 error flag.

kGPT_Chnl3ErrFlag 

Channel 3 error flag.

kGPT_Chnl4ErrFlag 

Channel 4 error flag.

kGPT_Chnl5ErrFlag 

Channel 5 error flag.

kGPT_TimeOverflowFlag 

Time overflow flag.

kGPT_Dma0OverflowFlag 

DMA0 overflow flag.

kGPT_Dma1OverflowFlag 

DMA1 overflow flag.

kGPT_AllFlags 

All flags.

Enumerator
kGPT_CntUpdateMode_Normal 

Used in any ratio between counter clock and APB clock.

Every 3-4 counter ticks are updated to CNT_VAL

kGPT_CntUpdateMode_Fast 

Used when counter clock is at least 5 times slower than APB clock.

Every counter tick is updated to CNT_VAL

kGPT_CntUpdateMode_Off 

Do not update to CNT_VAL.

Enumerator
kGPT_SampClkDiv_Divide_1 

Divide by 1.

kGPT_SampClkDiv_Divide_2 

Divide by 2.

kGPT_SampClkDiv_Divide_4 

Divide by 4.

kGPT_SampClkDiv_Divide_8 

Divide by 8.

kGPT_SampClkDiv_Divide_16 

Divide by 16.

kGPT_SampClkDiv_Divide_32 

Divide by 32.

kGPT_SampClkDiv_Divide_64 

Divide by 64.

kGPT_SampClkDiv_Divide_128 

Divide by 128.

Function Documentation

status_t GPT_Init ( GPT_Type *  base,
const gpt_config_t *  config 
)
Note
This API should be called at the beginning of the application which is using the GPT driver. If the GPT instance has only TPM features, please use the TPM driver.
Parameters
baseGPT peripheral base address
configPointer to the user configuration structure.
Returns
kStatus_Success indicates success; Else indicates failure.
void GPT_Deinit ( GPT_Type *  base)
Parameters
baseGPT peripheral base address
void GPT_GetDefaultConfig ( gpt_config_t *  config)

The default values are:

* config->src = kGPT_SystemClock;
* config->div = kGPT_ClkDiv_Divide_1;
* config->prescale = 0U;
* config->cntUpdateMode = kGPT_CntUpdateMode_Normal;
* config->stopCntInDebug = true;
* config->cntUppVal = 0xFFFFFFFFU;
* config->icDiv = kGPT_SampClkDiv_Divide_1;
* config->icFilter = kGPT_InputCapFilter_None;
*
Parameters
configPointer to the user configuration structure.
void GPT_SetupInputCapture ( GPT_Type *  base,
gpt_chnl_t  chnlNumber,
gpt_input_capture_edge_t  captureMode 
)

When the edge specified in the captureMode argument occurs on the channel, the GPT counter is captured into the CMR0 register. The user has to read the CMR0 register separately to get this value.

Parameters
baseGPT peripheral base address
chnlNumberThe channel number
captureModeSpecifies which edge to capture
void GPT_TriggerInputCapture ( GPT_Type *  base,
gpt_chnl_t  chnlNumber 
)

Edge and filter is ignored.

Parameters
baseGPT peripheral base address
chnlNumberThe channel number
uint32_t GPT_GetCapturedValue ( GPT_Type *  base,
gpt_chnl_t  chnlNumber 
)
Parameters
baseGPT peripheral base address
chnlNumberThe channel number
Returns
The captured counter value.
void GPT_SetupOneshotPulse ( GPT_Type *  base,
gpt_chnl_t  chnlNumber,
gpt_chnl_pol_t  pol,
uint32_t  delayTicks,
uint32_t  dutyTicks 
)
Parameters
baseGPT peripheral base address
chnlNumberThe channel number
polChannel output polarity reset value.
delayTicksDelay width before triggering the pulse, the uint of this value is timer ticks.
dutyTicksPulse width, the uint of this value is timer ticks.
void GPT_SetupOneshotEdge ( GPT_Type *  base,
gpt_chnl_t  chnlNumber,
gpt_chnl_pol_t  pol,
uint32_t  delayTicks 
)
Parameters
baseGPT peripheral base address
chnlNumberThe channel number
polChannel output polarity reset value.
delayTicksDelay width before changing the edge, the uint of this value is timer ticks.
status_t GPT_SetupPwm ( GPT_Type *  base,
gpt_chnl_t  chnlNumber,
gpt_chnl_pol_t  pol,
uint32_t  dutyPercent,
gpt_pwm_mode_t  mode,
uint32_t  pwmFreq_Hz,
uint32_t  srcClock_Hz 
)

Call this function to configure the PWM signal period, mode, duty cycle, and edge. Use this function to configure all GPT channels that are used to output a PWM signal.

Parameters
baseGPT peripheral base address
chnlNumberThe channel number.
polPWM output polarity reset value.
dutyPercentPWM pulse width, value should be between 0 to 100
modePWM operation mode, options available in enumeration gpt_pwm_mode_t
pwmFreq_HzPWM signal frequency in Hz
srcClock_HzGPT counter clock in Hz
Returns
kStatus_Success if the PWM setup was successful kStatus_Error on failure
status_t GPT_SetupPwmMode ( GPT_Type *  base,
gpt_chnl_t  chnlNumber,
gpt_chnl_pol_t  pol,
uint32_t  periodTicks,
uint32_t  dutyTicks,
gpt_pwm_mode_t  mode 
)

Call this function to configure the PWM signal mode, duty cycle in ticks, and edge. Use this function to configure all GPT channels that are used to output a PWM signal. Please note that: This API is similar with GPT_SetupPwm() API, but will not set the timer period, and this API will set channel match value in timer ticks, not period percent.

Parameters
baseGPT peripheral base address
chnlNumberThe channel number.
polPWM output polarity reset value.
periodTicksPWM period width, the uint of this value is timer ticks.
dutyTicksPWM pulse width, the uint of this value is timer ticks.
modePWM operation mode, options available in enumeration gpt_pwm_mode_t
Returns
kStatus_Success if the PWM setup was successful kStatus_Error on failure
status_t GPT_UpdatePwmDutycycle ( GPT_Type *  base,
gpt_chnl_t  chnlNumber,
uint8_t  dutyPercent 
)
Parameters
baseGPT peripheral base address
chnlNumberThe channel number.
dutyPercentNew PWM pulse width; The value should be between 0 to 100 0=inactive signal(0% duty cycle)... 100=active signal (100% duty cycle)
Returns
kStatus_Success if the PWM update was successful kStatus_Error on failure
status_t GPT_PausePwm ( GPT_Type *  base,
gpt_chnl_t  chnlNumber 
)
Parameters
baseGPT peripheral base address
chnlNumberThe channel number.
Returns
kStatus_Success if the PWM update was successful kStatus_Error on failure
void GPT_EnableInterrupts ( GPT_Type *  base,
uint32_t  mask 
)
Parameters
baseGPT peripheral base address
maskThe interrupts to enable. This is a logical OR of members of the enumeration gpt_interrupt_enable_t
void GPT_DisableInterrupts ( GPT_Type *  base,
uint32_t  mask 
)
Parameters
baseGPT peripheral base address
maskThe interrupts to enable. This is a logical OR of members of the enumeration gpt_interrupt_enable_t
uint32_t GPT_GetEnabledInterrupts ( GPT_Type *  base)
Parameters
baseGPT peripheral base address
Returns
The enabled interrupts. This is the logical OR of members of the enumeration gpt_interrupt_enable_t
uint32_t GPT_GetStatusFlags ( GPT_Type *  base)
Parameters
baseGPT peripheral base address
Returns
The status flags. This is the logical OR of members of the enumeration gpt_status_flags_t
void GPT_ClearStatusFlags ( GPT_Type *  base,
uint32_t  mask 
)
Parameters
baseGPT peripheral base address
maskThe status flags to clear. This is a logical OR of members of the enumeration gpt_status_flags_t
void GPT_SetTimerPeriod ( GPT_Type *  base,
uint32_t  ticks 
)

Timers counts from 0 until it equals the count value set here. The count value is written to the CNT_UPP_VAL register. The period update take effects during the next counter-reach-upper event. To guarantee an immediate update, use GPT_ResetTimer() after setting the period.

Note
Call the utility macros provided in the fsl_common.h to convert usec or msec to ticks.
Parameters
baseGPT peripheral base address
ticksA timer period in units of ticks, which should be equal or greater than 1.
uint32_t GPT_GetCurrentTimerCount ( GPT_Type *  base)

This function returns the real-time timer counting value in a range from 0 to a timer period.

Note
Call the utility macros provided in the fsl_common.h to convert ticks to usec or msec.
Parameters
baseGPT peripheral base address
Returns
The current counter value in ticks
void GPT_StartTimer ( GPT_Type *  base)
Parameters
baseGPT peripheral base address
void GPT_StopTimer ( GPT_Type *  base)
Parameters
baseGPT peripheral base address
void GPT_ResetTimer ( GPT_Type *  base)
Parameters
baseGPT peripheral base address