MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

The MCUXpresso SDK provides a peripheral driver for the Inter-Integrated Circuit (I2C) module of MCUXpresso SDK devices.

The I2C driver includes functional APIs and transactional APIs.

Functional APIs target the low-level APIs. Functional APIs can be used for the I2C master/slave initialization/configuration/operation for optimization/customization purpose. Using the functional APIs requires knowing the I2C master peripheral and how to organize functional APIs to meet the application requirements. The I2C functional operation groups provide the functional APIs set.

Transactional APIs target the high-level APIs. The transactional APIs can be used to enable the peripheral quickly and also in the application if the code size and performance of transactional APIs satisfy the requirements. If the code size and performance are critical requirements, see the transactional API implementation and write custom code using the functional APIs or accessing the hardware registers.

Transactional APIs support asynchronous transfer. This means that the functions I2C_MasterTransferNonBlocking() set up the interrupt non-blocking transfer. When the transfer completes, the upper layer is notified through a callback function with the status.

Typical use case

Master Operation in functional method

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/i2c

Master Operation in interrupt transactional method

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/i2c

Master Operation in DMA transactional method

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/i2c

Slave Operation in functional method

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/i2c

Slave Operation in interrupt transactional method

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/i2c

Data Structures

struct  i2c_master_config_t
 I2C master configuration structure. More...
 
struct  i2c_slave_config_t
 I2C slave configuration structure. More...
 
struct  i2c_master_transfer_t
 I2C master transfer configuration structure. More...
 
struct  i2c_master_handle_t
 I2C master transfer handle. More...
 
struct  i2c_slave_transfer_t
 I2C slave transfer configuration structure. More...
 
struct  i2c_slave_handle_t
 I2C slave transfer handle. More...
 

Macros

#define I2C_RETRY_TIMES   0U /* Default defines to zero, driver keeps checking status flag untill it changes. */
 Retry times when checking status flags. More...
 

Typedefs

typedef void(* i2c_master_transfer_callback_t )(I2C_Type *base, i2c_master_handle_t *handle, status_t completionStatus, void *userData)
 I2C master transfer callback function definition. More...
 
typedef void(* i2c_slave_transfer_callback_t )(I2C_Type *base, i2c_slave_transfer_t *transfer, void *userData)
 I2C slave transfer callback function definition. More...
 
typedef void(* i2c_isr_t )(I2C_Type *base, void *i2cHandle)
 brief Typedef for interrupt handler. More...
 

Enumerations

enum  {
  kStatus_I2C_Busy = MAKE_STATUS(kStatusGroup_I2C, 0),
  kStatus_I2C_Idle = MAKE_STATUS(kStatusGroup_I2C, 1),
  kStatus_I2C_Nak = MAKE_STATUS(kStatusGroup_I2C, 2),
  kStatus_I2C_ArbitrationLost = MAKE_STATUS(kStatusGroup_I2C, 3),
  kStatus_I2C_Timeout,
  kStatus_I2C_Addr_Nak = MAKE_STATUS(kStatusGroup_I2C, 5),
  kStatus_I2C_GeneralCall_Nak,
  kStatus_I2C_RxHardwareOverrun = MAKE_STATUS(kStatusGroup_I2C, 7),
  kStatus_I2C_TxFifoFlushed = MAKE_STATUS(kStatusGroup_I2C, 8)
}
 I2C API status codes, used by bus operation APIs and transactional APIs as return value to indicate the bus's current status as the API's execution result, or used in the callback to indicate transfer results. More...
 
enum  _i2c_status_flags {
  kI2C_RxUnderflowInterruptFlag,
  kI2C_RxOverflowInterruptFlag,
  kI2C_RxDataReadyInterruptFlag,
  kI2C_TxOverflowInterruptFlag = I2C_IC_RAW_INTR_STAT_TX_OVER_MASK,
  kI2C_TxRequestInterruptFlag,
  kI2C_TxAbortInterruptFlag = I2C_IC_RAW_INTR_STAT_TX_ABRT_MASK,
  kI2C_BusBusyInterruptFlag,
  kI2C_StopDetectInterruptFlag,
  kI2C_StartDetectInterruptFlag,
  kI2C_ActiveFlag,
  kI2C_TxFifoNotFullFlag = I2C_IC_STATUS_TFNF_MASK << 25U,
  kI2C_TxFifoEmptyFlag = I2C_IC_STATUS_TFE_MASK << 25U,
  kI2C_RxFifoNotEmptyFlag = I2C_IC_STATUS_RFNE_MASK << 25U,
  kI2C_RxFifoFullFlag = I2C_IC_STATUS_RFF_MASK << 25U
}
 I2C common hardware status flags. More...
 
enum  _i2c_master_status_flags {
  kI2C_Master7bitAddressNackFlag,
  kI2C_Master10bitAddressNack1Flag,
  kI2C_Master10bitAddressNack2Flag,
  kI2C_MasterDataNackFlag,
  kI2C_MasterGeneralCallNackFlag,
  kI2C_MasterGeneralCallReadFlag,
  kI2C_MasterHighSpeedCodeAckFlag,
  kI2C_MasterStartByteAckFlag,
  kI2C_MasterHighSpeedRestartDisabledFlag,
  kI2C_MasterStartWithRestartDisabledFlag,
  kI2C_Master10bitAddressReadRestartDisabledFlag,
  kI2C_MasterOperateWhenDisabledFlag,
  kI2C_MasterArbitrationLostFlag,
  kI2C_MasterActiveFlag,
  kI2C_MasterAutoClearFlags,
  kI2C_MasterAllClearFlags
}
 I2C master hardware status flags. More...
 
enum  _i2c_slave_status_flags {
  kI2C_SlaveReadRequestInterruptFlag,
  kI2C_SlaveNackInterruptFlag,
  kI2C_SlaveGeneralCallAckInterruptFlag,
  kI2C_SlaveFlushTxFifoFlag,
  kI2C_SlaveArbitrationLostFlag,
  kI2C_SlaveReadWhenRequestedDataFlag,
  kI2C_SlaveDisabledWhileBusy = I2C_IC_ENABLE_STATUS_SLV_DISABLED_WHILE_BUSY_MASK << 16U,
  kI2C_SlaveRxDataLost,
  kI2C_SlaveActiveFlag,
  kI2C_SlaveAutoClearFlags,
  kI2C_SlaveAllClearFlags
}
 I2C slave hardware status flags. More...
 
enum  _i2c_interrupt_enable {
  kI2C_RxUnderflowInterruptEnable = I2C_IC_INTR_MASK_M_RX_UNDER_MASK,
  kI2C_RxOverflowInterruptEnable = I2C_IC_INTR_MASK_M_RX_OVER_MASK,
  kI2C_RxDataReadyInterruptEnable = I2C_IC_INTR_MASK_M_RX_FULL_MASK,
  kI2C_TxOverflowInterruptEnable = I2C_IC_INTR_MASK_M_TX_OVER_MASK,
  kI2C_TxRequestInterruptEnable = I2C_IC_INTR_MASK_M_TX_EMPTY_MASK,
  kI2C_SlaveReadRequestInterruptEnable,
  kI2C_TxAbortInterruptEnable = I2C_IC_INTR_MASK_M_TX_ABRT_MASK,
  kI2C_SlaveNackInterruptEnable = I2C_IC_INTR_MASK_M_RX_DONE_MASK,
  kI2C_BusBusyInterruptEnable = I2C_IC_INTR_MASK_M_ACTIVITY_MASK,
  kI2C_StopDetectInterruptEnable,
  kI2C_StartDetectInterruptEnable,
  kI2C_SlaveGeneralCallAckInterruptEnable
}
 I2C interrupt enable/disable source. More...
 
enum  i2c_master_speed_mode_t {
  kI2C_MasterSpeedStandard = 0x1U,
  kI2C_MasterSpeedFast = 0X2U,
  kI2C_MasterSpeedHigh = 0X3U
}
 Master speed mode. More...
 
enum  i2c_address_mode_t {
  kI2C_AddressMatch7bit = 0x0U,
  kI2C_AddressMatch10bit = 0X1U
}
 Addressing mode, normal 7-bit address or 10-bit address. More...
 
enum  _i2c_dma_enable_flags {
  kQSPI_DmaRx = 0x1U,
  kQSPI_DmaTx = 0x2U
}
 I2C DMA configuration for Transmit and Receive. More...
 
enum  i2c_direction_t {
  kI2C_Write = 0U,
  kI2C_Read = 1U
}
 Master transfer direction. More...
 
enum  i2c_slave_transfer_event_t {
  kI2C_SlaveStartDetectEvent = 0x01U,
  kI2C_SlaveGenaralcallEvent = 0x02U,
  kI2C_SlaveTransmitEvent = 0x04U,
  kI2C_SlaveReceiveEvent = 0x08U,
  kI2C_SlaveCompletionEvent,
  kI2C_SlaveAllEvents
}
 Set of slave transfer events. More...
 

Functions

uint32_t I2C_GetInstance (I2C_Type *base)
 Gets instance number for I2C module. More...
 

Variables

const IRQn_Type s_I2cIrqs []
 Pointers to i2c IRQ number for each instance. More...
 
void * s_i2cHandles []
 Pointers to i2c handles for each instance. More...
 
i2c_isr_t s_i2cMasterIsr
 Pointer to master IRQ handler for each instance. More...
 

Driver version

#define FSL_I2C_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))
 

Hardware Status Flags Sub-group

static uint32_t I2C_MasterGetStatusFlags (I2C_Type *base)
 Gets the I2C master hardware status flags. More...
 
void I2C_MasterClearStatusFlags (I2C_Type *base, uint32_t statusFlags)
 Clears the I2C master status flags. More...
 
static uint32_t I2C_SlaveGetStatusFlags (I2C_Type *base)
 Gets the I2C slave hardware status flags. More...
 
void I2C_SlaveClearStatusFlags (I2C_Type *base, uint32_t statusFlags)
 Clears the I2C slave status flags. More...
 

Interrupt Sub-group

static void I2C_EnableInterrupts (I2C_Type *base, uint16_t interrupts)
 Enables I2C interrupt source. More...
 
static void I2C_DisableInterrupts (I2C_Type *base, uint16_t interrupts)
 Disables I2C interrupt source. More...
 
static uint16_t I2C_GetEnabledInterrupts (I2C_Type *base)
 Get all the enabled interrupt sources. More...
 

Module Init/Deinit Sub-group

void I2C_MasterGetDefaultConfig (i2c_master_config_t *masterConfig)
 Sets the I2C master configuration structure to default values. More...
 
void I2C_MasterInit (I2C_Type *base, const i2c_master_config_t *masterConfig, uint32_t sourceClock_Hz)
 Initializes the I2C peripheral to operate as master. More...
 
void I2C_MasterDeinit (I2C_Type *base)
 De-initializes the I2C peripheral. More...
 
void I2C_SlaveGetDefaultConfig (i2c_slave_config_t *slaveConfig)
 Sets the I2C slave configuration structure to default values. More...
 
void I2C_SlaveInit (I2C_Type *base, const i2c_slave_config_t *slaveConfig)
 Initializes the I2C peripheral to operate as slave. More...
 
void I2C_SlaveDeinit (I2C_Type *base)
 De-initializes the I2C peripheral. More...
 

Common Peripheral Configuration Sub-group

static void I2C_SetRxWaterMark (I2C_Type *base, uint8_t rxWaterMark)
 Sets I2C rx FIFO watermark. More...
 
static void I2C_SetTxWaterMark (I2C_Type *base, uint8_t txWaterMark)
 Sets I2C tx FIFO watermark. More...
 
static void I2C_Enable (I2C_Type *base, bool enable)
 Enables or disables the I2C module. More...
 
static void I2C_EnableMaster (I2C_Type *base, bool enable)
 Enables the I2C module as master or slave. More...
 
static uint8_t I2C_GetTxFifoDataCount (I2C_Type *base)
 Gets the data count in tx FIFO. More...
 
static uint8_t I2C_GetRxFifoDataCount (I2C_Type *base)
 Gets the data count in rx FIFO. More...
 
static uint8_t I2C_GetTxFifoDepth (I2C_Type *base)
 Gets tx FIFO depth. More...
 
static uint8_t I2C_GetRxFifoDepth (I2C_Type *base)
 Gets rx FIFO depth. More...
 
static void I2C_SetSdaHoldTime (I2C_Type *base, uint16_t sdaHoldTime)
 Sets I2C SDA hold time. More...
 
static void I2C_SetSdaSetupTime (I2C_Type *base, uint16_t sdaSetupTime)
 Sets I2C SDA setup time. More...
 
static void I2C_EnableAckGeneralCall (I2C_Type *base, bool enable)
 Enables I2C module to response ack to general call. More...
 
static bool I2C_IsEnabled (I2C_Type *base)
 Returns whether the I2C module is enabled. More...
 
static void I2C_SetGlitchFilter (I2C_Type *base, uint8_t glitchFilter)
 Sets I2C glitch filter width of normal and fast mode. More...
 
static void I2C_SetGlitchFilterHighSpeed (I2C_Type *base, uint8_t glitchFilter)
 Sets I2C glitch filter width of high speed mode. More...
 

Master Peripheral Configuration Sub-group

static void I2C_MasterSetHighSpeedAddress (I2C_Type *base, uint8_t address)
 Sets I2C master high speed mode address. More...
 
static bool I2C_IsMaster (I2C_Type *base)
 Returns whether the I2C module is in master mode. More...
 
static void I2C_MasterSetAddressingMode (I2C_Type *base, i2c_address_mode_t addressingMode)
 Sets I2C master addressing mode. More...
 
static void I2C_MasterSetTargetAddress (I2C_Type *base, uint16_t address)
 Sets target address for I2C master transaction. More...
 
static void I2C_MasterEnableGeneralCall (I2C_Type *base, bool enable)
 Choose whether to perform general call command. More...
 
void I2C_MasterSetSpeedMode (I2C_Type *base, i2c_master_speed_mode_t speed, uint32_t sourceClock_Hz)
 Sets the I2C transaction speed mode. More...
 

Slave Peripheral Configuration Sub-group

static bool I2C_IsSlave (I2C_Type *base)
 Returns whether the I2C module is in slave mode. More...
 
static void I2C_SlaveSetAddressingMode (I2C_Type *base, i2c_address_mode_t addressingMode, uint16_t address)
 Sets I2C slave addressing mode and address. More...
 

Common Bus Operation Sub-Group

static uint8_t I2C_ReadByte (I2C_Type *base)
 Reads one byte from data register directly. More...
 
static void I2C_WriteByte (I2C_Type *base, uint8_t data)
 Writes one byte to the data register directly. More...
 

DMA Configuration Sub-Group

static void I2C_EnableDMA (I2C_Type *base, uint8_t mask)
 Disables the I2C DMA requests. More...
 
static void I2C_DisableDMA (I2C_Type *base, uint8_t mask)
 Enables the I2C DMA requests. More...
 
static void I2C_SetDmaTxWaterMark (I2C_Type *base, uint8_t txLevel)
 Sets I2C tx DMA trigger level. More...
 
static void I2C_SetDmaRxWaterMark (I2C_Type *base, uint8_t rxLevel)
 Sets I2C rx DMA trigger level. More...
 
static uint32_t I2C_GetDataRegAddr (I2C_Type *base)
 Gets I2C read/write register address. More...
 

Master Bus Operation Sub-Group

static void I2C_MasterWriteDummy (I2C_Type *base)
 Writes dummy data data register and issue read command to generate clock. More...
 
status_t I2C_MasterCheckAndClearError (I2C_Type *base, uint32_t status)
 Convert provided status flags to status code, and clear any errors if present. More...
 
status_t I2C_MasterWriteBlocking (I2C_Type *base, const uint8_t *data, size_t txSize)
 Sends a piece of data to I2C bus in master mode in blocking way. More...
 
status_t I2C_MasterReadBlocking (I2C_Type *base, uint8_t *data, size_t rxSize)
 Receives a piece of data from I2C bus in master mode in blocking way. More...
 

Slave Bus Operation Sub-Group

static void I2C_SlaveNackNextByte (I2C_Type *base, bool enable)
 Enables slave to send nack after receiving next byte of data. More...
 
status_t I2C_SlaveCheckAndClearError (I2C_Type *base, uint32_t status)
 Convert provided status flags to status code, and clear any errors if present. More...
 
status_t I2C_SlaveWriteBlocking (I2C_Type *base, const uint8_t *data, size_t txSize)
 Sends a piece of data to I2C bus in slave mode in blocking way. More...
 
status_t I2C_SlaveReadBlocking (I2C_Type *base, uint8_t *data, size_t rxSize)
 Receives a piece of data from I2C bus in slave mode in blocking way. More...
 

Master Transfer Sub-group

status_t I2C_MasterTransferBlocking (I2C_Type *base, i2c_master_transfer_t *transferConfig)
 Performs a master polling transfer on the I2C bus. More...
 
void I2C_MasterTransferCreateHandle (I2C_Type *base, i2c_master_handle_t *handle, i2c_master_transfer_callback_t callback, void *userData)
 Initializes the I2C master transfer in interrupt way. More...
 
status_t I2C_MasterTransferNonBlocking (I2C_Type *base, i2c_master_handle_t *handle, i2c_master_transfer_t *transfer)
 Initiates a master transfer on the I2C bus in interrupt way. More...
 
status_t I2C_MasterTransferGetCount (I2C_Type *base, i2c_master_handle_t *handle, size_t *count)
 Gets the master transfer count and status during a interrupt transfer. More...
 
void I2C_MasterTransferAbort (I2C_Type *base, i2c_master_handle_t *handle)
 Aborts an in-process transfer in interrupt way. More...
 

Slave Transfer Sub-group

void I2C_SlaveTransferCreateHandle (I2C_Type *base, i2c_slave_handle_t *handle, i2c_slave_transfer_callback_t callback, void *userData)
 Initializes the I2C slave transfer in interrupt way. More...
 
status_t I2C_SlaveTransferNonBlocking (I2C_Type *base, i2c_slave_handle_t *handle, uint8_t eventMask)
 Sets I2C slave ready to process bus events. More...
 
status_t I2C_SlaveTransferGetCount (I2C_Type *base, i2c_slave_handle_t *handle, size_t *count)
 Gets how many bytes slave have transferred in curent data buffer. More...
 
void I2C_SlaveTransferAbort (I2C_Type *base, i2c_slave_handle_t *handle)
 Aborts the slave transfer. More...
 

Data Structure Documentation

struct i2c_master_config_t

This structure includes all the master operation needed features, user can configure these features one by one manually, or call I2C_MasterGetDefaultConfig to set the structure to default value. Then, call I2C_MasterInit to initialize I2C module. After initialization, the I2C module can only operate as master. To deinitialize I2C, call I2C_MasterDeinit.

Data Fields

bool enable
 Enable the I2C peripheral as master during initialization. More...
 
i2c_master_speed_mode_t speed
 The speed I2C master operates. More...
 
i2c_address_mode_t addressingMode
 Addressing mode. More...
 
uint8_t highSpeedMasterCodeAddress
 Master code address in high speed mode, only 0-7 is avaliable. More...
 
uint8_t rxFifoWaterMark
 Rx FIFO watermark that controls the rx interrupt trigger level. More...
 
uint8_t txFifoWaterMark
 Tx FIFO watermark that controls the tx interrupt trigger level. More...
 
uint16_t dataHoldTime
 The number of clock source cycles of the data hold time tHD:DAT. More...
 
uint16_t dataSetupTime
 The number of clock source cycles of the data setup time tSU:DAT. More...
 
uint8_t glitchFilter
 The number of clock source cycles of the longest glitch to be filtered in standard and fast mode. More...
 
uint8_t glitchFilterHighSpeed
 The number of clock source cycles of the longest glitch to be filtered in high speed mode. More...
 

Field Documentation

bool i2c_master_config_t::enable

I2C_IC_CON[IC_SLAVE_DISABLE], I2C_IC_CON[master_mode], I2C_IC_ENABLE[ENABLE]

i2c_master_speed_mode_t i2c_master_config_t::speed

I2C_IC_CON[SPEED]

i2c_address_mode_t i2c_master_config_t::addressingMode

I2C_IC_TAR[IC_10BITADDR_MASTER]

uint8_t i2c_master_config_t::highSpeedMasterCodeAddress

I2C_IC_HS_MADDR[IC_HS_MAR]

uint8_t i2c_master_config_t::rxFifoWaterMark

I2C_IC_RX_TL[RX_TL]

uint8_t i2c_master_config_t::txFifoWaterMark

I2C_IC_TX_TL[TX_TL]

uint16_t i2c_master_config_t::dataHoldTime

I2C_IC_SDA_HOLD[IC_SDA_HOLD]

uint16_t i2c_master_config_t::dataSetupTime

I2C_IC_SDA_SETUP[SDA_SETUP]

uint8_t i2c_master_config_t::glitchFilter

I2C_IC_FS_SPKLEN[IC_FS_SPKLEN]

uint8_t i2c_master_config_t::glitchFilterHighSpeed

I2C_IC_HS_SPKLEN[IC_HS_SPKLEN]

struct i2c_slave_config_t

This structure includes all the slave operation needed features, user can configure these features one by one manually, or call I2C_SlaveGetDefaultConfig to set the structure to default value. Then, call I2C_SlaveInit to initialize I2C module. After initialization, the I2C module can only operate as slave. To deinitialize I2C, call I2C_SlaveDeinit.

Data Fields

bool enable
 Enable the I2C peripheral as slave during initialization. More...
 
i2c_address_mode_t addressingMode
 Addressing mode. More...
 
uint16_t slaveAddress
 Slave address. More...
 
uint8_t rxFifoWaterMark
 Rx FIFO watermark that controls the rx interrupt trigger level. More...
 
uint8_t txFifoWaterMark
 Tx FIFO watermark that controls the tx interrupt trigger level. More...
 
uint16_t dataHoldTime
 The number of clock source cycles of the data hold time tHD:DAT. More...
 
uint16_t dataSetupTime
 The number of clock source cycles of the data setup time tSU:DAT. More...
 
bool ackGeneralCall
 True to let slave response general call with Ack. More...
 
uint8_t glitchFilter
 The number of clock source cycles of the longest glitch to be filtered in standard and fast mode. More...
 
uint8_t glitchFilterHighSpeed
 The number of clock source cycles of the longest glitch to be filtered in high speed mode. More...
 

Field Documentation

bool i2c_slave_config_t::enable

I2C_IC_CON[IC_SLAVE_DISABLE], I2C_IC_CON[master_mode], I2C_IC_ENABLE[ENABLE]

i2c_address_mode_t i2c_slave_config_t::addressingMode

I2C_IC_CON[IC_10BITADDR_SLAVE]

uint16_t i2c_slave_config_t::slaveAddress

I2C_IC_SAR[IC_SAR]

uint8_t i2c_slave_config_t::rxFifoWaterMark

I2C_IC_RX_TL[RX_TL]

uint8_t i2c_slave_config_t::txFifoWaterMark

I2C_IC_TX_TL[TX_TL]

uint16_t i2c_slave_config_t::dataHoldTime

I2C_IC_SDA_HOLD[IC_SDA_HOLD]

uint16_t i2c_slave_config_t::dataSetupTime

I2C_IC_SDA_SETUP[SDA_SETUP]

bool i2c_slave_config_t::ackGeneralCall

I2C_IC_ACK_GENERAL_CALL[ACK_GEN_CALL]

uint8_t i2c_slave_config_t::glitchFilter

I2C_IC_FS_SPKLEN[IC_FS_SPKLEN]

uint8_t i2c_slave_config_t::glitchFilterHighSpeed

I2C_IC_HS_SPKLEN[IC_HS_SPKLEN]

struct i2c_master_transfer_t

This structure definition includes all the user configurable features, that are used to control single I2C transfer of master mode, in polling way or in interrupt way.

Data Fields

uint16_t slaveAddress
 7-bit slave address, set to 0 to issue general call. More...
 
i2c_direction_t direction
 Transfer direction, kI2C_Write or kI2C_Read. More...
 
uint32_t subaddress
 Pointer to command code. More...
 
size_t subaddressSize
 Size of the command code, max value 4. More...
 
uint8_t *volatile data
 Pointer to the send/receive data buffer. More...
 
volatile size_t dataSize
 Transfer size. More...
 

Field Documentation

uint16_t i2c_master_transfer_t::slaveAddress
i2c_direction_t i2c_master_transfer_t::direction
uint32_t i2c_master_transfer_t::subaddress
size_t i2c_master_transfer_t::subaddressSize
uint8_t* volatile i2c_master_transfer_t::data
volatile size_t i2c_master_transfer_t::dataSize
struct _i2c_master_handle

Forward declaration of the I2C master transfer handle structure.

Note
If user wants to use the transactional API to transfer data in interrupt way in master mode, one I2C instance should and can only be allocated one master handle.
The handle is maintained by I2C driver internally, which means the transfer state is retained and user shall not modify its state state in application level. If user only wish to use transactional APIs without understanding its machanism, it is not necessary to understand these members.

Data Fields

uint8_t state
 A transfer state maintained during transfer. More...
 
i2c_master_transfer_t transfer
 I2C master transfer structure. More...
 
size_t transmitSize
 Total bytes to be transferred. More...
 
size_t receiveSize
 Total bytes to be received. More...
 
i2c_master_transfer_callback_t completionCallback
 Callback function invoked when the transfer is finished. More...
 
void * userData
 User configurable pointer to any data, function, structure etc that user wish to use in the callback.
 

Field Documentation

uint8_t i2c_master_handle_t::state
i2c_master_transfer_t i2c_master_handle_t::transfer
size_t i2c_master_handle_t::transmitSize
size_t i2c_master_handle_t::receiveSize
i2c_master_transfer_callback_t i2c_master_handle_t::completionCallback
struct i2c_slave_transfer_t

Covers slave transfer data buffer pointer, data size and the events user want driver to alert.

Note
Unlike master who controls the transfer flow, slave has to monitor any bus event and change its configuration accordingly. So this slave transfer configuration structure is also used as second parameter of callback, for user to change the transfer configuration in the callback. The read-only member eEvent shows which event occured that causes the callback being invoked.

Data Fields

uint8_t *volatile data
 Pointer to the buffer of data to send, or to store received data. More...
 
volatile uint16_t dataSize
 Transfer size. More...
 
i2c_slave_transfer_event_t event
 The event that caused the callback being invoked. More...
 
status_t completionStatus
 Success or error code describing how the transfer completed. More...
 

Field Documentation

uint8_t* volatile i2c_slave_transfer_t::data
volatile uint16_t i2c_slave_transfer_t::dataSize
i2c_slave_transfer_event_t i2c_slave_transfer_t::event

Read-only.

status_t i2c_slave_transfer_t::completionStatus

Only applies for kI2C_SlaveCompletionEvent.

struct i2c_slave_handle_t
Note
If user wants to use the transactional API to transfer data in slave mode, one I2C instance should and can only be allocated one handle.
The handle is maintained by I2C driver internally, which means the transfer state is retained and user shall not modify its state isBusy in application level. If user only wish to use transactional APIs without understanding its machanism, it is not necessary to understand these members.

Data Fields

i2c_slave_transfer_t transfer
 I2C slave transfer structure. More...
 
size_t transferredCount
 The number of bytes actually transferred for curent data buffer. More...
 
bool isBusy
 Whether transfer is busy. More...
 
uint8_t eventMask
 Mask of the events. More...
 
i2c_slave_transfer_callback_t callback
 Callback function invoked at the transfer event. More...
 
status_t completionStatus
 
                            I2C slave transfer complete status, indicating how the transfer ends, such as

kStatus_I2C_Nak indicates the slave was nacked by master before all the data was sent. More...

 
void * userData
 User configurable pointer to any data, function, structure etc that user wish to use in the callback. More...
 

Field Documentation

i2c_slave_transfer_t i2c_slave_handle_t::transfer
size_t i2c_slave_handle_t::transferredCount
bool i2c_slave_handle_t::isBusy
uint8_t i2c_slave_handle_t::eventMask

When these enents occur during transfer driver will alert user using callback.

i2c_slave_transfer_callback_t i2c_slave_handle_t::callback
status_t i2c_slave_handle_t::completionStatus

This parameter is only useful when eEvent is kI2C_SlaveCompletionEvent.

void* i2c_slave_handle_t::userData

Macro Definition Documentation

#define I2C_RETRY_TIMES   0U /* Default defines to zero, driver keeps checking status flag untill it changes. */

Typedef Documentation

typedef void(* i2c_master_transfer_callback_t)(I2C_Type *base, i2c_master_handle_t *handle, status_t completionStatus, void *userData)

Defines the interface of user callback function used in master interrupt transfer. The callback function shall be defined and declared in application level by user. Before starting master transfer by calling I2C_MasterTransferNonBlocking, call I2C_MasterTransferCreateHandle to install the user callback. When master transfer ends successfully or failed due to any event like arbitration lost or nacked by slave, user callback will be invoked by driver. And then user can decide what to do next in the callback according to its third parameter completionStatus that indicates how the transfer ends.

Parameters
baseThe I2C peripheral base address.
handleI2C transfer handle, which contains the information of base pointer, completionStatus and user data.
completionStatusEither kStatus_Success or an error code describing how the transfer completed.
userDataPointer to user configurable structure.
typedef void(* i2c_slave_transfer_callback_t)(I2C_Type *base, i2c_slave_transfer_t *transfer, void *userData)

Defines the interface of slave user callback function. The callback function shall be defined and declared in application level by user. Before calling I2C_SlaveTransferNonBlocking to let I2C slave ready to process bus events, call I2C_SlaveTransferCreateHandle first to install the user callback to slave handle. When I2C slave meets user selected events, callback will be invoked and user can decide the following steps in the callback. All the events that can trigger callback are listed in i2c_slave_transfer_event_t.

Parameters
baseBase address for the I2C instance on which the event occurred.
transferPointer to transfer descriptor containing values passed to and/or from the callback.
userDataPointer to user configurable structure.
typedef void(* i2c_isr_t)(I2C_Type *base, void *i2cHandle)

Enumeration Type Documentation

anonymous enum
Enumerator
kStatus_I2C_Busy 

I2C bus is busy.

kStatus_I2C_Idle 

I2C Bus is idle.

kStatus_I2C_Nak 

I2C detected NACK on bus.

When in SMBus mode, this means the receiver nacks transmitter before PEC byte.

kStatus_I2C_ArbitrationLost 

I2C lost arbitration during addressing.

kStatus_I2C_Timeout 

Timeout happens when waiting for status flags to change.

kStatus_I2C_Addr_Nak 

NACK was detected during the address probe.

kStatus_I2C_GeneralCall_Nak 

NACK was detected after issuing general call.

kStatus_I2C_RxHardwareOverrun 

I2C rx receiver overrun.

kStatus_I2C_TxFifoFlushed 

I2C tx FIFO is flushed by hardware.

These enumerations can be ORed together to form bit masks. The masks can be used together with masks in _i2c_master_status_flags as parameter by I2C_MasterClearStatusFlags or as return value by I2C_MasterGetStatusFlags. Or together with masks in _i2c_slave_status_flags as parameter by I2C_SlaveClearStatusFlags or as return value by I2C_SlaveGetStatusFlags

Enumerator
kI2C_RxUnderflowInterruptFlag 

Sets when software tries to read from empty rx FIFO.

bit 0

kI2C_RxOverflowInterruptFlag 

Sets when new data received and the rx FIFO is already full.

bit 1

kI2C_RxDataReadyInterruptFlag 

Sets when data in rx FIFO reaches or is above rx watermark.

bit 2

kI2C_TxOverflowInterruptFlag 

Sets when software tries to push data to tx FIFO and it's already full.

bit 3

kI2C_TxRequestInterruptFlag 

Sets when data in tx FIFO is at or below tx FIFO watermark.

bit 4

kI2C_TxAbortInterruptFlag 

Sets when any of the below status from kI2C_Master7bitAddressNackFlag to kI2C_MasterArbitrationLostFlag is set, results in the tx FIFO being flushed.

Clear this flag will also clear these status flags automatically. bit 6

kI2C_BusBusyInterruptFlag 

Sets when there is I2C activity on bus.

bit 8

kI2C_StopDetectInterruptFlag 

Sets when stop condition is detected.

bit 9

kI2C_StartDetectInterruptFlag 

Sets when start condition is detected.

bit 10

kI2C_ActiveFlag 

Sets when I2C module is in active transfer state.

bit 25

kI2C_TxFifoNotFullFlag 

Sets when I2C tx FIFO is not full.

bit 26

kI2C_TxFifoEmptyFlag 

Sets when I2C txFIFO is completely empty.

bit 27

kI2C_RxFifoNotEmptyFlag 

Sets when I2C rx FIFO is not empty.

bit 28

kI2C_RxFifoFullFlag 

Sets when I2C rx FIFO is completely full.

bit 29

These enumerations can be ORed together to form bit masks. The masks can be used as parameter by I2C_MasterClearStatusFlags or as return value by I2C_MasterGetStatusFlags.

Enumerator
kI2C_Master7bitAddressNackFlag 

Sets when I2C master is nacked in 7-bit addressing.

bit 12

kI2C_Master10bitAddressNack1Flag 

Sets when I2C master is nacked of first byte of address in 10-bit addressing.

bit 13

kI2C_Master10bitAddressNack2Flag 

Sets when I2C master is nacked of second byte of address in 10-bit addressing.

bit 14

kI2C_MasterDataNackFlag 

Sets when I2C master is nacked in data sending.

bit 15

kI2C_MasterGeneralCallNackFlag 

Sets when I2C master is nacked after issueing general call.

bit 16

kI2C_MasterGeneralCallReadFlag 

Sets when I2C master uses read command after issueing general call.

bit 17

kI2C_MasterHighSpeedCodeAckFlag 

Sets when I2C master is in high speed mode and the high speed master code was acknowledged.

bit 18

kI2C_MasterStartByteAckFlag 

Sets when I2C master has sent a START byte and the START byte was acknowledged.

bit 19

kI2C_MasterHighSpeedRestartDisabledFlag 

Sets when I2C master tries to transfer data in high speed mode with restart disabled.

bit 20

kI2C_MasterStartWithRestartDisabledFlag 

Sets when master tries to send a start with restart disabled.

bit 21

kI2C_Master10bitAddressReadRestartDisabledFlag 

Sets when I2C master issues read command in 10-bit addessing with restart disabled.

bit 22

kI2C_MasterOperateWhenDisabledFlag 

Sets when software wants to initiate a master operation with master mode disabled.

bit 23

kI2C_MasterArbitrationLostFlag 

Sets when master loses arbitration or kI2C_SlaveArbitrationLostFlag is set.

bit 24

kI2C_MasterActiveFlag 

Sets when I2C master operation is active.

bit 30

kI2C_MasterAutoClearFlags 

These flags are cleared automatically according to module status, or when other status bit is cleared.

eg. once tx FIFO is not empty kI2C_TxFifoEmptyFlag is cleared automatically. eg. status bits from kI2C_Master7bitAddressNackFlag to kI2C_MasterArbitrationLostFlag are cleared when kI2C_TxAbortInterruptFlag is cleared.

kI2C_MasterAllClearFlags 

All flags which are clearable.

These enumerations can be ORed together to form bit masks. The masks can be used as parameter by I2C_SlaveClearStatusFlags, or as return value by I2C_SlaveGetStatusFlags.

Enumerator
kI2C_SlaveReadRequestInterruptFlag 

Sets when I2C as slave and master tries to read data from it.

bit 5

kI2C_SlaveNackInterruptFlag 

Sets when I2C as slave transmiter and was nacked by master, indicating tx complete.

bit 7

kI2C_SlaveGeneralCallAckInterruptFlag 

Sets when general call address is received and acknowledged.

bit 11

kI2C_SlaveFlushTxFifoFlag 

Sets when I2C slave receives a read command but there are still old data remaining in tx FIFO.

Cleared when kI2C_TxAbortInterruptFlag is cleared. bit 13

kI2C_SlaveArbitrationLostFlag 

Sets when data on bus is not the same as slave sends.

Cleared when kI2C_TxAbortInterruptFlag is cleared. bit 14

kI2C_SlaveReadWhenRequestedDataFlag 

Sets when I2C slave is request data from master but use read command.

Cleared when kI2C_TxAbortInterruptFlag is cleared. bit 15

kI2C_SlaveDisabledWhileBusy 

Sets when I2C slave is busy while disabled.

If slave is addressed when disabled, slave will nack the master even address matched, if slave is receiveing slave will nack the transfer immediately. Cleared when module is re-eanbled. bit 16

kI2C_SlaveRxDataLost 
   Sets when I2C slave is actively

receiving data when disabled, and at least one byte have been received.

Cleared when module is re-eanbled. bit 17

kI2C_SlaveActiveFlag 

Sets when I2C slave operation is active.

bit 31

kI2C_SlaveAutoClearFlags 

These flags are cleared automatically according to module status, or when other status bit is cleared.

eg. once tx FIFO is not empty kI2C_TxFifoEmptyFlag is cleared automatically. eg. kI2C_SlaveFlushTxFifoFlag, kI2C_SlaveArbitrationLostFlag and kI2C_SlaveReadWhenRequestedDataFlag are cleared when kI2C_TxAbortInterruptFlag is cleared.

kI2C_SlaveAllClearFlags 

All flags which are clearable.

These enumerations can be ORed together to form bit masks. The masks can be used as parameter by I2C_EnableInterrupts, I2C_DisableInterrupts, or as return value by I2C_GetEnabledInterrupts.

Enumerator
kI2C_RxUnderflowInterruptEnable 

Rx FIFO underflow interrupt.

bit 0

kI2C_RxOverflowInterruptEnable 

Rx FIFO overflow interrupt.

bit 1

kI2C_RxDataReadyInterruptEnable 

Rx data ready interrupt.

bit 2

kI2C_TxOverflowInterruptEnable 

Tx FIFO overflow interrupt.

bit 3

kI2C_TxRequestInterruptEnable 

Tx data request interrupt.

bit 4

kI2C_SlaveReadRequestInterruptEnable 

I2C slave requested data by master interrupt.

bit 5

kI2C_TxAbortInterruptEnable 

Tx abort interrupt.

bit 6

kI2C_SlaveNackInterruptEnable 

I2C slave nack interrupt.

bit 7

kI2C_BusBusyInterruptEnable 

I2C bus busy interrupt.

bit 8

kI2C_StopDetectInterruptEnable 

I2C stop condition detect interrupt.

bit 9

kI2C_StartDetectInterruptEnable 

I2C start condition detect interrupt.

bit 10

kI2C_SlaveGeneralCallAckInterruptEnable 

I2C ganaral call detect and acknowledge interrupt.

bit 11

Enumerator
kI2C_MasterSpeedStandard 

Standard mode, 100kbps.

kI2C_MasterSpeedFast 

Fast mode, 400kbps.

kI2C_MasterSpeedHigh 

High speed mode, 3.4Mbps.

Enumerator
kI2C_AddressMatch7bit 

7-bit addressing mode.

kI2C_AddressMatch10bit 

10-bit addressing mode.

Enumerator
kQSPI_DmaRx 

Receive DMA Enable Flag.

kQSPI_DmaTx 

Transmit DMA Enable Flag.

Enumerator
kI2C_Write 

Master transmit.

kI2C_Read 

Master receive.

This enumeration lists all the protocol level events that may happen during slave transfer. They can be used for two related purposes:

  1. User can select certain events and combined them by OR operation to form a mask, and use the mask to configure slave transfer configuration stucture i2c_slave_transfer_t::u8EventMask. If any of these selected events happens, driver will alert user by invoking callback.
  2. When slave callback is invoked, user has to know which specific event occured. Callback uses slave transfer configuration structure i2c_slave_transfer_t as 2nd parameter, its member i2c_slave_transfer_t::eEvent shows which event just happened.
Enumerator
kI2C_SlaveStartDetectEvent 

A start/repeated start was detected.

kI2C_SlaveGenaralcallEvent 

Received the general call address after a start or repeated start.

kI2C_SlaveTransmitEvent 

Slave runs out of data to transmit, request a new data buffer.

kI2C_SlaveReceiveEvent 

Slave runs out of space to store received data, request a new data buffer.

kI2C_SlaveCompletionEvent 

Slave detects a stop signal, or slave is nacked by master during master-receive, or slave has finished transmit/receive previously configured amount of data.

kI2C_SlaveAllEvents 

A bit mask of all available events.

Function Documentation

static uint32_t I2C_MasterGetStatusFlags ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
Returns
the mask of status flags, can be a single flag or several flags in _i2c_master_status_flags ORed together
void I2C_MasterClearStatusFlags ( I2C_Type *  base,
uint32_t  statusFlags 
)
Parameters
baseI2C base pointer
statusFlagsThe status flag mask, can be a single flag or several flags in _i2c_status_flags ORed together.
static uint32_t I2C_SlaveGetStatusFlags ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
Returns
the mask of status flags, can be a single flag or several flags in _i2c_status_flags ORed together
void I2C_SlaveClearStatusFlags ( I2C_Type *  base,
uint32_t  statusFlags 
)
Parameters
baseI2C base pointer
statusFlagsThe status flag mask, can be a single flag or several flags in _i2c_slave_status_flags ORed together
static void I2C_EnableInterrupts ( I2C_Type *  base,
uint16_t  interrupts 
)
inlinestatic
Parameters
baseI2C base pointer
interruptsThe interrupt source mask, can be a single source or several sources in _i2c_interrupt_enable ORed together
static void I2C_DisableInterrupts ( I2C_Type *  base,
uint16_t  interrupts 
)
inlinestatic
Parameters
baseI2C base pointer
interruptsThe interrupt source mask, can be a single source or several sources in _i2c_interrupt_enable ORed together
static uint16_t I2C_GetEnabledInterrupts ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
Returns
The interrupt source mask, can be a single source or several sources in _i2c_interrupt_enable ORed together
void I2C_MasterGetDefaultConfig ( i2c_master_config_t *  masterConfig)

The purpose of this API is to initialize the configuration structure to default value for I2C_MasterInit to use. Use the unchanged structure in I2C_MasterInit or modify the structure before calling I2C_MasterInit. This is an example:

* I2C_MasterInit(I2C0, &config, 12000000U);
*
Parameters
masterConfigPointer to the master configuration structure
void I2C_MasterInit ( I2C_Type *  base,
const i2c_master_config_t *  masterConfig,
uint32_t  sourceClock_Hz 
)

This API initialize the I2C module for master operation.

Note
If FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL is enbaled by user, the init function will not ungate I2C clock source before initialization, to avoid hardfault, user has to manually enable ungate the clock source before calling the API

The configuration structure can be filled manully or be set with default values by calling I2C_MasterGetDefaultConfig. This is an example.

* I2C_MasterInit(I2C0, &config, 12000000U);
*
Parameters
baseI2C base pointer
masterConfigPointer to the master configuration structure
sourceClock_HzFrequency in Hertz of the I2C functional clock source
void I2C_MasterDeinit ( I2C_Type *  base)

Call this API to disable the I2C module.

Parameters
baseI2C base pointer
void I2C_SlaveGetDefaultConfig ( i2c_slave_config_t *  slaveConfig)

The purpose of this API is to initialize the configuration structure for I2C_SlaveInit to use. Use the unchanged initialized structure in I2C_SlaveInit or modify the structure before calling I2C_SlaveInit. This is an example.

* config.slaveAdress = 0x7FU;
*
Parameters
slaveConfigPointer to the slave configuration structure
void I2C_SlaveInit ( I2C_Type *  base,
const i2c_slave_config_t *  slaveConfig 
)

This API initialize the I2C module for slave operation. User can also configure whether to enable the module in the function.

Note
If FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL is enbaled by user, the init function will not ungate I2C clock source before initialization, to avoid hardfault, user has to manually ungate the clock source before calling the API

The configuration structure can be filled manully or be set with default values by calling I2C_SlaveGetDefaultConfig. This is an example.

* sConfig.address = 0x2AU;
* I2C_SlaveInit(I2C0, &sConfig);
*
Parameters
baseI2C base pointer
slaveConfigPointer to the slave configuration structure
void I2C_SlaveDeinit ( I2C_Type *  base)

Call this API to disable the I2C module.

Parameters
baseI2C base pointer
static void I2C_SetRxWaterMark ( I2C_Type *  base,
uint8_t  rxWaterMark 
)
inlinestatic
Parameters
baseI2C base pointer
rxWaterMarkrx watermark level
static void I2C_SetTxWaterMark ( I2C_Type *  base,
uint8_t  txWaterMark 
)
inlinestatic
Parameters
baseI2C base pointer
txWaterMarktx watermark level
static void I2C_Enable ( I2C_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseI2C base pointer
enablePass true to enable and false to disable the module
static void I2C_EnableMaster ( I2C_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseI2C base pointer
enablePass true to enable as master and false to enable as slave
static uint8_t I2C_GetTxFifoDataCount ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
Returns
The data count in tx FIFO
static uint8_t I2C_GetRxFifoDataCount ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
Returns
The data count in rx FIFO
static uint8_t I2C_GetTxFifoDepth ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
Returns
The tx FIFO depth
static uint8_t I2C_GetRxFifoDepth ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
Returns
The rx FIFO depth
static void I2C_SetSdaHoldTime ( I2C_Type *  base,
uint16_t  sdaHoldTime 
)
inlinestatic
Parameters
baseI2C base pointer
sdaHoldTimeNumber of clock source cycles of SDA hold time
static void I2C_SetSdaSetupTime ( I2C_Type *  base,
uint16_t  sdaSetupTime 
)
inlinestatic
Parameters
baseI2C base pointer
sdaSetupTimeNumber of clock source cycles of SDA setup time
static void I2C_EnableAckGeneralCall ( I2C_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseI2C base pointer
enablePass true to enable and false to disable
static bool I2C_IsEnabled ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
Returns
True for enabled, false for disabled.
static void I2C_SetGlitchFilter ( I2C_Type *  base,
uint8_t  glitchFilter 
)
inlinestatic
Parameters
baseI2C base pointer
glitchFilterNumber of clock source cycles of max glitch time
static void I2C_SetGlitchFilterHighSpeed ( I2C_Type *  base,
uint8_t  glitchFilter 
)
inlinestatic
Parameters
baseI2C base pointer
glitchFilterNumber of clock source cycles of max glitch time
static void I2C_MasterSetHighSpeedAddress ( I2C_Type *  base,
uint8_t  address 
)
inlinestatic
Parameters
baseI2C base pointer
addressHigh speed address, only low 3 bits are avaliable
static bool I2C_IsMaster ( I2C_Type *  base)
inlinestatic
Note
Although I2C can not be master and slave at the same time, when I2C is not in master mode does not mean it's in slave mode, the master and slave function may both be disabled.
Parameters
baseI2C base pointer
Returns
True for master mode enabled, false for disabled.
static void I2C_MasterSetAddressingMode ( I2C_Type *  base,
i2c_address_mode_t  addressingMode 
)
inlinestatic
Parameters
baseI2C base pointer
addressingModeThe I2C addressing mode master operates
static void I2C_MasterSetTargetAddress ( I2C_Type *  base,
uint16_t  address 
)
inlinestatic
Parameters
baseI2C base pointer
addressThe I2C addressing mode master operates
static void I2C_MasterEnableGeneralCall ( I2C_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseI2C base pointer
enableTrue to issue general call, false to issue common start byte according to target address
void I2C_MasterSetSpeedMode ( I2C_Type *  base,
i2c_master_speed_mode_t  speed,
uint32_t  sourceClock_Hz 
)

After the I2C module is initialized as master, user can call this function to change the transfer baud rate. There are 3 speed modes to choos from, kI2C_MasterSpeedStandard for 100kbps, kI2C_MasterSpeedFast for 400kbps and kI2C_MasterSpeedHigh for 3.4Mbps.

Parameters
baseI2C base pointer.
speedMaster transfer speed mode to be configured
sourceClock_HzI2C peripheral clock frequency in Hz
static bool I2C_IsSlave ( I2C_Type *  base)
inlinestatic
Note
Although I2C can not be master and slave at the same time, when I2C is not in slave mode does not mean it's in master mode, the master and slave function may both be disabled.
Parameters
baseI2C base pointer
Returns
True for slave mode enabled, false for disabled.
static void I2C_SlaveSetAddressingMode ( I2C_Type *  base,
i2c_address_mode_t  addressingMode,
uint16_t  address 
)
inlinestatic
Parameters
baseI2C base pointer
addressingModeThe I2C addressing mode slave resonses to
addressThe I2C address, for 7-bit only low 7 bits are valid and for 10-bit only low 10 bits are valid
static uint8_t I2C_ReadByte ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
Returns
The data read from data register.
static void I2C_WriteByte ( I2C_Type *  base,
uint8_t  data 
)
inlinestatic
Note
If using I2C as master to perform read operation, user needs to write dummy to data register to generate clock, do not use this API to write dummy since this API will issue write command simultaneously, use I2C_MasterWriteDummy.
Parameters
baseI2C base pointer
dataThe byte to write.
static void I2C_EnableDMA ( I2C_Type *  base,
uint8_t  mask 
)
inlinestatic
Parameters
baseI2C base pointer
maskEnable mask formed by enums in _i2c_dma_enable_flags
static void I2C_DisableDMA ( I2C_Type *  base,
uint8_t  mask 
)
inlinestatic
Parameters
baseI2C base pointer
maskDisable mask formed by enums in _i2c_dma_enable_flags
static void I2C_SetDmaTxWaterMark ( I2C_Type *  base,
uint8_t  txLevel 
)
inlinestatic
Parameters
baseI2C base pointer
txLeveltx DMA trigger level
static void I2C_SetDmaRxWaterMark ( I2C_Type *  base,
uint8_t  rxLevel 
)
inlinestatic
Parameters
baseI2C base pointer
rxLevelrx DMA trigger level
static uint32_t I2C_GetDataRegAddr ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
Returns
The I2C Data Register address.
static void I2C_MasterWriteDummy ( I2C_Type *  base)
inlinestatic
Note
If using I2C as master to perform read operation, user needs to write dummy to data register to generate clock, use this API not I2C_WriteByte to write dummy, since I2C_WriteByte issue write command simultaneously.
Parameters
baseI2C base pointer
status_t I2C_MasterCheckAndClearError ( I2C_Type *  base,
uint32_t  status 
)
Note
: The API only checks the error status that occured on bus, error caused by user misuse such as kI2C_RxUnderflowInterruptFlag, kI2C_TxOverflowInterruptFlag or kI2C_MasterOperateWhenDisabledFlag will not be checked
Parameters
baseThe I2C peripheral base address.
statusStatus flags to check.
Return values
kStatus_Success
kStatus_I2C_RxHardwareOverrunMaster rx FIFO overflow
kStatus_I2C_GeneralCall_NakMaster nacked after issueing general call
kStatus_I2C_ArbitrationLostMaster lost arbitration when addressing
kStatus_I2C_NakMaster nacked during data transmitting
kStatus_I2C_Addr_NakMaster nacked during slave probing
status_t I2C_MasterWriteBlocking ( I2C_Type *  base,
const uint8_t *  data,
size_t  txSize 
)

Call this function when using I2C as master to send certain bytes of data to bus. This function uses the blocking way, which means it does not return until all the data is sent to bus.

Note
The I2C module generates START/STOP/RESTART automatically. When tx FIFO state changes from empty to not empty, start signal is generated; when tx FIFO is empty again, stop signal is generated; when read command follows a write command, restart signal is generated in between. So stop signal will be generated after this API returns, and before calling this API if tx FIFO is empty, start signal will be generated first automatically, if tx FIFO is not empty and the last command in tx FIFO is write, restart signal will be generated first automatically.
Parameters
baseI2C base pointer.
dataThe pointer to the data to be transmitted.
txSizeThe length in bytes of the data to be transmitted.
Return values
kStatus_SuccessSuccessfully complete the data transmission.
kStatus_I2C_ArbitrationLostTransfer error, arbitration lost.
kStatus_I2C_NakTransfer error, receive NAK during transfer.
kStatus_I2C_Addr_NakTransfer error, receive NAK during addressing, only applies when tx FIFO is empty before calling this API.
kStatus_I2C_TimeoutTransfer error, timeout happens when waiting for status flags to change.
status_t I2C_MasterReadBlocking ( I2C_Type *  base,
uint8_t *  data,
size_t  rxSize 
)

Call this function when using I2C as master to receive certain bytes of data from bus. This function uses the blocking way, which means it does not return until all the data is received or is nacked by slave.

Note
When doing read operation, software needs to push dummy data to tx FIFO with read command to generate clock, plus I2C module generates START/STOP/RESTART automatically, meaning when tx FIFO state changes from empty to not empty, start signal is generated, when tx FIFO is empty again, stop signal is generated, when read command follows a write command, restart signal is generated in between. So stop signal will be generated after this API returns, and before calling this API if tx FIFO is empty, start signal will be generated first automatically, if tx FIFO is not empty and the last command in tx FIFO is write, restart signal will be generated first automatically.
Parameters
baseI2C base pointer.
dataThe pointer to the data to store the received data.
rxSizeThe length in bytes of the data to be received.
Return values
kStatus_SuccessSuccessfully complete the data transmission.
kStatus_I2C_TimeoutSend stop signal failed, timeout.
static void I2C_SlaveNackNextByte ( I2C_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseI2C base pointer
enablePass true to enable nack and false to disable
status_t I2C_SlaveCheckAndClearError ( I2C_Type *  base,
uint32_t  status 
)
Note
: The API only checks the error status that occured on bus, error caused by user misuse such as kI2C_RxUnderflowInterruptFlag, kI2C_TxOverflowInterruptFlag, kI2C_SlaveReadWhenRequestedDataFlag or kI2C_SlaveDisabledWhileBusy will not be checked
Parameters
baseThe I2C peripheral base address.
statusStatus flags to check.
Return values
kStatus_Success
kStatus_I2C_RxHardwareOverrunSlave rx FIFO overflow
kStatus_I2C_TxFifoFlushedSlave is addressed and is requested data but there are still old data remaining in tx FIFO
kStatus_I2C_ArbitrationLostData on SDA is not the same as slave transmitted
kStatus_I2C_NakSlave nacked by master
status_t I2C_SlaveWriteBlocking ( I2C_Type *  base,
const uint8_t *  data,
size_t  txSize 
)

Call this funtion to let I2C slave poll register status until it is addressed, then slave sends txSize of data to bus until all the data has been sent to bus or untill it is nacked.

Parameters
baseI2C base pointer.
dataThe pointer to the data to be transferred.
txSizeThe length in bytes of the data to be transferred.
Return values
kStatus_Success
kStatus_I2C_TxFifoFlushedSlave is addressed and is requested data but there are still old data remaining in tx FIFO
kStatus_I2C_ArbitrationLostData on SDA is not the same as slave transmitted
kStatus_I2C_NakSlave nacked by master
status_t I2C_SlaveReadBlocking ( I2C_Type *  base,
uint8_t *  data,
size_t  rxSize 
)

Call this funtion to let I2C slave poll register status until it is addressed, then slave receives rxSize of data until all the data has been received.

Parameters
baseI2C base pointer.
dataThe pointer to the data to store the received data.
rxSizeThe length in bytes of the data to be received.
Return values
kStatus_SuccessSuccessfully complete data receive.
kStatus_I2C_TimeoutWait status flag timeout.
status_t I2C_MasterTransferBlocking ( I2C_Type *  base,
i2c_master_transfer_t *  transferConfig 
)
Note
The API does not return until the transfer succeeds or fails due to arbitration lost or receiving a NAK.
Parameters
baseI2C base pointer.
transferConfigPointer to the transfer configuration structure.
Return values
kStatus_SuccessSuccessfully complete the data transmission.
kStatus_I2C_BusyPrevious transmission still not finished.
kStatus_I2C_TimeoutTransfer error, timeout happens when waiting for status flags to change.
kStatus_I2C_ArbitrationLostTransfer error, arbitration lost.
kStatus_I2C_NakTransfer error, receive NAK during transfer.
kStatus_I2C_Addr_NakTransfer error, receive NAK during slave probing.
kStatus_I2C_GeneralCall_NakTransfer error, receive NAK after issueing general call.
void I2C_MasterTransferCreateHandle ( I2C_Type *  base,
i2c_master_handle_t *  handle,
i2c_master_transfer_callback_t  callback,
void *  userData 
)

This function is responsible for initializig master transfer handle, installing user callback, registering master IRQ handling function and opening global interrupt.

Parameters
baseI2C base pointer.
handlepointer to i2c_master_transfer_handle_t structure to store the transfer state.
callbackpointer to user callback function.
userDataUser configurable pointer to any data, function, structure etc that user wish to use in the callback
status_t I2C_MasterTransferNonBlocking ( I2C_Type *  base,
i2c_master_handle_t *  handle,
i2c_master_transfer_t *  transfer 
)
Note
Transfer in interrupt way is non-blocking which means this API returns immediately after transfer initiates. User can call I2C_MasterTransferGetCount to get the count of data that master has transmitted/received and check transfer status. If the return status is kStatus_NoTransferInProgress, the transfer is finished. Also if user installs a user callback when calling I2C_MasterTransferCreateHandle before, the callback will be invoked when transfer finishes.
Parameters
baseI2C base pointer
handlepointer to i2c_master_transfer_handle_t structure which stores the transfer state.
transferPointer to the transfer configuration structure.
Return values
kStatus_SuccessSuccessfully start the data transmission.
kStatus_I2C_BusyPrevious transmission still not finished.
status_t I2C_MasterTransferGetCount ( I2C_Type *  base,
i2c_master_handle_t *  handle,
size_t *  count 
)
Parameters
baseI2C base pointer.
handlepointer to i2c_master_transfer_handle_t structure which stores the transfer state.
countPointer to number of bytes transferred so far by the non-blocking transaction.
Return values
kStatus_InvalidArgumentcount is Invalid.
kStatus_NoTransferInProgressCurent no transfer is in progress.
kStatus_SuccessSuccessfully obtained the count.
void I2C_MasterTransferAbort ( I2C_Type *  base,
i2c_master_handle_t *  handle 
)
Note
This API can be called at any time after a transfer of interrupt way initiates and before it finishes to abort the transfer early.
Parameters
baseI2C base pointer.
handlepointer to i2c_master_handle_t structure which stores the transfer state
void I2C_SlaveTransferCreateHandle ( I2C_Type *  base,
i2c_slave_handle_t *  handle,
i2c_slave_transfer_callback_t  callback,
void *  userData 
)

This function is responsible for initializig slave transfer handle, installing user callback, registering master IRQ handling function and opening global interrupt.

Parameters
baseI2C base pointer
handlepointer to i2c_slave_handle_t structure to store the transfer state
callbackpointer to user callback function
userDataUser configurable pointer to any data, function, structure etc that user wish to use in the callback
status_t I2C_SlaveTransferNonBlocking ( I2C_Type *  base,
i2c_slave_handle_t *  handle,
uint8_t  eventMask 
)

Call this API to let I2C start monitoring bus events driven by I2C master on bus. When user specified event occurs, callback will be invoked passes event information to the callback.

Note
When kI2C_SlaveTransmitEvent and kI2C_SlaveReceiveEvent occured, slave callback will always be revoked regardless which events user choose to enable. This means user need not configure them in the eventMask. If user wants to enable all the events, use kI2C_SlaveAllEvents for convenience.
Parameters
baseThe I2C peripheral base address.
handlePointer to i2c_slave_handle_t structure which stores the transfer state.
eventMaskBit mask formed by OR operation of event(s) in i2c_slave_transfer_event_t enumerators. When these events occur the callback will be invoked.
Return values
kStatus_I2C_BusyI2C slave has already been started on this handle.
status_t I2C_SlaveTransferGetCount ( I2C_Type *  base,
i2c_slave_handle_t *  handle,
size_t *  count 
)
Parameters
baseI2C base pointer.
handlepointer to i2c_slave_handle_t structure.
countNumber of bytes slave have transferred after the last start/repeated start.
Return values
kStatus_InvalidArgumentcount is Invalid.
kStatus_NoTransferInProgressCurent no transfer is in progress.
kStatus_SuccessSuccessfully obtained the count.
void I2C_SlaveTransferAbort ( I2C_Type *  base,
i2c_slave_handle_t *  handle 
)
Note
This API can be called at any time to stop slave for handling further bus events.
Parameters
baseI2C base pointer.
handlepointer to i2c_slave_handle_t structure which stores the transfer state.
uint32_t I2C_GetInstance ( I2C_Type *  base)
Parameters
baseI2C base pointer.
Return values
Thenumber of the instance.

Variable Documentation

const IRQn_Type s_I2cIrqs[]
void* s_i2cHandles[]
i2c_isr_t s_i2cMasterIsr