MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

Data Structures

struct  uart_dmac_handle_t
 UART DMAC handle. More...
 

Typedefs

typedef void(* uart_dmac_transfer_callback_t )(UART_Type *base, uart_dmac_handle_t *handle, status_t status, void *userData)
 UART transfer callback function. More...
 

Driver version

#define FSL_UART_DMAC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))
 UART DMAC driver version. More...
 

DMAC transactional APIs

void UART_TransferCreateHandleDMAC (UART_Type *base, uart_dmac_handle_t *handle, uart_dmac_transfer_callback_t callback, void *userData, dmac_handle_t *txDmaHandle, dmac_handle_t *rxDmaHandle)
 Initializes the UART handle which is used in transactional functions and sets the callback. More...
 
status_t UART_TransferSendDMAC (UART_Type *base, uart_dmac_handle_t *handle, uart_transfer_t *xfer)
 Sends data using DMAC. More...
 
status_t UART_TransferReceiveDMAC (UART_Type *base, uart_dmac_handle_t *handle, uart_transfer_t *xfer)
 Receives data using DMAC. More...
 
void UART_TransferAbortSendDMAC (UART_Type *base, uart_dmac_handle_t *handle)
 Aborts the send data using DMAC. More...
 
void UART_TransferAbortReceiveDMAC (UART_Type *base, uart_dmac_handle_t *handle)
 Aborts the received data using DMAC. More...
 

Data Structure Documentation

struct _uart_dmac_handle

Data Fields

UART_Type * base
 UART peripheral base address. More...
 
uart_dmac_transfer_callback_t callback
 Callback function. More...
 
void * userData
 UART callback function parameter. More...
 
dmac_handle_t * txDmaHandle
 The DMAC TX channel used. More...
 
dmac_handle_t * rxDmaHandle
 The DMAC RX channel used. More...
 
volatile uint8_t txState
 TX transfer state. More...
 
volatile uint8_t rxState
 RX transfer state.
 

Field Documentation

UART_Type* uart_dmac_handle_t::base
uart_dmac_transfer_callback_t uart_dmac_handle_t::callback
void* uart_dmac_handle_t::userData
dmac_handle_t* uart_dmac_handle_t::txDmaHandle
dmac_handle_t* uart_dmac_handle_t::rxDmaHandle
volatile uint8_t uart_dmac_handle_t::txState

Macro Definition Documentation

#define FSL_UART_DMAC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))

Typedef Documentation

typedef void(* uart_dmac_transfer_callback_t)(UART_Type *base, uart_dmac_handle_t *handle, status_t status, void *userData)

Function Documentation

void UART_TransferCreateHandleDMAC ( UART_Type *  base,
uart_dmac_handle_t *  handle,
uart_dmac_transfer_callback_t  callback,
void *  userData,
dmac_handle_t *  txDmaHandle,
dmac_handle_t *  rxDmaHandle 
)
Parameters
baseUART peripheral base address.
handlePointer to the uart_dmac_handle_t structure.
callbackUART callback, NULL means no callback.
userDataUser callback function data.
rxDmaHandleUser requested DMAC handle for the RX DMAC transfer.
txDmaHandleUser requested DMAC handle for the TX DMAC transfer.
status_t UART_TransferSendDMAC ( UART_Type *  base,
uart_dmac_handle_t *  handle,
uart_transfer_t *  xfer 
)

This function sends data using DMAC. This is non-blocking function, which returns right away. When all data is sent, the send callback function is called.

Parameters
baseUART peripheral base address.
handleUART handle pointer.
xferUART DMAC transfer structure. See uart_transfer_t.
Return values
kStatus_Successif succeeded; otherwise failed.
kStatus_UART_TxBusyPrevious transfer ongoing.
kStatus_InvalidArgumentInvalid argument.
status_t UART_TransferReceiveDMAC ( UART_Type *  base,
uart_dmac_handle_t *  handle,
uart_transfer_t *  xfer 
)

This function receives data using DMAC. This is non-blocking function, which returns right away. When all data is received, the receive callback function is called.

Parameters
baseUART peripheral base address.
handlePointer to the uart_dmac_handle_t structure.
xferUART DMAC transfer structure. See uart_transfer_t.
Return values
kStatus_Successif succeeded; otherwise failed.
kStatus_UART_RxBusyPrevious transfer on going.
kStatus_InvalidArgumentInvalid argument.
void UART_TransferAbortSendDMAC ( UART_Type *  base,
uart_dmac_handle_t *  handle 
)

This function aborts the sent data using DMAC.

Note
This function only aborts the tx DMAC transfer not disable the DMA function, since disable DMA function will disable tx and rx together. If user wants to abort both tx/rx DMAC transfer, use UART_EnableDMA(base, false).
Parameters
baseUART peripheral base address.
handlePointer to uart_dmac_handle_t structure.
void UART_TransferAbortReceiveDMAC ( UART_Type *  base,
uart_dmac_handle_t *  handle 
)

This function abort receive data which using DMAC.

Note
This function only aborts the rx DMAC transfer not disable the DMA function, since disable DMA function will disable tx and rx together. If user wants to abort both tx/rx DMAC transfer, use UART_EnableDMA(base, false).
Parameters
baseUART peripheral base address.
handlePointer to uart_dmac_handle_t structure.