![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
This section describes the programming interface of the DSPI Peripheral driver. The DSPI driver configures DSPI module and provides the functional and transactional interfaces to build the DSPI application.
Data Structures | |
struct | dspi_master_edma_handle_t |
DSPI master eDMA transfer handle structure used for the transactional API. More... | |
struct | dspi_slave_edma_handle_t |
DSPI slave eDMA transfer handle structure used for the transactional API. More... | |
Typedefs | |
typedef void(* | dspi_master_edma_transfer_callback_t )(SPI_Type *base, dspi_master_edma_handle_t *handle, status_t status, void *userData) |
Completion callback function pointer type. More... | |
typedef void(* | dspi_slave_edma_transfer_callback_t )(SPI_Type *base, dspi_slave_edma_handle_t *handle, status_t status, void *userData) |
Completion callback function pointer type. More... | |
Functions | |
void | DSPI_MasterTransferCreateHandleEDMA (SPI_Type *base, dspi_master_edma_handle_t *handle, dspi_master_edma_transfer_callback_t callback, void *userData, edma_handle_t *edmaRxRegToRxDataHandle, edma_handle_t *edmaTxDataToIntermediaryHandle, edma_handle_t *edmaIntermediaryToTxRegHandle) |
Initializes the DSPI master eDMA handle. More... | |
status_t | DSPI_MasterTransferEDMA (SPI_Type *base, dspi_master_edma_handle_t *handle, dspi_transfer_t *transfer) |
DSPI master transfer data using eDMA. More... | |
void | DSPI_MasterTransferAbortEDMA (SPI_Type *base, dspi_master_edma_handle_t *handle) |
DSPI master aborts a transfer which is using eDMA. More... | |
status_t | DSPI_MasterTransferGetCountEDMA (SPI_Type *base, dspi_master_edma_handle_t *handle, size_t *count) |
Gets the master eDMA transfer count. More... | |
void | DSPI_SlaveTransferCreateHandleEDMA (SPI_Type *base, dspi_slave_edma_handle_t *handle, dspi_slave_edma_transfer_callback_t callback, void *userData, edma_handle_t *edmaRxRegToRxDataHandle, edma_handle_t *edmaTxDataToTxRegHandle) |
Initializes the DSPI slave eDMA handle. More... | |
status_t | DSPI_SlaveTransferEDMA (SPI_Type *base, dspi_slave_edma_handle_t *handle, dspi_transfer_t *transfer) |
DSPI slave transfer data using eDMA. More... | |
void | DSPI_SlaveTransferAbortEDMA (SPI_Type *base, dspi_slave_edma_handle_t *handle) |
DSPI slave aborts a transfer which is using eDMA. More... | |
status_t | DSPI_SlaveTransferGetCountEDMA (SPI_Type *base, dspi_slave_edma_handle_t *handle, size_t *count) |
Gets the slave eDMA transfer count. More... | |
struct _dspi_master_edma_handle |
Forward declaration of the DSPI eDMA master handle typedefs.
Data Fields | |
uint32_t | bitsPerFrame |
The desired number of bits per frame. More... | |
volatile uint32_t | command |
The desired data command. More... | |
volatile uint32_t | lastCommand |
The desired last data command. More... | |
uint8_t | fifoSize |
FIFO dataSize. More... | |
volatile bool | isPcsActiveAfterTransfer |
Indicates whether the PCS signal keeps active after the last frame transfer. More... | |
uint8_t | nbytes |
eDMA minor byte transfer count initially configured. More... | |
volatile uint8_t | state |
DSPI transfer state , _dspi_transfer_state. More... | |
uint8_t *volatile | txData |
Send buffer. More... | |
uint8_t *volatile | rxData |
Receive buffer. More... | |
volatile size_t | remainingSendByteCount |
A number of bytes remaining to send. More... | |
volatile size_t | remainingReceiveByteCount |
A number of bytes remaining to receive. More... | |
size_t | totalByteCount |
A number of transfer bytes. | |
uint32_t | rxBuffIfNull |
Used if there is not rxData for DMA purpose. More... | |
uint32_t | txBuffIfNull |
Used if there is not txData for DMA purpose. More... | |
dspi_master_edma_transfer_callback_t | callback |
Completion callback. More... | |
void * | userData |
Callback user data. More... | |
edma_handle_t * | edmaRxRegToRxDataHandle |
edma_handle_t handle point used for RxReg to RxData buff | |
edma_handle_t * | edmaTxDataToIntermediaryHandle |
edma_handle_t handle point used for TxData to Intermediary | |
edma_handle_t * | edmaIntermediaryToTxRegHandle |
edma_handle_t handle point used for Intermediary to TxReg | |
edma_tcd_t | dspiSoftwareTCD [2] |
SoftwareTCD , internal used. | |
uint32_t dspi_master_edma_handle_t::bitsPerFrame |
volatile uint32_t dspi_master_edma_handle_t::command |
volatile uint32_t dspi_master_edma_handle_t::lastCommand |
uint8_t dspi_master_edma_handle_t::fifoSize |
volatile bool dspi_master_edma_handle_t::isPcsActiveAfterTransfer |
uint8_t dspi_master_edma_handle_t::nbytes |
volatile uint8_t dspi_master_edma_handle_t::state |
uint8_t* volatile dspi_master_edma_handle_t::txData |
uint8_t* volatile dspi_master_edma_handle_t::rxData |
volatile size_t dspi_master_edma_handle_t::remainingSendByteCount |
volatile size_t dspi_master_edma_handle_t::remainingReceiveByteCount |
uint32_t dspi_master_edma_handle_t::rxBuffIfNull |
uint32_t dspi_master_edma_handle_t::txBuffIfNull |
dspi_master_edma_transfer_callback_t dspi_master_edma_handle_t::callback |
void* dspi_master_edma_handle_t::userData |
struct _dspi_slave_edma_handle |
Forward declaration of the DSPI eDMA slave handle typedefs.
Data Fields | |
uint32_t | bitsPerFrame |
The desired number of bits per frame. More... | |
uint8_t *volatile | txData |
Send buffer. More... | |
uint8_t *volatile | rxData |
Receive buffer. More... | |
volatile size_t | remainingSendByteCount |
A number of bytes remaining to send. More... | |
volatile size_t | remainingReceiveByteCount |
A number of bytes remaining to receive. More... | |
size_t | totalByteCount |
A number of transfer bytes. | |
uint32_t | rxBuffIfNull |
Used if there is not rxData for DMA purpose. More... | |
uint32_t | txBuffIfNull |
Used if there is not txData for DMA purpose. More... | |
uint32_t | txLastData |
Used if there is an extra byte when 16bits per frame for DMA purpose. More... | |
uint8_t | nbytes |
eDMA minor byte transfer count initially configured. More... | |
volatile uint8_t | state |
DSPI transfer state. More... | |
dspi_slave_edma_transfer_callback_t | callback |
Completion callback. More... | |
void * | userData |
Callback user data. More... | |
edma_handle_t * | edmaRxRegToRxDataHandle |
edma_handle_t handle point used for RxReg to RxData buff | |
edma_handle_t * | edmaTxDataToTxRegHandle |
edma_handle_t handle point used for TxData to TxReg | |
uint32_t dspi_slave_edma_handle_t::bitsPerFrame |
uint8_t* volatile dspi_slave_edma_handle_t::txData |
uint8_t* volatile dspi_slave_edma_handle_t::rxData |
volatile size_t dspi_slave_edma_handle_t::remainingSendByteCount |
volatile size_t dspi_slave_edma_handle_t::remainingReceiveByteCount |
uint32_t dspi_slave_edma_handle_t::rxBuffIfNull |
uint32_t dspi_slave_edma_handle_t::txBuffIfNull |
uint32_t dspi_slave_edma_handle_t::txLastData |
uint8_t dspi_slave_edma_handle_t::nbytes |
volatile uint8_t dspi_slave_edma_handle_t::state |
dspi_slave_edma_transfer_callback_t dspi_slave_edma_handle_t::callback |
void* dspi_slave_edma_handle_t::userData |
typedef void(* dspi_master_edma_transfer_callback_t)(SPI_Type *base, dspi_master_edma_handle_t *handle, status_t status, void *userData) |
base | DSPI peripheral base address. |
handle | A pointer to the handle for the DSPI master. |
status | Success or error code describing whether the transfer completed. |
userData | An arbitrary pointer-dataSized value passed from the application. |
typedef void(* dspi_slave_edma_transfer_callback_t)(SPI_Type *base, dspi_slave_edma_handle_t *handle, status_t status, void *userData) |
base | DSPI peripheral base address. |
handle | A pointer to the handle for the DSPI slave. |
status | Success or error code describing whether the transfer completed. |
userData | An arbitrary pointer-dataSized value passed from the application. |
void DSPI_MasterTransferCreateHandleEDMA | ( | SPI_Type * | base, |
dspi_master_edma_handle_t * | handle, | ||
dspi_master_edma_transfer_callback_t | callback, | ||
void * | userData, | ||
edma_handle_t * | edmaRxRegToRxDataHandle, | ||
edma_handle_t * | edmaTxDataToIntermediaryHandle, | ||
edma_handle_t * | edmaIntermediaryToTxRegHandle | ||
) |
This function initializes the DSPI eDMA handle which can be used for other DSPI transactional APIs. Usually, for a specified DSPI instance, call this API once to get the initialized handle.
Note that DSPI eDMA has separated (RX and TX as two sources) or shared (RX and TX are the same source) DMA request source. (1) For the separated DMA request source, enable and set the RX DMAMUX source for edmaRxRegToRxDataHandle and TX DMAMUX source for edmaIntermediaryToTxRegHandle. (2) For the shared DMA request source, enable and set the RX/RX DMAMUX source for the edmaRxRegToRxDataHandle.
base | DSPI peripheral base address. |
handle | DSPI handle pointer to dspi_master_edma_handle_t. |
callback | DSPI callback. |
userData | A callback function parameter. |
edmaRxRegToRxDataHandle | edmaRxRegToRxDataHandle pointer to edma_handle_t. |
edmaTxDataToIntermediaryHandle | edmaTxDataToIntermediaryHandle pointer to edma_handle_t. |
edmaIntermediaryToTxRegHandle | edmaIntermediaryToTxRegHandle pointer to edma_handle_t. |
status_t DSPI_MasterTransferEDMA | ( | SPI_Type * | base, |
dspi_master_edma_handle_t * | handle, | ||
dspi_transfer_t * | transfer | ||
) |
This function transfers data using eDMA. This is a non-blocking function, which returns right away. When all data is transferred, the callback function is called.
base | DSPI peripheral base address. |
handle | A pointer to the dspi_master_edma_handle_t structure which stores the transfer state. |
transfer | A pointer to the dspi_transfer_t structure. |
void DSPI_MasterTransferAbortEDMA | ( | SPI_Type * | base, |
dspi_master_edma_handle_t * | handle | ||
) |
This function aborts a transfer which is using eDMA.
base | DSPI peripheral base address. |
handle | A pointer to the dspi_master_edma_handle_t structure which stores the transfer state. |
status_t DSPI_MasterTransferGetCountEDMA | ( | SPI_Type * | base, |
dspi_master_edma_handle_t * | handle, | ||
size_t * | count | ||
) |
This function gets the master eDMA transfer count.
base | DSPI peripheral base address. |
handle | A pointer to the dspi_master_edma_handle_t structure which stores the transfer state. |
count | A number of bytes transferred by the non-blocking transaction. |
void DSPI_SlaveTransferCreateHandleEDMA | ( | SPI_Type * | base, |
dspi_slave_edma_handle_t * | handle, | ||
dspi_slave_edma_transfer_callback_t | callback, | ||
void * | userData, | ||
edma_handle_t * | edmaRxRegToRxDataHandle, | ||
edma_handle_t * | edmaTxDataToTxRegHandle | ||
) |
This function initializes the DSPI eDMA handle which can be used for other DSPI transactional APIs. Usually, for a specified DSPI instance, call this API once to get the initialized handle.
Note that DSPI eDMA has separated (RN and TX in 2 sources) or shared (RX and TX are the same source) DMA request source. (1)For the separated DMA request source, enable and set the RX DMAMUX source for edmaRxRegToRxDataHandle and TX DMAMUX source for edmaTxDataToTxRegHandle. (2)For the shared DMA request source, enable and set the RX/RX DMAMUX source for the edmaRxRegToRxDataHandle.
base | DSPI peripheral base address. |
handle | DSPI handle pointer to dspi_slave_edma_handle_t. |
callback | DSPI callback. |
userData | A callback function parameter. |
edmaRxRegToRxDataHandle | edmaRxRegToRxDataHandle pointer to edma_handle_t. |
edmaTxDataToTxRegHandle | edmaTxDataToTxRegHandle pointer to edma_handle_t. |
status_t DSPI_SlaveTransferEDMA | ( | SPI_Type * | base, |
dspi_slave_edma_handle_t * | handle, | ||
dspi_transfer_t * | transfer | ||
) |
This function transfers data using eDMA. This is a non-blocking function, which returns right away. When all data is transferred, the callback function is called. Note that the slave eDMA transfer doesn't support transfer_size is 1 when the bitsPerFrame is greater than eight.
base | DSPI peripheral base address. |
handle | A pointer to the dspi_slave_edma_handle_t structure which stores the transfer state. |
transfer | A pointer to the dspi_transfer_t structure. |
void DSPI_SlaveTransferAbortEDMA | ( | SPI_Type * | base, |
dspi_slave_edma_handle_t * | handle | ||
) |
This function aborts a transfer which is using eDMA.
base | DSPI peripheral base address. |
handle | A pointer to the dspi_slave_edma_handle_t structure which stores the transfer state. |
status_t DSPI_SlaveTransferGetCountEDMA | ( | SPI_Type * | base, |
dspi_slave_edma_handle_t * | handle, | ||
size_t * | count | ||
) |
This function gets the slave eDMA transfer count.
base | DSPI peripheral base address. |
handle | A pointer to the dspi_slave_edma_handle_t structure which stores the transfer state. |
count | A number of bytes transferred so far by the non-blocking transaction. |