MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Clock Driver

Overview

The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.

Get frequency

A centralized function CLOCK_GetFreq gets different clock type frequencies by passing a clock name. For example, pass a kCLOCK_CoreSysClk to get the core clock and pass a kCLOCK_BusClk to get the bus clock. Additionally, there are separate functions to get the frequency. For example, use CLOCK_GetCoreSysClkFreq to get the core clock frequency and CLOCK_GetBusClkFreq to get the bus clock frequency. Using these functions reduces the image size.

External clock frequency

The external clocks EXTAL0/EXTAL1/EXTAL32 are decided by the board level design. The Clock driver uses variables g_xtal0Freq/g_xtal1Freq/g_xtal32Freq to save clock frequencies. Likewise, the APIs CLOCK_SetXtal0Freq, CLOCK_SetXtal1Freq, and CLOCK_SetXtal32Freq are used to set these variables.
The upper layer must set these values correctly. For example, after OSC0(SYSOSC) is initialized using CLOCK_InitOsc0 or CLOCK_InitSysOsc, the upper layer should call the CLOCK_SetXtal0Freq. Otherwise, the clock frequency get functions may not receive valid values. This is useful for multicore platforms where only one core calls CLOCK_InitOsc0 to initialize OSC0 and other cores call CLOCK_SetXtal0Freq.

Data Structures

struct  clock_usb_pll_config_t
 PLL configuration for USB. More...
 
struct  clock_sys_pll_config_t
 PLL configuration for System Fout = Fref * (loopDivider + (float)Numerator/Denominator) More...
 
struct  clock_audio_pll_config_t
 PLL configuration for AUDIO. More...
 
struct  clock_enet_pll_config_t
 PLL configuration for ENET. More...
 

Macros

#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0
 Configure whether driver controls clock. More...
 
#define EDMA_CLOCKS
 Clock ip name array for EDMA. More...
 
#define ENET_CLOCKS
 Clock ip name array for ENET. More...
 
#define LPUART_CLOCKS
 Clock ip name array for LPUART. More...
 
#define LPSPI_CLOCKS
 Clock ip name array for LPSPI. More...
 
#define LPI2C_CLOCKS
 Clock ip name array for LPI2C. More...
 
#define SNVS_HP_CLOCKS
 Clock ip name array for SNVS HP. More...
 
#define SNVS_LP_CLOCKS
 Clock ip name array for SNVS LP. More...
 
#define CAAM_CLOCKS
 Clock ip name array for CAAM. More...
 
#define PCTL_CLOCKS
 Clock ip name array for PCTL. More...
 
#define MIPFIL_CLOCKS
 Clock ip name array for MICFIL. More...
 
#define FLEXSPI_CLOCKS
 Clock ip name array for FLEXSPI. More...
 
#define FLEXIO_CLOCKS
 Clock ip name array for FLEXIO. More...
 
#define FLEXCAN_CLOCKS
 Clock ip name array for FLEXCAN. More...
 
#define SAI_CLOCKS
 Clock ip name array for SAI. More...
 
#define SJC_CLOCKS
 Clock ip name array for SJC. More...
 
#define SPDIF_CLOCKS
 Clock ip name array for SPDIF. More...
 
#define ROMC_CLOCKS
 Clock ip name array for ROMC. More...
 
#define IIM_CLOCKS
 Clock ip name array for IIM. More...
 
#define LPSPI_PERIPH_CLOCKS
 Clock array for LPSPI Peripheral clock. More...
 
#define LPUART_PERIPH_CLOCKS
 Clock array for LPUART Peripheral clock. More...
 
#define LPI2C_PERIPH_CLOCKS
 Clock array for LPI2C Peripheral clock. More...
 
#define TPSMP_CLOCKS
 Clock ip name array for TPSMP. More...
 
#define ESAI_CLOCKS
 Clock ip name array for ESAI. More...
 
#define TPM_CLOCKS
 Clock ip name array for TPM. More...
 
#define FLEXCAN_PERIPH_CLOCKS
 Clock array for FLEXCAN Peripheral clock. More...
 
#define LPTMR_PERIPH_CLOCKS
 Clock array for LPTMR Peripheral clock. More...
 
#define LPTMR_CLOCKS
 Clock ip name array for LPTMR. More...
 
#define LPIT_PERIPH_CLOCKS
 Clock array for LPIT Peripheral clock. More...
 
#define LPIT_CLOCKS
 Clock ip name array for LPIT. More...
 
#define WDOG_CLOCKS
 Clock ip name array for WDOG. More...
 
#define USDHC_CLOCKS
 Clock ip name array for uSDHC. More...
 
#define EMVSIM_CLOCKS
 Clock ip name array for EMVSIM. More...
 
#define CRC_CLOCKS
 Clock ip name array for CRC. More...
 
#define CRC_CLOCKS
 Clock ip name array for CRC. More...
 
#define CAAM_MEM_CLOCKS
 Clock array for CAAM Memory. More...
 
#define CAAM_CTRL_CLOCKS
 Clock array for CAAM controller. More...
 
#define LPDAC_CLOCKS
 Clock ip name array for DAC. More...
 
#define ADC_CLOCKS
 Clock ip name array for ADC. More...
 
#define TRGMUX_CLOCKS
 Clock ip name array for TRGMUX. More...
 
#define IEE_CLOCKS
 Clock ip name array for IEE. More...
 
#define TPIU_CLOCKS
 Clock ip name array for TPIU. More...
 
#define IOMUXC_CLOCKS
 Clock ip name array for IOMUXC. More...
 
#define FSL_CLOCK_MMDC_IPG_GATE_COUNT   1U
 MMDC IPG clock. More...
 
#define MMDC_ACLK_CLOCKS
 MMDC ACLK. More...
 
#define RGPIO_CLOCKS
 Clock ip name array for RGPIO. More...
 
#define SIM_CLOCKS
 Clock ip name array for SIM. More...
 
#define FLEXBUS_CLOCKS
 Clock ip name array for FLEXBUS. More...
 
#define DMAMUX_CLOCKS
 Clock ip name array for DMAMUX. More...
 
#define SDRAM_CLOCKS
 Clock ip name array for SDRAM. More...
 
#define FSL_CLOCK_XRDC_GATE_COUNT   0U
 XRDC clock gate number. More...
 
#define IRC_CLK_FREQ   24000000U
 IRC clock frequency.
 
#define RTC_CLK_FREQ   32768U
 RTC clock frequency.
 
#define kCLOCK_CoreSysClk   kCLOCK_CpuClk
 For compatible with other platforms without CCM. More...
 
#define CLOCK_GetCoreSysClkFreq   CLOCK_GetCpuClkFreq
 For compatible with other platforms without CCM. More...
 

Enumerations

enum  clock_name_t {
  kCLOCK_CpuClk,
  kCLOCK_AxiClk,
  kCLOCK_AhbClk,
  kCLOCK_IpgClk,
  kCLOCK_FlexBusClk,
  kCLOCK_RcOscClk,
  kCLOCK_XtalOscClk,
  kCLOCK_OscClk,
  kCLOCK_RtcClk,
  kCLOCK_Usb1PllClk,
  kCLOCK_Usb1PllPfd0Clk,
  kCLOCK_Usb1PllPfd1Clk,
  kCLOCK_Usb1PllPfd2Clk,
  kCLOCK_Usb1PllPfd3Clk,
  kCLOCK_Usb2PllClk,
  kCLOCK_SysPllClk,
  kCLOCK_SysPllPfd0Clk,
  kCLOCK_SysPllPfd1Clk,
  kCLOCK_SysPllPfd2Clk,
  kCLOCK_SysPllPfd3Clk,
  kCLOCK_EnetPll0Clk,
  kCLOCK_EnetPll1Clk,
  kCLOCK_EnetPll2Clk,
  kCLOCK_AudioPllClk
}
 Clock name used to get clock frequency. More...
 
enum  clock_ip_name_t { ,
  kCLOCK_Dma1 = (0U << 8U) | CCM_CCGR0_DMA1_CLK_ENABLE_SHIFT,
  kCLOCK_Dma0 = (0U << 8U) | CCM_CCGR0_DMA0_CLK_ENABLE_SHIFT,
  kCLOCK_Enet0 = (0U << 8U) | CCM_CCGR0_ENET_CLK_ENABLE_SHIFT,
  kCLOCK_Lpuart3 = (1U << 8U) | CCM_CCGR1_LPUART3_CLK_ENABLE_SHIFT,
  kCLOCK_Lpuart2 = (1U << 8U) | CCM_CCGR1_LPUART2_CLK_ENABLE_SHIFT,
  kCLOCK_Lpuart1 = (1U << 8U) | CCM_CCGR1_LPUART1_CLK_ENABLE_SHIFT,
  kCLOCK_Lpuart0 = (1U << 8U) | CCM_CCGR1_LPUART0_CLK_ENABLE_SHIFT,
  kCLOCK_Lpspi3 = (1U << 8U) | CCM_CCGR1_LPSPI3_CLK_ENABLE_SHIFT,
  kCLOCK_Lpspi2 = (1U << 8U) | CCM_CCGR1_LPSPI2_CLK_ENABLE_SHIFT,
  kCLOCK_Lpspi1 = (1U << 8U) | CCM_CCGR1_LPSPI1_CLK_ENABLE_SHIFT,
  kCLOCK_Lpspi0 = (1U << 8U) | CCM_CCGR1_LPSPI0_CLK_ENABLE_SHIFT,
  kCLOCK_Lpi2c3 = (1U << 8U) | CCM_CCGR1_LPI2C3_CLK_ENABLE_SHIFT,
  kCLOCK_Lpi2c2 = (1U << 8U) | CCM_CCGR1_LPI2C2_CLK_ENABLE_SHIFT,
  kCLOCK_Lpi2c1 = (1U << 8U) | CCM_CCGR1_LPI2C1_CLK_ENABLE_SHIFT,
  kCLOCK_Lpi2c0 = (1U << 8U) | CCM_CCGR1_LPI2C0_CLK_ENABLE_SHIFT,
  kCLOCK_SnvsHp0 = (1U << 8U) | CCM_CCGR1_SNVS_HP_CLK_ENABLE_SHIFT,
  kCLOCK_MmdcAClk = (1U << 8U) | CCM_CCGR1_MMDC_CORE_ACLK_FAST_CORE_P0_CLK_ENABLE_SHIFT,
  kCLOCK_Caam0 = (2U << 8U) | CCM_CCGR2_CAAM_WRAPPER_IPG_CLK_ENABLE_SHIFT,
  kCLOCK_Pctl5 = (2U << 8U) | CCM_CCGR2_PCTL5_CLK_ENABLE_SHIFT,
  kCLOCK_Pctl4 = (2U << 8U) | CCM_CCGR2_PCTL4_CLK_ENABLE_SHIFT,
  kCLOCK_Pctl3 = (2U << 8U) | CCM_CCGR2_PCTL3_CLK_ENABLE_SHIFT,
  kCLOCK_Pctl2 = (2U << 8U) | CCM_CCGR2_PCTL2_CLK_ENABLE_SHIFT,
  kCLOCK_Pctl1 = (2U << 8U) | CCM_CCGR2_PCTL1_CLK_ENABLE_SHIFT,
  kCLOCK_Pctl0 = (2U << 8U) | CCM_CCGR2_PCTL0_CLK_ENABLE_SHIFT,
  kCLOCK_Flexspi1 = (2U << 8U) | CCM_CCGR2_FLEXSPI1_CLK_ENABLE_SHIFT,
  kCLOCK_Flexspi0 = (2U << 8U) | CCM_CCGR2_FLEXSPI0_CLK_ENABLE_SHIFT,
  kCLOCK_Flexio1 = (2U << 8U) | CCM_CCGR2_FLEXIO1_CLK_ENABLE_SHIFT,
  kCLOCK_Flexio0 = (2U << 8U) | CCM_CCGR2_FLEXIO0_CLK_ENABLE_SHIFT,
  kCLOCK_Sai1 = (2U << 8U) | CCM_CCGR2_SAI1_CLK_ENABLE_SHIFT,
  kCLOCK_Sai0 = (2U << 8U) | CCM_CCGR2_SAI0_CLK_ENABLE_SHIFT,
  kCLOCK_Sjc0 = (3U << 8U) | CCM_CCGR3_SJC_CLK_ENABLE_SHIFT,
  kCLOCK_Romc0 = (3U << 8U) | CCM_CCGR3_ROMC_CLK_ENABLE_SHIFT,
  kCLOCK_Iim0 = (3U << 8U) | CCM_CCGR3_IIM_CLK_ENABLE_SHIFT,
  kCLOCK_Lpspi3Periph = (3U << 8U) | CCM_CCGR3_LPSPI3_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lpspi2Periph = (3U << 8U) | CCM_CCGR3_LPSPI2_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lpspi1Periph = (3U << 8U) | CCM_CCGR3_LPSPI1_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lpspi0Periph = (3U << 8U) | CCM_CCGR3_LPSPI0_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lpuart3Periph = (3U << 8U) | CCM_CCGR3_LPUART3_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lpuart2Periph = (3U << 8U) | CCM_CCGR3_LPUART2_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lpuart1Periph = (3U << 8U) | CCM_CCGR3_LPUART1_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lpuart0Periph = (3U << 8U) | CCM_CCGR3_LPUART0_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lpi2c3Periph = (3U << 8U) | CCM_CCGR3_LPI2C3_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lpi2c2Periph = (3U << 8U) | CCM_CCGR3_LPI2C2_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lpi2c1Periph = (3U << 8U) | CCM_CCGR3_LPI2C1_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lpi2c0Periph = (3U << 8U) | CCM_CCGR3_LPI2C0_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Tpsmp0 = (4U << 8U) | CCM_CCGR4_TPSMP_CLK_ENABLE_SHIFT,
  kCLOCK_Esai0 = (4U << 8U) | CCM_CCGR4_ESAI_CLK_ENABLE_SHIFT,
  kCLOCK_Tpm3 = (4U << 8U) | CCM_CCGR4_TPM3_CLK_ENABLE_SHIFT,
  kCLOCK_Tpm2 = (4U << 8U) | CCM_CCGR4_TPM2_CLK_ENABLE_SHIFT,
  kCLOCK_Tpm1 = (4U << 8U) | CCM_CCGR4_TPM1_CLK_ENABLE_SHIFT,
  kCLOCK_Tpm0 = (4U << 8U) | CCM_CCGR4_TPM0_CLK_ENABLE_SHIFT,
  kCLOCK_Lptmr1Periph = (4U << 8U) | CCM_CCGR4_LPTMR1_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lptmr1 = (4U << 8U) | CCM_CCGR4_LPTMR1_CLK_ENABLE_SHIFT,
  kCLOCK_Lptmr0Periph = (4U << 8U) | CCM_CCGR4_LPTMR0_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lptmr0 = (4U << 8U) | CCM_CCGR4_LPTMR0_CLK_ENABLE_SHIFT,
  kCLOCK_Lpit1Periph = (4U << 8U) | CCM_CCGR4_LPIT1_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lpit1 = (4U << 8U) | CCM_CCGR4_LPIT1_CLK_ENABLE_SHIFT,
  kCLOCK_Lpit0Periph = (4U << 8U) | CCM_CCGR4_LPIT0_SERIAL_CLK_ENABLE_SHIFT,
  kCLOCK_Lpit0 = (4U << 8U) | CCM_CCGR4_LPIT0_CLK_ENABLE_SHIFT,
  kCLOCK_Wdog0 = (5U << 8U) | CCM_CCGR5_WDOG_CLK_ENABLE_SHIFT,
  kCLOCK_Usdhc1 = (5U << 8U) | CCM_CCGR5_USDHC1_CLK_ENABLE_SHIFT,
  kCLOCK_Usdhc0 = (5U << 8U) | CCM_CCGR5_USDHC0_CLK_ENABLE_SHIFT,
  kCLOCK_Emvsim1 = (5U << 8U) | CCM_CCGR5_EMVSIM1_CLK_ENABLE_SHIFT,
  kCLOCK_Emvsim0 = (5U << 8U) | CCM_CCGR5_EMVSIM0_CLK_ENABLE_SHIFT,
  kCLOCK_Crc0 = (5U << 8U) | CCM_CCGR5_CRC_CLK_ENABLE_SHIFT,
  kCLOCK_Usbhs0 = (5U << 8U) | CCM_CCGR5_USBOH3_CLK_ENABLE_SHIFT,
  kCLOCK_CaamController0 = (5U << 8U) | CCM_CCGR5_CAAM_WRAPPER_CLK_ENABLE_SHIFT,
  kCLOCK_CaamMemory0 = (5U << 8U) | CCM_CCGR5_CAAM_SECURE_MEM_CLK_ENABLE_SHIFT,
  kCLOCK_Lpdac1 = (5U << 8U) | CCM_CCGR5_DAC1_CLK_ENABLE_SHIFT,
  kCLOCK_Lpdac0 = (5U << 8U) | CCM_CCGR5_DAC0_CLK_ENABLE_SHIFT,
  kCLOCK_Adc1 = (5U << 8U) | CCM_CCGR5_ADC1_CLK_ENABLE_SHIFT,
  kCLOCK_Adc0 = (5U << 8U) | CCM_CCGR5_ADC0_CLK_ENABLE_SHIFT,
  kCLOCK_Trgmux0 = (5U << 8U) | CCM_CCGR5_TRGMUX_CLK_ENABLE_SHIFT,
  kCLOCK_Iee0 = (5U << 8U) | CCM_CCGR5_IEE_CLK_ENABLE_SHIFT,
  kCLOCK_Tpiu0 = (5U << 8U) | CCM_CCGR5_TPIU_CLK_ENABLE_SHIFT,
  kCLOCK_Mmdc0 = (6U << 8U) | CCM_CCGR6_MMDC_CORE_IPG_CLK_P0_CLK_ENABLE_SHIFT,
  kCLOCK_Iomuxc1 = (6U << 8U) | CCM_CCGR6_IOMUXC1_CLK_ENABLE_SHIFT,
  kCLOCK_Iomuxc0 = (6U << 8U) | CCM_CCGR6_IOMUXC0_CLK_ENABLE_SHIFT,
  kCLOCK_Sdramc0 = (7U << 8U) | CCM_CCGR7_SDRAMC_CLK_ENABLE_SHIFT,
  kCLOCK_Flexbus0 = (7U << 8U) | CCM_CCGR7_FLEXBUS_CLK_ENABLE_SHIFT,
  kCLOCK_Sim0 = (7U << 8U) | CCM_CCGR7_SIM_CLK_ENABLE_SHIFT,
  kCLOCK_Dmamux1 = (7U << 8U) | CCM_CCGR7_DMAMUX1_CLK_ENABLE_SHIFT,
  kCLOCK_Dmamux0 = (7U << 8U) | CCM_CCGR7_DMAMUX0_CLK_ENABLE_SHIFT,
  kCLOCK_SnvsLp0 = (7U << 8U) | CCM_CCGR7_SNVS_LP_CLK_ENABLE_SHIFT,
  kCLOCK_Rgpio0 = (7U << 8U) | CCM_CCGR7_RGPIO_CLK_ENABLE_SHIFT
}
 CCM CCGR gate control for each module independently. More...
 
enum  clock_osc_t {
  kCLOCK_RcOsc = 0U,
  kCLOCK_XtalOsc = 1U
}
 OSC 24M sorce select. More...
 
enum  clock_gate_value_t {
  kCLOCK_ClockNotNeeded = 0U,
  kCLOCK_ClockNeededRun = 1U,
  kCLOCK_ClockNeededAll = 2U,
  kCLOCK_ClockNeededRunWait = 3U
}
 Clock gate value. More...
 
enum  clock_mode_t {
  kCLOCK_ModeRun = 0U,
  kCLOCK_ModeWait = 1U,
  kCLOCK_ModeStop = 2U
}
 System clock mode. More...
 
enum  _clock_interrupt {
  kCLOCK_MmdcPodfUpdateInterrupt = CCM_CIMR_MASK_MMDC_PODF_LOADED_MASK,
  kCLOCK_MmdcClkSelUpdateInterrupt = CCM_CIMR_MASK_MMDC_CLK_SEL_LOADED_MASK,
  kCLOCK_OnChipOscReadyInterrupt = CCM_CIMR_MASK_COSC_READY_MASK,
  kCLOCK_PllLrfInterrupt = CCM_CIMR_MASK_LRF_PLL_MASK
}
 CCM interrupt source. More...
 
enum  clock_mux_t {
  kCLOCK_SysPllMux = CCM_TUPLE(CCSR, CCM_CCSR_SYS_PLL_SW_CLK_SEL_SHIFT, CCM_CCSR_SYS_PLL_SW_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Usb1PllMux = CCM_TUPLE(CCSR, CCM_CCSR_USB1_PLL_SW_CLK_SEL_SHIFT, CCM_CCSR_USB1_PLL_SW_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_OscIrcMux = CCM_TUPLE(CSYSCMR, CCM_CSYSCMR_OSC_FIR_CLK_SEL_SHIFT, CCM_CSYSCMR_OSC_FIR_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_SysClkMux = CCM_TUPLE(CSYSCMR, CCM_CSYSCMR_SYS_CLK_SEL_SHIFT, CCM_CSYSCMR_SYS_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Enet1588Mux = CCM_TUPLE(CSCMR1, CCM_CSCMR1_ENET_1588_CLK_SEL_SHIFT, CCM_CSCMR1_ENET_1588_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Lpspi23Mux = CCM_TUPLE(CSCMR1, CCM_CSCMR1_LPSPI23_CLK_SEL_SHIFT, CCM_CSCMR1_LPSPI23_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Lpspi01Mux = CCM_TUPLE(CSCMR1, CCM_CSCMR1_LPSPI01_CLK_SEL_SHIFT, CCM_CSCMR1_LPSPI01_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Flexspi1Mux = CCM_TUPLE(CSCMR1, CCM_CSCMR1_FLEXSPI1_CLK_SEL_SHIFT, CCM_CSCMR1_FLEXSPI1_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Flexspi0Mux = CCM_TUPLE(CSCMR1, CCM_CSCMR1_FLEXSPI0_CLK_SEL_SHIFT, CCM_CSCMR1_FLEXSPI0_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_EnetRmiiMux = CCM_TUPLE(CSCMR1, CCM_CSCMR1_ENET_RMII_CLK_SEL_SHIFT, CCM_CSCMR1_ENET_RMII_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Usdhc1Mux = CCM_TUPLE(CSCMR1, CCM_CSCMR1_USDHC1_CLK_SEL_SHIFT, CCM_CSCMR1_USDHC1_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Usdhc0Mux = CCM_TUPLE(CSCMR1, CCM_CSCMR1_USDHC0_CLK_SEL_SHIFT, CCM_CSCMR1_USDHC0_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_MmdcMux = CCM_TUPLE(CSCMR1, CCM_CSCMR1_MMDC_CH0_CLK_SEL_SHIFT, CCM_CSCMR1_MMDC_CH0_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Tpm23Mux = CCM_TUPLE(CSCMR2, CCM_CSCMR2_TPM23_CLK_SEL_SHIFT, CCM_CSCMR2_TPM23_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Tpm01Mux = CCM_TUPLE(CSCMR2, CCM_CSCMR2_TPM01_CLK_SEL_SHIFT, CCM_CSCMR2_TPM01_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_LpitMux = CCM_TUPLE(CSCMR2, CCM_CSCMR2_LPIT_CLK_SEL_SHIFT, CCM_CSCMR2_LPIT_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_FlexioMux = CCM_TUPLE(CSCMR2, CCM_CSCMR2_FLEXIO_CLK_SEL_SHIFT, CCM_CSCMR2_FLEXIO_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_EmvsimMux = CCM_TUPLE(CSCMR2, CCM_CSCMR2_EMVSIM_CLK_SEL_SHIFT, CCM_CSCMR2_EMVSIM_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Lpi2c23Mux = CCM_TUPLE(CSCMR2, CCM_CSCMR2_LPI2C23_CLK_SEL_SHIFT, CCM_CSCMR2_LPI2C23_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Lpi2c01Mux = CCM_TUPLE(CSCMR2, CCM_CSCMR2_LPI2C01_CLK_SEL_SHIFT, CCM_CSCMR2_LPI2C01_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Lpuart23Mux = CCM_TUPLE(CSCMR2, CCM_CSCMR2_LPUART23_CLK_SEL_SHIFT, CCM_CSCMR2_LPUART23_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Lpuart01Mux = CCM_TUPLE(CSCMR2, CCM_CSCMR2_LPUART01_CLK_SEL_SHIFT, CCM_CSCMR2_LPUART01_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_TpiuMux = CCM_TUPLE(CSCMR3, CCM_CSCMR3_TPIU_CLK_SEL_SHIFT, CCM_CSCMR3_TPIU_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Sai1Mux = CCM_TUPLE(CSCMR3, CCM_CSCMR3_SAI1_CLK_SEL_SHIFT, CCM_CSCMR3_SAI1_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Sai0Mux = CCM_TUPLE(CSCMR3, CCM_CSCMR3_SAI0_CLK_SEL_SHIFT, CCM_CSCMR3_SAI0_CLK_SEL_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_EsaiMux = CCM_TUPLE(CSCMR3, CCM_CSCMR3_ESAI_CLK_SEL_SHIFT, CCM_CSCMR3_ESAI_CLK_SEL_MASK, CCM_NO_BUSY_WAIT)
}
 MUX control names for clock mux setting. More...
 
enum  clock_div_t {
  kCLOCK_ArmDiv = CCM_TUPLE(CSYSCDR, CCM_CSYSCDR_CPU_PODF_SHIFT, CCM_CSYSCDR_CPU_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_AxiDiv = CCM_TUPLE(CSYSCDR, CCM_CSYSCDR_AXI_PODF_SHIFT, CCM_CSYSCDR_AXI_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_AhbDiv = CCM_TUPLE(CSYSCDR, CCM_CSYSCDR_AHB_PODF_SHIFT, CCM_CSYSCDR_AHB_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_IpgDiv = CCM_TUPLE(CSYSCDR, CCM_CSYSCDR_IPG_PODF_SHIFT, CCM_CSYSCDR_IPG_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_FlexBusDiv = CCM_TUPLE(CSYSCDR, CCM_CSYSCDR_FB_PODF_SHIFT, CCM_CSYSCDR_FB_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_EnetRmiiDiv = CCM_TUPLE(CSCDR1, CCM_CSCDR1_ENET_RMII_PODF_SHIFT, CCM_CSCDR1_ENET_RMII_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_TpiuDiv = CCM_TUPLE(CSCDR1, CCM_CSCDR1_TPIU_PODF_SHIFT, CCM_CSCDR1_TPIU_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Flexspi1Div = CCM_TUPLE(CSCDR1, CCM_CSCDR1_FLEXSPI1_PODF_SHIFT, CCM_CSCDR1_FLEXSPI1_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Flexspi0Div = CCM_TUPLE(CSCDR1, CCM_CSCDR1_FLEXSPI0_PODF_SHIFT, CCM_CSCDR1_FLEXSPI0_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Usdhc1Div = CCM_TUPLE(CSCDR1, CCM_CSCDR1_USDHC1_PODF_SHIFT, CCM_CSCDR1_USDHC1_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Usdhc0Div = CCM_TUPLE(CSCDR1, CCM_CSCDR1_USDHC0_PODF_SHIFT, CCM_CSCDR1_USDHC0_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_MmdcDiv = CCM_TUPLE(CSCDR1, CCM_CSCDR1_MMDC_PODF_SHIFT, CCM_CSCDR1_MMDC_PODF_MASK, CCM_CDHIPR_MMDC_CH0_PODF_CHANGED_SHIFT),
  kCLOCK_Lpuart23Div = CCM_TUPLE(CSCDR2, CCM_CSCDR2_LPUART23_PODF_SHIFT, CCM_CSCDR2_LPUART23_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Lpuart01Div = CCM_TUPLE(CSCDR2, CCM_CSCDR2_LPUART01_PODF_SHIFT, CCM_CSCDR2_LPUART01_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Lpspi23Div = CCM_TUPLE(CSCDR2, CCM_CSCDR2_LPSPI23_PODF_SHIFT, CCM_CSCDR2_LPSPI23_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Lpspi01Div = CCM_TUPLE(CSCDR2, CCM_CSCDR2_LPSPI01_PODF_SHIFT, CCM_CSCDR2_LPSPI01_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_LptmrDiv = CCM_TUPLE(CSCDR3, CCM_CSCDR3_LPTMR_PODF_SHIFT, CCM_CSCDR3_LPTMR_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_LpitDiv = CCM_TUPLE(CSCDR3, CCM_CSCDR3_LPIT_PODF_SHIFT, CCM_CSCDR3_LPIT_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Lpi2c23Div = CCM_TUPLE(CSCDR3, CCM_CSCDR3_LPI2C23_PODF_SHIFT, CCM_CSCDR3_LPI2C23_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Lpi2c01Div = CCM_TUPLE(CSCDR3, CCM_CSCDR3_LPI2C01_PODF_SHIFT, CCM_CSCDR3_LPI2C01_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_EmvsimDiv = CCM_TUPLE(CSCDR4, CCM_CSCDR4_EMVSIM_PODF_SHIFT, CCM_CSCDR4_EMVSIM_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_FlexioDiv = CCM_TUPLE(CSCDR4, CCM_CSCDR4_FLEXIO_PODF_SHIFT, CCM_CSCDR4_FLEXIO_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Tpm23Div = CCM_TUPLE(CSCDR5, CCM_CSCDR5_TPM23_PODF_SHIFT, CCM_CSCDR5_TPM23_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Tpm01Div = CCM_TUPLE(CSCDR5, CCM_CSCDR5_TPM01_PODF_SHIFT, CCM_CSCDR5_TPM01_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_EsaiDiv = CCM_TUPLE(CSCDR6, CCM_CSCDR6_ESAI_PODF_SHIFT, CCM_CSCDR6_ESAI_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Sai1Div = CCM_TUPLE(CSCDR7, CCM_CSCDR7_SAI1_PODF_SHIFT, CCM_CSCDR7_SAI1_PODF_MASK, CCM_NO_BUSY_WAIT),
  kCLOCK_Sai0Div = CCM_TUPLE(CSCDR7, CCM_CSCDR7_SAI0_PODF_SHIFT, CCM_CSCDR7_SAI0_PODF_MASK, CCM_NO_BUSY_WAIT)
}
 DIV control names for clock div setting. More...
 
enum  clock_pll_t {
  kCLOCK_PllSys,
  kCLOCK_PllUsb1,
  kCLOCK_PllAudio,
  kCLOCK_PllEnet0,
  kCLOCK_PllEnet1,
  kCLOCK_PllEnet2,
  kCLOCK_PllUsb2
}
 PLL name. More...
 
enum  clock_pfd_t {
  kCLOCK_Pfd0 = 0U,
  kCLOCK_Pfd1 = 1U,
  kCLOCK_Pfd2 = 2U,
  kCLOCK_Pfd3 = 3U
}
 PLL PFD name. More...
 
enum  clock_usb_src_t {
  kCLOCK_Usb480M = 0,
  kCLOCK_UsbSrcUnused = 0xFFFFFFFFU
}
 USB clock source definition. More...
 
enum  clock_usb_phy_src_t { kCLOCK_Usbphy480M = 0 }
 Source of the USB HS PHY. More...
 

Variables

uint32_t g_xtal0Freq
 External XTAL (24M OSC/SYSOSC) clock frequency. More...
 
uint32_t g_xtal32Freq
 External RTC XTAL (32K OSC) clock frequency. More...
 

Driver version

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
 CLOCK driver version 2.0.0. More...
 

Clock gate, mux, and divider.

static void CLOCK_SetMux (clock_mux_t mux, uint32_t value)
 Set CCM MUX node to certain value. More...
 
static uint32_t CLOCK_GetMux (clock_mux_t mux)
 Get CCM MUX value. More...
 
static void CLOCK_SetDiv (clock_div_t divider, uint32_t value)
 Set CCM DIV node to certain value. More...
 
static uint32_t CLOCK_GetDiv (clock_div_t divider)
 Get CCM DIV node value. More...
 
static void CLOCK_ControlGate (clock_ip_name_t name, clock_gate_value_t value)
 Control the clock gate for specific IP. More...
 
static void CLOCK_EnableClock (clock_ip_name_t name)
 Enable the clock for specific IP. More...
 
static void CLOCK_DisableClock (clock_ip_name_t name)
 Disable the clock for specific IP. More...
 
static void CLOCK_SetMode (clock_mode_t mode)
 Setting the low power mode that system will enter on next assertion of dsm_request signal. More...
 

CCM Interrupts

static void CLOCK_EnableInterrupts (uint32_t mask)
 Enable/not mask CCM interrupts. More...
 
static void CLOCK_DisableInterrupts (uint32_t mask)
 Disable/mask CCM interrupts. More...
 
static uint32_t CLOCK_GetInterruptStatus (void)
 Get CCM interrupt status flags. More...
 
static void CLOCK_ClearInterruptStatus (uint32_t mask)
 Clear interrupt status flags. More...
 

CCM Get frequency

uint32_t CLOCK_GetFreq (clock_name_t clockName)
 Gets the clock frequency for a specific clock name. More...
 
uint32_t CLOCK_GetCpuClkFreq (void)
 Get the CCM CPU/core/system frequency. More...
 
uint32_t CLOCK_GetAxiBusClkFreq (void)
 Get the CCM AXI bus frequency. More...
 
uint32_t CLOCK_GetAhbBusClkFreq (void)
 Get the CCM AHB bus frequency. More...
 
uint32_t CLOCK_GetIpgBusClkFreq (void)
 Get the CCM IPG bus frequency. More...
 
uint32_t CLOCK_GetFlexBusClkFreq (void)
 Get the CCM FlexBus frequency. More...
 
static uint32_t CLOCK_GetRcOscFreq (void)
 Get the RCOSC (internel IRC) clock frequency. More...
 
static uint32_t CLOCK_GetXtalOscFreq (void)
 Get the external IRC clock frequency. More...
 
uint32_t CLOCK_GetOscFreq (void)
 Get the OSC clock frequency selected by ANATOP HW_ANADIG_LOWPWR_CTRL[OSC_SEL]. More...
 
uint32_t CLOCK_GetRtcFreq (void)
 Get the RTC clock frequency. More...
 

OSC operations

void CLOCK_InitExternalClk (bool bypassXtalOsc)
 Initialize the external 24MHz clock. More...
 
void CLOCK_DeinitExternalClk (void)
 Deinitialize the external 24MHz clock. More...
 
void CLOCK_SwitchOsc (clock_osc_t osc)
 Switch the OSC. More...
 
static void CLOCK_InitRtcRingOsc (void)
 Initializes the ANATOP RTC ring OSC. More...
 
static void CLOCK_DeinitRtcRingOsc (void)
 De-initializes the ANATOP RTC ring OSC. More...
 
static void CLOCK_SetXtal0Freq (uint32_t freq)
 Set the XTAL0 frequency based on board setting. More...
 
static void CLOCK_SetXtal32Freq (uint32_t freq)
 Set the XTAL32 frequency based on board setting. More...
 
void CLOCK_InitRcOsc24M (void)
 Initialize the RC oscillator 24MHz clock.
 
void CLOCK_DeinitRcOsc24M (void)
 Power down the RCOSC 24M clock.
 

PLL/PFD operations

void CLOCK_InitSysPll (const clock_sys_pll_config_t *config)
 Initialize the System PLL. More...
 
void CLOCK_DeinitSysPll (void)
 De-initialize the System PLL.
 
void CLOCK_InitUsb1Pll (const clock_usb_pll_config_t *config)
 Initialize the USB1 PLL. More...
 
void CLOCK_DeinitUsb1Pll (void)
 Deinitialize the USB1 PLL.
 
void CLOCK_InitUsb2Pll (const clock_usb_pll_config_t *config)
 Initialize the USB2 PLL. More...
 
void CLOCK_DeinitUsb2Pll (void)
 Deinitialize the USB2 PLL.
 
void CLOCK_InitAudioPll (const clock_audio_pll_config_t *config)
 Initializes the Audio PLL. More...
 
void CLOCK_DeinitAudioPll (void)
 De-initialize the Audio PLL.
 
void CLOCK_InitEnetPll (const clock_enet_pll_config_t *config)
 Initialize the ENET PLL. More...
 
void CLOCK_DeinitEnetPll (void)
 Deinitialize the ENET PLL. More...
 
uint32_t CLOCK_GetPllFreq (clock_pll_t pll)
 Get current PLL output frequency. More...
 
void CLOCK_InitSysPfd (clock_pfd_t pfd, uint8_t pfdFrac)
 Initialize the System PLL PFD. More...
 
void CLOCK_DeinitSysPfd (clock_pfd_t pfd)
 De-initialize the System PLL PFD. More...
 
void CLOCK_InitUsb1Pfd (clock_pfd_t pfd, uint8_t pfdFrac)
 Initialize the USB1 PLL PFD. More...
 
void CLOCK_DeinitUsb1Pfd (clock_pfd_t pfd)
 De-initialize the USB1 PLL PFD. More...
 
uint32_t CLOCK_GetSysPfdFreq (clock_pfd_t pfd)
 Get current System PLL PFD output frequency. More...
 
uint32_t CLOCK_GetUsb1PfdFreq (clock_pfd_t pfd)
 Get current USB1 PLL PFD output frequency. More...
 
bool CLOCK_EnableUsbhs0Clock (clock_usb_src_t src, uint32_t freq)
 Enable USB HS clock. More...
 
bool CLOCK_EnableUsbhs0PhyPllClock (clock_usb_phy_src_t src, uint32_t freq)
 Enable USB HS PHY PLL clock. More...
 
void CLOCK_DisableUsbhs0PhyPllClock (void)
 Disable USB HS PHY PLL clock. More...
 
bool CLOCK_EnableUsbhs1Clock (clock_usb_src_t src, uint32_t freq)
 Enable USB HS clock. More...
 
bool CLOCK_EnableUsbhs1PhyPllClock (clock_usb_phy_src_t src, uint32_t freq)
 Enable USB HS PHY PLL clock. More...
 
void CLOCK_DisableUsbhs1PhyPllClock (void)
 Disable USB HS PHY PLL clock. More...
 

Data Structure Documentation

struct clock_usb_pll_config_t

Data Fields

uint8_t loopDivider
 PLL loop divider. More...
 

Field Documentation

uint8_t clock_usb_pll_config_t::loopDivider

0 - Fout=Fref*20; 1 - Fout=Fref*22

struct clock_sys_pll_config_t

Data Fields

uint8_t loopDivider
 PLL loop divider. More...
 
uint32_t numerator
 30 bit numerator of fractional loop divider. More...
 
uint32_t denominator
 30 bit denominator of fractional loop divider
 

Field Documentation

uint8_t clock_sys_pll_config_t::loopDivider

Intended to be 1 (528M). 0 - Fout=Fref*20; 1 - Fout=Fref*22

uint32_t clock_sys_pll_config_t::numerator
struct clock_audio_pll_config_t

Fout = Fref * (loopDivider + (float)Numerator/Denominator) / postDivider.

Data Fields

uint8_t loopDivider
 PLL loop divider. More...
 
uint8_t postDivider
 Divider after the PLL, should only be 1, 2, 4, 8, 16. More...
 
uint32_t numerator
 30 bit numerator of fractional loop divider. More...
 
uint32_t denominator
 30 bit denominator of fractional loop divider
 

Field Documentation

uint8_t clock_audio_pll_config_t::loopDivider

Valid range for DIV_SELECT divider value: 27~54.

uint8_t clock_audio_pll_config_t::postDivider
uint32_t clock_audio_pll_config_t::numerator
struct clock_enet_pll_config_t

Data Fields

bool enableClkOutput0
 Power on and enable PLL clock output for ENET0 (ref_enetpll0). More...
 
bool enableClkOutput1
 Power on and enable PLL clock output for ENET1 (ref_enetpll1). More...
 
bool enableClkOutput2
 Power on and enable PLL clock output for ENET2 (ref_enetpll2). More...
 
uint8_t loopDivider0
 Controls the frequency of the ENET0 reference clock. More...
 
uint8_t loopDivider1
 Controls the frequency of the ENET1 reference clock. More...
 

Field Documentation

bool clock_enet_pll_config_t::enableClkOutput0
bool clock_enet_pll_config_t::enableClkOutput1
bool clock_enet_pll_config_t::enableClkOutput2
uint8_t clock_enet_pll_config_t::loopDivider0

b00 25MHz b01 50MHz b10 100MHz (not 50% duty cycle) b11 125MHz

uint8_t clock_enet_pll_config_t::loopDivider1

b00 25MHz b01 50MHz b10 100MHz (not 50% duty cycle) b11 125MHz

Macro Definition Documentation

#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0

When set to 0, peripheral drivers will enable clock in initialize function and disable clock in de-initialize function. When set to 1, peripheral driver will not control the clock, application could control the clock out of the driver.

Note
All drivers share this feature switcher. If it is set to 1, application should handle clock enable and disable for all drivers.
#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 0, 0))
#define EDMA_CLOCKS
Value:
{ \
}
DMA1 Clock Gate.
Definition: fsl_clock.h:455
DMA0 Clock Gate.
Definition: fsl_clock.h:456
#define ENET_CLOCKS
Value:
{ \
}
ENET Clock Gate.
Definition: fsl_clock.h:457
#define LPUART_CLOCKS
Value:
{ \
}
LPUART1 Clock Gate.
Definition: fsl_clock.h:462
LPUART0 Clock Gate.
Definition: fsl_clock.h:463
LPUART2 Clock Gate.
Definition: fsl_clock.h:461
LPUART3 Clock Gate.
Definition: fsl_clock.h:460
#define LPSPI_CLOCKS
Value:
{ \
}
LPSPI1 Clock Gate.
Definition: fsl_clock.h:467
LPSPI3 Clock Gate.
Definition: fsl_clock.h:465
LPSPI2 Clock Gate.
Definition: fsl_clock.h:466
LPSPI0 Clock Gate.
Definition: fsl_clock.h:468
#define LPI2C_CLOCKS
Value:
{ \
}
LPI2C1 Debug Clock Gate.
Definition: fsl_clock.h:472
LPI2C0 Debug Clock Gate.
Definition: fsl_clock.h:473
LPI2C3 Debug Clock Gate.
Definition: fsl_clock.h:470
LPI2C2 Debug Clock Gate.
Definition: fsl_clock.h:471
#define SNVS_HP_CLOCKS
Value:
{ \
}
SNVS HP Clock Gate.
Definition: fsl_clock.h:475
#define SNVS_LP_CLOCKS
Value:
{ \
}
SNVS LP Clock Gate.
Definition: fsl_clock.h:577
#define CAAM_CLOCKS
Value:
{ \
}
CAAM Clock Gate.
Definition: fsl_clock.h:479
#define PCTL_CLOCKS
Value:
{ \
}
PCTL1 Clock Gate.
Definition: fsl_clock.h:485
PCTL4 Clock Gate.
Definition: fsl_clock.h:482
PCTL2 Clock Gate.
Definition: fsl_clock.h:484
PCTL0 Clock Gate.
Definition: fsl_clock.h:486
PCTL5 Clock Gate.
Definition: fsl_clock.h:481
PCTL3 Clock Gate.
Definition: fsl_clock.h:483
#define MIPFIL_CLOCKS
Value:
{ \
kCLOCK_Micfil0 \
}
#define FLEXSPI_CLOCKS
Value:
{ \
}
FLEXSPI0 Clock Gate.
Definition: fsl_clock.h:489
FLEXSPI1 Clock Gate.
Definition: fsl_clock.h:488
#define FLEXIO_CLOCKS
Value:
{ \
}
FLEXIO1 Clock Gate.
Definition: fsl_clock.h:491
FLEXIO0 Clock Gate.
Definition: fsl_clock.h:492
#define FLEXCAN_CLOCKS
Value:
{ \
kCLOCK_Flexcan0, kCLOCK_Flexcan1 \
}
#define SAI_CLOCKS
Value:
{ \
}
SAI0 Clock Gate.
Definition: fsl_clock.h:496
SAI1 Clock Gate.
Definition: fsl_clock.h:495
#define SJC_CLOCKS
Value:
{ \
}
SJC Clock Gate.
Definition: fsl_clock.h:499
#define SPDIF_CLOCKS
Value:
{ \
kCLOCK_Spdif0 \
}
#define ROMC_CLOCKS
Value:
{ \
}
ROMC Clock Gate.
Definition: fsl_clock.h:500
#define IIM_CLOCKS
Value:
{ \
}
IIM Clock Gate.
Definition: fsl_clock.h:501
#define LPSPI_PERIPH_CLOCKS
Value:
{ \
}
LPSPI3 Peripheral Clock Gate.
Definition: fsl_clock.h:503
LPSPI0 Peripheral Clock Gate.
Definition: fsl_clock.h:506
LPSPI1 Peripheral Clock Gate.
Definition: fsl_clock.h:505
LPSPI2 Peripheral Clock Gate.
Definition: fsl_clock.h:504
#define LPUART_PERIPH_CLOCKS
Value:
{ \
}
LPUART2 Peripheral Clock Gate.
Definition: fsl_clock.h:509
LPUART1 Peripheral Clock Gate.
Definition: fsl_clock.h:510
LPUART0 Peripheral Clock Gate.
Definition: fsl_clock.h:511
LPUART3 Peripheral Clock Gate.
Definition: fsl_clock.h:508
#define LPI2C_PERIPH_CLOCKS
Value:
{ \
}
LPI2C3 Peripheral Clock Gate.
Definition: fsl_clock.h:513
LPI2C0 Peripheral Clock Gate.
Definition: fsl_clock.h:516
LPI2C2 Peripheral Clock Gate.
Definition: fsl_clock.h:514
LPI2C1 Peripheral Clock Gate.
Definition: fsl_clock.h:515
#define TPSMP_CLOCKS
Value:
{ \
}
TPSMP Clock Gate.
Definition: fsl_clock.h:519
#define ESAI_CLOCKS
Value:
{ \
}
ESAI Clock Gate.
Definition: fsl_clock.h:520
#define TPM_CLOCKS
Value:
{ \
}
TPM3 Clock Gate.
Definition: fsl_clock.h:522
TPM1 Clock Gate.
Definition: fsl_clock.h:524
TPM2 Clock Gate.
Definition: fsl_clock.h:523
TPM0 Clock Gate.
Definition: fsl_clock.h:525
#define FLEXCAN_PERIPH_CLOCKS
Value:
{ \
kCLOCK_Flexcan0Periph, kCLOCK_Flexcan1Periph, \
}
#define LPTMR_PERIPH_CLOCKS
Value:
{ \
}
LPTMR0 Peripheral Clock Gate.
Definition: fsl_clock.h:530
LPTMR1 Peripheral Clock Gate.
Definition: fsl_clock.h:528
#define LPTMR_CLOCKS
Value:
{ \
}
LPTMR0 Bus Clock Gate.
Definition: fsl_clock.h:531
LPTMR1 Bus Clock Gate.
Definition: fsl_clock.h:529
#define LPIT_PERIPH_CLOCKS
Value:
{ \
}
LPIT0 Peripheral Clock Gate.
Definition: fsl_clock.h:535
LPIT1 Peripheral Clock Gate.
Definition: fsl_clock.h:533
#define LPIT_CLOCKS
Value:
{ \
}
LPIT0 Bus Clock Gate.
Definition: fsl_clock.h:536
LPIT1 Bus Clock Gate.
Definition: fsl_clock.h:534
#define WDOG_CLOCKS
Value:
{ \
}
WDOG Clock Gate.
Definition: fsl_clock.h:539
#define USDHC_CLOCKS
Value:
{ \
}
USDHC0 Clock Gate.
Definition: fsl_clock.h:542
USDHC1 Clock Gate.
Definition: fsl_clock.h:541
#define EMVSIM_CLOCKS
Value:
{ \
}
EMVSIM0 Clock Gate.
Definition: fsl_clock.h:545
EMVSIM1 Clock Gate.
Definition: fsl_clock.h:544
#define CRC_CLOCKS
Value:
{ \
}
CRC Clock Gate.
Definition: fsl_clock.h:547
#define CRC_CLOCKS
Value:
{ \
}
CRC Clock Gate.
Definition: fsl_clock.h:547
#define CAAM_MEM_CLOCKS
Value:
{ \
}
CAAM memory Clock Gate.
Definition: fsl_clock.h:552
#define CAAM_CTRL_CLOCKS
Value:
{ \
}
CAAM controller Clock Gate.
Definition: fsl_clock.h:551
#define LPDAC_CLOCKS
Value:
{ \
}
DAC1 Clock Gate.
Definition: fsl_clock.h:554
DAC0 Clock Gate.
Definition: fsl_clock.h:555
#define ADC_CLOCKS
Value:
{ \
}
ADC1 Clock Gate.
Definition: fsl_clock.h:557
ADC0 Clock Gate.
Definition: fsl_clock.h:558
#define TRGMUX_CLOCKS
Value:
{ \
}
Trigger MUX Clock Gate.
Definition: fsl_clock.h:560
#define IEE_CLOCKS
Value:
{ \
}
IEE Clock Gate.
Definition: fsl_clock.h:561
#define TPIU_CLOCKS
Value:
{ \
}
TPIU Clock Gate.
Definition: fsl_clock.h:562
#define IOMUXC_CLOCKS
Value:
{ \
}
IOMUXC1 Clock Gate.
Definition: fsl_clock.h:567
IOMUXC0 Clock Gate.
Definition: fsl_clock.h:568
#define FSL_CLOCK_MMDC_IPG_GATE_COUNT   1U
#define MMDC_ACLK_CLOCKS
Value:
{ \
}
MMDC ACLK.
Definition: fsl_clock.h:476
#define RGPIO_CLOCKS
Value:
{ \
}
RGPIO Clock Gate.
Definition: fsl_clock.h:578
#define SIM_CLOCKS
Value:
{ \
}
SIM Clock Gate.
Definition: fsl_clock.h:573
#define FLEXBUS_CLOCKS
Value:
{ \
}
FLEXBUS Clock Gate.
Definition: fsl_clock.h:572
#define DMAMUX_CLOCKS
Value:
{ \
}
DMAMUX1 Clock Gate.
Definition: fsl_clock.h:575
DMAMUX0 Clock Gate.
Definition: fsl_clock.h:576
#define SDRAM_CLOCKS
Value:
{ \
}
SDRAMC Clock Gate.
Definition: fsl_clock.h:571
#define FSL_CLOCK_XRDC_GATE_COUNT   0U
#define kCLOCK_CoreSysClk   kCLOCK_CpuClk
#define CLOCK_GetCoreSysClkFreq   CLOCK_GetCpuClkFreq

Enumeration Type Documentation

Enumerator
kCLOCK_CpuClk 

CPU clock.

kCLOCK_AxiClk 

AXI bus clock.

kCLOCK_AhbClk 

AHB bus clock.

kCLOCK_IpgClk 

IPG bus clock.

kCLOCK_FlexBusClk 

FlexBus clock.

kCLOCK_RcOscClk 

RCOSC clock (internal IRC).

kCLOCK_XtalOscClk 

External OSC clock.

kCLOCK_OscClk 

OSC clock selected by ANATOP HW_ANADIG_LOWPWR_CTRL[OSC_SEL].

kCLOCK_RtcClk 

RTC clock.

(RTCCLK)

kCLOCK_Usb1PllClk 

USB1PLLCLK.

kCLOCK_Usb1PllPfd0Clk 

USB1PLLPDF0CLK.

kCLOCK_Usb1PllPfd1Clk 

USB1PLLPFD1CLK.

kCLOCK_Usb1PllPfd2Clk 

USB1PLLPFD2CLK.

kCLOCK_Usb1PllPfd3Clk 

USB1PLLPFD3CLK.

kCLOCK_Usb2PllClk 

USB2PLLCLK.

kCLOCK_SysPllClk 

SYSPLLCLK.

kCLOCK_SysPllPfd0Clk 

SYSPLLPDF0CLK.

kCLOCK_SysPllPfd1Clk 

SYSPLLPFD1CLK.

kCLOCK_SysPllPfd2Clk 

SYSPLLPFD2CLK.

kCLOCK_SysPllPfd3Clk 

SYSPLLPFD3CLK.

kCLOCK_EnetPll0Clk 

Enet PLLCLK ref_enetpll0.

kCLOCK_EnetPll1Clk 

Enet PLLCLK ref_enetpll1.

kCLOCK_EnetPll2Clk 

Enet PLLCLK ref_enetpll2.

kCLOCK_AudioPllClk 

Audio PLLCLK.

Enumerator
kCLOCK_Dma1 

DMA1 Clock Gate.

kCLOCK_Dma0 

DMA0 Clock Gate.

kCLOCK_Enet0 

ENET Clock Gate.

kCLOCK_Lpuart3 

LPUART3 Clock Gate.

kCLOCK_Lpuart2 

LPUART2 Clock Gate.

kCLOCK_Lpuart1 

LPUART1 Clock Gate.

kCLOCK_Lpuart0 

LPUART0 Clock Gate.

kCLOCK_Lpspi3 

LPSPI3 Clock Gate.

kCLOCK_Lpspi2 

LPSPI2 Clock Gate.

kCLOCK_Lpspi1 

LPSPI1 Clock Gate.

kCLOCK_Lpspi0 

LPSPI0 Clock Gate.

kCLOCK_Lpi2c3 

LPI2C3 Debug Clock Gate.

kCLOCK_Lpi2c2 

LPI2C2 Debug Clock Gate.

kCLOCK_Lpi2c1 

LPI2C1 Debug Clock Gate.

kCLOCK_Lpi2c0 

LPI2C0 Debug Clock Gate.

kCLOCK_SnvsHp0 

SNVS HP Clock Gate.

kCLOCK_MmdcAClk 

MMDC ACLK.

kCLOCK_Caam0 

CAAM Clock Gate.

kCLOCK_Pctl5 

PCTL5 Clock Gate.

kCLOCK_Pctl4 

PCTL4 Clock Gate.

kCLOCK_Pctl3 

PCTL3 Clock Gate.

kCLOCK_Pctl2 

PCTL2 Clock Gate.

kCLOCK_Pctl1 

PCTL1 Clock Gate.

kCLOCK_Pctl0 

PCTL0 Clock Gate.

kCLOCK_Flexspi1 

FLEXSPI1 Clock Gate.

kCLOCK_Flexspi0 

FLEXSPI0 Clock Gate.

kCLOCK_Flexio1 

FLEXIO1 Clock Gate.

kCLOCK_Flexio0 

FLEXIO0 Clock Gate.

kCLOCK_Sai1 

SAI1 Clock Gate.

kCLOCK_Sai0 

SAI0 Clock Gate.

kCLOCK_Sjc0 

SJC Clock Gate.

kCLOCK_Romc0 

ROMC Clock Gate.

kCLOCK_Iim0 

IIM Clock Gate.

kCLOCK_Lpspi3Periph 

LPSPI3 Peripheral Clock Gate.

kCLOCK_Lpspi2Periph 

LPSPI2 Peripheral Clock Gate.

kCLOCK_Lpspi1Periph 

LPSPI1 Peripheral Clock Gate.

kCLOCK_Lpspi0Periph 

LPSPI0 Peripheral Clock Gate.

kCLOCK_Lpuart3Periph 

LPUART3 Peripheral Clock Gate.

kCLOCK_Lpuart2Periph 

LPUART2 Peripheral Clock Gate.

kCLOCK_Lpuart1Periph 

LPUART1 Peripheral Clock Gate.

kCLOCK_Lpuart0Periph 

LPUART0 Peripheral Clock Gate.

kCLOCK_Lpi2c3Periph 

LPI2C3 Peripheral Clock Gate.

kCLOCK_Lpi2c2Periph 

LPI2C2 Peripheral Clock Gate.

kCLOCK_Lpi2c1Periph 

LPI2C1 Peripheral Clock Gate.

kCLOCK_Lpi2c0Periph 

LPI2C0 Peripheral Clock Gate.

kCLOCK_Tpsmp0 

TPSMP Clock Gate.

kCLOCK_Esai0 

ESAI Clock Gate.

kCLOCK_Tpm3 

TPM3 Clock Gate.

kCLOCK_Tpm2 

TPM2 Clock Gate.

kCLOCK_Tpm1 

TPM1 Clock Gate.

kCLOCK_Tpm0 

TPM0 Clock Gate.

kCLOCK_Lptmr1Periph 

LPTMR1 Peripheral Clock Gate.

kCLOCK_Lptmr1 

LPTMR1 Bus Clock Gate.

kCLOCK_Lptmr0Periph 

LPTMR0 Peripheral Clock Gate.

kCLOCK_Lptmr0 

LPTMR0 Bus Clock Gate.

kCLOCK_Lpit1Periph 

LPIT1 Peripheral Clock Gate.

kCLOCK_Lpit1 

LPIT1 Bus Clock Gate.

kCLOCK_Lpit0Periph 

LPIT0 Peripheral Clock Gate.

kCLOCK_Lpit0 

LPIT0 Bus Clock Gate.

kCLOCK_Wdog0 

WDOG Clock Gate.

kCLOCK_Usdhc1 

USDHC1 Clock Gate.

kCLOCK_Usdhc0 

USDHC0 Clock Gate.

kCLOCK_Emvsim1 

EMVSIM1 Clock Gate.

kCLOCK_Emvsim0 

EMVSIM0 Clock Gate.

kCLOCK_Crc0 

CRC Clock Gate.

kCLOCK_Usbhs0 

USB Clock Gate.

kCLOCK_CaamController0 

CAAM controller Clock Gate.

kCLOCK_CaamMemory0 

CAAM memory Clock Gate.

kCLOCK_Lpdac1 

DAC1 Clock Gate.

kCLOCK_Lpdac0 

DAC0 Clock Gate.

kCLOCK_Adc1 

ADC1 Clock Gate.

kCLOCK_Adc0 

ADC0 Clock Gate.

kCLOCK_Trgmux0 

Trigger MUX Clock Gate.

kCLOCK_Iee0 

IEE Clock Gate.

kCLOCK_Tpiu0 

TPIU Clock Gate.

kCLOCK_Mmdc0 

MMDC channel0 ipg Clock Gate.

kCLOCK_Iomuxc1 

IOMUXC1 Clock Gate.

kCLOCK_Iomuxc0 

IOMUXC0 Clock Gate.

kCLOCK_Sdramc0 

SDRAMC Clock Gate.

kCLOCK_Flexbus0 

FLEXBUS Clock Gate.

kCLOCK_Sim0 

SIM Clock Gate.

kCLOCK_Dmamux1 

DMAMUX1 Clock Gate.

kCLOCK_Dmamux0 

DMAMUX0 Clock Gate.

kCLOCK_SnvsLp0 

SNVS LP Clock Gate.

kCLOCK_Rgpio0 

RGPIO Clock Gate.

Enumerator
kCLOCK_RcOsc 

On chip OSC.

kCLOCK_XtalOsc 

24M Xtal OSC

Enumerator
kCLOCK_ClockNotNeeded 

Clock is off during all modes.

kCLOCK_ClockNeededRun 

Clock is on in run mode, but off in WAIT and STOP modes.

kCLOCK_ClockNeededAll 

Clock is on in all modes.

kCLOCK_ClockNeededRunWait 

Clock is on during all modes, except STOP mode.

Enumerator
kCLOCK_ModeRun 

Remain in run mode.

kCLOCK_ModeWait 

Transfer to wait mode.

kCLOCK_ModeStop 

Transfer to stop mode.

Enumerator
kCLOCK_MmdcPodfUpdateInterrupt 

Interrupt due to update of mask_mmdc_podf.

kCLOCK_MmdcClkSelUpdateInterrupt 

Interrupt due to update of mask_mmdc_clk_sel.

kCLOCK_OnChipOscReadyInterrupt 

On board oscillator ready.

kCLOCK_PllLrfInterrupt 

Interrupt due to lrf of PLLs.

These constants define the mux control names for clock mux setting.

  • 0:7: REG offset to CCM_BASE in bytes.
  • 8:15: Root clock setting bit field shift.
  • 16:31: Root clock setting bit field width.
Enumerator
kCLOCK_SysPllMux 

SYSTEM PLL SW Clock mux.

kCLOCK_Usb1PllMux 

USB1 PLL SW Clock mux.

kCLOCK_OscIrcMux 

IRC or external OSC Clock.

kCLOCK_SysClkMux 

System Clock mux.

kCLOCK_Enet1588Mux 

ENET 1588 Clock mux.

kCLOCK_Lpspi23Mux 

LPSPI2 and LPSPI3 Clock mux.

kCLOCK_Lpspi01Mux 

LPSPI0 and LPSPI1 Clock mux.

kCLOCK_Flexspi1Mux 

FLEXSPI1 Clock2 mux.

kCLOCK_Flexspi0Mux 

FLEXSPI0 Clock mux.

kCLOCK_EnetRmiiMux 

ENET RMII Clock mux.

kCLOCK_Usdhc1Mux 

USDHC1 Clock mux.

kCLOCK_Usdhc0Mux 

USDHC0 Clock mux.

kCLOCK_MmdcMux 

MMDC Clock mux.

kCLOCK_Tpm23Mux 

TPM2 and TPM3 Clock mux.

kCLOCK_Tpm01Mux 

TPM0 and TPM1 Clock mux.

kCLOCK_LpitMux 

LPIT Clock mux.

kCLOCK_FlexioMux 

FLEXIO Clock mux.

kCLOCK_EmvsimMux 

EMVSIM Clock mux.

kCLOCK_Lpi2c23Mux 

LPI2C2 and LPI2C3 Clock mux.

kCLOCK_Lpi2c01Mux 

LPI2C0 and LPI2C1 Clock mux.

kCLOCK_Lpuart23Mux 

LPUART2 and LPUART3 Clock mux.

kCLOCK_Lpuart01Mux 

LPUART0 and LPUART1 Clock mux.

kCLOCK_TpiuMux 

TPIU Clock mux.

kCLOCK_Sai1Mux 

SAI1 Clock mux.

kCLOCK_Sai0Mux 

SAI0 Pre Clock mux.

kCLOCK_EsaiMux 

ESAI Clock mux.

These constants define div control names for clock div setting.

  • 0:7: REG offset to CCM_BASE in bytes.
  • 8:15: Root clock setting bit field shift.
  • 16:31: Root clock setting bit field width.
Enumerator
kCLOCK_ArmDiv 

core div name

kCLOCK_AxiDiv 

axi div name

kCLOCK_AhbDiv 

ahb div name

kCLOCK_IpgDiv 

ipg div name

kCLOCK_FlexBusDiv 

FB Clock post divider.

kCLOCK_EnetRmiiDiv 

ENET RMII Clock post divider.

kCLOCK_TpiuDiv 

TPIU post divider.

kCLOCK_Flexspi1Div 

FLEXSPI1 Clock post divider.

kCLOCK_Flexspi0Div 

FLEXSPI0 Clock post divider.

kCLOCK_Usdhc1Div 

USDHC1 Clock post divider.

kCLOCK_Usdhc0Div 

USDHC0 Clock post divider.

kCLOCK_MmdcDiv 

MMDC Clock post divider.

kCLOCK_Lpuart23Div 

LPUART2 and LPUART3 Clock post divider.

kCLOCK_Lpuart01Div 

LPUART0 and LPUART1 Clock post divider.

kCLOCK_Lpspi23Div 

LPSPI2 and LPSPI3 Clock post divider .

kCLOCK_Lpspi01Div 

LPSPI0 and LPSPI1 Clock post divider .

kCLOCK_LptmrDiv 

LPTMR Clock post divider .

kCLOCK_LpitDiv 

LPIT Clock post divider.

kCLOCK_Lpi2c23Div 

LPI2C2 and LPI2C3 Clock post divider.

kCLOCK_Lpi2c01Div 

LPI2C0 and LPI2C1 Clock post divider.

kCLOCK_EmvsimDiv 

EMVSIM Clock post divider .

kCLOCK_FlexioDiv 

FLEXIO Clock post divider .

kCLOCK_Tpm23Div 

TPM2 and TPM3 Clock post divider.

kCLOCK_Tpm01Div 

TPM0 and TPM1 Clock post divider.

kCLOCK_EsaiDiv 

ESAI Clock post divider.

kCLOCK_Sai1Div 

SAI1 Clock post divider.

kCLOCK_Sai0Div 

SAI0 Clock post divider.

Enumerator
kCLOCK_PllSys 

PLL SYS.

kCLOCK_PllUsb1 

PLL USB1.

kCLOCK_PllAudio 

PLL Audio.

kCLOCK_PllEnet0 

PLL Enet0.

kCLOCK_PllEnet1 

PLL Enet1.

kCLOCK_PllEnet2 

PLL Enet2.

kCLOCK_PllUsb2 

PLL USB2.

Enumerator
kCLOCK_Pfd0 

PLL PFD0.

kCLOCK_Pfd1 

PLL PFD1.

kCLOCK_Pfd2 

PLL PFD2.

kCLOCK_Pfd3 

PLL PFD3.

Enumerator
kCLOCK_Usb480M 

Use 480M.

kCLOCK_UsbSrcUnused 

Used when the function does not care the clock source.

Enumerator
kCLOCK_Usbphy480M 

Use 480M.

Function Documentation

static void CLOCK_SetMux ( clock_mux_t  mux,
uint32_t  value 
)
inlinestatic
Parameters
muxWhich mux node to set, see clock_mux_t.
valueClock mux value to set, different mux has different value range.
static uint32_t CLOCK_GetMux ( clock_mux_t  mux)
inlinestatic
Parameters
muxWhich mux node to get, see clock_mux_t.
Returns
Clock mux value.
static void CLOCK_SetDiv ( clock_div_t  divider,
uint32_t  value 
)
inlinestatic
Parameters
dividerWhich div node to set, see clock_div_t.
valueClock div value to set, different divider has different value range.
static uint32_t CLOCK_GetDiv ( clock_div_t  divider)
inlinestatic
Parameters
dividerWhich div node to get, see clock_div_t.
static void CLOCK_ControlGate ( clock_ip_name_t  name,
clock_gate_value_t  value 
)
inlinestatic
Parameters
nameWhich clock to enable, see clock_ip_name_t.
valueClock gate value to set, see clock_gate_value_t.
static void CLOCK_EnableClock ( clock_ip_name_t  name)
inlinestatic
Parameters
nameWhich clock to enable, see clock_ip_name_t.
static void CLOCK_DisableClock ( clock_ip_name_t  name)
inlinestatic
Parameters
nameWhich clock to disable, see clock_ip_name_t.
static void CLOCK_SetMode ( clock_mode_t  mode)
inlinestatic
Parameters
modeWhich mode to enter, see clock_mode_t.
static void CLOCK_EnableInterrupts ( uint32_t  mask)
inlinestatic

The mask is a logical OR of enumeration members. See _clock_interrupt. This example shows how to enable/not mask the on-chip OSC ready and PLL LRF interrupts:

Parameters
maskThe interrupts to enable. Logical OR of _clock_interrupt.
static void CLOCK_DisableInterrupts ( uint32_t  mask)
inlinestatic

The mask is a logical OR of enumeration members. See _clock_interrupt. This example shows how to disable/mask the on-chip OSC ready and PLL LRF interrupts:

Parameters
maskThe interrupts to disable. Logical OR of _clock_interrupt.
static uint32_t CLOCK_GetInterruptStatus ( void  )
inlinestatic

The interrupt status flags are returned as the logical OR value of the enumerators _clock_interrupt. To check a specific interrupt enable status, compare the return value with enumerators in _clock_interrupt. For example, to check whether the on-chip OSC ready interrupt is enabled:

* uint32_t interruptStatus = CLOCK_GetInterruptStatus();
*
* if (kCLOCK_OnChipOscReadyInterrupt & interruptStatus)
* {
* ...
* }
*
*
Returns
The interrupts status flags to get. Logical OR of _clock_interrupt.
static void CLOCK_ClearInterruptStatus ( uint32_t  mask)
inlinestatic

The interrupt status flags are input as the logical OR value of the enumerators _clock_interrupt.

Parameters
maskThe interrupts status flags to get. Logical OR of _clock_interrupt.
uint32_t CLOCK_GetFreq ( clock_name_t  clockName)

This function checks the current clock configurations and then calculates the clock frequency for a specific clock name defined in clock_name_t.

Parameters
clockNameClock names defined in clock_name_t
Returns
Clock frequency value in hertz
uint32_t CLOCK_GetCpuClkFreq ( void  )
Returns
Clock frequency; If the clock is invalid, returns 0.
uint32_t CLOCK_GetAxiBusClkFreq ( void  )
Returns
Clock frequency; If the clock is invalid, returns 0.
uint32_t CLOCK_GetAhbBusClkFreq ( void  )
Returns
Clock frequency; If the clock is invalid, returns 0.
uint32_t CLOCK_GetIpgBusClkFreq ( void  )
Returns
Clock frequency; If the clock is invalid, returns 0.
uint32_t CLOCK_GetFlexBusClkFreq ( void  )
Returns
Clock frequency; If the clock is invalid, returns 0.
static uint32_t CLOCK_GetRcOscFreq ( void  )
inlinestatic
Returns
Clock frequency.
static uint32_t CLOCK_GetXtalOscFreq ( void  )
inlinestatic
Returns
Clock frequency.
uint32_t CLOCK_GetOscFreq ( void  )
Returns
Clock frequency; If the clock is invalid, returns 0.
uint32_t CLOCK_GetRtcFreq ( void  )
Returns
Clock frequency; If the clock is invalid, returns 0.
void CLOCK_InitExternalClk ( bool  bypassXtalOsc)

This function supports two modes:

  1. Use external crystal oscillator.
  2. Bypass the external crystal oscillator, using input source clock directly.

After this function, please call CLOCK_SetXtal0Freq to inform clock driver the external clock frequency.

Parameters
bypassXtalOscPass in true to bypass the external crystal oscillator.
void CLOCK_DeinitExternalClk ( void  )

This function disables the external 24MHz clock.

After this function, please call CLOCK_SetXtal0Freq to set external clock frequency to 0.

void CLOCK_SwitchOsc ( clock_osc_t  osc)

This function switches the OSC source for SoC.

Parameters
oscOSC source to switch to.
static void CLOCK_InitRtcRingOsc ( void  )
inlinestatic

This function enables the internal ring oscillator that can be used in lieu of an external 32k crystal. The accuracy is relatively poor ~(10-40KHz) over process and environmental conditions. The crystal oscillator is automatically chosen to source the rtc clock if present. The choice is made based on the output of the clock monitor block.

static void CLOCK_DeinitRtcRingOsc ( void  )
inlinestatic

This function disables the ANATOP RTC ring OSC.

static void CLOCK_SetXtal0Freq ( uint32_t  freq)
inlinestatic
Parameters
freqThe XTAL0/EXTAL0 input clock frequency in Hz.
static void CLOCK_SetXtal32Freq ( uint32_t  freq)
inlinestatic
Parameters
freqThe XTAL32/EXTAL32 input clock frequency in Hz.
void CLOCK_InitSysPll ( const clock_sys_pll_config_t *  config)

This function initializes the System PLL with specific settings

Parameters
configConfiguration to set to PLL.
void CLOCK_InitUsb1Pll ( const clock_usb_pll_config_t *  config)

This function initializes the USB1 PLL with specific settings

Parameters
configConfiguration to set to PLL.
void CLOCK_InitUsb2Pll ( const clock_usb_pll_config_t *  config)

This function initializes the USB2 PLL with specific settings

Parameters
configConfiguration to set to PLL.
void CLOCK_InitAudioPll ( const clock_audio_pll_config_t *  config)

This function initializes the Audio PLL with specific settings

Parameters
configConfiguration to set to PLL.
void CLOCK_InitEnetPll ( const clock_enet_pll_config_t *  config)

This function initializes the ENET PLL with specific settings.

Parameters
configConfiguration to set to PLL.
void CLOCK_DeinitEnetPll ( void  )

This function disables the ENET PLL.

uint32_t CLOCK_GetPllFreq ( clock_pll_t  pll)

This function get current output frequency of specific PLL

Parameters
pllpll name to get frequency.
Returns
The PLL output frequency in hertz.
void CLOCK_InitSysPfd ( clock_pfd_t  pfd,
uint8_t  pfdFrac 
)

This function initializes the System PLL PFD. During new value setting, the clock output is disabled to prevent glitch.

Parameters
pfdWhich PFD clock to enable.
pfdFracThe PFD FRAC value.
Note
It is recommended that PFD settings are kept between 12-35.
void CLOCK_DeinitSysPfd ( clock_pfd_t  pfd)

This function disables the System PLL PFD.

Parameters
pfdWhich PFD clock to disable.
void CLOCK_InitUsb1Pfd ( clock_pfd_t  pfd,
uint8_t  pfdFrac 
)

This function initializes the USB1 PLL PFD. During new value setting, the clock output is disabled to prevent glitch.

Parameters
pfdWhich PFD clock to enable.
pfdFracThe PFD FRAC value.
Note
It is recommended that PFD settings are kept between 12-35.
void CLOCK_DeinitUsb1Pfd ( clock_pfd_t  pfd)

This function disables the USB1 PLL PFD.

Parameters
pfdWhich PFD clock to disable.
uint32_t CLOCK_GetSysPfdFreq ( clock_pfd_t  pfd)

This function get current output frequency of specific System PLL PFD

Parameters
pfdpfd name to get frequency.
Returns
The PFD output frequency in hertz.
uint32_t CLOCK_GetUsb1PfdFreq ( clock_pfd_t  pfd)

This function get current output frequency of specific USB1 PLL PFD

Parameters
pfdpfd name to get frequency.
Returns
The PFD output frequency in hertz.
bool CLOCK_EnableUsbhs0Clock ( clock_usb_src_t  src,
uint32_t  freq 
)

This function only enables the access to USB HS prepheral, upper layer should first call the CLOCK_EnableUsbhs0PhyPllClock to enable the PHY clock to use USB HS.

Parameters
srcUSB HS does not care about the clock source, here must be kCLOCK_UsbSrcUnused.
freqUSB HS does not care about the clock source, so this parameter is ignored.
Return values
trueThe clock is set successfully.
falseThe clock source is invalid to get proper USB HS clock.
bool CLOCK_EnableUsbhs0PhyPllClock ( clock_usb_phy_src_t  src,
uint32_t  freq 
)

This function enables the internal 480MHz USB PHY PLL clock.

Parameters
srcUSB HS PHY PLL clock source.
freqThe frequency specified by src.
Return values
trueThe clock is set successfully.
falseThe clock source is invalid to get proper USB HS clock.
void CLOCK_DisableUsbhs0PhyPllClock ( void  )

This function disables USB HS PHY PLL clock.

bool CLOCK_EnableUsbhs1Clock ( clock_usb_src_t  src,
uint32_t  freq 
)

This function only enables the access to USB HS prepheral, upper layer should first call the CLOCK_EnableUsbhs0PhyPllClock to enable the PHY clock to use USB HS.

Parameters
srcUSB HS does not care about the clock source, here must be kCLOCK_UsbSrcUnused.
freqUSB HS does not care about the clock source, so this parameter is ignored.
Return values
trueThe clock is set successfully.
falseThe clock source is invalid to get proper USB HS clock.
bool CLOCK_EnableUsbhs1PhyPllClock ( clock_usb_phy_src_t  src,
uint32_t  freq 
)

This function enables the internal 480MHz USB PHY PLL clock.

Parameters
srcUSB HS PHY PLL clock source.
freqThe frequency specified by src.
Return values
trueThe clock is set successfully.
falseThe clock source is invalid to get proper USB HS clock.
void CLOCK_DisableUsbhs1PhyPllClock ( void  )

This function disables USB HS PHY PLL clock.

Variable Documentation

uint32_t g_xtal0Freq

The XTAL (24M OSC/SYSOSC) clock frequency in Hz, when the clock is setup, use the function CLOCK_SetXtalFreq to set the value in to clock driver. For example, if XTAL is 24MHz,

* CLOCK_InitExternalClk(false); // Setup the 24M OSC/SYSOSC
* CLOCK_SetXtalFreq(240000000); // Set the XTAL value to clock driver.
*
uint32_t g_xtal32Freq

The RTC XTAL (32K OSC) clock frequency in Hz, when the clock is setup, use the function CLOCK_SetRtcXtalFreq to set the value in to clock driver.