MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
MMDC: Multi Mode DDR Controller Driver

Overview

The MCUXpresso SDK provides a peripheral driver for the Multi Mode DDR Controller block of MCUXpresso SDK devices.

The MMDC is configurable high performance and optimized DDR controller that support LPDDR2 x16 memory type. The MMDC driver provide function API to config the MMDC core and PHY register.

Typical use case

This example shows how to use the MMDC driver to initialize the external 16 bit DDR device. Initialize the MMDC controller and run the initialization sequence. The external DDR device is initialized and the DDR read and write is available.

Initialize the LPDDR2 Controller and external device.

{
.tCKE_Clocks = 3U,
.tCKSRE_Clocks = 2U,
.tCKSRX_Clocks = 2U,
.tRFC_Clocks = 40U,
.tXSR_Clocks = 43U,
.tXP_Clocks = 3U,
.tFAW_Clocks = 16U,
.tCL_Clocks = 3U,
.tMRD_Clocks = 3U,
.tRAS_Clocks = 13U,
.tWR_Clocks = 5U,
.tRTP_Clocks = 3U,
.tWTR_Clocks = 4U,
.tRRD_Clocks = 4U,
.ralat_Clocks = 5U,
.walat_Clocks = 0U,
.tRC_Clocks = 19U,
.tRCD_Clocks = 6U,
.tRP_Clocks = 6U,
.tRPA_Clocks = 7U,
.tCWL_Clocks = 1U,
.tRSTtoCKE_Clocks = 14U,
.tXPR_Clocks = 159U,
.tRTWSAME_Clocks = 2U,
.tWTRDIFF_Clocks = 3U,
.tWTWDIFF_Clocks = 3U,
.tRTWDIFF_Clocks = 2U,
.tRTRDIFF_Clocks = 2U,
.tDAI_Clocks = 3001U,
};
{
.caDelay = 0x47U,
.rDQOffset0 = 0x33333333U,
.rDQOffset1 = 0x33333333U,
.wDQOffset0 = 0xf3333333U,
.wDQOffset1 = 0xf3333333U,
.ddrCKDutyCtl0 = kMMDC_DutyHighPercent50,
.ddrCKDutyCtl1 = kMMDC_DutyHighPercent50,
};
{
.earlyCompTimer = 21U,
.hwZQFreq = kMMDC_ZQCalFreq1ms,
.cmpOutSample = 15U,
.tZQCl_Clocks = 144U,
.tZQCs_Clocks = 112U,
.tZQInit_Clocks = 400U,
.cmpOutSample = 7,
.hwPullDownOffset = 0U,
.hwPullUpOffset = 0U,
};
mmdc_config_t userConfig;
mmdc_write_calibration_config_t writeCal;
mmdc_auto_refresh_t autoRefresh;
readCal.readDelay0 = 0x40U;
readCal.readDelay1 = 0x40U;
writeCal.mode = kMMDC_CalWithPreDefine;
writeCal.writeDelay0 = 0x40U;
writeCal.writeDelay1 = 0x40U;
config.MR1 = 0x82U;
config.MR2 = 0x01U;
config.MR3 = 0x01U;
autoRefresh.refreshCnt = 0;
autoRefresh.refreshRate = 4;
/*
* config->bankInterleave = true;
* config->secondDDRClock = true;
* config->enableOnlyCS0 = true;
* config->devType = kMMDC_DDR3;
* config->devSize = 0x40000000U;
* config->devBank = kMMDC_Bank8;
* config->rowWidth = kMMDC_Row16Bits;
* config->colWidth = kMMDC_Col10Bits;
* config->burstLen = kMMDC_BurstLen8;
* config->odtByte1Config = kMMDC_RttNom60ohm;
* config->odtByte0Config = kMMDC_RttNom60ohm;
* config->enableActiveReadOdt = false;
* config->enableInactiveReadOdt = true;
* config->enableActiveWriteOdt = true;
* config->enableInactiveWriteOdt = true;
*/
MMDC_GetDefaultConfig(&userConfig);
userConfig.devType = kMMDC_LPDDR2_S4;
userConfig.devSize = EXAMPLE_DDR_SIZE;
userConfig.rowWidth = EXAMPLE_DDR_ROW_WIDTH;
userConfig.colWidth = EXAMPLE_DDR_COL_WIDTH;
userConfig.burstLen = EXAMPLE_DDR_BURST_LEN;
userConfig.timing = &timing;
userConfig.deviceConfig[0] = &config;
userConfig.readCalibration[0] = &readCal;
userConfig.writeCalibration[0] = &writeCal;
userConfig.tuning = &tuning;
userConfig.autoRefresh = &autoRefresh;
userConfig.zqCalibration = &zqCal;
/* MMDC Initialization. */
if (MMDC_Init(EXAMPLE_MMDC, &userConfig) != kStatus_Success)
{
PRINTF("\r\n MMDC Init Failed. \r\n");
}

Data Structures

struct  mmdc_readDQS_calibration_config_t
 MMDC read DQS gating calibration configuration collection. More...
 
struct  mmdc_writeLeveling_calibration_config_t
 MMDC write leveling calibration configuration collection. More...
 
struct  mmdc_read_calibration_config_t
 MMDC read calibration configuration collection. More...
 
struct  mmdc_fine_tuning_config_t
 MMDC write calibration configuration collection. More...
 
struct  mmdc_odt_config_t
 MMDC odt configuration collection. More...
 
struct  mmdc_power_config_t
 MMDC power configutation collection. More...
 
struct  mmdc_zq_config_t
 MMDC ZQ configuration collection. More...
 
struct  mmdc_cmd_config_t
 MMDC cmd configuration collection. More...
 
struct  mmdc_device_timing_t
 MMDC device device timing configuration collection. More...
 
struct  mmdc_auto_refresh_t
 MMDC auto refresh configuration collection. More...
 
struct  mmdc_exaccess_config_t
 MMDC exclusive access configuration collection. More...
 
struct  mmdc_profiling_config_t
 MMDC module profiling configuration collection. More...
 
struct  mmdc_performance_config_t
 MMDC performance configuration collection. More...
 
struct  mmdc_device_config_t
 MMDC module relate configuration collection. More...
 
struct  mmdc_config_t
 MMDC module relate configuration collection. More...
 

Typedefs

typedef void(* MMDC_SwitchFrequency )(MMDC_Type *, void *, void *, uint32_t)
 MMDC switch frequency api prototype. More...
 

Enumerations

enum  _mmdc_status {
  kStatus_MMDC_ErrorDGCalibration = MAKE_STATUS(kStatusGroup_MMDC, 1),
  kStatus_MMDC_ErrorReadCalibration = MAKE_STATUS(kStatusGroup_MMDC, 2),
  kStatus_MMDC_ErrorWriteCalibration = MAKE_STATUS(kStatusGroup_MMDC, 3),
  kStatus_MMDC_ErrorWriteLevelingCalibration = MAKE_STATUS(kStatusGroup_MMDC, 4),
  kStatus_MMDC_WaitFlagTimeout = MAKE_STATUS(kStatusGroup_MMDC, 5)
}
 MMDC status return codes. More...
 
enum  mmdc_device_type_t {
  kMMDC_LPDDR2_S4 = 0x0U,
  kMMDC_LPDDR2_S2 = 0x1U,
  kMMDC_DDR3 = 0x2U
}
 LPDDR2 device list. More...
 
enum  mmdc_device_bank_num_t {
  kMMDC_Bank8 = 0U,
  kMMDC_Bank4 = 1U
}
 LPDDR2 device bank number. More...
 
enum  mmdc_row_addr_width_t {
  kMMDC_Row11Bits = 0U,
  kMMDC_Row12Bits = 1U,
  kMMDC_Row13Bits = 2U,
  kMMDC_Row14Bits = 3U,
  kMMDC_Row15Bits = 4U,
  kMMDC_Row16Bits = 5U
}
 define for row addr width More...
 
enum  mmdc_col_addr_width_t {
  kMMDC_Col9Bits = 0U,
  kMMDC_Col10Bits = 1U,
  kMMDC_Col11Bits = 2U,
  kMMDC_Col8Bits = 3U,
  kMMDC_Col12Bits = 4U
}
 define for col addr width More...
 
enum  mmdc_burst_len_t {
  kMMDC_BurstLen4 = 0U,
  kMMDC_BurstLen8,
  kMMDC_BurstLen16
}
 define for burst length More...
 
enum  mmdc_cmd_type_t {
  kMMDC_NormalOperation = 0x0U,
  kMMDC_AutoRefresh = 0x2U,
  kMMDC_WriteModeRegister = 0x3U,
  kMMDC_ZQCalibration = 0x04U,
  kMMDC_PreChargeAll = 0x05U,
  kMMDC_ReadModeRegister = 0x6U
}
 define for command type auto refresh cmd: select correct CMD_CS before issue this cmd write mode register cmd: DDR2/DDR3: CMD_CS,CMD_BA,CMD_ADDR_LSB,CMD_ADDR_MSB LPDDR2: CMD_CS,MR_OP,MR_ADDR ZQ calibration cmd: DDR2/DDR3: CMD_CS,{CMD_ADDR_MSB,CMD_ADDR_LSB}=0x400,or 0x0 LPDDR2: through MRW cmd PreChargeAll cmd: selecet correct CMD_CS MRR cmd: only for LPDDR2/LPDDR3 device,must set correct CMD_CS,MR_ADDR More...
 
enum  mmdc_zq_calmode_t {
  kMMDC_ZQCaltoIOHW = 0x4U,
  kMMDC_ZQCaltoIODeviceLong = 0x01U,
  kMMDC_ZQCaltoDeviceOnly = 0x02U,
  kMMDC_ZQCaltoIODeviceLongShort,
  kMMDC_ZQFinetuning = 0x0AU,
  kMMDC_DisZQFinetuning = 0x0BU
}
 MMDC ZQ calibration type. More...
 
enum  mmdc_zq_calfreq_t {
  kMMDC_ZQCalFreq1ms = 0x0U,
  kMMDC_ZQCalFreq2ms = 0x1U,
  kMMDC_ZQCalFreq4ms = 0x2U,
  kMMDC_ZQCalFreq1s = 0x6U,
  kMMDC_ZQCalFreq16s = 0xEU,
  kMMDC_ZQCalFreq32s = 0xFU
}
 MMDC ZQ calibration frequency. More...
 
enum  mmdc_refresh_sel_t {
  kMMDC_RefreshTrigBy64K = 0U,
  kMMDC_RefreshTrigBy32K,
  kMMDC_RefreshTrigDDRCycles,
  kMMDC_RefreshTrigNone
}
 define MMDC refresh selector-select source of the clock that will trigger each refresh cycle. More...
 
enum  mmdc_profiling_action_t {
  kMMDC_EnProfilingWithID,
  kMMDC_FreezeProfiling,
  kMMDC_CheckOverFlow
}
 define MMDC profiling action define . More...
 
enum  mmdc_calibration_type_t {
  kMMDC_CalWithPreSetValue,
  kMMDC_CalWithMPR,
  kMMDC_CalWithPreDefine
}
 MMDC calibration type define . More...
 
enum  mmdc_calibaration_waitcycles_t {
  kMMDC_Wait16DDRCycles = 0U,
  kMMDC_Wait32DDRCycles = 0x01U
}
 define MMDC wait cycles before comparing data during calibration. More...
 
enum  mmdc_fine_tuning_dutycycle_t {
  kMMDC_DutyHighPercent48_5 = 0x1U,
  kMMDC_DutyHighPercent50 = 0x2U,
  kMMDC_DutyHighPercent51_5 = 0x4U
}
 define MMDC parameter fine tuning duty cyle. More...
 
enum  mmdc_termination_config_t {
  kMMDC_RttNomDisabled = 0x0U,
  kMMDC_RttNom120ohm = 0x1U,
  kMMDC_RttNom60ohm = 0x2U,
  kMMDC_RttNom40ohm = 0x3U,
  kMMDC_RttNom30ohm = 0x4U,
  kMMDC_RttNom24ohm = 0x5U,
  kMMDC_RttNom20ohm = 0x6U,
  kMMDC_RttNom17ohm = 0x7U
}
 define MMDC on chip termination configurations. More...
 
enum  _mmdc_lpddr2_derate {
  kMMDC_NoUpdateDerate = 0U,
  kMMDC_UpdateRefreshRate = 0x01U,
  kMMDC_DerateTiming = 0x02U,
  kMMDC_DisableDerate = 0x04U
}
 define LPDDR2 device derating type. More...
 
enum  _mmdc_exaccess_type {
  kMMDC_ExMonitorID0 = 0x01U,
  kMMDC_ExMonitorID1 = 0x02U,
  kMMDC_ExMonitorID2 = 0x04U,
  kMMDC_ExMonitorID3 = 0x08U,
  kMMDC_ExAccessResponse = 0x10U
}
 MMDC exclusive acess config type. More...
 

Driver version

#define FSL_MMDC_DRIVER_VERSION   (MAKE_VERSION(2U, 1U, 2U))
 MMDC driver Version 2.1.2.
 
#define MMDC_TIMEOUT   (500U)
 MMDC retry times.
 
#define MMDC_READ_DQS_FINE_TUNING_MASK   (0x77777777U)
 < More...
 
#define MMDC_WRITE_DQS_FINE_TUNING_MASK   (0xF3333333U)
 < More...
 
#define MMDC_PRE_DEFINE_VALUE_DEFAULT   (0xCCU)
 < More...
 
#define MMDC_MEASUREUNIT_ERR_FREQ   (100000000U)
 < More...
 

Initialization and deinitialization

void MMDC_GetDefaultConfig (mmdc_config_t *config)
 MMDC module get the default configutation get timing/power/zq configuration. More...
 
status_t MMDC_Init (MMDC_Type *base, mmdc_config_t *config)
 MMDC module initialization function. More...
 
void MMDC_Deinit (MMDC_Type *base)
 MMDC module deinit function. More...
 

device operation

void MMDC_HandleCommand (MMDC_Type *base, mmdc_cmd_config_t *config)
 MMDC module process the command,support transfer multi cmd in once function call. More...
 
status_t MMDC_GetReadData (MMDC_Type *base, uint32_t *data)
 MMDC get the read data. More...
 
void MMDC_EnhancePerformance (MMDC_Type *base, const mmdc_performance_config_t *config)
 MMDC module enhance performance function. More...
 
void MMDC_EnableAutoRefresh (MMDC_Type *base, mmdc_auto_refresh_t *config)
 Enable MMDC module periodic refresh scheme config. More...
 
static void MMDC_DisableAutoRefresh (MMDC_Type *base)
 Disable MMDC module periodic refresh scheme. More...
 
void MMDC_EnablePowerSaving (MMDC_Type *base, mmdc_power_config_t *config)
 MMDC enable automatic power saving. More...
 
static void MMDC_DisablePowerSaving (MMDC_Type *base)
 uint8_t targetCS, More...
 
void MMDC_Profiling (MMDC_Type *base, mmdc_profiling_config_t *config)
 MMDC profiling mechanism. More...
 
status_t MMDC_LPDDR2UpdateDerate (MMDC_Type *base, mmdc_auto_refresh_t *config, uint32_t type)
 MMDC update device refresh rate and derate timing for LPDDR2 device only. More...
 
status_t MMDC_MonitorLPDDR2OperationTemp (MMDC_Type *base, uint32_t *mr4)
 MMDC device operation temp monitor function. More...
 
status_t MMDC_ReadDQSGatingCalibration (MMDC_Type *base, mmdc_readDQS_calibration_config_t *config)
 MMDC module read DQS gating calibration function. More...
 
status_t MMDC_WriteLevelingCalibration (MMDC_Type *base, mmdc_writeLeveling_calibration_config_t *config)
 MMDC module write leveling calibration function. More...
 
status_t MMDC_WriteCalibration (MMDC_Type *base, mmdc_write_calibration_config_t *config)
 MMDC module write calibration function. More...
 
status_t MMDC_ReadCalibration (MMDC_Type *base, mmdc_read_calibration_config_t *config)
 MMDC module read calibration function. More...
 
void MMDC_DoFineTuning (MMDC_Type *base, mmdc_device_type_t devType, mmdc_fine_tuning_config_t *config)
 MMDC module read calibration function. More...
 
void MMDC_SetTiming (MMDC_Type *base, mmdc_device_type_t devType, mmdc_device_timing_t *timing)
 set timing parameter More...
 
void MMDC_DeviceInit (MMDC_Type *base, mmdc_device_type_t devType, uint8_t targetCS, mmdc_device_config_t *devConfig)
 Initialize MMDC controlled device. More...
 
status_t MMDC_EnterConfigurationMode (MMDC_Type *base, bool enable)
 MMDC module enter/exit configuration mode function. More...
 
void MMDC_DoZQCalibration (MMDC_Type *base, mmdc_device_type_t devType, mmdc_zq_config_t *zqCal)
 MMDC do ZQ calibration function. More...
 
status_t MMDC_EnableLowPowerMode (MMDC_Type *base, bool enable)
 MMDC enable/disable low power mode Once enable device will enter self-refresh mode. More...
 
status_t MMDC_EnableDVFSMode (MMDC_Type *base, bool enable)
 MMDC enable/disable dynamic frequency change mode Once enable device will enter self-refresh mode. More...
 
void MMDC_Reset (MMDC_Type *base)
 MMDC module reset function when you call this function will reset all internal register user need bo module init function bue do not need to do device init. More...
 
static void MMDC_SwitchDeviceFrequency (MMDC_Type *base, void *ccm, void *iomux, uint32_t param, uint32_t codeAddr)
 define the mmdc switch frequency. More...
 

debug

static void MMDC_EnableSBS (MMDC_Type *base, bool enable)
 MMDC enable/disable the SBS-step by step debug feature. More...
 
static void MMDC_TriggerSBS (MMDC_Type *base)
 MMDC trigger the MMDC dispatch the one pending request to device. More...
 
static uint32_t MMDC_GetAXIAddrBySBS (MMDC_Type *base)
 MMDC get AXI ddr which was dispatched by MMDC in SBS mode. More...
 
static uint32_t MMDC_GetAXIAttributeBySBS (MMDC_Type *base)
 MMDC get AXI attribute which was dispatched by MMDC in SBS mode. More...
 
static void MMDC_EnableProfiling (MMDC_Type *base, bool enable)
 MMDC enable/disable profiling feature. More...
 
static void MMDC_ResumeProfiling (MMDC_Type *base)
 MMDC resume profiling. More...
 
static void MMDC_ResetProfiling (MMDC_Type *base)
 MMDC reset profiling. More...
 
void MMDC_ExclusiveAccess (MMDC_Type *base, mmdc_exaccess_config_t *config, uint32_t type)
 MMDC exclusive access config function,config the monitor ID and response. More...
 

Data Structure Documentation

struct mmdc_readDQS_calibration_config_t

Data Fields

mmdc_calibration_type_t mode
 select calibration mode. More...
 
mmdc_calibaration_waitcycles_t waitCycles
 MMDC wait cycles before comparing sample data. More...
 
uint8_t dqsGatingHalfDelay0
 Read DQS gating half cycles delay count for Byte0. More...
 
uint8_t dqsGatingAbsDelay0
 Absolute read DQS gating delay offset for Byte0, So the total read DQS gating delay is (dqsGatingHalfDelay0)*0.5*cycle + (dqsGatingAbsDelay0)*1/256*cycle. More...
 
uint8_t dqsGatingHalfDelay1
 Read DQS gating half cycles delay count for Byte1. More...
 
uint8_t dqsGatingAbsDelay1
 Absolute read DQS gating delay offset for Byte1, So the total read DQS gating delay is (dqsGatingHalfDelay1)*0.5*cycle + (dqsGatingAbsDelay1)*1/256*cycle. More...
 
uint8_t readDelay0
 When using hardware calibration(MPR/Predefined mode), user should input RD_DL_ABS_OFFSET to place read DQS inside the read DQ window. More...
 
uint8_t readDelay1
 When using hardware calibration(MPR/Predefined mode), user should input RD_DL_ABS_OFFSET to place read DQS inside the read DQ window. More...
 

Field Documentation

mmdc_calibration_type_t mmdc_readDQS_calibration_config_t::mode
mmdc_calibaration_waitcycles_t mmdc_readDQS_calibration_config_t::waitCycles
uint8_t mmdc_readDQS_calibration_config_t::dqsGatingHalfDelay0
uint8_t mmdc_readDQS_calibration_config_t::dqsGatingAbsDelay0
uint8_t mmdc_readDQS_calibration_config_t::dqsGatingHalfDelay1
uint8_t mmdc_readDQS_calibration_config_t::dqsGatingAbsDelay1
uint8_t mmdc_readDQS_calibration_config_t::readDelay0
uint8_t mmdc_readDQS_calibration_config_t::readDelay1
struct mmdc_writeLeveling_calibration_config_t

Data Fields

mmdc_calibration_type_t mode
 select calibration mode. More...
 
uint8_t wLevelingOneDelay0
 Write leveling one cycles delay count for Byte0.
 
uint8_t wLevelingHalfDelay0
 Write leveling half cycles delay count for Byte0.
 
uint8_t wLevelingAbsDelay0
 
             Absolute Write leveling delay offset for Byte0, So the total delay is the sum of

(wLevelingAbsDelay0/256*cycle) + (wLevelingHalfDelay0*halfcycle) + (wLevelingOneDelay0*cycle). More...

 
uint8_t wLevelingOneDelay1
 Write leveling one cycles delay count for Byte1.
 
uint8_t wLevelingHalfDelay1
 Write leveling half cycles delay count for Byte1.
 
uint8_t wLevelingAbsDelay1
 
             Absolute Write leveling delay offset for Byte1, So the total delay is the sum of

(wLevelingAbsDelay1/256*cycle) + (wLevelingHalfDelay1*halfcycle) + (wLevelingOneDelay1*cycle). More...

 

Field Documentation

mmdc_calibration_type_t mmdc_writeLeveling_calibration_config_t::mode
uint8_t mmdc_writeLeveling_calibration_config_t::wLevelingAbsDelay0
uint8_t mmdc_writeLeveling_calibration_config_t::wLevelingAbsDelay1
struct mmdc_read_calibration_config_t

Data Fields

mmdc_calibration_type_t mode
 select calibration mode. More...
 
uint8_t readDelay0
 delay between read DQS strobe and read data of Byte0, RD_DL_ABS_OFFSET0. More...
 
uint8_t readDelay1
 delay between read DQS strobe and read data of Byte1, RD_DL_ABS_OFFSET1. More...
 

Field Documentation

mmdc_calibration_type_t mmdc_read_calibration_config_t::mode
uint8_t mmdc_read_calibration_config_t::readDelay0

The delay of the delay-line would be (RD_DL_ABS_OFFSET0 / 256) * MMDC AXIclock (fast clock). when using hardware calibration(MPR/Predefined mode), user should input RD_DL_ABS_OFFSET0 to place read DQS inside the read DQ window.

uint8_t mmdc_read_calibration_config_t::readDelay1

The delay of the delay-line would be (RD_DL_ABS_OFFSET1 / 256) * MMDC AXIclock (fast clock). when using hardware calibration(MPR/Predefined mode), user should input RD_DL_ABS_OFFSET1 to place read DQS inside the read DQ window.

struct mmdc_fine_tuning_config_t

Data Fields

uint32_t rDQOffset0
 fine-tuning adjustment to every bit in the read DQ byte0 relative to the read DQS, max dealy units can be add is 7
 
uint32_t rDQOffset1
 fine-tuning adjustment to every bit in the read DQ byte1 relative to the read DQS, max dealy units can be add is 7
 
uint32_t wDQOffset0
 fine-tuning adjustment to every bit in the write DQ byte0 relative to the write DQS, max dealy units can be add is 7
 
uint32_t wDQOffset1
 fine-tuning adjustment to every bit in the write DQ byte1 relative to the write DQS, max dealy units can be add is 7
 
uint32_t caDelay
 CA delay line fine tuning parameter. More...
 
mmdc_fine_tuning_dutycycle_t rDQDuty0
 Read DQS duty cycle fine tuning control of Byte1.
 
mmdc_fine_tuning_dutycycle_t rDQDuty1
 Read DQS duty cycle fine tuning control of Byte0.
 
mmdc_fine_tuning_dutycycle_t ddrCKDutyCtl0
 Primary duty cycle fine tuning control of DDR clock.
 
mmdc_fine_tuning_dutycycle_t ddrCKDutyCtl1
 Secondary duty cycle fine tuning control of DDR clock.
 
mmdc_fine_tuning_dutycycle_t wDQDuty0
 Write DQS duty cycle fine tuning control of Byte0.
 
mmdc_fine_tuning_dutycycle_t wDQDuty1
 Write DQS duty cycle fine tuning control of Byte1.
 

Field Documentation

uint32_t mmdc_fine_tuning_config_t::caDelay
struct mmdc_odt_config_t

Data Fields

mmdc_termination_config_t odtByte0Config
 On chip ODT byte1 resistor. More...
 
bool enableActiveReadOdt
 On chip ODT byte0 resistor. More...
 
bool enableInactiveReadOdt
 Active read CS ODT enable. More...
 
bool enableActiveWriteOdt
 Inactive read CS ODT enable. More...
 
bool enableInactiveWriteOdt
 Active write CS ODT enable. More...
 

Field Documentation

mmdc_termination_config_t mmdc_odt_config_t::odtByte0Config
bool mmdc_odt_config_t::enableActiveReadOdt
bool mmdc_odt_config_t::enableInactiveReadOdt
bool mmdc_odt_config_t::enableActiveWriteOdt
bool mmdc_odt_config_t::enableInactiveWriteOdt
struct mmdc_power_config_t

Data Fields

bool wIdle
 get write request buffer Idle status
 
bool rIdle
 get read request buffer Idle status
 
bool isInAutoPS
 indicate mmdc if in a automatic power saving mode
 
uint8_t idleClockToPS
 define the idle clock which device will automatically enter auto self-refresh mode ,default is 1024 clock cycles, max is 16320 cycles,calucate formula is idleClockToPS * 64 = idle clock note: idleClockToPS = 0 is forbidden
 
uint8_t idleClockToPrecharge0
 define the idle clock which device will automatically precharged. More...
 
uint8_t idleClockToPD0
 define the idle clock which device will enter power down, default is disable ,max clock is 32768 clocks, calucate formula idleClockToPD *16 = idle clock
 
uint8_t idleClockToPrecharge1
 define the idle clock which device will automatically precharged. More...
 
uint8_t idleClockToPD1
 define the idle clock which device will enter power down, default is disable ,max clock is 32768 clocks, calucate formula idleClockToPD *16 = idle clock
 

Field Documentation

uint8_t mmdc_power_config_t::idleClockToPrecharge0

default is disable ,max clock is 128 clocks, calucate formula 2^idleClockToPrecharge = idle clock

uint8_t mmdc_power_config_t::idleClockToPrecharge1

default is disable ,max clock is 128 clocks, calucate formula 2^idleClockToPrecharge = idle clock

struct mmdc_zq_config_t

Data Fields

mmdc_zq_calmode_t mode
 zq calibration mode. More...
 
uint8_t earlyCompTimer
 this field define the interval between the warming up of the comp of the ultra cal pad and the begining of the ZQ cal process with pads
 
uint16_t tZQCl_Clocks
 This is the period of time that the MMDC has to wait after sending a short ZQ calibration and before sending other commands,max value 112 cycles,see RM for more detail ,lpddr2 device default is 360ns.
 
uint16_t tZQCs_Clocks
 This is the period of time that the MMDC has to wait after sending a long ZQ calibration and before sending other commands.
 
uint16_t tZQInit_Clocks
 This is the period of time that the MMDC has to wait after sending a init ZQ calibration and before sending other commands.lpddr2 device default is 1us.
 
mmdc_zq_calfreq_t hwZQFreq
 ZQ periodic calibration freq.
 
uint8_t cmpOutSample
 define the amount of cycle between driving the ZQ signal to pad and till sampling the cmp enable output
 
uint8_t hwPullDownOffset
 define ZQ hardware pull down offset, used for fine tuning
 
uint8_t hwPullUpOffset
 define ZQ hardware pull up offset, used for fine tuning
 

Field Documentation

mmdc_zq_calmode_t mmdc_zq_config_t::mode
struct mmdc_cmd_config_t

Data Fields

uint8_t argMsb
 define the CMD_ADDR_MSB_MR_OP, for lpddr2 device this field is mode register oprand
 
uint8_t argLsb
 define the CMD_ADDR_LSB_MR_ADDR,for lpddr2 device this field is mode register addr
 
uint8_t bankAddr
 define the bank address,this field not relate with lpddr2 device
 
uint8_t targetCS
 select which CS to drive low. More...
 
mmdc_cmd_type_t cmd
 define the cmd to be send
 

Field Documentation

uint8_t mmdc_cmd_config_t::targetCS
struct mmdc_device_timing_t

clocks is ddr clock,(a+b), a is the value write to reigster,b is offset

Data Fields

uint8_t tRFC_Clocks
 
Refresh cmd to active or refresh cmd time

default is (0x32+1) clocks,max is (255+1) clocks

 
uint8_t tCKSRX_Clocks
 
Valid clock before self-refresh exit,self-refresh timing

default is 2 clocks,max is 7 clocks

 
uint8_t tCKSRE_Clocks
 
Valid clock after self-refresh entry,self-refresh timing

default is 2 clocks.max is 7 clocks

 
uint8_t tXSR_Clocks
 
exit self refresh to a valid cmd,self-refresh timing

min value should set to 0x16,represent 23 clocks,max is 256 clocks

 
uint8_t tCKE_Clocks
 CKE minimum pulse width,default is (3+1) clocks,max is (7+1) clocks.
 
uint8_t tCL_Clocks
 CAS read latency,default is(3+3) clocks, max is (8+3) clocks.
 
uint8_t tCWL_Clocks
 CAS write latency, default is (3+1)clocks, max is (6+1) clocks.
 
uint8_t ralat_Clocks
 define write additional latency in misc, default is disable, max is (7+2)clocks
 
uint8_t walat_Clocks
 define read additional latency in misc, default is disable, max is 3 clocks
 
uint8_t tFAW_Clocks
 Four bank active window,all bank,default is (6+1) clocks,max is (31+1)clocks.
 
uint8_t tRAS_Clocks
 row active time,Active to Precharge cmd period,same bank,default is (9+1) clocks ,max is (30+1)clocks
 
uint8_t tRC_Clocks
 Active to active or refresh cmd period,default is (0+1)clocks,max is (62+1)clocks.
 
uint8_t tRCD_Clocks
 Active cmd to internal read/write delay time,default is 0+1 clocks,max is 14+1 clocks.
 
uint8_t tRP_Clocks
 Precharge cmd period-per bank,default is 0+1 clock,max is 14+1 clocks.
 
uint8_t tRPA_Clocks
 Precharge cmd period-all bank,default is 0+1 clock,max is 14+1 clocks.
 
uint8_t tWR_Clocks
 Write recovery time,default is 0+1 clock,max is 7+1 clocks.
 
uint8_t tMRD_Clocks
 Mode register set cmd cycle,should set to max(tMRR,tMRW), default is 1+1 clock,max is 15+1 clocks.
 
uint8_t tRTP_Clocks
 Internal read cmd to pre-charge cmd delay,default is 2+1 clock,max is 7+1 clocks.
 
uint8_t tWTR_Clocks
 Internal write cmd to read cmd delay,default is 2+1 clock,max is 7+1 clocks.
 
uint8_t tRRD_Clocks
 active bankA to active bankB ,Internal read cmd to pre-charge cmd, default is 0+1 clock,max is 6+1 clocks
 
uint8_t tXP_Clocks
 exit power down to any cmd, default (1+1) clocks, max is (7 +1) clocks
 
uint8_t tRSTtoCKE_Clocks
 idle time until first reset is assert,default is 14-2 clock,max is 0X3f-2 clocks,for LPDDR2 device default is 200us
 
uint32_t tDAI_Clocks
 Maximum device auto initialization period for LPDDR2, not relavant to DDR3. More...
 
uint8_t tRTWSAME_Clocks
 
Read to write commands delay for same chip select, total delay is calculated

according to: BL/2 + RTW_SAME + (tCL-tCWL) + RALAT

 
uint8_t tWTRDIFF_Clocks
 
Write to read commands delay for different chip select, total delay is calculated

according to: BL/2 + WTR_DIFF + (tCL-tCWL) + RALAT

 
uint8_t tWTWDIFF_Clocks
 
Write to write commands delay for different chip select, total delay is

calculated according to: BL/2 + WTW_DIFF

 
uint8_t tRTWDIFF_Clocks
 
Read to write commands delay for different chip select, total delay is calculated

according to: BL/2 + RTW_DIFF + (tCL - tCWL) + RALAT

 
uint8_t tRTRDIFF_Clocks
 Read to read commands delay for different chip select. More...
 
uint8_t tXPDLL_Clocks
 Exit precharge power down with DLL frozen to commands requiring DLL, not relavant to LPDDR2. More...
 
uint16_t tDLLK_Clocks
 DLL locking time, not relavant to LPDDR2. More...
 
uint8_t tXPR_Clocks
 CLKE High to a valid command, not relevant to LPDDR2. More...
 
uint8_t tSDEtoRST_Clocks
 Time from SDE enable until DDR #reset is high, not relavant to LPDDR2. More...
 
uint8_t tAOFPD_Clocks
 Asynchronous RTT turn-off delay, not relavant to LPDDR2. More...
 
uint8_t tAONPD_Clocks
 Asynchronous RTT turn-on delay, not relavant to LPDDR2. More...
 
uint8_t tODTIdleOff_Clocks
 ODT turn off latency, not relavant to LPDDR2. More...
 

Field Documentation

uint32_t mmdc_device_timing_t::tDAI_Clocks
uint8_t mmdc_device_timing_t::tRTRDIFF_Clocks

total delay is calculated according to: BL/2 + RTR_DIFF

uint8_t mmdc_device_timing_t::tXPDLL_Clocks
uint16_t mmdc_device_timing_t::tDLLK_Clocks
uint8_t mmdc_device_timing_t::tXPR_Clocks
uint8_t mmdc_device_timing_t::tSDEtoRST_Clocks
uint8_t mmdc_device_timing_t::tAOFPD_Clocks
uint8_t mmdc_device_timing_t::tAONPD_Clocks
uint8_t mmdc_device_timing_t::tODTIdleOff_Clocks
struct mmdc_auto_refresh_t

Data Fields

uint16_t refreshCnt
 
define refresh counter which is how many DDR clock cycles arrive

will trigger auto refresh, only applied when choose refreshTrigSrc as kMMDC_RefreshTrigDDRCycles

 
uint16_t refreshRate
 refresh rate-means how much cmd will send once auto refresh being trigger
 
mmdc_refresh_sel_t refreshTrigSrc
 select refresh trigger clock source
 
struct mmdc_exaccess_config_t

Data Fields

uint16_t excMonitorID0
 exclusive monitor ID 0
 
uint16_t excMonitorID1
 exclusive monitor ID 1
 
uint16_t excMonitorID2
 exclusive monitor ID 2
 
uint16_t excMonitorID3
 exclusive monitor ID 3
 
bool secErrLock
 define if lock ARCR_SEC_ERR_EN this bit can't update if locked
 
bool secErrEn
 This bit defines whether security read/write access violation result in SLV Error response or in OKAY response.
 
bool excErrEn
 This bit defines whether exclusive read/write access violation of AXI 6.2.4 rule result in SLV Error response or in OKAY response . More...
 

Field Documentation

bool mmdc_exaccess_config_t::excErrEn

Default value is 0x1 response is SLV Error

struct mmdc_profiling_config_t

Data Fields

mmdc_profiling_action_t type
 profiling action
 
bool overFlowCount
 profiling cycle counter over flag
 
uint16_t axiIDMask
 profiling AXI ID mask
 
uint16_t axiID
 profiling AXI ID
 
uint32_t totalCount
 total cycle count-readonly
 
uint32_t busyCount
 busy count-readonly
 
uint32_t readCount
 total read count-readonly
 
uint32_t writeCount
 total write count-readonly
 
uint32_t readByteCount
 read byte count-readonly
 
uint32_t writeByteCount
 total write byte count-readonly
 
struct mmdc_performance_config_t

Data Fields

bool enArbitration
 define if enable arbitration in MAARCR
 
bool enReordering
 define if enable reordering in MAARCR
 
bool enRCH
 define if enable real time channel in MAARCR
 
uint32_t ratePageHit
 static score taken into account in case the pending access has a page hit in MAARCR
 
uint32_t rateAccessHit
 
static score taken into account in case the pending access

is same as before in MAARCR

 
uint32_t dynJump
 dynamic score give to any pending access in case it was not chosen in arbitration in MAARCR
 
uint32_t dynMax
 dynamic score max value in MAARCR
 
uint32_t guard
 use to prevent a starvation of access
 
uint32_t cmdPredict
 define cmd prediction work mode in misc
 
struct mmdc_device_config_t
struct mmdc_config_t

Data Fields

mmdc_device_type_t devType
 define device type
 
uint32_t devSize
 define the size of the device
 
mmdc_device_bank_num_t devBank
 define device total bank number
 
mmdc_row_addr_width_t rowWidth
 define row width in MDCTL
 
mmdc_col_addr_width_t colWidth
 define col width in MDCTL
 
mmdc_burst_len_t burstLen
 define burst length MDCTL
 
bool bankInterleave
 define indicate bank interleave on/off in misc
 
bool secondDDRClock
 define gating the secondary DDR clock in misc
 
bool enableOnlyCS0
 Only enable CS0.
 
mmdc_odt_config_t * ODTConfig
 Pointer to on die termination config, NULL means disable, for LPDDR2, pass NULL. More...
 
mmdc_zq_config_t * zqCalibration
 Pointer to device timing structure. More...
 
mmdc_device_config_t * deviceConfig [2]
 Pointer to ZQ calibration config, NULL means do not need. More...
 
mmdc_readDQS_calibration_config_t * readDQSCalibration [2]
 Pointer to device configuration CS0/CS1, NULL means do not need. More...
 
mmdc_writeLeveling_calibration_config_t * wLevelingCalibration [2]
 Pointer to read DQS calibration config CS0/CS1, NULL meansdo not need, for LPDDR2, pass NULL. More...
 
mmdc_read_calibration_config_t * readCalibration [2]
 Pointer to write leveling calibration config, NULL means do not need, for LPDDR2, pass NULL. More...
 
mmdc_write_calibration_config_t * writeCalibration [2]
 Pointer to read calibration config CS0/CS1, NULL means do not need. More...
 
mmdc_fine_tuning_config_t * tuning
 Pointer to write calibration config CS0/CS1, NULL means do not need. More...
 
mmdc_auto_refresh_t * autoRefresh
 Pointer to fine tuning config, NULL means do not need. More...
 
mmdc_power_config_t * powerConfig
 Pointer to auto refresh config structure, NULL means do not need. More...
 

Field Documentation

mmdc_odt_config_t* mmdc_config_t::ODTConfig
mmdc_zq_config_t* mmdc_config_t::zqCalibration
mmdc_device_config_t* mmdc_config_t::deviceConfig[2]
mmdc_readDQS_calibration_config_t* mmdc_config_t::readDQSCalibration[2]
mmdc_writeLeveling_calibration_config_t* mmdc_config_t::wLevelingCalibration[2]
mmdc_read_calibration_config_t* mmdc_config_t::readCalibration[2]
mmdc_write_calibration_config_t* mmdc_config_t::writeCalibration[2]
mmdc_fine_tuning_config_t* mmdc_config_t::tuning
mmdc_auto_refresh_t* mmdc_config_t::autoRefresh
mmdc_power_config_t* mmdc_config_t::powerConfig

Macro Definition Documentation

#define MMDC_READ_DQS_FINE_TUNING_MASK   (0x77777777U)

define the read DQS fine tuning mask value

#define MMDC_WRITE_DQS_FINE_TUNING_MASK   (0xF3333333U)

define the write DQS fine tuning mask value

#define MMDC_PRE_DEFINE_VALUE_DEFAULT   (0xCCU)

define the calibration predefine value

#define MMDC_MEASUREUNIT_ERR_FREQ   (100000000U)

according to ERR005778 description

Typedef Documentation

typedef void(* MMDC_SwitchFrequency)(MMDC_Type *, void *, void *, uint32_t)

Enumeration Type Documentation

Enumerator
kStatus_MMDC_ErrorDGCalibration 

MMDC error DG calibration.

kStatus_MMDC_ErrorReadCalibration 

MMDC error read calibration.

kStatus_MMDC_ErrorWriteCalibration 

MMDC error write calibration.

kStatus_MMDC_ErrorWriteLevelingCalibration 

MMDC error write leveling calibration.

kStatus_MMDC_WaitFlagTimeout 

MMDC wait flag timeout.

Enumerator
kMMDC_LPDDR2_S4 

LPDDR2-S4.

kMMDC_LPDDR2_S2 

LPDDR2-S2.

kMMDC_DDR3 

DDR3 device.

Enumerator
kMMDC_Bank8 

bank number 8

kMMDC_Bank4 

bank number 4

Enumerator
kMMDC_Row11Bits 

row addr 11 bits

kMMDC_Row12Bits 

row addr 12 bits

kMMDC_Row13Bits 

row addr 13 bits

kMMDC_Row14Bits 

row addr 14 bits

kMMDC_Row15Bits 

row addr 15 bits

kMMDC_Row16Bits 

row addr 16 bits

Enumerator
kMMDC_Col9Bits 

col addr 9 bits

kMMDC_Col10Bits 

col addr 10 bits

kMMDC_Col11Bits 

col addr 11 bits

kMMDC_Col8Bits 

col addr 8 bits

kMMDC_Col12Bits 

col addr 12 bits

Enumerator
kMMDC_BurstLen4 

brust len 4

kMMDC_BurstLen8 

burst len 8

kMMDC_BurstLen16 

reserved

Enumerator
kMMDC_NormalOperation 

normal operation cmd

kMMDC_AutoRefresh 

auto refresh cmd

kMMDC_WriteModeRegister 

load mode register for DDR2/DDR3,MRW for LPDDR2

kMMDC_ZQCalibration 

ZQ calibration cmd.

kMMDC_PreChargeAll 

Precharge all cmd.

kMMDC_ReadModeRegister 

mode register read cmd

Enumerator
kMMDC_ZQCaltoIOHW 

ZQ calibration to IO pads only through HW.

kMMDC_ZQCaltoIODeviceLong 

ZQ calibration to IO pads together with ZQ long cmd to device.

kMMDC_ZQCaltoDeviceOnly 

ZQ calibration to device with long/short cmd.

kMMDC_ZQCaltoIODeviceLongShort 

ZQ calibration to IO pads together with ZQ calibration cmd long/short to device.

kMMDC_ZQFinetuning 

HW ZQ res offset fine tuning.

kMMDC_DisZQFinetuning 

disable HW ZQ res offset

Enumerator
kMMDC_ZQCalFreq1ms 

ZQ calibration is peformed every 1ms.

kMMDC_ZQCalFreq2ms 

ZQ calibration is peformed every 2ms.

kMMDC_ZQCalFreq4ms 

ZQ calibration is peformed every 4ms.

kMMDC_ZQCalFreq1s 

ZQ calibration is peformed every 1s.

kMMDC_ZQCalFreq16s 

ZQ calibration is peformed every 16s.

kMMDC_ZQCalFreq32s 

ZQ calibration is peformed every 32s.

Enumerator
kMMDC_RefreshTrigBy64K 

refresh trigger frequency 64K

kMMDC_RefreshTrigBy32K 

refresh trigger frequency 32K

kMMDC_RefreshTrigDDRCycles 

refresh trigger every amount of cycles that are configured in REF_CNT field

kMMDC_RefreshTrigNone 

auto refresh disable

Enumerator
kMMDC_EnProfilingWithID 

enable profiling with special ID

kMMDC_FreezeProfiling 

freeze profiling

kMMDC_CheckOverFlow 

check the counter overflow

Enumerator
kMMDC_CalWithPreSetValue 

calibration with preset value

kMMDC_CalWithMPR 

HW calibration with the MPR.

kMMDC_CalWithPreDefine 

calibration with Pre-defined value

Enumerator
kMMDC_Wait16DDRCycles 

wait 16 DDR cycles before comparing sample data

kMMDC_Wait32DDRCycles 

wait 32 DDR cycles before comparing sample data

Enumerator
kMMDC_DutyHighPercent48_5 

51.5% low 48.5% high

kMMDC_DutyHighPercent50 

50% duty cycle

kMMDC_DutyHighPercent51_5 

48.5% low 51.5% high

Enumerator
kMMDC_RttNomDisabled 

Rtt_Nom Disabled.

kMMDC_RttNom120ohm 

Rtt_Nom 120 Ohm.

kMMDC_RttNom60ohm 

Rtt_Nom 60 Ohm.

kMMDC_RttNom40ohm 

Rtt_Nom 40 Ohm.

kMMDC_RttNom30ohm 

Rtt_Nom 30 Ohm.

kMMDC_RttNom24ohm 

Rtt_Nom 24 Ohm.

kMMDC_RttNom20ohm 

Rtt_Nom 20 Ohm.

kMMDC_RttNom17ohm 

Rtt_Nom 17 Ohm.

Enumerator
kMMDC_NoUpdateDerate 

no derate

kMMDC_UpdateRefreshRate 

refresh rate derate

kMMDC_DerateTiming 

derating relate timing

kMMDC_DisableDerate 

derating disable

Enumerator
kMMDC_ExMonitorID0 

config the exclusive access ID0

kMMDC_ExMonitorID1 

config the exclusive access ID1

kMMDC_ExMonitorID2 

config the exclusive access ID2

kMMDC_ExMonitorID3 

config the exclusive access ID3

kMMDC_ExAccessResponse 

config the exclusive access reponse

Function Documentation

void MMDC_GetDefaultConfig ( mmdc_config_t *  config)
Parameters
baseMMDC peripheral base address
mmdcconfig collection pointer config->bankInterleave = true; config->secondDDRClock = true; config->enableOnlyCS0 = true; config->devType = kMMDC_DDR3; config->devSize = 0x40000000U; config->devBank = kMMDC_Bank8; config->rowWidth = kMMDC_Row16Bits; config->colWidth = kMMDC_Col10Bits; config->burstLen = kMMDC_BurstLen8; config->ODTConfig = NULL; config->timing = NULL; config->zqCalibration = NULL; config->deviceConfig[0] = NULL; config->deviceConfig[1] = NULL; config->readDQSCalibration[0] = NULL; config->readDQSCalibration[1] = NULL; config->wLevelingCalibration[0] = NULL; config->wLevelingCalibration[1] = NULL; config->readCalibration[0] = NULL; config->readCalibration[1] = NULL; config->writeCalibration[0] = NULL; config->writeCalibration[1] = NULL; config->tuning = NULL; config->autoRefresh = NULL; config->powerConfig = NULL;
status_t MMDC_Init ( MMDC_Type *  base,
mmdc_config_t *  config 
)
Parameters
baseMMDC peripheral base address
mmdcconfig collection pointer
Return values
kStatus_SuccessInitialization succeed
kStatus_MMDC_ErrorDGCalibrationError happened during hardware DQS gate calibration
kStatus_MMDC_ErrorReadCalibrationError happened during hardware read calibration
kStatus_MMDC_ErrorWriteCalibrationError happened during hardware write calibration
kStatus_MMDC_ErrorWriteLevelingCalibrationError happened during hardware write leveling calibration
void MMDC_Deinit ( MMDC_Type *  base)
Parameters
baseMMDC peripheral base address
void MMDC_HandleCommand ( MMDC_Type *  base,
mmdc_cmd_config_t *  config 
)
Parameters
baseMMDC peripheral base address
cmdconfiguration collection
status_t MMDC_GetReadData ( MMDC_Type *  base,
uint32_t *  data 
)
Parameters
baseMMDC peripheral base address
thepointer which used to store read data
Return values
kStatus_SuccessRead data succeed
kStatus_MMDC_WaitFlagTimeoutRead data flag wait timeout
void MMDC_EnhancePerformance ( MMDC_Type *  base,
const mmdc_performance_config_t *  config 
)
Parameters
baseMMDC peripheral base address
performanceconfiguration collection
void MMDC_EnableAutoRefresh ( MMDC_Type *  base,
mmdc_auto_refresh_t *  config 
)
Parameters
baseMMDC peripheral base address
mmdcauto refresh configuration collection
static void MMDC_DisableAutoRefresh ( MMDC_Type *  base)
inlinestatic
Parameters
baseMMDC peripheral base address
void MMDC_EnablePowerSaving ( MMDC_Type *  base,
mmdc_power_config_t *  config 
)
Parameters
baseMMDC peripheral base address
mmdcdevice configuration collection, pointer for the configuration.
static void MMDC_DisablePowerSaving ( MMDC_Type *  base)
inlinestatic

MMDC disable automatic power saving.

Parameters
baseMMDC peripheral base address
void MMDC_Profiling ( MMDC_Type *  base,
mmdc_profiling_config_t *  config 
)
Parameters
baseMMDC peripheral base address
mmdcprofiling status and control
status_t MMDC_LPDDR2UpdateDerate ( MMDC_Type *  base,
mmdc_auto_refresh_t *  config,
uint32_t  type 
)
Parameters
baseMMDC peripheral base address
autorefresh configuration collection,can set to NULL,when do not change refresh rate
deratingtype
Return values
kStatus_SuccessRead data succeed
kStatus_MMDC_WaitFlagTimeoutLPDDR2 AC timing/refresh derate wait flag timeout
status_t MMDC_MonitorLPDDR2OperationTemp ( MMDC_Type *  base,
uint32_t *  mr4 
)
Parameters
baseMMDC peripheral base address
MR4pointer,use to store the mode register4 value
Return values
kStatus_SuccessRead data succeed
kStatus_MMDC_WaitFlagTimeoutGet MR4 data flag timeout
status_t MMDC_ReadDQSGatingCalibration ( MMDC_Type *  base,
mmdc_readDQS_calibration_config_t *  config 
)
Parameters
baseMMDC peripheral base address
configcalibration configuration collection
Return values
kStatus_SuccessRead data succeed
kStatus_MMDC_ErrorDGCalibrationRead DQS data gate hardware calibration error
status_t MMDC_WriteLevelingCalibration ( MMDC_Type *  base,
mmdc_writeLeveling_calibration_config_t *  config 
)
Parameters
baseMMDC peripheral base address
configcalibration configuration collection
Return values
kStatus_SuccessRead data succeed
kStatus_MMDC_ErrorWriteLevelingCalibrationwrite leveling hardware calibration error
status_t MMDC_WriteCalibration ( MMDC_Type *  base,
mmdc_write_calibration_config_t *  config 
)
Parameters
baseMMDC peripheral base address
configcalibration configuration collection
Return values
kStatus_SuccessRead data succeed
kStatus_MMDC_ErrorWriteCalibrationwrite hardware calibration error
status_t MMDC_ReadCalibration ( MMDC_Type *  base,
mmdc_read_calibration_config_t *  config 
)
Parameters
baseMMDC peripheral base address
configcalibration configuration collection
Return values
kStatus_SuccessRead data succeed
kStatus_MMDC_ErrorReadCalibrationread hardware calibration error
void MMDC_DoFineTuning ( MMDC_Type *  base,
mmdc_device_type_t  devType,
mmdc_fine_tuning_config_t *  config 
)
Parameters
baseMMDC peripheral base address
devTypeMMDC device type
configfine tuning configuration collection
void MMDC_SetTiming ( MMDC_Type *  base,
mmdc_device_type_t  devType,
mmdc_device_timing_t *  timing 
)
Parameters
MMDCperipheral base address
timingpointer to timing structure
void MMDC_DeviceInit ( MMDC_Type *  base,
mmdc_device_type_t  devType,
uint8_t  targetCS,
mmdc_device_config_t *  devConfig 
)
Parameters
MMDCbase address
devicebasic config info pointer
status_t MMDC_EnterConfigurationMode ( MMDC_Type *  base,
bool  enable 
)
Parameters
baseMMDC peripheral base address
enableenter/exit flag
Return values
kStatus_SuccessRead data succeed
kStatus_MMDC_WaitFlagTimeoutEnter configuration mode time out
void MMDC_DoZQCalibration ( MMDC_Type *  base,
mmdc_device_type_t  devType,
mmdc_zq_config_t *  zqCal 
)
Parameters
baseMMDC peripheral base address
devTypedevice type
zqCalinfo pointer
status_t MMDC_EnableLowPowerMode ( MMDC_Type *  base,
bool  enable 
)
Parameters
baseMMDC peripheral base address
enableenable/disable flag
Return values
kStatus_SuccessRead data succeed
kStatus_MMDC_WaitFlagTimeoutEnter low power mode timeout
status_t MMDC_EnableDVFSMode ( MMDC_Type *  base,
bool  enable 
)
Parameters
baseMMDC peripheral base address
enableenable/disable flag
Return values
kStatus_SuccessRead data succeed
kStatus_MMDC_WaitFlagTimeoutEnter DVFS mode timeout
void MMDC_Reset ( MMDC_Type *  base)
Parameters
baseMMDC peripheral base address
static void MMDC_SwitchDeviceFrequency ( MMDC_Type *  base,
void *  ccm,
void *  iomux,
uint32_t  param,
uint32_t  codeAddr 
)
inlinestatic
Parameters
MMDCbase address
CCMbase address
iomuxbase address
targetfrequency value for LPDDR2 and parameter address for DDR3
assemblyswitch frequency code address
static void MMDC_EnableSBS ( MMDC_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseMMDC peripheral base address
static void MMDC_TriggerSBS ( MMDC_Type *  base)
inlinestatic
Parameters
baseMMDC peripheral base address
static uint32_t MMDC_GetAXIAddrBySBS ( MMDC_Type *  base)
inlinestatic
Parameters
baseMMDC peripheral base address
static uint32_t MMDC_GetAXIAttributeBySBS ( MMDC_Type *  base)
inlinestatic
Parameters
baseMMDC peripheral base address
static void MMDC_EnableProfiling ( MMDC_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseMMDC peripheral base address
enableor disable flag
static void MMDC_ResumeProfiling ( MMDC_Type *  base)
inlinestatic
Parameters
baseMMDC peripheral base address
static void MMDC_ResetProfiling ( MMDC_Type *  base)
inlinestatic
Parameters
baseMMDC peripheral base address
void MMDC_ExclusiveAccess ( MMDC_Type *  base,
mmdc_exaccess_config_t *  config,
uint32_t  type 
)
Parameters
baseMMDC peripheral base address
exclusiveaccess config collection
exclusiveaccess config type