The Smart Card UART driver uses a standard UART peripheral which supports the ISO-7816 standard. The driver supports transmission functionality in the CPU mode. The driver also supports non-blocking (asynchronous) type of data transfers. The blocking (synchronous) transfer is supported only by the RTOS adaptation layer.
|
| void | SMARTCARD_UART_GetDefaultConfig (smartcard_card_params_t *cardParams) |
| | Fills in the smartcard_card_params structure with default values according to the EMV 4.3 specification. More...
|
| |
| status_t | SMARTCARD_UART_Init (UART_Type *base, smartcard_context_t *context, uint32_t srcClock_Hz) |
| | Initializes a UART peripheral for the Smart card/ISO-7816 operation. More...
|
| |
| void | SMARTCARD_UART_Deinit (UART_Type *base) |
| | This function disables the UART interrupts, disables the transmitter and receiver, and flushes the FIFOs (for modules that support FIFOs) and gates UART clock in SIM. More...
|
| |
| int32_t | SMARTCARD_UART_GetTransferRemainingBytes (UART_Type *base, smartcard_context_t *context) |
| | Returns whether the previous UART transfer has finished. More...
|
| |
| status_t | SMARTCARD_UART_AbortTransfer (UART_Type *base, smartcard_context_t *context) |
| | Terminates an asynchronous UART transfer early. More...
|
| |
| status_t | SMARTCARD_UART_TransferNonBlocking (UART_Type *base, smartcard_context_t *context, smartcard_xfer_t *xfer) |
| | Transfers data using interrupts. More...
|
| |
| status_t | SMARTCARD_UART_Control (UART_Type *base, smartcard_context_t *context, smartcard_control_t control, uint32_t param) |
| | Controls the UART module per different user requests. More...
|
| |
| void | SMARTCARD_UART_IRQHandler (UART_Type *base, smartcard_context_t *context) |
| | Interrupt handler for UART. More...
|
| |
| void | SMARTCARD_UART_ErrIRQHandler (UART_Type *base, smartcard_context_t *context) |
| | Error interrupt handler for UART. More...
|
| |
| void | SMARTCARD_UART_TSExpiryCallback (UART_Type *base, smartcard_context_t *context) |
| | Handles initial TS character timer time-out event. More...
|
| |
- Parameters
-
| cardParams | The configuration structure of type smartcard_interface_config_t. Function fill in members: Fi = 372; Di = 1; currentD = 1; WI = 0x0A; GTN = 0x00; with default values. |
| status_t SMARTCARD_UART_Init |
( |
UART_Type * |
base, |
|
|
smartcard_context_t * |
context, |
|
|
uint32_t |
srcClock_Hz |
|
) |
| |
This function un-gates the UART clock, initializes the module to EMV default settings, configures the IRQ, enables the module-level interrupt to the core, and initializes the driver context.
- Parameters
-
| base | The UART peripheral base address. |
| context | A pointer to a smart card driver context structure. |
| srcClock_Hz | Smart card clock generation module source clock. |
- Returns
- An error code or kStatus_SMARTCARD_Success.
| void SMARTCARD_UART_Deinit |
( |
UART_Type * |
base | ) |
|
- Parameters
-
| base | The UART peripheral base address. |
| int32_t SMARTCARD_UART_GetTransferRemainingBytes |
( |
UART_Type * |
base, |
|
|
smartcard_context_t * |
context |
|
) |
| |
When performing an async transfer, call this function to ascertain the context of the current transfer: in progress (or busy) or complete (success). If the transfer is still in progress, the user can obtain the number of words that have not been transferred by reading xSize of smart card context structure.
- Parameters
-
| base | The UART peripheral base address. |
| context | A pointer to a Smart card driver context structure. |
- Returns
- The number of bytes not transferred.
During an async UART transfer, the user can terminate the transfer early if the transfer is still in progress.
- Parameters
-
| base | The UART peripheral base address. |
| context | A pointer to a Smart card driver context structure. |
- Return values
-
| kStatus_SMARTCARD_Success | The transfer abort was successful. |
| kStatus_SMARTCARD_NoTransmitInProgress | No transmission is currently in progress. |
A non-blocking (also known as asynchronous) function means that the function returns immediately after initiating the transfer function. The application has to get the transfer status to see when the transfer is complete. In other words, after calling non-blocking (asynchronous) transfer function, the application must get the transfer status to check if transmit is completed or not.
- Parameters
-
| base | The UART peripheral base address. |
| context | A pointer to a Smart card driver context structure. |
| xfer | A pointer to Smart card transfer structure where the linked buffers and sizes are stored. |
- Returns
- An error code or kStatus_SMARTCARD_Success.
- Parameters
-
| base | The UART peripheral base address. |
| context | A pointer to a smart card driver context structure. |
| control | Smart card command type. |
| param | Integer value specific to a control command. |
return An kStatus_SMARTCARD_OtherError in case of error return kStatus_SMARTCARD_Success in success
This handler uses the buffers stored in the smartcard_context_t structures to transfer data. The Smart card driver requires this function to call when the UART interrupt occurs.
- Parameters
-
| base | The UART peripheral base address. |
| context | A pointer to a Smart card driver context structure. |
This function handles error conditions during a transfer.
- Parameters
-
| base | The UART peripheral base address. |
| context | A pointer to a Smart card driver context structure. |
- Parameters
-
| base | The UART peripheral base address. |
| context | A pointer to a Smart card driver context structure. |