MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

Data Structures

struct  uart_rtos_config_t
 UART configuration structure. More...
 

UART RTOS Operation

int UART_RTOS_Init (uart_rtos_handle_t *handle, uart_handle_t *t_handle, const uart_rtos_config_t *cfg)
 Initializes a UART instance for operation in RTOS. More...
 
int UART_RTOS_Deinit (uart_rtos_handle_t *handle)
 Deinitializes a UART instance for operation. More...
 

UART transactional Operation

int UART_RTOS_Send (uart_rtos_handle_t *handle, const uint8_t *buffer, uint32_t length)
 Sends data in the background. More...
 
int UART_RTOS_Receive (uart_rtos_handle_t *handle, uint8_t *buffer, uint32_t length, size_t *received)
 Receives data. More...
 

Data Structure Documentation

struct uart_rtos_config_t

Data Fields

UART_Type * base
 UART base address.
 
uint32_t srcclk
 UART source clock in Hz.
 
uint32_t baudrate
 Desired communication speed.
 
uart_parity_mode_t parity
 Parity setting.
 
uart_stop_bit_count_t stopbits
 Number of stop bits to use.
 
uint8_t * buffer
 Buffer for background reception.
 
uint32_t buffer_size
 Size of buffer for background reception.
 

Function Documentation

int UART_RTOS_Init ( uart_rtos_handle_t *  handle,
uart_handle_t *  t_handle,
const uart_rtos_config_t *  cfg 
)
Parameters
handleThe RTOS UART handle, the pointer to an allocated space for RTOS context.
t_handleThe pointer to the allocated space to store the transactional layer internal state.
cfgThe pointer to the parameters required to configure the UART after initialization.
Returns
0 succeed; otherwise fail.
int UART_RTOS_Deinit ( uart_rtos_handle_t *  handle)

This function deinitializes the UART module, sets all register values to reset value, and frees the resources.

Parameters
handleThe RTOS UART handle.
int UART_RTOS_Send ( uart_rtos_handle_t *  handle,
const uint8_t *  buffer,
uint32_t  length 
)

This function sends data. It is a synchronous API. If the hardware buffer is full, the task is in the blocked state.

Parameters
handleThe RTOS UART handle.
bufferThe pointer to the buffer to send.
lengthThe number of bytes to send.
int UART_RTOS_Receive ( uart_rtos_handle_t *  handle,
uint8_t *  buffer,
uint32_t  length,
size_t *  received 
)

This function receives data from UART. It is a synchronous API. If data is immediately available, it is returned immediately and the number of bytes received.

Parameters
handleThe RTOS UART handle.
bufferThe pointer to the buffer to write received data.
lengthThe number of bytes to receive.
receivedThe pointer to a variable of size_t where the number of received data is filled.