![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | lpsci_rtos_config_t |
| LPSCI RTOS configuration structure. More... | |
Driver version | |
| #define | FSL_LPSCI_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 0, 4)) |
| LPSCI freertos driver version 2.0.4. More... | |
LPSCI RTOS Operation | |
| int | LPSCI_RTOS_Init (lpsci_rtos_handle_t *handle, lpsci_handle_t *t_handle, const lpsci_rtos_config_t *cfg) |
| Initializes an LPSCI instance for operation in RTOS. More... | |
| int | LPSCI_RTOS_Deinit (lpsci_rtos_handle_t *handle) |
| Deinitializes an LPSCI instance for operation. More... | |
LPSCI transactional Operation | |
| int | LPSCI_RTOS_Send (lpsci_rtos_handle_t *handle, const uint8_t *buffer, uint32_t length) |
| Send data in background. More... | |
| int | LPSCI_RTOS_Receive (lpsci_rtos_handle_t *handle, uint8_t *buffer, uint32_t length, size_t *received) |
| Receives data. More... | |
| struct lpsci_rtos_config_t |
Data Fields | |
| UART0_Type * | base |
| LPSCI base address. | |
| uint32_t | srcclk |
| LPSCI source clock in Hz. | |
| uint32_t | baudrate |
| Desired communication speed. | |
| lpsci_parity_mode_t | parity |
| Parity setting. | |
| lpsci_stop_bit_count_t | stopbits |
| Number of stop bits to use. | |
| uint8_t * | buffer |
| Buffer for background reception. | |
| uint32_t | buffer_size |
| Size of buffer for background reception. | |
| #define FSL_LPSCI_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 0, 4)) |
| int LPSCI_RTOS_Init | ( | lpsci_rtos_handle_t * | handle, |
| lpsci_handle_t * | t_handle, | ||
| const lpsci_rtos_config_t * | cfg | ||
| ) |
| handle | The RTOS LPSCI handle, the pointer to allocated space for RTOS context. |
| t_handle | The pointer to allocated space where to store transactional layer internal state. |
| cfg | The pointer to the parameters required to configure the LPSCI after initialization. |
| int LPSCI_RTOS_Deinit | ( | lpsci_rtos_handle_t * | handle | ) |
This function deinitializes the LPSCI modulem, set all register value to reset value and releases the resources.
| handle | The RTOS LPSCI handle. |
| int LPSCI_RTOS_Send | ( | lpsci_rtos_handle_t * | handle, |
| const uint8_t * | buffer, | ||
| uint32_t | length | ||
| ) |
This function sends data. It is synchronous API. If the HW buffer is full, the task is in the blocked state.
| handle | The RTOS LPSCI handle. |
| buffer | The pointer to buffer to send. |
| length | The number of bytes to send. |
| int LPSCI_RTOS_Receive | ( | lpsci_rtos_handle_t * | handle, |
| uint8_t * | buffer, | ||
| uint32_t | length, | ||
| size_t * | received | ||
| ) |
It is synchronous API.
This function receives data from LPSCI. If any data is immediately available it is returned immediately and the number of bytes received.
| handle | The RTOS LPSCI handle. |
| buffer | The pointer to buffer where to write received data. |
| length | The number of bytes to receive. |
| received | The pointer to variable of size_t where the number of received data is filled. |