![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | sai_dma_handle_t | 
| SAI DMA transfer handle, users should not touch the content of the handle.  More... | |
Typedefs | |
| typedef void(* | sai_dma_callback_t )(I2S_Type *base, sai_dma_handle_t *handle, status_t status, void *userData) | 
| Define SAI DMA callback.  | |
Driver version | |
| #define | FSL_SAI_DMA_DRIVER_VERSION (MAKE_VERSION(2, 1, 4)) | 
| Version 2.1.4.  | |
DMA Transactional | |
| void | SAI_TransferTxCreateHandleDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_dma_callback_t callback, void *userData, dma_handle_t *dmaHandle) | 
| Initializes the SAI master DMA handle.  More... | |
| void | SAI_TransferRxCreateHandleDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_dma_callback_t callback, void *userData, dma_handle_t *dmaHandle) | 
| Initializes the SAI slave DMA handle.  More... | |
| void | SAI_TransferTxSetFormatDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz) | 
| Configures the SAI Tx audio format.  More... | |
| void | SAI_TransferRxSetFormatDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz) | 
| Configures the SAI Rx audio format.  More... | |
| status_t | SAI_TransferSendDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transfer_t *xfer) | 
| Performs a non-blocking SAI transfer using DMA.  More... | |
| status_t | SAI_TransferReceiveDMA (I2S_Type *base, sai_dma_handle_t *handle, sai_transfer_t *xfer) | 
| Performs a non-blocking SAI transfer using DMA.  More... | |
| void | SAI_TransferAbortSendDMA (I2S_Type *base, sai_dma_handle_t *handle) | 
| Aborts a SAI transfer using DMA.  More... | |
| void | SAI_TransferAbortReceiveDMA (I2S_Type *base, sai_dma_handle_t *handle) | 
| Aborts a SAI transfer using DMA.  More... | |
| status_t | SAI_TransferGetSendCountDMA (I2S_Type *base, sai_dma_handle_t *handle, size_t *count) | 
| Gets byte count sent by SAI.  More... | |
| status_t | SAI_TransferGetReceiveCountDMA (I2S_Type *base, sai_dma_handle_t *handle, size_t *count) | 
| Gets byte count received by SAI.  More... | |
| struct _sai_dma_handle | 
Data Fields | |
| dma_handle_t * | dmaHandle | 
| DMA handler for SAI send.  | |
| uint8_t | bytesPerFrame | 
| Bytes in a frame.  | |
| uint8_t | channel | 
| Which Data channel SAI use.  | |
| uint32_t | state | 
| SAI DMA transfer internal state.  | |
| sai_dma_callback_t | callback | 
| Callback for users while transfer finish or error occured.  | |
| void * | userData | 
| User callback parameter.  | |
| sai_transfer_t | saiQueue [SAI_XFER_QUEUE_SIZE] | 
| Transfer queue storing queued transfer.  More... | |
| size_t | transferSize [SAI_XFER_QUEUE_SIZE] | 
| Data bytes need to transfer.  | |
| volatile uint8_t | queueUser | 
| Index for user to queue transfer.  More... | |
| volatile uint8_t | queueDriver | 
| Index for driver to get the transfer data and size.  | |
| sai_transfer_t sai_dma_handle_t::saiQueue[SAI_XFER_QUEUE_SIZE] | 
| volatile uint8_t sai_dma_handle_t::queueUser | 
| void SAI_TransferTxCreateHandleDMA | ( | I2S_Type * | base, | 
| sai_dma_handle_t * | handle, | ||
| sai_dma_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | dmaHandle | ||
| ) | 
This function initializes the SAI master DMA handle, which can be used for other SAI master transactional APIs. Usually, for a specified SAI instance, call this API once to get the initialized handle.
| base | SAI base pointer. | 
| handle | SAI DMA handle pointer. | 
| base | SAI peripheral base address. | 
| callback | Pointer to user callback function. | 
| userData | User parameter passed to the callback function. | 
| dmaHandle | DMA handle pointer, this handle shall be static allocated by users. | 
| void SAI_TransferRxCreateHandleDMA | ( | I2S_Type * | base, | 
| sai_dma_handle_t * | handle, | ||
| sai_dma_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | dmaHandle | ||
| ) | 
This function initializes the SAI slave DMA handle, which can be used for other SAI master transactional APIs. Usually, for a specified SAI instance, call this API once to get the initialized handle.
| base | SAI base pointer. | 
| handle | SAI DMA handle pointer. | 
| base | SAI peripheral base address. | 
| callback | Pointer to user callback function. | 
| userData | User parameter passed to the callback function. | 
| dmaHandle | DMA handle pointer, this handle shall be static allocated by users. | 
| void SAI_TransferTxSetFormatDMA | ( | I2S_Type * | base, | 
| sai_dma_handle_t * | handle, | ||
| sai_transfer_format_t * | format, | ||
| uint32_t | mclkSourceClockHz, | ||
| uint32_t | bclkSourceClockHz | ||
| ) | 
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred. This function also sets the eDMA parameter according to the format.
| base | SAI base pointer. | 
| handle | SAI DMA handle pointer. | 
| format | Pointer to SAI audio data format structure. | 
| mclkSourceClockHz | SAI master clock source frequency in Hz. | 
| bclkSourceClockHz | SAI bit clock source frequency in Hz. If bit clock source is master. clock, this value should equals to masterClockHz in format. | 
| kStatus_Success | Audio format set successfully. | 
| kStatus_InvalidArgument | The input arguments is invalid. | 
| void SAI_TransferRxSetFormatDMA | ( | I2S_Type * | base, | 
| sai_dma_handle_t * | handle, | ||
| sai_transfer_format_t * | format, | ||
| uint32_t | mclkSourceClockHz, | ||
| uint32_t | bclkSourceClockHz | ||
| ) | 
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred. This function also sets eDMA parameter according to format.
| base | SAI base pointer. | 
| handle | SAI DMA handle pointer. | 
| format | Pointer to SAI audio data format structure. | 
| mclkSourceClockHz | SAI master clock source frequency in Hz. | 
| bclkSourceClockHz | SAI bit clock source frequency in Hz. If bit clock source is master. clock, this value should equals to masterClockHz in format. | 
| kStatus_Success | Audio format set successfully. | 
| kStatus_InvalidArgument | The input arguments is invalid. | 
| status_t SAI_TransferSendDMA | ( | I2S_Type * | base, | 
| sai_dma_handle_t * | handle, | ||
| sai_transfer_t * | xfer | ||
| ) | 
| base | SAI base pointer. | 
| handle | SAI DMA handle pointer. | 
| xfer | Pointer to DMA transfer structure. | 
| kStatus_Success | Successfully start the data receive. | 
| kStatus_SAI_TxBusy | Previous receive still not finished. | 
| kStatus_InvalidArgument | The input parameter is invalid. | 
| status_t SAI_TransferReceiveDMA | ( | I2S_Type * | base, | 
| sai_dma_handle_t * | handle, | ||
| sai_transfer_t * | xfer | ||
| ) | 
| base | SAI base pointer | 
| handle | SAI DMA handle pointer. | 
| xfer | Pointer to DMA transfer structure. | 
| kStatus_Success | Successfully start the data receive. | 
| kStatus_SAI_RxBusy | Previous receive still not finished. | 
| kStatus_InvalidArgument | The input parameter is invalid. | 
| void SAI_TransferAbortSendDMA | ( | I2S_Type * | base, | 
| sai_dma_handle_t * | handle | ||
| ) | 
| base | SAI base pointer. | 
| handle | SAI DMA handle pointer. | 
| void SAI_TransferAbortReceiveDMA | ( | I2S_Type * | base, | 
| sai_dma_handle_t * | handle | ||
| ) | 
| base | SAI base pointer. | 
| handle | SAI DMA handle pointer. | 
| status_t SAI_TransferGetSendCountDMA | ( | I2S_Type * | base, | 
| sai_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | SAI base pointer. | 
| handle | SAI DMA handle pointer. | 
| count | Bytes count sent by SAI. | 
| kStatus_Success | Succeed get the transfer count. | 
| kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. | 
| status_t SAI_TransferGetReceiveCountDMA | ( | I2S_Type * | base, | 
| sai_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | SAI base pointer. | 
| handle | SAI DMA handle pointer. | 
| count | Bytes count received by SAI. | 
| kStatus_Success | Succeed get the transfer count. | 
| kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |