![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
The MCUXpresso SDK provides a driver for the Timer PWM Module (TPM) of MCUXpresso SDK devices.
The TPM driver supports the generation of PWM signals, input capture, and output compare modes. On some SoCs, the driver supports the generation of combined PWM signals, dual-edge capture, and quadrature decoder modes. The driver also supports configuring each of the TPM fault inputs. The fault input is available only on some SoCs.
The function TPM_Init() initializes the TPM with a specified configurations. The function TPM_GetDefaultConfig() gets the default configurations. On some SoCs, the initialization function issues a software reset to reset the TPM internal logic. The initialization function configures the TPM's behavior when it receives a trigger input and its operation in doze and debug modes.
The function TPM_Deinit() disables the TPM counter and turns off the module clock.
The function TPM_SetupPwm() sets up TPM channels for the PWM output. The function can set up the PWM signal properties for multiple channels. Each channel has its own tpm_chnl_pwm_signal_param_t structure that is used to specify the output signals duty cycle and level-mode. However, the same PWM period and PWM mode is applied to all channels requesting a PWM output. The signal duty cycle is provided as a percentage of the PWM period. Its value should be between 0 and 100 where 0=inactive signal (0% duty cycle) and 100=always active signal (100% duty cycle). When generating a combined PWM signal, the channel number passed refers to a channel pair number, for example 0 refers to channel 0 and 1, 1 refers to channels 2 and 3.
The function TPM_UpdatePwmDutycycle() updates the PWM signal duty cycle of a particular TPM channel.
The function TPM_UpdateChnlEdgeLevelSelect() updates the level select bits of a particular TPM channel. This can be used to disable the PWM output when making changes to the PWM signal.
The function TPM_SetupInputCapture() sets up a TPM channel for input capture. The user can specify the capture edge.
The function TPM_SetupDualEdgeCapture() can be used to measure the pulse width of a signal. This is available only for certain SoCs. A channel pair is used during the capture with the input signal coming through a channel that can be configured. The user can specify the capture edge for each channel and any filter value to be used when processing the input signal.
The function TPM_SetupOutputCompare() sets up a TPM channel for output comparison. The user can specify the channel output on a successful comparison and a comparison value.
The function TPM_SetupQuadDecode() sets up TPM channels 0 and 1 for quad decode, which is available only for certain SoCs. The user can specify the quad decode mode, polarity, and filter properties for each input signal.
The function TPM_SetupFault() sets up the properties for each fault, which is available only for certain SoCs. The user can specify the fault polarity and whether to use a filter on a fault input. The overall fault filter value and fault control mode are set up during initialization.
Provides functions to get and clear the TPM status.
Provides functions to enable/disable TPM interrupts and get current enabled interrupts.
Output the PWM signal on 2 TPM channels with different duty cycles. Periodically update the PWM signal duty cycle. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/tpm
Data Structures | |
| struct | tpm_chnl_pwm_signal_param_t |
| Options to configure a TPM channel's PWM signal. More... | |
| struct | tpm_config_t |
| TPM config structure. More... | |
Enumerations | |
| enum | tpm_chnl_t { kTPM_Chnl_0 = 0U, kTPM_Chnl_1, kTPM_Chnl_2, kTPM_Chnl_3, kTPM_Chnl_4, kTPM_Chnl_5, kTPM_Chnl_6, kTPM_Chnl_7 } |
| List of TPM channels. More... | |
| enum | tpm_pwm_mode_t { kTPM_EdgeAlignedPwm = 0U, kTPM_CenterAlignedPwm } |
| TPM PWM operation modes. More... | |
| enum | tpm_pwm_level_select_t { kTPM_NoPwmSignal = 0U, kTPM_LowTrue, kTPM_HighTrue } |
| TPM PWM output pulse mode: high-true, low-true or no output. More... | |
| enum | tpm_trigger_select_t |
| Trigger options available. More... | |
| enum | tpm_output_compare_mode_t { kTPM_NoOutputSignal = (1U << TPM_CnSC_MSA_SHIFT), kTPM_ToggleOnMatch = ((1U << TPM_CnSC_MSA_SHIFT) | (1U << TPM_CnSC_ELSA_SHIFT)), kTPM_ClearOnMatch = ((1U << TPM_CnSC_MSA_SHIFT) | (2U << TPM_CnSC_ELSA_SHIFT)), kTPM_SetOnMatch = ((1U << TPM_CnSC_MSA_SHIFT) | (3U << TPM_CnSC_ELSA_SHIFT)), kTPM_HighPulseOutput = ((3U << TPM_CnSC_MSA_SHIFT) | (1U << TPM_CnSC_ELSA_SHIFT)), kTPM_LowPulseOutput = ((3U << TPM_CnSC_MSA_SHIFT) | (2U << TPM_CnSC_ELSA_SHIFT)) } |
| TPM output compare modes. More... | |
| enum | tpm_input_capture_edge_t { kTPM_RisingEdge = (1U << TPM_CnSC_ELSA_SHIFT), kTPM_FallingEdge = (2U << TPM_CnSC_ELSA_SHIFT), kTPM_RiseAndFallEdge = (3U << TPM_CnSC_ELSA_SHIFT) } |
| TPM input capture edge. More... | |
| enum | tpm_clock_source_t { kTPM_SystemClock = 1U, kTPM_ExternalClock } |
| TPM clock source selection. More... | |
| enum | tpm_clock_prescale_t { kTPM_Prescale_Divide_1 = 0U, kTPM_Prescale_Divide_2, kTPM_Prescale_Divide_4, kTPM_Prescale_Divide_8, kTPM_Prescale_Divide_16, kTPM_Prescale_Divide_32, kTPM_Prescale_Divide_64, kTPM_Prescale_Divide_128 } |
| TPM prescale value selection for the clock source. More... | |
| enum | tpm_interrupt_enable_t { kTPM_Chnl0InterruptEnable = (1U << 0), kTPM_Chnl1InterruptEnable = (1U << 1), kTPM_Chnl2InterruptEnable = (1U << 2), kTPM_Chnl3InterruptEnable = (1U << 3), kTPM_Chnl4InterruptEnable = (1U << 4), kTPM_Chnl5InterruptEnable = (1U << 5), kTPM_Chnl6InterruptEnable = (1U << 6), kTPM_Chnl7InterruptEnable = (1U << 7), kTPM_TimeOverflowInterruptEnable = (1U << 8) } |
| List of TPM interrupts. More... | |
| enum | tpm_status_flags_t { kTPM_Chnl0Flag = (1U << 0), kTPM_Chnl1Flag = (1U << 1), kTPM_Chnl2Flag = (1U << 2), kTPM_Chnl3Flag = (1U << 3), kTPM_Chnl4Flag = (1U << 4), kTPM_Chnl5Flag = (1U << 5), kTPM_Chnl6Flag = (1U << 6), kTPM_Chnl7Flag = (1U << 7), kTPM_TimeOverflowFlag = (1U << 8) } |
| List of TPM flags. More... | |
Driver version | |
| #define | FSL_TPM_DRIVER_VERSION (MAKE_VERSION(2, 0, 2)) |
| Version 2.0.2. | |
Initialization and deinitialization | |
| void | TPM_Init (TPM_Type *base, const tpm_config_t *config) |
| Ungates the TPM clock and configures the peripheral for basic operation. More... | |
| void | TPM_Deinit (TPM_Type *base) |
| Stops the counter and gates the TPM clock. More... | |
| void | TPM_GetDefaultConfig (tpm_config_t *config) |
| Fill in the TPM config struct with the default settings. More... | |
Channel mode operations | |
| status_t | TPM_SetupPwm (TPM_Type *base, const tpm_chnl_pwm_signal_param_t *chnlParams, uint8_t numOfChnls, tpm_pwm_mode_t mode, uint32_t pwmFreq_Hz, uint32_t srcClock_Hz) |
| Configures the PWM signal parameters. More... | |
| void | TPM_UpdatePwmDutycycle (TPM_Type *base, tpm_chnl_t chnlNumber, tpm_pwm_mode_t currentPwmMode, uint8_t dutyCyclePercent) |
| Update the duty cycle of an active PWM signal. More... | |
| void | TPM_UpdateChnlEdgeLevelSelect (TPM_Type *base, tpm_chnl_t chnlNumber, uint8_t level) |
| Update the edge level selection for a channel. More... | |
| void | TPM_SetupInputCapture (TPM_Type *base, tpm_chnl_t chnlNumber, tpm_input_capture_edge_t captureMode) |
| Enables capturing an input signal on the channel using the function parameters. More... | |
| void | TPM_SetupOutputCompare (TPM_Type *base, tpm_chnl_t chnlNumber, tpm_output_compare_mode_t compareMode, uint32_t compareValue) |
| Configures the TPM to generate timed pulses. More... | |
Interrupt Interface | |
| void | TPM_EnableInterrupts (TPM_Type *base, uint32_t mask) |
| Enables the selected TPM interrupts. More... | |
| void | TPM_DisableInterrupts (TPM_Type *base, uint32_t mask) |
| Disables the selected TPM interrupts. More... | |
| uint32_t | TPM_GetEnabledInterrupts (TPM_Type *base) |
| Gets the enabled TPM interrupts. More... | |
Status Interface | |
| static uint32_t | TPM_GetStatusFlags (TPM_Type *base) |
| Gets the TPM status flags. More... | |
| static void | TPM_ClearStatusFlags (TPM_Type *base, uint32_t mask) |
| Clears the TPM status flags. More... | |
Read and write the timer period | |
| static void | TPM_SetTimerPeriod (TPM_Type *base, uint32_t ticks) |
| Sets the timer period in units of ticks. More... | |
| static uint32_t | TPM_GetCurrentTimerCount (TPM_Type *base) |
| Reads the current timer counting value. More... | |
Timer Start and Stop | |
| static void | TPM_StartTimer (TPM_Type *base, tpm_clock_source_t clockSource) |
| Starts the TPM counter. More... | |
| static void | TPM_StopTimer (TPM_Type *base) |
| Stops the TPM counter. More... | |
| struct tpm_chnl_pwm_signal_param_t |
Data Fields | |
| tpm_chnl_t | chnlNumber |
| TPM channel to configure. More... | |
| tpm_pwm_level_select_t | level |
| PWM output active level select. | |
| uint8_t | dutyCyclePercent |
| PWM pulse width, value should be between 0 to 100 0=inactive signal(0% duty cycle)... More... | |
| tpm_chnl_t tpm_chnl_pwm_signal_param_t::chnlNumber |
In combined mode (available in some SoC's, this represents the channel pair number
| uint8_t tpm_chnl_pwm_signal_param_t::dutyCyclePercent |
100=always active signal (100% duty cycle)
| struct tpm_config_t |
This structure holds the configuration settings for the TPM peripheral. To initialize this structure to reasonable defaults, call the TPM_GetDefaultConfig() function and pass a pointer to your config structure instance.
The config struct can be made const so it resides in flash
Data Fields | |
| tpm_clock_prescale_t | prescale |
| Select TPM clock prescale value. | |
| bool | useGlobalTimeBase |
| true: Use of an external global time base is enabled; false: disabled | |
| tpm_trigger_select_t | triggerSelect |
| Input trigger to use for controlling the counter operation. | |
| bool | enableDoze |
| true: TPM counter is paused in doze mode; false: TPM counter continues in doze mode | |
| bool | enableDebugMode |
| true: TPM counter continues in debug mode; false: TPM counter is paused in debug mode | |
| bool | enableReloadOnTrigger |
| true: TPM counter is reloaded on trigger; false: TPM counter not reloaded | |
| bool | enableStopOnOverflow |
| true: TPM counter stops after overflow; false: TPM counter continues running after overflow | |
| bool | enableStartOnTrigger |
| true: TPM counter only starts when a trigger is detected; false: TPM counter starts immediately | |
| enum tpm_chnl_t |
| enum tpm_pwm_mode_t |
| enum tpm_trigger_select_t |
This is used for both internal & external trigger sources (external option available in certain SoC's)
| enum tpm_clock_source_t |
| enum tpm_clock_prescale_t |
| enum tpm_status_flags_t |
| void TPM_Init | ( | TPM_Type * | base, |
| const tpm_config_t * | config | ||
| ) |
| base | TPM peripheral base address |
| config | Pointer to user's TPM config structure. |
| void TPM_Deinit | ( | TPM_Type * | base | ) |
| base | TPM peripheral base address |
| void TPM_GetDefaultConfig | ( | tpm_config_t * | config | ) |
The default values are:
| config | Pointer to user's TPM config structure. |
| status_t TPM_SetupPwm | ( | TPM_Type * | base, |
| const tpm_chnl_pwm_signal_param_t * | chnlParams, | ||
| uint8_t | numOfChnls, | ||
| tpm_pwm_mode_t | mode, | ||
| uint32_t | pwmFreq_Hz, | ||
| uint32_t | srcClock_Hz | ||
| ) |
User calls this function to configure the PWM signals period, mode, dutycycle and edge. Use this function to configure all the TPM channels that will be used to output a PWM signal
| base | TPM peripheral base address |
| chnlParams | Array of PWM channel parameters to configure the channel(s) |
| numOfChnls | Number of channels to configure, this should be the size of the array passed in |
| mode | PWM operation mode, options available in enumeration tpm_pwm_mode_t |
| pwmFreq_Hz | PWM signal frequency in Hz |
| srcClock_Hz | TPM counter clock in Hz |
| void TPM_UpdatePwmDutycycle | ( | TPM_Type * | base, |
| tpm_chnl_t | chnlNumber, | ||
| tpm_pwm_mode_t | currentPwmMode, | ||
| uint8_t | dutyCyclePercent | ||
| ) |
| base | TPM peripheral base address |
| chnlNumber | The channel number. In combined mode, this represents the channel pair number |
| currentPwmMode | The current PWM mode set during PWM setup |
| dutyCyclePercent | New PWM pulse width, value should be between 0 to 100 0=inactive signal(0% duty cycle)... 100=active signal (100% duty cycle) |
| void TPM_UpdateChnlEdgeLevelSelect | ( | TPM_Type * | base, |
| tpm_chnl_t | chnlNumber, | ||
| uint8_t | level | ||
| ) |
| base | TPM peripheral base address |
| chnlNumber | The channel number |
| level | The level to be set to the ELSnB:ELSnA field; valid values are 00, 01, 10, 11. See the appropriate SoC reference manual for details about this field. |
| void TPM_SetupInputCapture | ( | TPM_Type * | base, |
| tpm_chnl_t | chnlNumber, | ||
| tpm_input_capture_edge_t | captureMode | ||
| ) |
When the edge specified in the captureMode argument occurs on the channel, the TPM counter is captured into the CnV register. The user has to read the CnV register separately to get this value.
| base | TPM peripheral base address |
| chnlNumber | The channel number |
| captureMode | Specifies which edge to capture |
| void TPM_SetupOutputCompare | ( | TPM_Type * | base, |
| tpm_chnl_t | chnlNumber, | ||
| tpm_output_compare_mode_t | compareMode, | ||
| uint32_t | compareValue | ||
| ) |
When the TPM counter matches the value of compareVal argument (this is written into CnV reg), the channel output is changed based on what is specified in the compareMode argument.
| base | TPM peripheral base address |
| chnlNumber | The channel number |
| compareMode | Action to take on the channel output when the compare condition is met |
| compareValue | Value to be programmed in the CnV register. |
| void TPM_EnableInterrupts | ( | TPM_Type * | base, |
| uint32_t | mask | ||
| ) |
| base | TPM peripheral base address |
| mask | The interrupts to enable. This is a logical OR of members of the enumeration tpm_interrupt_enable_t |
| void TPM_DisableInterrupts | ( | TPM_Type * | base, |
| uint32_t | mask | ||
| ) |
| base | TPM peripheral base address |
| mask | The interrupts to disable. This is a logical OR of members of the enumeration tpm_interrupt_enable_t |
| uint32_t TPM_GetEnabledInterrupts | ( | TPM_Type * | base | ) |
| base | TPM peripheral base address |
|
inlinestatic |
| base | TPM peripheral base address |
|
inlinestatic |
| base | TPM peripheral base address |
| mask | The status flags to clear. This is a logical OR of members of the enumeration tpm_status_flags_t |
|
inlinestatic |
Timers counts from 0 until it equals the count value set here. The count value is written to the MOD register.
| base | TPM peripheral base address |
| ticks | A timer period in units of ticks, which should be equal or greater than 1. |
|
inlinestatic |
This function returns the real-time timer counting value in a range from 0 to a timer period.
| base | TPM peripheral base address |
|
inlinestatic |
| base | TPM peripheral base address |
| clockSource | TPM clock source; once clock source is set the counter will start running |
|
inlinestatic |
| base | TPM peripheral base address |