The MCUXpresso SDK provides a driver for the Input multiplexing (INPUTMUX).
It configures the inputs to the pin interrupt block, DMA trigger, and frequency measure function. Once configured, the clock is not needed for the inputmux.
Input Multiplexing Driver operation
INPUTMUX_AttachSignal function configures the specified input
Typical use case
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/inputmux
void INPUTMUX_Init |
( |
INPUTMUX_Type * |
base | ) |
|
This function enables the INPUTMUX clock.
- Parameters
-
base | Base address of the INPUTMUX peripheral. |
- Return values
-
void INPUTMUX_AttachSignal |
( |
INPUTMUX_Type * |
base, |
|
|
uint32_t |
index, |
|
|
inputmux_connection_t |
connection |
|
) |
| |
This function gates the INPUTPMUX clock.
- Parameters
-
base | Base address of the INPUTMUX peripheral. |
index | Destination peripheral to attach the signal to. |
connection | Selects connection. |
- Return values
-
void INPUTMUX_Deinit |
( |
INPUTMUX_Type * |
base | ) |
|
This function disables the INPUTMUX clock.
- Parameters
-
base | Base address of the INPUTMUX peripheral. |
- Return values
-