The MCUXpresso SDK provides driver for the Analog Front End (AFE) module of MCUXpresso SDK devices.
The Analog Front End or AFE is an integrated module that is comprised of ΣΔADCs, PGA, filtering and phase compensation blocks. The AFE is responsible for measuring the phase voltage, phase current and neutral current.
Function groups
Channel configuration structures
The driver uses instances of the channel configuration structures to configuration and initialization AFE channel. This structure holds the settings of the AFE measurement channel. The settings include AFE hardware/software triggering, AFE continuous/Single conversion mode, AFE channel mode, AFE channel analog gain, AFE channel oversampling ration. The AFE channel mode selects whether the bypass mode is enabled or disabled and the external clock selection.
User configuration structures
The AFE driver uses instances of the user configuration structure afe_config_t for the AFE driver configuration. This structure holds the configuration which is common for all AFE channels. The settings include AFE low power mode, AFE result format, AFE clock divider mode, AFE clock source mode, and AFE start up delay of modulators.
AFE Initialization
To initialize the AFE driver, for a typical use case, call the AFE_GetDefaultConfig() function which populates the structure. Then, call the AFE_Init() function and pass the base address of the AFE peripheral and a pointer to the user configuration structure.
To configure the AFE channel, for a typical use case call the AFE_GetDefaultChnConfig() function which populates the structure. Then, call the AFE_SetChnConfig() function and pass the base address of the AFE peripheral and a pointer to the channel configuration structure.
AFE Conversion
The driver contains functions for software triggering, a channel delay after trigger setting, a result (raw or converted to right justified), reading and waiting functions.
If the software triggering is enabled (hwTriggerEnable parameter in afe_chn_config_t is a false value), call the AFE_SoftTriggerConv() function to start conversion.
Typical use case
AFE Initialization
afeExampleStruct.startupCount = 80U;
AFE Conversion
while (1)
{
PRINTF("Press any key to trigger AFE conversion\r\n");
GETCHAR();
{
}
PRINTF("result0 = %d \r\n", result0);
}
|
| enum | _afe_channel_status_flag {
kAFE_Channel0OverflowFlag = AFE_SR_OVR0_MASK,
kAFE_Channel1OverflowFlag = AFE_SR_OVR1_MASK,
kAFE_Channel2OverflowFlag = AFE_SR_OVR2_MASK,
kAFE_Channel0ReadyFlag = AFE_SR_RDY0_MASK,
kAFE_Channel1ReadyFlag = AFE_SR_RDY1_MASK,
kAFE_Channel2ReadyFlag = AFE_SR_RDY2_MASK,
kAFE_Channel0ConversionCompleteFlag = AFE_SR_COC0_MASK,
kAFE_Channel1ConversionCompleteFlag = AFE_SR_COC1_MASK,
kAFE_Channel2ConversionCompleteFlag = AFE_SR_COC2_MASK,
kAFE_Channel3OverflowFlag = AFE_SR_OVR3_MASK,
kAFE_Channel3ReadyFlag = AFE_SR_RDY3_MASK,
kAFE_Channel3ConversionCompleteFlag = AFE_SR_COC3_MASK
} |
| | Defines the type of status flags. More...
|
| |
| enum | _afe_channel_interrupt_enable {
kAFE_Channel0InterruptEnable = AFE_DI_INTEN0_MASK,
kAFE_Channel1InterruptEnable = AFE_DI_INTEN1_MASK,
kAFE_Channel2InterruptEnable = AFE_DI_INTEN2_MASK,
kAFE_Channel3InterruptEnable = AFE_DI_INTEN3_MASK
} |
| | Defines AFE interrupt enable. More...
|
| |
| enum | _afe_channel_dma_enable {
kAFE_Channel0DMAEnable = AFE_DI_DMAEN0_MASK,
kAFE_Channel1DMAEnable = AFE_DI_DMAEN1_MASK,
kAFE_Channel2DMAEnable = AFE_DI_DMAEN2_MASK,
kAFE_Channel3DMAEnable = AFE_DI_DMAEN3_MASK
} |
| | Defines AFE DMA enable. More...
|
| |
| enum | _afe_software_trigger_command {
kAFE_Channel0Trigger = AFE_CR_SOFT_TRG0_MASK,
kAFE_Channel1Trigger = AFE_CR_SOFT_TRG1_MASK,
kAFE_Channel2Trigger = AFE_CR_SOFT_TRG2_MASK,
kAFE_Channel3Trigger = AFE_CR_SOFT_TRG3_MASK
} |
| | Defines AFE channel trigger flag. More...
|
| |
| enum | afe_decimator_oversample_ratio_t {
kAFE_DecimatorOversampleRatio64 = 0U,
kAFE_DecimatorOversampleRatio128 = 1U,
kAFE_DecimatorOversampleRatio256 = 2U,
kAFE_DecimatorOversampleRatio512 = 3U,
kAFE_DecimatorOversampleRatio1024 = 4U,
kAFE_DecimatorOversampleRatio2048 = 5U
} |
| | AFE OSR modes. More...
|
| |
| enum | afe_result_format_t {
kAFE_ResultFormatLeft = 0U,
kAFE_ResultFormatRight = 1U
} |
| | Defines the AFE result format modes. More...
|
| |
| enum | afe_clock_divider_t {
kAFE_ClockDivider1 = 0U,
kAFE_ClockDivider2 = 1U,
kAFE_ClockDivider4 = 2U,
kAFE_ClockDivider8 = 3U,
kAFE_ClockDivider16 = 4U,
kAFE_ClockDivider32 = 5U,
kAFE_ClockDivider64 = 6U,
kAFE_ClockDivider128 = 7U,
kAFE_ClockDivider256 = 8U
} |
| | Defines the AFE clock divider modes. More...
|
| |
| enum | afe_clock_source_t {
kAFE_ClockSource0 = 0U,
kAFE_ClockSource1 = 1U,
kAFE_ClockSource2 = 2U,
kAFE_ClockSource3 = 3U
} |
| | Defines the AFE clock source modes. More...
|
| |
| enum | afe_pga_gain_t {
kAFE_PgaDisable = 0U,
kAFE_PgaGain1 = 1U,
kAFE_PgaGain2 = 2U,
kAFE_PgaGain4 = 3U,
kAFE_PgaGain8 = 4U,
kAFE_PgaGain16 = 5U,
kAFE_PgaGain32 = 6U
} |
| | Defines the PGA's values. More...
|
| |
| enum | afe_bypass_mode_t {
kAFE_BypassInternalClockPositiveEdge = 0U,
kAFE_BypassExternalClockPositiveEdge = 1U,
kAFE_BypassInternalClockNegativeEdge = 2U,
kAFE_BypassExternalClockNegativeEdge = 3U,
kAFE_BypassDisable = 4U
} |
| | Defines the bypass modes. More...
|
| |
|
| void | AFE_SetChannelConfig (AFE_Type *base, uint32_t channel, const afe_channel_config_t *config) |
| | Configure the selected AFE channel. More...
|
| |
| void | AFE_GetDefaultChannelConfig (afe_channel_config_t *config) |
| | Fills the channel configuration structure. More...
|
| |
| uint32_t | AFE_GetChannelConversionValue (AFE_Type *base, uint32_t channel) |
| | Reads the raw conversion value. More...
|
| |
| static void | AFE_DoSoftwareTriggerChannel (AFE_Type *base, uint32_t mask) |
| | Triggers the AFE conversion by software. More...
|
| |
| static uint32_t | AFE_GetChannelStatusFlags (AFE_Type *base) |
| | Gets the AFE status flag state. More...
|
| |
| void | AFE_SetChannelPhaseDelayValue (AFE_Type *base, uint32_t channel, uint32_t value) |
| | Sets phase delays value. More...
|
| |
| static void | AFE_SetChannelPhasetDelayOk (AFE_Type *base) |
| | Asserts the phase delay setting. More...
|
| |
| static void | AFE_EnableChannelInterrupts (AFE_Type *base, uint32_t mask) |
| | Enables AFE interrupt. More...
|
| |
| static void | AFE_DisableChannelInterrupts (AFE_Type *base, uint32_t mask) |
| | Disables AFE interrupt. More...
|
| |
| static uint32_t | AFE_GetEnabledChannelInterrupts (AFE_Type *base) |
| | Returns mask of all enabled AFE interrupts. More...
|
| |
| void | AFE_EnableChannelDMA (AFE_Type *base, uint32_t mask, bool enable) |
| | Enables/Disables AFE DMA. More...
|
| |
| struct afe_channel_config_t |
This structure keeps the configuration for the AFE channel.
| bool afe_channel_config_t::enableHardwareTrigger |
| bool afe_channel_config_t::enableContinuousConversion |
This structure keeps the configuration for the AFE module.
| bool afe_config_t::enableLowPower |
| uint8_t afe_config_t::startupCount |
| Enumerator |
|---|
| kAFE_Channel0OverflowFlag |
Channel 0 previous conversion result has not been read and new data has already arrived.
|
| kAFE_Channel1OverflowFlag |
Channel 1 previous conversion result has not been read and new data has already arrived.
|
| kAFE_Channel2OverflowFlag |
Channel 2 previous conversion result has not been read and new data has already arrived.
|
| kAFE_Channel0ReadyFlag |
Channel 0 is ready to conversion.
|
| kAFE_Channel1ReadyFlag |
Channel 1 is ready to conversion.
|
| kAFE_Channel2ReadyFlag |
Channel 2 is ready to conversion.
|
| kAFE_Channel0ConversionCompleteFlag |
Channel 0 conversion is complete.
|
| kAFE_Channel1ConversionCompleteFlag |
Channel 1 conversion is complete.
|
| kAFE_Channel2ConversionCompleteFlag |
Channel 2 conversion is complete.
|
| kAFE_Channel3OverflowFlag |
Channel 3 previous conversion result has not been read and new data has already arrived.
|
| kAFE_Channel3ReadyFlag |
Channel 3 is ready to conversion.
|
| kAFE_Channel3ConversionCompleteFlag |
Channel 3 conversion is complete.
|
| Enumerator |
|---|
| kAFE_Channel0InterruptEnable |
Channel 0 Interrupt.
|
| kAFE_Channel1InterruptEnable |
Channel 1 Interrupt.
|
| kAFE_Channel2InterruptEnable |
Channel 2 Interrupt.
|
| kAFE_Channel3InterruptEnable |
Channel 3 Interrupt.
|
| Enumerator |
|---|
| kAFE_Channel0DMAEnable |
Channel 0 DMA.
|
| kAFE_Channel1DMAEnable |
Channel 1 DMA.
|
| kAFE_Channel2DMAEnable |
Channel 2 DMA.
|
| kAFE_Channel3DMAEnable |
Channel 3 DMA.
|
| Enumerator |
|---|
| kAFE_Channel0Trigger |
Channel 0 software trigger.
|
| kAFE_Channel1Trigger |
Channel 1 software trigger.
|
| kAFE_Channel2Trigger |
Channel 2 software trigger.
|
| kAFE_Channel3Trigger |
Channel 3 software trigger.
|
| Enumerator |
|---|
| kAFE_DecimatorOversampleRatio64 |
Decimator over sample ratio is 64.
|
| kAFE_DecimatorOversampleRatio128 |
Decimator over sample ratio is 128.
|
| kAFE_DecimatorOversampleRatio256 |
Decimator over sample ratio is 256.
|
| kAFE_DecimatorOversampleRatio512 |
Decimator over sample ratio is 512.
|
| kAFE_DecimatorOversampleRatio1024 |
Decimator over sample ratio is 1024.
|
| kAFE_DecimatorOversampleRatio2048 |
Decimator over sample ratio is 2048.
|
| Enumerator |
|---|
| kAFE_ResultFormatLeft |
Left justified result format.
|
| kAFE_ResultFormatRight |
Right justified result format.
|
| Enumerator |
|---|
| kAFE_ClockDivider1 |
Clock divided by 1.
|
| kAFE_ClockDivider2 |
Clock divided by 2.
|
| kAFE_ClockDivider4 |
Clock divided by 4.
|
| kAFE_ClockDivider8 |
Clock divided by 8.
|
| kAFE_ClockDivider16 |
Clock divided by 16.
|
| kAFE_ClockDivider32 |
Clock divided by 32.
|
| kAFE_ClockDivider64 |
Clock divided by 64.
|
| kAFE_ClockDivider128 |
Clock divided by 128.
|
| kAFE_ClockDivider256 |
Clock divided by 256.
|
| Enumerator |
|---|
| kAFE_ClockSource0 |
Modulator clock source 0.
|
| kAFE_ClockSource1 |
Modulator clock source 1.
|
| kAFE_ClockSource2 |
Modulator clock source 2.
|
| kAFE_ClockSource3 |
Modulator clock source 3.
|
| Enumerator |
|---|
| kAFE_PgaDisable |
PGA disabled.
|
| kAFE_PgaGain1 |
Input gained by 1.
|
| kAFE_PgaGain2 |
Input gained by 2.
|
| kAFE_PgaGain4 |
Input gained by 4.
|
| kAFE_PgaGain8 |
Input gained by 8.
|
| kAFE_PgaGain16 |
Input gained by 16.
|
| kAFE_PgaGain32 |
Input gained by 32.
|
| Enumerator |
|---|
| kAFE_BypassInternalClockPositiveEdge |
Bypassed channel mode - internal clock selected, positive edge for registering data by the decimation filter.
|
| kAFE_BypassExternalClockPositiveEdge |
Bypassed channel mode - external clock selected, positive edge for registering data by the decimation filter.
|
| kAFE_BypassInternalClockNegativeEdge |
Bypassed channel mode - internal clock selected, negative edge for registering data by the decimation filter.
|
| kAFE_BypassExternalClockNegativeEdge |
Bypassed channel mode - external clock selected, negative edge for registering data by the decimation filter.
|
| kAFE_BypassDisable |
Normal channel mode.
|
| void AFE_Init |
( |
AFE_Type * |
base, |
|
|
const afe_config_t * |
config |
|
) |
| |
This function configures the AFE module for the configuration which are shared by all channels.
- Parameters
-
| base | AFE peripheral base address. |
| config | Pointer to structure of "afe_config_t". |
| void AFE_Deinit |
( |
AFE_Type * |
base | ) |
|
This function disables clock.
- Parameters
-
| base | AFE peripheral base address. |
This function fills the afe_config_t structure with default settings. Defaut value are:
* config->enableLowPower = false;
* config->startupCount = 2U;
*
- Parameters
-
| config | Pointer to structure of "afe_config_t". |
| static void AFE_SoftwareReset |
( |
AFE_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
This function is to reset all the ADCs, PGAs, decimation filters and clock configuration bits. When asserted as "false", all ADCs, PGAs and decimation filters are disabled. Clock Configuration bits are reset. When asserted as "true", all ADCs, PGAs and decimation filters are enabled.
- Parameters
-
| base | AFE peripheral base address. |
| enable | Assert the reset command. |
| static void AFE_Enable |
( |
AFE_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
This function enables AFE and filter.
- Parameters
-
| base | AFE peripheral base address. |
| enable | Enable the AFE module or not. |
| void AFE_SetChannelConfig |
( |
AFE_Type * |
base, |
|
|
uint32_t |
channel, |
|
|
const afe_channel_config_t * |
config |
|
) |
| |
This function configures the selected AFE channel.
- Parameters
-
| base | AFE peripheral base address. |
| channel | AFE channel index. |
| config | Pointer to structure of "afe_channel_config_t". |
This function fills the afe_channel_config_t structure with default settings. Default value are:
* config->enableHardwareTrigger = false;
* config->enableContinuousConversion = false;
* config->channelMode = kAFE_Normal;
*
- Parameters
-
| config | Pointer to structure of "afe_channel_config_t". |
| uint32_t AFE_GetChannelConversionValue |
( |
AFE_Type * |
base, |
|
|
uint32_t |
channel |
|
) |
| |
This function returns the raw conversion value of the selected channel.
- Parameters
-
| base | AFE peripheral base address. |
| channel | AFE channel index. |
- Returns
- Conversion value.
- Note
- The returned value could be left or right adjusted according to the AFE module configuration.
| static void AFE_DoSoftwareTriggerChannel |
( |
AFE_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
This function triggers the AFE conversion by executing a software command. It starts the conversion on selected channels if the software trigger option is selected for the channels.
- Parameters
-
| base | AFE peripheral base address. |
| mask | AFE channel mask software trigger. The parameter can be combination of the following source if defined:
- kAFE_Channel0Trigger
- kAFE_Channel1Trigger
- kAFE_Channel2Trigger
- kAFE_Channel3Trigger
|
| static uint32_t AFE_GetChannelStatusFlags |
( |
AFE_Type * |
base | ) |
|
|
inlinestatic |
This function gets all AFE status.
- Parameters
-
| base | AFE peripheral base address. |
- Returns
- the mask of these status flag bits.
| void AFE_SetChannelPhaseDelayValue |
( |
AFE_Type * |
base, |
|
|
uint32_t |
channel, |
|
|
uint32_t |
value |
|
) |
| |
This function sets the phase delays for channels. This delay is inserted before the trigger response of the decimation filters. The delay is used to provide a phase compensation between AFE channels in step of prescaled modulator clock periods.
- Parameters
-
| base | AFE peripheral base address. |
| channel | AFE channel index. |
| value | delay time value. |
| static void AFE_SetChannelPhasetDelayOk |
( |
AFE_Type * |
base | ) |
|
|
inlinestatic |
This function should be called after all desired channel's delay registers are loaded. Values in channel's delay registers are active after calling this function and after the conversation starts.
- Parameters
-
| base | AFE peripheral base address. |
| static void AFE_EnableChannelInterrupts |
( |
AFE_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
This function enables one channel interrupt.
- Parameters
-
| base | AFE peripheral base address. |
| mask | AFE channel interrupt mask. The parameter can be combination of the following source if defined:
- kAFE_Channel0InterruptEnable
- kAFE_Channel1InterruptEnable
- kAFE_Channel2InterruptEnable
- kAFE_Channel3InterruptEnable
|
| static void AFE_DisableChannelInterrupts |
( |
AFE_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
This function disables one channel interrupt.
- Parameters
-
| base | AFE peripheral base address. |
| mask | AFE channel interrupt mask. The parameter can be combination of the following source if defined:
- kAFE_Channel0InterruptEnable
- kAFE_Channel1InterruptEnable
- kAFE_Channel2InterruptEnable
- kAFE_Channel3InterruptEnable
|
| static uint32_t AFE_GetEnabledChannelInterrupts |
( |
AFE_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | AFE peripheral base address. |
- Returns
- Return the mask of these interrupt enable/disable bits.
| void AFE_EnableChannelDMA |
( |
AFE_Type * |
base, |
|
|
uint32_t |
mask, |
|
|
bool |
enable |
|
) |
| |
This function enables/disables one channel DMA request.
- Parameters
-
| base | AFE peripheral base address. |
| mask | AFE channel dma mask. |
| enable | Pass true to enable interrupt, false to disable. The parameter can be combination of the following source if defined:
- kAFE_Channel0DMAEnable
- kAFE_Channel1DMAEnable
- kAFE_Channel2DMAEnable
- kAFE_Channel3DMAEnable
|