MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

Data Structures

struct  flexcan_edma_handle_t
 FlexCAN eDMA handle. More...
 

Typedefs

typedef void(* flexcan_edma_transfer_callback_t )(CAN_Type *base, flexcan_edma_handle_t *handle, status_t status, void *userData)
 FlexCAN transfer callback function. More...
 

Driver version

#define FSL_FLEXCAN_EDMA_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))
 FlexCAN EDMA driver version 2.2.0. More...
 

eDMA transactional

void FLEXCAN_TransferCreateHandleEDMA (CAN_Type *base, flexcan_edma_handle_t *handle, flexcan_edma_transfer_callback_t callback, void *userData, edma_handle_t *rxFifoEdmaHandle)
 Initializes the FlexCAN handle, which is used in transactional functions. More...
 
status_t FLEXCAN_TransferReceiveFifoEDMA (CAN_Type *base, flexcan_edma_handle_t *handle, flexcan_fifo_transfer_t *xfer)
 Receives the CAN Message from the Rx FIFO using eDMA. More...
 
void FLEXCAN_TransferAbortReceiveFifoEDMA (CAN_Type *base, flexcan_edma_handle_t *handle)
 Aborts the receive process which used eDMA. More...
 

Data Structure Documentation

struct _flexcan_edma_handle

Data Fields

flexcan_edma_transfer_callback_t callback
 Callback function. More...
 
void * userData
 FlexCAN callback function parameter. More...
 
edma_handle_t * rxFifoEdmaHandle
 The EDMA Rx FIFO channel used. More...
 
volatile uint8_t rxFifoState
 Rx FIFO transfer state. More...
 

Field Documentation

flexcan_edma_transfer_callback_t flexcan_edma_handle_t::callback
void* flexcan_edma_handle_t::userData
edma_handle_t* flexcan_edma_handle_t::rxFifoEdmaHandle
volatile uint8_t flexcan_edma_handle_t::rxFifoState

Macro Definition Documentation

#define FSL_FLEXCAN_EDMA_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0))

Typedef Documentation

typedef void(* flexcan_edma_transfer_callback_t)(CAN_Type *base, flexcan_edma_handle_t *handle, status_t status, void *userData)

Function Documentation

void FLEXCAN_TransferCreateHandleEDMA ( CAN_Type *  base,
flexcan_edma_handle_t *  handle,
flexcan_edma_transfer_callback_t  callback,
void *  userData,
edma_handle_t *  rxFifoEdmaHandle 
)
Parameters
baseFlexCAN peripheral base address.
handlePointer to flexcan_edma_handle_t structure.
callbackThe callback function.
userDataThe parameter of the callback function.
rxFifoEdmaHandleUser-requested DMA handle for Rx FIFO DMA transfer.
status_t FLEXCAN_TransferReceiveFifoEDMA ( CAN_Type *  base,
flexcan_edma_handle_t *  handle,
flexcan_fifo_transfer_t *  xfer 
)

This function receives the CAN Message using eDMA. This is a non-blocking function, which returns right away. After the CAN Message is received, the receive callback function is called.

Parameters
baseFlexCAN peripheral base address.
handlePointer to flexcan_edma_handle_t structure.
xferFlexCAN Rx FIFO EDMA transfer structure, see flexcan_fifo_transfer_t.
Return values
kStatus_Successif succeed, others failed.
kStatus_FLEXCAN_RxFifoBusyPrevious transfer ongoing.
void FLEXCAN_TransferAbortReceiveFifoEDMA ( CAN_Type *  base,
flexcan_edma_handle_t *  handle 
)

This function aborts the receive process which used eDMA.

Parameters
baseFlexCAN peripheral base address.
handlePointer to flexcan_edma_handle_t structure.