![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | lpsci_dma_handle_t |
| LPSCI DMA handle. More... | |
Typedefs | |
| typedef void(* | lpsci_dma_transfer_callback_t )(UART0_Type *base, lpsci_dma_handle_t *handle, status_t status, void *userData) |
| LPSCI transfer callback function. More... | |
eDMA transactional | |
| void | LPSCI_TransferCreateHandleDMA (UART0_Type *base, lpsci_dma_handle_t *handle, lpsci_dma_transfer_callback_t callback, void *userData, dma_handle_t *txDmaHandle, dma_handle_t *rxDmaHandle) |
| Initializes the LPSCI handle which is used in transactional functions. More... | |
| status_t | LPSCI_TransferSendDMA (UART0_Type *base, lpsci_dma_handle_t *handle, lpsci_transfer_t *xfer) |
| Sends data using DMA. More... | |
| status_t | LPSCI_TransferReceiveDMA (UART0_Type *base, lpsci_dma_handle_t *handle, lpsci_transfer_t *xfer) |
| Receives data using DMA. More... | |
| void | LPSCI_TransferAbortSendDMA (UART0_Type *base, lpsci_dma_handle_t *handle) |
| Aborts the sent data using DMA. More... | |
| void | LPSCI_TransferAbortReceiveDMA (UART0_Type *base, lpsci_dma_handle_t *handle) |
| Aborts the receive data using DMA. More... | |
| status_t | LPSCI_TransferGetSendCountDMA (UART0_Type *base, lpsci_dma_handle_t *handle, uint32_t *count) |
| Gets the number of bytes written to the LPSCI TX register. More... | |
| status_t | LPSCI_TransferGetReceiveCountDMA (UART0_Type *base, lpsci_dma_handle_t *handle, uint32_t *count) |
| Gets the number of bytes that have been received. More... | |
| struct _lpsci_dma_handle |
Data Fields | |
| UART0_Type * | base |
| LPSCI peripheral base address. More... | |
| lpsci_dma_transfer_callback_t | callback |
| Callback function. More... | |
| void * | userData |
| UART callback function parameter. More... | |
| size_t | rxDataSizeAll |
| Size of the data to receive. More... | |
| size_t | txDataSizeAll |
| Size of the data to send out. More... | |
| dma_handle_t * | txDmaHandle |
| The DMA TX channel used. More... | |
| dma_handle_t * | rxDmaHandle |
| The DMA RX channel used. More... | |
| volatile uint8_t | txState |
| TX transfer state. More... | |
| volatile uint8_t | rxState |
| RX transfer state. | |
| UART0_Type* lpsci_dma_handle_t::base |
| lpsci_dma_transfer_callback_t lpsci_dma_handle_t::callback |
| void* lpsci_dma_handle_t::userData |
| size_t lpsci_dma_handle_t::rxDataSizeAll |
| size_t lpsci_dma_handle_t::txDataSizeAll |
| dma_handle_t* lpsci_dma_handle_t::txDmaHandle |
| dma_handle_t* lpsci_dma_handle_t::rxDmaHandle |
| volatile uint8_t lpsci_dma_handle_t::txState |
| typedef void(* lpsci_dma_transfer_callback_t)(UART0_Type *base, lpsci_dma_handle_t *handle, status_t status, void *userData) |
| void LPSCI_TransferCreateHandleDMA | ( | UART0_Type * | base, |
| lpsci_dma_handle_t * | handle, | ||
| lpsci_dma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | txDmaHandle, | ||
| dma_handle_t * | rxDmaHandle | ||
| ) |
| handle | Pointer to lpsci_dma_handle_t structure |
| base | LPSCI peripheral base address |
| rxDmaHandle | User requested DMA handle for RX DMA transfer |
| txDmaHandle | User requested DMA handle for TX DMA transfer |
| status_t LPSCI_TransferSendDMA | ( | UART0_Type * | base, |
| lpsci_dma_handle_t * | handle, | ||
| lpsci_transfer_t * | xfer | ||
| ) |
This function sends data using DMA. This is a non-blocking function, which returns immediately. When all data is sent, the send callback function is called.
| handle | LPSCI handle pointer. |
| xfer | LPSCI DMA transfer structure, see lpsci_transfer_t. |
| kStatus_Success | if successful, others failed. |
| kStatus_LPSCI_TxBusy | Previous transfer on going. |
| kStatus_InvalidArgument | Invalid argument. |
| status_t LPSCI_TransferReceiveDMA | ( | UART0_Type * | base, |
| lpsci_dma_handle_t * | handle, | ||
| lpsci_transfer_t * | xfer | ||
| ) |
This function receives data using DMA. This is a non-blocking function, which returns immediately. When all data is received, the receive callback function is called.
| handle | Pointer to lpsci_dma_handle_t structure |
| xfer | LPSCI DMA transfer structure, see lpsci_transfer_t. |
| kStatus_Success | if successful, others failed. |
| kStatus_LPSCI_RxBusy | Previous transfer on going. |
| kStatus_InvalidArgument | Invalid argument. |
| void LPSCI_TransferAbortSendDMA | ( | UART0_Type * | base, |
| lpsci_dma_handle_t * | handle | ||
| ) |
This function aborts the sent data using DMA.
| handle | Pointer to lpsci_dma_handle_t structure. |
| void LPSCI_TransferAbortReceiveDMA | ( | UART0_Type * | base, |
| lpsci_dma_handle_t * | handle | ||
| ) |
This function aborts the receive data using DMA.
| handle | Pointer to lpsci_dma_handle_t structure. |
| status_t LPSCI_TransferGetSendCountDMA | ( | UART0_Type * | base, |
| lpsci_dma_handle_t * | handle, | ||
| uint32_t * | count | ||
| ) |
This function gets the number of bytes that have been written to the LPSCI TX register by DMA.
| base | LPSCI peripheral base address. |
| handle | LPSCI handle pointer. |
| count | Send bytes count. |
| kStatus_NoTransferInProgress | No send in progress. |
| kStatus_InvalidArgument | Parameter is invalid. |
| kStatus_Success | Get successfully through the parameter count; |
| status_t LPSCI_TransferGetReceiveCountDMA | ( | UART0_Type * | base, |
| lpsci_dma_handle_t * | handle, | ||
| uint32_t * | count | ||
| ) |
This function gets the number of bytes that have been received.
| base | LPSCI peripheral base address. |
| handle | LPSCI handle pointer. |
| count | Receive bytes count. |
| kStatus_NoTransferInProgress | No receive in progress. |
| kStatus_InvalidArgument | Parameter is invalid. |
| kStatus_Success | Get successfully through the parameter count; |