![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | sdiocard_usr_param_t | 
| card user parameter, user can define the parameter according the board, card capability  More... | |
| struct | sdio_card_t | 
| SDIO card state.  More... | |
Macros | |
| #define | FSL_SDIO_DRIVER_VERSION (MAKE_VERSION(2U, 2U, 6U)) /*2.2.6*/ | 
| Middleware version.  More... | |
SDIOCARD Function | |
| status_t | SDIO_Init (sdio_card_t *card) | 
| SDIO card init function.  More... | |
| void | SDIO_Deinit (sdio_card_t *card) | 
| SDIO card deinit, include card and host deinit.  More... | |
| status_t | SDIO_CardInit (sdio_card_t *card) | 
| Initializes the card.  More... | |
| void | SDIO_CardDeinit (sdio_card_t *card) | 
| Deinitializes the card.  More... | |
| status_t | SDIO_HostInit (sdio_card_t *card) | 
| initialize the host.  More... | |
| void | SDIO_HostDeinit (sdio_card_t *card) | 
| Deinitializes the host.  More... | |
| void | SDIO_HostReset (SDMMCHOST_CONFIG *host) | 
| reset the host.  More... | |
| void | SDIO_PowerOnCard (SDMMCHOST_TYPE *base, const sdmmchost_pwr_card_t *pwr) | 
| power on card.  More... | |
| void | SDIO_PowerOffCard (SDMMCHOST_TYPE *base, const sdmmchost_pwr_card_t *pwr) | 
| power on card.  More... | |
| status_t | SDIO_CardInActive (sdio_card_t *card) | 
| set SDIO card to inactive state  More... | |
| status_t | SDIO_IO_Write_Direct (sdio_card_t *card, sdio_func_num_t func, uint32_t regAddr, uint8_t *data, bool raw) | 
| IO direct write transfer function.  More... | |
| status_t | SDIO_IO_Read_Direct (sdio_card_t *card, sdio_func_num_t func, uint32_t regAddr, uint8_t *data) | 
| IO direct read transfer function.  More... | |
| status_t | SDIO_IO_Write_Extended (sdio_card_t *card, sdio_func_num_t func, uint32_t regAddr, uint8_t *buffer, uint32_t count, uint32_t flags) | 
| IO extended write transfer function.  More... | |
| status_t | SDIO_IO_Read_Extended (sdio_card_t *card, sdio_func_num_t func, uint32_t regAddr, uint8_t *buffer, uint32_t count, uint32_t flags) | 
| IO extended read transfer function.  More... | |
| status_t | SDIO_GetCardCapability (sdio_card_t *card, sdio_func_num_t func) | 
| get SDIO card capability  More... | |
| status_t | SDIO_SetBlockSize (sdio_card_t *card, sdio_func_num_t func, uint32_t blockSize) | 
| set SDIO card block size  More... | |
| status_t | SDIO_CardReset (sdio_card_t *card) | 
| set SDIO card reset  More... | |
| status_t | SDIO_SetDataBusWidth (sdio_card_t *card, sdio_bus_width_t busWidth) | 
| set SDIO card data bus width  More... | |
| status_t | SDIO_SwitchToHighSpeed (sdio_card_t *card) | 
| switch the card to high speed  More... | |
| status_t | SDIO_ReadCIS (sdio_card_t *card, sdio_func_num_t func, const uint32_t *tupleList, uint32_t tupleNum) | 
| read SDIO card CIS for each function  More... | |
| status_t | SDIO_EnableIOInterrupt (sdio_card_t *card, sdio_func_num_t func, bool enable) | 
| enable IO interrupt  More... | |
| status_t | SDIO_EnableIO (sdio_card_t *card, sdio_func_num_t func, bool enable) | 
| enable IO and wait IO ready  More... | |
| status_t | SDIO_SelectIO (sdio_card_t *card, sdio_func_num_t func) | 
| select IO  More... | |
| status_t | SDIO_AbortIO (sdio_card_t *card, sdio_func_num_t func) | 
| Abort IO transfer.  More... | |
| status_t | SDIO_WaitCardDetectStatus (SDMMCHOST_TYPE *hostBase, const sdmmchost_detect_card_t *cd, bool waitCardStatus) | 
| sdio wait card detect function.  More... | |
| bool | SDIO_IsCardPresent (sdio_card_t *card) | 
| sdio card present check function.  More... | |
| status_t | SDIO_IO_Transfer (sdio_card_t *card, sdio_command_t cmd, uint32_t argument, uint32_t blockSize, uint8_t *txData, uint8_t *rxData, uint16_t dataSize, uint32_t *response) | 
| sdio card io transfer function.  More... | |
| struct sdiocard_usr_param_t | 
Data Fields | |
| const sdmmchost_detect_card_t * | cd | 
| card detect type  | |
| const sdmmchost_pwr_card_t * | pwr | 
| power control configuration  | |
| struct sdio_card_t | 
Define the card structure including the necessary fields to identify and describe the card.
Data Fields | |
| SDMMCHOST_CONFIG | host | 
| Host information.  | |
| sdiocard_usr_param_t | usrParam | 
| user parameter  | |
| bool | isHostReady | 
| use this flag to indicate if need host re-init or not  | |
| bool | memPresentFlag | 
| indicate if memory present  | |
| uint32_t | busClock_Hz | 
| SD bus clock frequency united in Hz.  | |
| uint32_t | relativeAddress | 
| Relative address of the card.  | |
| uint8_t | sdVersion | 
| SD version.  | |
| uint8_t | sdioVersion | 
| SDIO version.  | |
| uint8_t | cccrVersioin | 
| CCCR version.  | |
| uint8_t | ioTotalNumber | 
| total number of IO function  | |
| uint32_t | cccrflags | 
| Flags in _sd_card_flag.  | |
| uint32_t | io0blockSize | 
| record the io0 block size  | |
| uint32_t | ocr | 
| Raw OCR content, only 24bit avalible for SDIO card.  | |
| uint32_t | commonCISPointer | 
| point to common CIS  | |
| sdio_fbr_t | ioFBR [7U] | 
| FBR table.  | |
| sdio_common_cis_t | commonCIS | 
| CIS table.  | |
| sdio_func_cis_t | funcCIS [7U] | 
| function CIS table  | |
| #define FSL_SDIO_DRIVER_VERSION (MAKE_VERSION(2U, 2U, 6U)) /*2.2.6*/ | 
| status_t SDIO_Init | ( | sdio_card_t * | card | ) | 
| card | Card descriptor. | 
| kStatus_SDMMC_GoIdleFailed | |
| kStatus_SDMMC_HandShakeOperationConditionFailed | |
| kStatus_SDMMC_SDIO_InvalidCard | |
| kStatus_SDMMC_SDIO_InvalidVoltage | |
| kStatus_SDMMC_SendRelativeAddressFailed | |
| kStatus_SDMMC_SelectCardFailed | |
| kStatus_SDMMC_SDIO_SwitchHighSpeedFail | |
| kStatus_SDMMC_SDIO_ReadCISFail | |
| kStatus_SDMMC_TransferFailed | |
| kStatus_Success | 
| void SDIO_Deinit | ( | sdio_card_t * | card | ) | 
| card | Card descriptor. | 
| status_t SDIO_CardInit | ( | sdio_card_t * | card | ) | 
This function initializes the card only, make sure the host is ready when call this function, otherwise it will return kStatus_SDMMC_HostNotReady.
| card | Card descriptor. | 
| kStatus_SDMMC_HostNotReady | host is not ready. | 
| kStatus_SDMMC_GoIdleFailed | Go idle failed. | 
| kStatus_SDMMC_NotSupportYet | Card not support. | 
| kStatus_SDMMC_SendOperationConditionFailed | Send operation condition failed. | 
| kStatus_SDMMC_AllSendCidFailed | Send CID failed. | 
| kStatus_SDMMC_SendRelativeAddressFailed | Send relative address failed. | 
| kStatus_SDMMC_SendCsdFailed | Send CSD failed. | 
| kStatus_SDMMC_SelectCardFailed | Send SELECT_CARD command failed. | 
| kStatus_SDMMC_SendScrFailed | Send SCR failed. | 
| kStatus_SDMMC_SetBusWidthFailed | Set bus width failed. | 
| kStatus_SDMMC_SwitchHighSpeedFailed | Switch high speed failed. | 
| kStatus_SDMMC_SetCardBlockSizeFailed | Set card block size failed. | 
| kStatus_Success | Operate successfully. | 
| void SDIO_CardDeinit | ( | sdio_card_t * | card | ) | 
This function deinitializes the specific card.
| card | Card descriptor. | 
| status_t SDIO_HostInit | ( | sdio_card_t * | card | ) | 
This function deinitializes the specific host.
| card | Card descriptor. | 
| void SDIO_HostDeinit | ( | sdio_card_t * | card | ) | 
This function deinitializes the host.
| card | Card descriptor. | 
| void SDIO_HostReset | ( | SDMMCHOST_CONFIG * | host | ) | 
This function reset the specific host.
| host | host descriptor. | 
| void SDIO_PowerOnCard | ( | SDMMCHOST_TYPE * | base, | 
| const sdmmchost_pwr_card_t * | pwr | ||
| ) | 
The power on operation depend on host or the user define power on function.
| base | host base address. | 
| pwr | user define power control configuration | 
| void SDIO_PowerOffCard | ( | SDMMCHOST_TYPE * | base, | 
| const sdmmchost_pwr_card_t * | pwr | ||
| ) | 
The power off operation depend on host or the user define power on function.
| base | host base address. | 
| pwr | user define power control configuration | 
| status_t SDIO_CardInActive | ( | sdio_card_t * | card | ) | 
| card | Card descriptor. | 
| kStatus_SDMMC_TransferFailed | |
| kStatus_Success | 
| status_t SDIO_IO_Write_Direct | ( | sdio_card_t * | card, | 
| sdio_func_num_t | func, | ||
| uint32_t | regAddr, | ||
| uint8_t * | data, | ||
| bool | raw | ||
| ) | 
| card | Card descriptor. | 
| function | IO numner | 
| register | address | 
| the | data pinter to write | 
| raw | flag, indicate read after write or write only | 
| kStatus_SDMMC_TransferFailed | |
| kStatus_Success | 
| status_t SDIO_IO_Read_Direct | ( | sdio_card_t * | card, | 
| sdio_func_num_t | func, | ||
| uint32_t | regAddr, | ||
| uint8_t * | data | ||
| ) | 
| card | Card descriptor. | 
| function | IO number | 
| register | address | 
| data | pointer to read | 
| kStatus_SDMMC_TransferFailed | |
| kStatus_Success | 
| status_t SDIO_IO_Write_Extended | ( | sdio_card_t * | card, | 
| sdio_func_num_t | func, | ||
| uint32_t | regAddr, | ||
| uint8_t * | buffer, | ||
| uint32_t | count, | ||
| uint32_t | flags | ||
| ) | 
| card | Card descriptor. | 
| function | IO number | 
| register | address | 
| data | buffer to write | 
| data | count | 
| write | flags | 
| kStatus_SDMMC_TransferFailed | |
| kStatus_SDMMC_SDIO_InvalidArgument | |
| kStatus_Success | 
| status_t SDIO_IO_Read_Extended | ( | sdio_card_t * | card, | 
| sdio_func_num_t | func, | ||
| uint32_t | regAddr, | ||
| uint8_t * | buffer, | ||
| uint32_t | count, | ||
| uint32_t | flags | ||
| ) | 
| card | Card descriptor. | 
| function | IO number | 
| register | address | 
| data | buffer to read | 
| data | count | 
| write | flags | 
| kStatus_SDMMC_TransferFailed | |
| kStatus_SDMMC_SDIO_InvalidArgument | |
| kStatus_Success | 
| status_t SDIO_GetCardCapability | ( | sdio_card_t * | card, | 
| sdio_func_num_t | func | ||
| ) | 
| card | Card descriptor. | 
| function | IO number | 
| kStatus_SDMMC_TransferFailed | |
| kStatus_Success | 
| status_t SDIO_SetBlockSize | ( | sdio_card_t * | card, | 
| sdio_func_num_t | func, | ||
| uint32_t | blockSize | ||
| ) | 
| card | Card descriptor. | 
| function | io number | 
| block | size | 
| kStatus_SDMMC_SetCardBlockSizeFailed | |
| kStatus_SDMMC_SDIO_InvalidArgument | |
| kStatus_Success | 
| status_t SDIO_CardReset | ( | sdio_card_t * | card | ) | 
| card | Card descriptor. | 
| kStatus_SDMMC_TransferFailed | |
| kStatus_Success | 
| status_t SDIO_SetDataBusWidth | ( | sdio_card_t * | card, | 
| sdio_bus_width_t | busWidth | ||
| ) | 
| card | Card descriptor. | 
| data | bus width | 
| kStatus_SDMMC_TransferFailed | |
| kStatus_Success | 
| status_t SDIO_SwitchToHighSpeed | ( | sdio_card_t * | card | ) | 
| card | Card descriptor. | 
| kStatus_SDMMC_TransferFailed | |
| kStatus_SDMMC_SDIO_SwitchHighSpeedFail | |
| kStatus_Success | 
| status_t SDIO_ReadCIS | ( | sdio_card_t * | card, | 
| sdio_func_num_t | func, | ||
| const uint32_t * | tupleList, | ||
| uint32_t | tupleNum | ||
| ) | 
| card | Card descriptor. | 
| function | io number | 
| tuple | code list | 
| tuple | code number | 
| kStatus_SDMMC_SDIO_ReadCISFail | |
| kStatus_SDMMC_TransferFailed | |
| kStatus_Success | 
| status_t SDIO_EnableIOInterrupt | ( | sdio_card_t * | card, | 
| sdio_func_num_t | func, | ||
| bool | enable | ||
| ) | 
| card | Card descriptor. | 
| function | IO number | 
| enable/disable | flag | 
| kStatus_SDMMC_TransferFailed | |
| kStatus_Success | 
| status_t SDIO_EnableIO | ( | sdio_card_t * | card, | 
| sdio_func_num_t | func, | ||
| bool | enable | ||
| ) | 
| card | Card descriptor. | 
| function | IO number | 
| enable/disable | flag | 
| kStatus_SDMMC_TransferFailed | |
| kStatus_Success | 
| status_t SDIO_SelectIO | ( | sdio_card_t * | card, | 
| sdio_func_num_t | func | ||
| ) | 
| card | Card descriptor. | 
| function | IO number | 
| kStatus_SDMMC_TransferFailed | |
| kStatus_Success | 
| status_t SDIO_AbortIO | ( | sdio_card_t * | card, | 
| sdio_func_num_t | func | ||
| ) | 
| card | Card descriptor. | 
| function | IO number | 
| kStatus_SDMMC_TransferFailed | |
| kStatus_Success | 
| status_t SDIO_WaitCardDetectStatus | ( | SDMMCHOST_TYPE * | hostBase, | 
| const sdmmchost_detect_card_t * | cd, | ||
| bool | waitCardStatus | ||
| ) | 
Detect card through GPIO, CD, DATA3.
| card | card descriptor. | 
| card | detect configuration | 
| waitCardStatus | wait card detect status | 
| bool SDIO_IsCardPresent | ( | sdio_card_t * | card | ) | 
| card | card descriptor. | 
| status_t SDIO_IO_Transfer | ( | sdio_card_t * | card, | 
| sdio_command_t | cmd, | ||
| uint32_t | argument, | ||
| uint32_t | blockSize, | ||
| uint8_t * | txData, | ||
| uint8_t * | rxData, | ||
| uint16_t | dataSize, | ||
| uint32_t * | response | ||
| ) | 
This function can be used for trnansfer direct/extend command. Please pay attention to the non-align data buffer address transfer, if data buffer address can not meet host controller internal DMA requirement, sdio driver will try to use internal align buffer if data size is not bigger than internal buffer size, Align address transfer always can get a better performance, so if application want sdio driver make sure buffer address align, please redefine the SDMMC_GLOBAL_BUFFER_SIZE macro to a value which is big enough for your application.
| card | card descriptor. | 
| cmd | command to transfer | 
| argument | argument to transfer | 
| blockSize | used for block mode. | 
| txData | tx buffer pointer or NULL | 
| rxData | rx buffer pointer or NULL | 
| dataSize | transfer data size | 
| response | reponse pointer, if application want read response back, please set it to a NON-NULL pointer. |