![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Driver version | |
| #define | FSL_DSPI_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 2, 0)) |
| DSPI FREERTOS driver version 2.2.0. More... | |
DSPI RTOS Operation | |
| status_t | DSPI_RTOS_Init (dspi_rtos_handle_t *handle, SPI_Type *base, const dspi_master_config_t *masterConfig, uint32_t srcClock_Hz) |
| Initializes the DSPI. More... | |
| status_t | DSPI_RTOS_Deinit (dspi_rtos_handle_t *handle) |
| Deinitializes the DSPI. More... | |
| status_t | DSPI_RTOS_Transfer (dspi_rtos_handle_t *handle, dspi_transfer_t *transfer) |
| Performs the SPI transfer. More... | |
| #define FSL_DSPI_FREERTOS_DRIVER_VERSION (MAKE_VERSION(2, 2, 0)) |
| status_t DSPI_RTOS_Init | ( | dspi_rtos_handle_t * | handle, |
| SPI_Type * | base, | ||
| const dspi_master_config_t * | masterConfig, | ||
| uint32_t | srcClock_Hz | ||
| ) |
This function initializes the DSPI module and the related RTOS context.
| handle | The RTOS DSPI handle, the pointer to an allocated space for RTOS context. |
| base | The pointer base address of the DSPI instance to initialize. |
| masterConfig | A configuration structure to set-up the DSPI in master mode. |
| srcClock_Hz | A frequency of the input clock of the DSPI module. |
| status_t DSPI_RTOS_Deinit | ( | dspi_rtos_handle_t * | handle | ) |
This function deinitializes the DSPI module and the related RTOS context.
| handle | The RTOS DSPI handle. |
| status_t DSPI_RTOS_Transfer | ( | dspi_rtos_handle_t * | handle, |
| dspi_transfer_t * | transfer | ||
| ) |
This function performs the SPI transfer according to the data given in the transfer structure.
| handle | The RTOS DSPI handle. |
| transfer | A structure specifying the transfer parameters. |