![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev. 0
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | ftfx_prefetch_speculation_status_t | 
| FTFx prefetch speculation status.  More... | |
| struct | ftfx_cache_config_t | 
| FTFx cache driver state information.  More... | |
Enumerations | |
| enum | _ftfx_cache_ram_func_constants { kFTFx_CACHE_RamFuncMaxSizeInWords = 16U } | 
| Constants for execute-in-RAM flash function.  More... | |
Functions | |
| status_t | FTFx_CACHE_Init (ftfx_cache_config_t *config) | 
| Initializes the global FTFx cache structure members.  More... | |
| status_t | FTFx_CACHE_ClearCachePrefetchSpeculation (ftfx_cache_config_t *config, bool isPreProcess) | 
| Process the cache/prefetch/speculation to the flash.  More... | |
| status_t | FTFx_CACHE_PflashSetPrefetchSpeculation (ftfx_prefetch_speculation_status_t *speculationStatus) | 
| Sets the PFlash prefetch speculation to the intended speculation status.  More... | |
| status_t | FTFx_CACHE_PflashGetPrefetchSpeculation (ftfx_prefetch_speculation_status_t *speculationStatus) | 
| Gets the PFlash prefetch speculation status.  More... | |
FTFx cache version | |
| #define | FSL_FTFX_CACHE_DRIVER_VERSION (MAKE_VERSION(1, 0, 0)) | 
| Flexnvm driver version for SDK.  More... | |
| struct ftfx_prefetch_speculation_status_t | 
Data Fields | |
| bool | instructionOff | 
| Instruction speculation.  More... | |
| bool | dataOff | 
| Data speculation.  More... | |
| bool ftfx_prefetch_speculation_status_t::instructionOff | 
| bool ftfx_prefetch_speculation_status_t::dataOff | 
| struct ftfx_cache_config_t | 
An instance of this structure is allocated by the user of the flash driver and passed into each of the driver APIs.
Data Fields | |
| uint8_t | flashMemoryIndex | 
| 0 - primary flash; 1 - secondary flash  | |
| uint32_t * | comBitOperFuncAddr | 
| An buffer point to the flash execute-in-RAM function.  More... | |
| uint32_t* ftfx_cache_config_t::comBitOperFuncAddr | 
| #define FSL_FTFX_CACHE_DRIVER_VERSION (MAKE_VERSION(1, 0, 0)) | 
Version 1.0.0.
| status_t FTFx_CACHE_Init | ( | ftfx_cache_config_t * | config | ) | 
This function checks and initializes the Flash module for the other FTFx cache APIs.
| config | Pointer to the storage for the driver runtime state. | 
| #kStatus_FTFx_Success | API was executed successfully. | 
| #kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| #kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| status_t FTFx_CACHE_ClearCachePrefetchSpeculation | ( | ftfx_cache_config_t * | config, | 
| bool | isPreProcess | ||
| ) | 
| config | A pointer to the storage for the driver runtime state. | 
| process | The possible option used to control flash cache/prefetch/speculation | 
| #kStatus_FTFx_Success | API was executed successfully. | 
| #kStatus_FTFx_InvalidArgument | Invalid argument is provided. | 
| #kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| status_t FTFx_CACHE_PflashSetPrefetchSpeculation | ( | ftfx_prefetch_speculation_status_t * | speculationStatus | ) | 
| speculationStatus | The expected protect status to set to the PFlash protection register. Each bit is | 
| #kStatus_FTFx_Success | API was executed successfully. | 
| #kStatus_FTFx_InvalidSpeculationOption | An invalid speculation option argument is provided. | 
| status_t FTFx_CACHE_PflashGetPrefetchSpeculation | ( | ftfx_prefetch_speculation_status_t * | speculationStatus | ) | 
| speculationStatus | Speculation status returned by the PFlash IP. | 
| #kStatus_FTFx_Success | API was executed successfully. |