![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | i2c_master_dma_handle_t |
| I2C master DMA transfer structure. More... | |
Typedefs | |
| typedef void(* | i2c_master_dma_transfer_callback_t )(I2C_Type *base, i2c_master_dma_handle_t *handle, status_t status, void *userData) |
| I2C master DMA transfer callback typedef. More... | |
Driver version | |
| #define | FSL_I2C_DMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 5)) |
| I2C DMA driver version 2.0.5. More... | |
I2C Block DMA Transfer Operation | |
| void | I2C_MasterTransferCreateHandleDMA (I2C_Type *base, i2c_master_dma_handle_t *handle, i2c_master_dma_transfer_callback_t callback, void *userData, dma_handle_t *dmaHandle) |
| Initializes the I2C handle which is used in transcational functions. More... | |
| status_t | I2C_MasterTransferDMA (I2C_Type *base, i2c_master_dma_handle_t *handle, i2c_master_transfer_t *xfer) |
| Performs a master DMA non-blocking transfer on the I2C bus. More... | |
| status_t | I2C_MasterTransferGetCountDMA (I2C_Type *base, i2c_master_dma_handle_t *handle, size_t *count) |
| Gets a master transfer status during a DMA non-blocking transfer. More... | |
| void | I2C_MasterTransferAbortDMA (I2C_Type *base, i2c_master_dma_handle_t *handle) |
| Aborts a master DMA non-blocking transfer early. More... | |
| struct _i2c_master_dma_handle |
I2C master DMA handle typedef.
Data Fields | |
| i2c_master_transfer_t | transfer |
| I2C master transfer struct. More... | |
| size_t | transferSize |
| Total bytes to be transferred. More... | |
| uint8_t | state |
| I2C master transfer status. More... | |
| dma_handle_t * | dmaHandle |
| The DMA handler used. More... | |
| i2c_master_dma_transfer_callback_t | completionCallback |
| A callback function called after the DMA transfer finished. More... | |
| void * | userData |
| A callback parameter passed to the callback function. More... | |
| i2c_master_transfer_t i2c_master_dma_handle_t::transfer |
| size_t i2c_master_dma_handle_t::transferSize |
| uint8_t i2c_master_dma_handle_t::state |
| dma_handle_t* i2c_master_dma_handle_t::dmaHandle |
| i2c_master_dma_transfer_callback_t i2c_master_dma_handle_t::completionCallback |
| void* i2c_master_dma_handle_t::userData |
| #define FSL_I2C_DMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 5)) |
| typedef void(* i2c_master_dma_transfer_callback_t)(I2C_Type *base, i2c_master_dma_handle_t *handle, status_t status, void *userData) |
| void I2C_MasterTransferCreateHandleDMA | ( | I2C_Type * | base, |
| i2c_master_dma_handle_t * | handle, | ||
| i2c_master_dma_transfer_callback_t | callback, | ||
| void * | userData, | ||
| dma_handle_t * | dmaHandle | ||
| ) |
| base | I2C peripheral base address |
| handle | Pointer to the i2c_master_dma_handle_t structure |
| callback | Pointer to the user callback function |
| userData | A user parameter passed to the callback function |
| dmaHandle | DMA handle pointer |
| status_t I2C_MasterTransferDMA | ( | I2C_Type * | base, |
| i2c_master_dma_handle_t * | handle, | ||
| i2c_master_transfer_t * | xfer | ||
| ) |
| base | I2C peripheral base address |
| handle | A pointer to the i2c_master_dma_handle_t structure |
| xfer | A pointer to the transfer structure of the i2c_master_transfer_t |
| kStatus_Success | Sucessfully completes the data transmission. |
| kStatus_I2C_Busy | A previous transmission is still not finished. |
| kStatus_I2C_Timeout | A transfer error, waits for the signal timeout. |
| kStatus_I2C_ArbitrationLost | A transfer error, arbitration lost. |
| kStataus_I2C_Nak | A transfer error, receives NAK during transfer. |
| status_t I2C_MasterTransferGetCountDMA | ( | I2C_Type * | base, |
| i2c_master_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | I2C peripheral base address |
| handle | A pointer to the i2c_master_dma_handle_t structure |
| count | A number of bytes transferred so far by the non-blocking transaction. |
| void I2C_MasterTransferAbortDMA | ( | I2C_Type * | base, |
| i2c_master_dma_handle_t * | handle | ||
| ) |
| base | I2C peripheral base address |
| handle | A pointer to the i2c_master_dma_handle_t structure. |