![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
SD card status.
#include <fsl_sdmmc_spec.h>
Data Fields | |
uint8_t | busWidth |
current buswidth | |
uint8_t | secureMode |
secured mode | |
uint16_t | cardType |
sdcard type | |
uint32_t | protectedSize |
size of protected area | |
uint8_t | speedClass |
speed class of card | |
uint8_t | performanceMove |
Performance of move indicated by 1[MB/S]step. | |
uint8_t | auSize |
size of AU | |
uint16_t | eraseSize |
number of AUs to be erased at a time | |
uint8_t | eraseTimeout |
timeout value for erasing areas specified by UNIT OF ERASE AU | |
uint8_t | eraseOffset |
fixed offset value added to erase time | |
uint8_t | uhsSpeedGrade |
speed grade for UHS mode | |
uint8_t | uhsAuSize |
size of AU for UHS mode | |