MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

Data Structures

struct  lpsci_dma_handle_t
 LPSCI DMA handle. More...
 

Typedefs

typedef void(* lpsci_dma_transfer_callback_t )(UART0_Type *base, lpsci_dma_handle_t *handle, status_t status, void *userData)
 LPSCI transfer callback function. More...
 

eDMA transactional

void LPSCI_TransferCreateHandleDMA (UART0_Type *base, lpsci_dma_handle_t *handle, lpsci_dma_transfer_callback_t callback, void *userData, dma_handle_t *txDmaHandle, dma_handle_t *rxDmaHandle)
 Initializes the LPSCI handle which is used in transactional functions. More...
 
status_t LPSCI_TransferSendDMA (UART0_Type *base, lpsci_dma_handle_t *handle, lpsci_transfer_t *xfer)
 Sends data using DMA. More...
 
status_t LPSCI_TransferReceiveDMA (UART0_Type *base, lpsci_dma_handle_t *handle, lpsci_transfer_t *xfer)
 Receives data using DMA. More...
 
void LPSCI_TransferAbortSendDMA (UART0_Type *base, lpsci_dma_handle_t *handle)
 Aborts the sent data using DMA. More...
 
void LPSCI_TransferAbortReceiveDMA (UART0_Type *base, lpsci_dma_handle_t *handle)
 Aborts the receive data using DMA. More...
 
status_t LPSCI_TransferGetSendCountDMA (UART0_Type *base, lpsci_dma_handle_t *handle, uint32_t *count)
 Gets the number of bytes written to the LPSCI TX register. More...
 
status_t LPSCI_TransferGetReceiveCountDMA (UART0_Type *base, lpsci_dma_handle_t *handle, uint32_t *count)
 Gets the number of bytes that have been received. More...
 

Data Structure Documentation

struct _lpsci_dma_handle

Data Fields

UART0_Type * base
 LPSCI peripheral base address. More...
 
lpsci_dma_transfer_callback_t callback
 Callback function. More...
 
void * userData
 UART callback function parameter. More...
 
size_t rxDataSizeAll
 Size of the data to receive. More...
 
size_t txDataSizeAll
 Size of the data to send out. More...
 
dma_handle_t * txDmaHandle
 The DMA TX channel used. More...
 
dma_handle_t * rxDmaHandle
 The DMA RX channel used. More...
 
volatile uint8_t txState
 TX transfer state. More...
 
volatile uint8_t rxState
 RX transfer state.
 

Field Documentation

UART0_Type* lpsci_dma_handle_t::base
lpsci_dma_transfer_callback_t lpsci_dma_handle_t::callback
void* lpsci_dma_handle_t::userData
size_t lpsci_dma_handle_t::rxDataSizeAll
size_t lpsci_dma_handle_t::txDataSizeAll
dma_handle_t* lpsci_dma_handle_t::txDmaHandle
dma_handle_t* lpsci_dma_handle_t::rxDmaHandle
volatile uint8_t lpsci_dma_handle_t::txState

Typedef Documentation

typedef void(* lpsci_dma_transfer_callback_t)(UART0_Type *base, lpsci_dma_handle_t *handle, status_t status, void *userData)

Function Documentation

void LPSCI_TransferCreateHandleDMA ( UART0_Type *  base,
lpsci_dma_handle_t *  handle,
lpsci_dma_transfer_callback_t  callback,
void *  userData,
dma_handle_t *  txDmaHandle,
dma_handle_t *  rxDmaHandle 
)
Parameters
handlePointer to lpsci_dma_handle_t structure
baseLPSCI peripheral base address
rxDmaHandleUser requested DMA handle for RX DMA transfer
txDmaHandleUser requested DMA handle for TX DMA transfer
status_t LPSCI_TransferSendDMA ( UART0_Type *  base,
lpsci_dma_handle_t *  handle,
lpsci_transfer_t *  xfer 
)

This function sends data using DMA. This is a non-blocking function, which returns immediately. When all data is sent, the send callback function is called.

Parameters
handleLPSCI handle pointer.
xferLPSCI DMA transfer structure, see lpsci_transfer_t.
Return values
kStatus_Successif successful, others failed.
kStatus_LPSCI_TxBusyPrevious transfer on going.
kStatus_InvalidArgumentInvalid argument.
status_t LPSCI_TransferReceiveDMA ( UART0_Type *  base,
lpsci_dma_handle_t *  handle,
lpsci_transfer_t *  xfer 
)

This function receives data using DMA. This is a non-blocking function, which returns immediately. When all data is received, the receive callback function is called.

Parameters
handlePointer to lpsci_dma_handle_t structure
xferLPSCI DMA transfer structure, see lpsci_transfer_t.
Return values
kStatus_Successif successful, others failed.
kStatus_LPSCI_RxBusyPrevious transfer on going.
kStatus_InvalidArgumentInvalid argument.
void LPSCI_TransferAbortSendDMA ( UART0_Type *  base,
lpsci_dma_handle_t *  handle 
)

This function aborts the sent data using DMA.

Parameters
handlePointer to lpsci_dma_handle_t structure.
void LPSCI_TransferAbortReceiveDMA ( UART0_Type *  base,
lpsci_dma_handle_t *  handle 
)

This function aborts the receive data using DMA.

Parameters
handlePointer to lpsci_dma_handle_t structure.
status_t LPSCI_TransferGetSendCountDMA ( UART0_Type *  base,
lpsci_dma_handle_t *  handle,
uint32_t *  count 
)

This function gets the number of bytes that have been written to the LPSCI TX register by DMA.

Parameters
baseLPSCI peripheral base address.
handleLPSCI handle pointer.
countSend bytes count.
Return values
kStatus_NoTransferInProgressNo send in progress.
kStatus_InvalidArgumentParameter is invalid.
kStatus_SuccessGet successfully through the parameter count;
status_t LPSCI_TransferGetReceiveCountDMA ( UART0_Type *  base,
lpsci_dma_handle_t *  handle,
uint32_t *  count 
)

This function gets the number of bytes that have been received.

Parameters
baseLPSCI peripheral base address.
handleLPSCI handle pointer.
countReceive bytes count.
Return values
kStatus_NoTransferInProgressNo receive in progress.
kStatus_InvalidArgumentParameter is invalid.
kStatus_SuccessGet successfully through the parameter count;