![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
sdio card FBR register
#include <fsl_sdmmc_spec.h>
Data Fields | |
| uint8_t | flags |
| current io flags | |
| uint8_t | ioStdFunctionCode |
| current io standard function code | |
| uint8_t | ioExtFunctionCode |
| current io extended function code | |
| uint32_t | ioPointerToCIS |
| current io pointer to CIS | |
| uint32_t | ioPointerToCSA |
| current io pointer to CSA | |
| uint16_t | ioBlockSize |
| current io block size | |