MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
ENET: Ethernet MAC Driver

Overview

The MCUXpresso SDK provides a peripheral driver for the 10/100 Mbps Ethernet MAC (ENET) module of MCUXpresso SDK devices.

The MII interface is the interface connected with MAC and PHY. the Serial management interface - MII management interface should be set before any access to the external PHY chip register. Call ENET_SetSMI() to initialize the MII management interface. Use ENET_StartSMIRead(), ENET_StartSMIWrite(), and ENET_ReadSMIData() to read/write to PHY registers. This function group sets up the MII and serial management SMI interface, gets data from the SMI interface, and starts the SMI read and write command. Use ENET_SetMII() to configure the MII before successfully getting data from the external PHY.

This group sets/gets the ENET mac address and the multicast group address filter. ENET_AddMulticastGroup() should be called to add the ENET MAC to the multicast group. The IEEE 1588 feature requires receiving the PTP message.

This group has the receive active API ENET_ActiveRead() and ENET_ActiveReadMultiRing() for single and multiple rings. The ENET_AVBConfigure() is provided to configure the AVB features to support the AVB frames transmission. Note that due to the AVB frames transmission scheme being a credit-based TX scheme, it is only supported with the Enhanced buffer descriptors. Because of this, the AVB configuration should only be done with the Enhanced buffer descriptor. When the AVB feature is required, make sure the the "ENET_ENHANCEDBUFFERDESCRIPTOR_MODE" is defined before using this feature.

  1. For single ring

For ENET receive, the ENET_GetRxFrameSize() function needs to be called to get the received data size. Then, call the ENET_ReadFrame() function to get the received data. If the received error occurs, call the ENET_GetRxErrBeforeReadFrame() function after ENET_GetRxFrameSize() and before ENET_ReadFrame() functions to get the detailed error information.

For ENET transmit, call the ENET_SendFrame() function to send the data out. The transmit data error information is only accessible for the IEEE 1588 enhanced buffer descriptor mode. When the ENET_ENHANCEDBUFFERDESCRIPTOR_MODE is defined, the ENET_GetTxErrAfterSendFrame() can be used to get the detail transmit error information. The transmit error information can only be updated by uDMA after the data is transmitted. The ENET_GetTxErrAfterSendFrame() function is recommended to be called on the transmit interrupt handler.

  1. For multiple-ring supported

The ENET driver now added a series transactional APIs with postfix "MultiRing" to support the extended multiple-ring for AVB feature. There are extended multiple-ring functions for receive side: ENET_GetRxErrBeforeReadFrameMultiRing(), ENET_GetRxFrameSizeMultiRing(), and ENET_ReadFrameMultiRing(). They are the similar to the single ring receive APIs and only add the "ringId" input param to identify the different ring index. For TX side add the ENET_SendFrameMultiRing, ENET_GetTxErrAfterSendFrameMultiRing(). They are the similar to the single ring transmit APIs and only add the "ringId" input param to identify the different ring index.

This function group configures the PTP IEEE 1588 feature, starts/stops/gets/sets/adjusts the PTP IEEE 1588 timer, gets the receive/transmit frame timestamp, and PTP IEEE 1588 timer channel feature setting.

The ENET_Ptp1588Configure() function needs to be called when the ENET_ENHANCEDBUFFERDESCRIPTOR_MODE is defined and the IEEE 1588 feature is required. The ENET_GetRxFrameTime() and ENET_GetTxFrameTime() functions are called by the PTP stack to get the timestamp captured by the ENET driver.

Typical use case

ENET Initialization, receive, and transmit operations

For the ENET_ENHANCEDBUFFERDESCRIPTOR_MODE undefined use case, use the legacy type buffer descriptor transmit/receive the frame as follows. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/enet For the ENET_ENHANCEDBUFFERDESCRIPTOR_MODE defined use case, add the PTP IEEE 1588 configuration to enable the PTP IEEE 1588 feature. The initialization occurs as follows. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/enet

Data Structures

struct  enet_rx_bd_struct_t
 Defines the receive buffer descriptor structure for the little endian system. More...
 
struct  enet_tx_bd_struct_t
 Defines the enhanced transmit buffer descriptor structure for the little endian system. More...
 
struct  enet_data_error_stats_t
 Defines the ENET data error statistics structure. More...
 
struct  enet_buffer_config_t
 Defines the receive buffer descriptor configuration structure. More...
 
struct  enet_ptp_time_t
 Defines the ENET PTP time stamp structure. More...
 
struct  enet_ptp_time_data_t
 Defines the structure for the ENET PTP message data and timestamp data. More...
 
struct  enet_ptp_time_data_ring_t
 Defines the ENET PTP ring buffer structure for the PTP message timestamp store. More...
 
struct  enet_ptp_config_t
 Defines the ENET PTP configuration structure. More...
 
struct  enet_config_t
 Defines the basic configuration structure for the ENET device. More...
 
struct  enet_handle_t
 Defines the ENET handler structure. More...
 

Macros

#define ENET_BUFFDESCRIPTOR_RX_ERR_MASK
 Defines the receive error status flag mask. More...
 

Typedefs

typedef void(* enet_callback_t )(ENET_Type *base, enet_handle_t *handle, enet_event_t event, void *userData)
 ENET callback function. More...
 

Enumerations

enum  _enet_status {
  kStatus_ENET_RxFrameError = MAKE_STATUS(kStatusGroup_ENET, 0U),
  kStatus_ENET_RxFrameFail = MAKE_STATUS(kStatusGroup_ENET, 1U),
  kStatus_ENET_RxFrameEmpty = MAKE_STATUS(kStatusGroup_ENET, 2U),
  kStatus_ENET_TxFrameOverLen = MAKE_STATUS(kStatusGroup_ENET, 3U),
  kStatus_ENET_TxFrameBusy = MAKE_STATUS(kStatusGroup_ENET, 4U),
  kStatus_ENET_TxFrameFail = MAKE_STATUS(kStatusGroup_ENET, 5U),
  kStatus_ENET_PtpTsRingFull = MAKE_STATUS(kStatusGroup_ENET, 6U),
  kStatus_ENET_PtpTsRingEmpty = MAKE_STATUS(kStatusGroup_ENET, 7U)
}
 Defines the status return codes for transaction. More...
 
enum  enet_mii_mode_t {
  kENET_MiiMode = 0U,
  kENET_RmiiMode = 1U
}
 Defines the MII/RMII/RGMII mode for data interface between the MAC and the PHY. More...
 
enum  enet_mii_speed_t {
  kENET_MiiSpeed10M = 0U,
  kENET_MiiSpeed100M = 1U
}
 Defines the 10/100/1000 Mbps speed for the MII data interface. More...
 
enum  enet_mii_duplex_t {
  kENET_MiiHalfDuplex = 0U,
  kENET_MiiFullDuplex
}
 Defines the half or full duplex for the MII data interface. More...
 
enum  enet_mii_write_t {
  kENET_MiiWriteNoCompliant = 0U,
  kENET_MiiWriteValidFrame
}
 Define the MII opcode for normal MDIO_CLAUSES_22 Frame. More...
 
enum  enet_mii_read_t {
  kENET_MiiReadValidFrame = 2U,
  kENET_MiiReadNoCompliant = 3U
}
 Defines the read operation for the MII management frame. More...
 
enum  enet_special_control_flag_t {
  kENET_ControlFlowControlEnable = 0x0001U,
  kENET_ControlRxPayloadCheckEnable = 0x0002U,
  kENET_ControlRxPadRemoveEnable = 0x0004U,
  kENET_ControlRxBroadCastRejectEnable = 0x0008U,
  kENET_ControlMacAddrInsert = 0x0010U,
  kENET_ControlStoreAndFwdDisable = 0x0020U,
  kENET_ControlSMIPreambleDisable = 0x0040U,
  kENET_ControlPromiscuousEnable = 0x0080U,
  kENET_ControlMIILoopEnable = 0x0100U,
  kENET_ControlVLANTagEnable = 0x0200U
}
 Defines a special configuration for ENET MAC controller. More...
 
enum  enet_interrupt_enable_t {
  kENET_BabrInterrupt = ENET_EIR_BABR_MASK,
  kENET_BabtInterrupt = ENET_EIR_BABT_MASK,
  kENET_GraceStopInterrupt = ENET_EIR_GRA_MASK,
  kENET_TxFrameInterrupt = ENET_EIR_TXF_MASK,
  kENET_TxBufferInterrupt = ENET_EIR_TXB_MASK,
  kENET_RxFrameInterrupt = ENET_EIR_RXF_MASK,
  kENET_RxBufferInterrupt = ENET_EIR_RXB_MASK,
  kENET_MiiInterrupt = ENET_EIR_MII_MASK,
  kENET_EBusERInterrupt = ENET_EIR_EBERR_MASK,
  kENET_LateCollisionInterrupt = ENET_EIR_LC_MASK,
  kENET_RetryLimitInterrupt = ENET_EIR_RL_MASK,
  kENET_UnderrunInterrupt = ENET_EIR_UN_MASK,
  kENET_PayloadRxInterrupt = ENET_EIR_PLR_MASK,
  kENET_WakeupInterrupt = ENET_EIR_WAKEUP_MASK,
  kENET_TsAvailInterrupt = ENET_EIR_TS_AVAIL_MASK,
  kENET_TsTimerInterrupt = ENET_EIR_TS_TIMER_MASK
}
 List of interrupts supported by the peripheral. More...
 
enum  enet_event_t {
  kENET_RxEvent,
  kENET_TxEvent,
  kENET_ErrEvent,
  kENET_WakeUpEvent,
  kENET_TimeStampEvent,
  kENET_TimeStampAvailEvent
}
 Defines the common interrupt event for callback use. More...
 
enum  enet_tx_accelerator_t {
  kENET_TxAccelIsShift16Enabled = ENET_TACC_SHIFT16_MASK,
  kENET_TxAccelIpCheckEnabled = ENET_TACC_IPCHK_MASK,
  kENET_TxAccelProtoCheckEnabled = ENET_TACC_PROCHK_MASK
}
 Defines the transmit accelerator configuration. More...
 
enum  enet_rx_accelerator_t {
  kENET_RxAccelPadRemoveEnabled = ENET_RACC_PADREM_MASK,
  kENET_RxAccelIpCheckEnabled = ENET_RACC_IPDIS_MASK,
  kENET_RxAccelProtoCheckEnabled = ENET_RACC_PRODIS_MASK,
  kENET_RxAccelMacCheckEnabled = ENET_RACC_LINEDIS_MASK,
  kENET_RxAccelisShift16Enabled = ENET_RACC_SHIFT16_MASK
}
 Defines the receive accelerator configuration. More...
 
enum  enet_ptp_event_type_t {
  kENET_PtpEventMsgType = 3U,
  kENET_PtpSrcPortIdLen = 10U,
  kENET_PtpEventPort = 319U,
  kENET_PtpGnrlPort = 320U
}
 Defines the ENET PTP message related constant. More...
 
enum  enet_ptp_timer_channel_t {
  kENET_PtpTimerChannel1 = 0U,
  kENET_PtpTimerChannel2,
  kENET_PtpTimerChannel3,
  kENET_PtpTimerChannel4
}
 Defines the IEEE 1588 PTP timer channel numbers. More...
 
enum  enet_ptp_timer_channel_mode_t {
  kENET_PtpChannelDisable = 0U,
  kENET_PtpChannelRisingCapture = 1U,
  kENET_PtpChannelFallingCapture = 2U,
  kENET_PtpChannelBothCapture = 3U,
  kENET_PtpChannelSoftCompare = 4U,
  kENET_PtpChannelToggleCompare = 5U,
  kENET_PtpChannelClearCompare = 6U,
  kENET_PtpChannelSetCompare = 7U,
  kENET_PtpChannelClearCompareSetOverflow = 10U,
  kENET_PtpChannelSetCompareClearOverflow = 11U,
  kENET_PtpChannelPulseLowonCompare = 14U,
  kENET_PtpChannelPulseHighonCompare = 15U
}
 Defines the capture or compare mode for IEEE 1588 PTP timer channels. More...
 

Driver version

#define FSL_ENET_DRIVER_VERSION   (MAKE_VERSION(2, 2, 3))
 Defines the driver version. More...
 

ENET DESCRIPTOR QUEUE

#define FSL_FEATURE_ENET_QUEUE   1 /* Singal queue for previous IP. */
 Defines the queue number. More...
 

Control and status region bit masks of the receive buffer descriptor.

#define ENET_BUFFDESCRIPTOR_RX_EMPTY_MASK   0x8000U
 Empty bit mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_SOFTOWNER1_MASK   0x4000U
 Software owner one mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_WRAP_MASK   0x2000U
 Next buffer descriptor is the start address. More...
 
#define ENET_BUFFDESCRIPTOR_RX_SOFTOWNER2_Mask   0x1000U
 Software owner two mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_LAST_MASK   0x0800U
 Last BD of the frame mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_MISS_MASK   0x0100U
 Received because of the promiscuous mode. More...
 
#define ENET_BUFFDESCRIPTOR_RX_BROADCAST_MASK   0x0080U
 Broadcast packet mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_MULTICAST_MASK   0x0040U
 Multicast packet mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_LENVLIOLATE_MASK   0x0020U
 Length violation mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_NOOCTET_MASK   0x0010U
 Non-octet aligned frame mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_CRC_MASK   0x0004U
 CRC error mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_OVERRUN_MASK   0x0002U
 FIFO overrun mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_TRUNC_MASK   0x0001U
 Frame is truncated mask. More...
 

Control and status bit masks of the transmit buffer descriptor.

#define ENET_BUFFDESCRIPTOR_TX_READY_MASK   0x8000U
 Ready bit mask. More...
 
#define ENET_BUFFDESCRIPTOR_TX_SOFTOWENER1_MASK   0x4000U
 Software owner one mask. More...
 
#define ENET_BUFFDESCRIPTOR_TX_WRAP_MASK   0x2000U
 Wrap buffer descriptor mask. More...
 
#define ENET_BUFFDESCRIPTOR_TX_SOFTOWENER2_MASK   0x1000U
 Software owner two mask. More...
 
#define ENET_BUFFDESCRIPTOR_TX_LAST_MASK   0x0800U
 Last BD of the frame mask. More...
 
#define ENET_BUFFDESCRIPTOR_TX_TRANMITCRC_MASK   0x0400U
 Transmit CRC mask. More...
 

First extended control region bit masks of the receive buffer descriptor.

#define ENET_BUFFDESCRIPTOR_RX_IPV4_MASK   0x0001U
 Ipv4 frame mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_IPV6_MASK   0x0002U
 Ipv6 frame mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_VLAN_MASK   0x0004U
 VLAN frame mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_PROTOCOLCHECKSUM_MASK   0x0010U
 Protocol checksum error mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_IPHEADCHECKSUM_MASK   0x0020U
 IP header checksum error mask. More...
 

Second extended control region bit masks of the receive buffer descriptor.

#define ENET_BUFFDESCRIPTOR_RX_INTERRUPT_MASK   0x0080U
 BD interrupt mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_UNICAST_MASK   0x0100U
 Unicast frame mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_COLLISION_MASK   0x0200U
 BD collision mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_PHYERR_MASK   0x0400U
 PHY error mask. More...
 
#define ENET_BUFFDESCRIPTOR_RX_MACERR_MASK   0x8000U
 Mac error mask. More...
 

First extended control region bit masks of the transmit buffer descriptor.

#define ENET_BUFFDESCRIPTOR_TX_ERR_MASK   0x8000U
 Transmit error mask. More...
 
#define ENET_BUFFDESCRIPTOR_TX_UNDERFLOWERR_MASK   0x2000U
 Underflow error mask. More...
 
#define ENET_BUFFDESCRIPTOR_TX_EXCCOLLISIONERR_MASK   0x1000U
 Excess collision error mask. More...
 
#define ENET_BUFFDESCRIPTOR_TX_FRAMEERR_MASK   0x0800U
 Frame error mask. More...
 
#define ENET_BUFFDESCRIPTOR_TX_LATECOLLISIONERR_MASK   0x0400U
 Late collision error mask. More...
 
#define ENET_BUFFDESCRIPTOR_TX_OVERFLOWERR_MASK   0x0200U
 Overflow error mask. More...
 
#define ENET_BUFFDESCRIPTOR_TX_TIMESTAMPERR_MASK   0x0100U
 Timestamp error mask. More...
 

Second extended control region bit masks of the transmit buffer descriptor.

#define ENET_BUFFDESCRIPTOR_TX_INTERRUPT_MASK   0x4000U
 Interrupt mask. More...
 
#define ENET_BUFFDESCRIPTOR_TX_TIMESTAMP_MASK   0x2000U
 Timestamp flag mask. More...
 

Defines some Ethernet parameters.

#define ENET_FRAME_MAX_FRAMELEN   1518U
 Default maximum Ethernet frame size. More...
 
#define ENET_FIFO_MIN_RX_FULL   5U
 ENET minimum receive FIFO full. More...
 
#define ENET_RX_MIN_BUFFERSIZE   256U
 ENET minimum buffer size. More...
 
#define ENET_PHY_MAXADDRESS   (ENET_MMFR_PA_MASK >> ENET_MMFR_PA_SHIFT)
 
#define ENET_TX_INTERRUPT   (kENET_TxFrameInterrupt | kENET_TxBufferInterrupt)
 
#define ENET_RX_INTERRUPT   (kENET_RxFrameInterrupt | kENET_RxBufferInterrupt)
 
#define ENET_TS_INTERRUPT   (kENET_TsTimerInterrupt | kENET_TsAvailInterrupt)
 
#define ENET_ERR_INTERRUPT
 
#define ENET_ERR_INTERRUPT
 

Initialization and De-initialization

void ENET_GetDefaultConfig (enet_config_t *config)
 Gets the ENET default configuration structure. More...
 
void ENET_Init (ENET_Type *base, enet_handle_t *handle, const enet_config_t *config, const enet_buffer_config_t *bufferConfig, uint8_t *macAddr, uint32_t srcClock_Hz)
 Initializes the ENET module. More...
 
void ENET_Deinit (ENET_Type *base)
 Deinitializes the ENET module. More...
 
static void ENET_Reset (ENET_Type *base)
 Resets the ENET module. More...
 

MII interface operation

void ENET_SetMII (ENET_Type *base, enet_mii_speed_t speed, enet_mii_duplex_t duplex)
 Sets the ENET MII speed and duplex. More...
 
void ENET_SetSMI (ENET_Type *base, uint32_t srcClock_Hz, bool isPreambleDisabled)
 Sets the ENET SMI(serial management interface)- MII management interface. More...
 
static bool ENET_GetSMI (ENET_Type *base)
 Gets the ENET SMI- MII management interface configuration. More...
 
static uint32_t ENET_ReadSMIData (ENET_Type *base)
 Reads data from the PHY register through an SMI interface. More...
 
void ENET_StartSMIRead (ENET_Type *base, uint32_t phyAddr, uint32_t phyReg, enet_mii_read_t operation)
 Starts an SMI (Serial Management Interface) read command. More...
 
void ENET_StartSMIWrite (ENET_Type *base, uint32_t phyAddr, uint32_t phyReg, enet_mii_write_t operation, uint32_t data)
 Starts an SMI write command. More...
 

MAC Address Filter

void ENET_SetMacAddr (ENET_Type *base, uint8_t *macAddr)
 Sets the ENET module Mac address. More...
 
void ENET_GetMacAddr (ENET_Type *base, uint8_t *macAddr)
 Gets the ENET module Mac address. More...
 
void ENET_AddMulticastGroup (ENET_Type *base, uint8_t *address)
 Adds the ENET device to a multicast group. More...
 
void ENET_LeaveMulticastGroup (ENET_Type *base, uint8_t *address)
 Moves the ENET device from a multicast group. More...
 

Other basic operation

static void ENET_ActiveRead (ENET_Type *base)
 Activates ENET read or receive. More...
 
static void ENET_EnableSleepMode (ENET_Type *base, bool enable)
 Enables/disables the MAC to enter sleep mode. More...
 
static void ENET_GetAccelFunction (ENET_Type *base, uint32_t *txAccelOption, uint32_t *rxAccelOption)
 Gets ENET transmit and receive accelerator functions from MAC controller. More...
 

Interrupts.

static void ENET_EnableInterrupts (ENET_Type *base, uint32_t mask)
 Enables the ENET interrupt. More...
 
static void ENET_DisableInterrupts (ENET_Type *base, uint32_t mask)
 Disables the ENET interrupt. More...
 
static uint32_t ENET_GetInterruptStatus (ENET_Type *base)
 Gets the ENET interrupt status flag. More...
 
static void ENET_ClearInterruptStatus (ENET_Type *base, uint32_t mask)
 Clears the ENET interrupt events status flag. More...
 

Transactional operation

void ENET_SetCallback (enet_handle_t *handle, enet_callback_t callback, void *userData)
 Sets the callback function. More...
 
void ENET_GetRxErrBeforeReadFrame (enet_handle_t *handle, enet_data_error_stats_t *eErrorStatic)
 Gets the error statistics of a received frame for ENET single ring. More...
 
status_t ENET_GetTxErrAfterSendFrame (enet_handle_t *handle, enet_data_error_stats_t *eErrorStatic)
 Gets the ENET transmit frame statistics after the data send for single ring. More...
 
status_t ENET_GetRxFrameSize (enet_handle_t *handle, uint32_t *length)
 Gets the size of the read frame for single ring. More...
 
status_t ENET_ReadFrame (ENET_Type *base, enet_handle_t *handle, uint8_t *data, uint32_t length)
 Reads a frame from the ENET device for single ring. More...
 
status_t ENET_SendFrame (ENET_Type *base, enet_handle_t *handle, const uint8_t *data, uint32_t length)
 Transmits an ENET frame for single ring. More...
 
void ENET_TransmitIRQHandler (ENET_Type *base, enet_handle_t *handle)
 The transmit IRQ handler. More...
 
void ENET_ReceiveIRQHandler (ENET_Type *base, enet_handle_t *handle)
 The receive IRQ handler. More...
 
void ENET_ErrorIRQHandler (ENET_Type *base, enet_handle_t *handle)
 Some special IRQ handler including the error, mii, wakeup irq handler. More...
 
void ENET_CommonFrame0IRQHandler (ENET_Type *base)
 the common IRQ handler for the tx/rx/error etc irq handler. More...
 

ENET PTP 1588 function operation

void ENET_Ptp1588Configure (ENET_Type *base, enet_handle_t *handle, enet_ptp_config_t *ptpConfig)
 Configures the ENET PTP IEEE 1588 feature with the basic configuration. More...
 
void ENET_Ptp1588StartTimer (ENET_Type *base, uint32_t ptpClkSrc)
 Starts the ENET PTP 1588 Timer. More...
 
static void ENET_Ptp1588StopTimer (ENET_Type *base)
 Stops the ENET PTP 1588 Timer. More...
 
void ENET_Ptp1588AdjustTimer (ENET_Type *base, uint32_t corrIncrease, uint32_t corrPeriod)
 Adjusts the ENET PTP 1588 timer. More...
 
static void ENET_Ptp1588SetChannelMode (ENET_Type *base, enet_ptp_timer_channel_t channel, enet_ptp_timer_channel_mode_t mode, bool intEnable)
 Sets the ENET PTP 1588 timer channel mode. More...
 
static void ENET_Ptp1588SetChannelCmpValue (ENET_Type *base, enet_ptp_timer_channel_t channel, uint32_t cmpValue)
 Sets the ENET PTP 1588 timer channel comparison value. More...
 
static bool ENET_Ptp1588GetChannelStatus (ENET_Type *base, enet_ptp_timer_channel_t channel)
 Gets the ENET PTP 1588 timer channel status. More...
 
static void ENET_Ptp1588ClearChannelStatus (ENET_Type *base, enet_ptp_timer_channel_t channel)
 Clears the ENET PTP 1588 timer channel status. More...
 
void ENET_Ptp1588GetTimer (ENET_Type *base, enet_handle_t *handle, enet_ptp_time_t *ptpTime)
 Gets the current ENET time from the PTP 1588 timer. More...
 
void ENET_Ptp1588SetTimer (ENET_Type *base, enet_handle_t *handle, enet_ptp_time_t *ptpTime)
 Sets the ENET PTP 1588 timer to the assigned time. More...
 
void ENET_Ptp1588TimerIRQHandler (ENET_Type *base, enet_handle_t *handle)
 The IEEE 1588 PTP time stamp interrupt handler. More...
 
status_t ENET_GetRxFrameTime (enet_handle_t *handle, enet_ptp_time_data_t *ptpTimeData)
 Gets the time stamp of the received frame. More...
 
status_t ENET_GetTxFrameTime (enet_handle_t *handle, enet_ptp_time_data_t *ptpTimeData)
 Gets the time stamp of the transmit frame. More...
 

Data Structure Documentation

struct enet_rx_bd_struct_t

Data Fields

uint16_t length
 Buffer descriptor data length. More...
 
uint16_t control
 Buffer descriptor control and status. More...
 
uint8_t * buffer
 Data buffer pointer. More...
 
uint16_t controlExtend0
 Extend buffer descriptor control0. More...
 
uint16_t controlExtend1
 Extend buffer descriptor control1. More...
 
uint16_t payloadCheckSum
 Internal payload checksum. More...
 
uint8_t headerLength
 Header length. More...
 
uint8_t protocolTyte
 Protocol type. More...
 
uint16_t controlExtend2
 Extend buffer descriptor control2. More...
 
uint32_t timestamp
 Timestamp. More...
 

Field Documentation

uint16_t enet_rx_bd_struct_t::length
uint16_t enet_rx_bd_struct_t::control
uint8_t* enet_rx_bd_struct_t::buffer
uint16_t enet_rx_bd_struct_t::controlExtend0
uint16_t enet_rx_bd_struct_t::controlExtend1
uint16_t enet_rx_bd_struct_t::payloadCheckSum
uint8_t enet_rx_bd_struct_t::headerLength
uint8_t enet_rx_bd_struct_t::protocolTyte
uint16_t enet_rx_bd_struct_t::controlExtend2
uint32_t enet_rx_bd_struct_t::timestamp
struct enet_tx_bd_struct_t

Data Fields

uint16_t length
 Buffer descriptor data length. More...
 
uint16_t control
 Buffer descriptor control and status. More...
 
uint8_t * buffer
 Data buffer pointer. More...
 
uint16_t controlExtend0
 Extend buffer descriptor control0. More...
 
uint16_t controlExtend1
 Extend buffer descriptor control1. More...
 
uint16_t controlExtend2
 Extend buffer descriptor control2. More...
 
uint32_t timestamp
 Timestamp. More...
 

Field Documentation

uint16_t enet_tx_bd_struct_t::length
uint16_t enet_tx_bd_struct_t::control
uint8_t* enet_tx_bd_struct_t::buffer
uint16_t enet_tx_bd_struct_t::controlExtend0
uint16_t enet_tx_bd_struct_t::controlExtend1
uint16_t enet_tx_bd_struct_t::controlExtend2
uint32_t enet_tx_bd_struct_t::timestamp
struct enet_data_error_stats_t

Data Fields

uint32_t statsRxLenGreaterErr
 Receive length greater than RCR[MAX_FL]. More...
 
uint32_t statsRxAlignErr
 Receive non-octet alignment/.
 
uint32_t statsRxFcsErr
 Receive CRC error. More...
 
uint32_t statsRxOverRunErr
 Receive over run. More...
 
uint32_t statsRxTruncateErr
 Receive truncate. More...
 
uint32_t statsRxProtocolChecksumErr
 Receive protocol checksum error. More...
 
uint32_t statsRxIpHeadChecksumErr
 Receive IP header checksum error. More...
 
uint32_t statsRxMacErr
 Receive Mac error. More...
 
uint32_t statsRxPhyErr
 Receive PHY error. More...
 
uint32_t statsRxCollisionErr
 Receive collision. More...
 
uint32_t statsTxErr
 The error happen when transmit the frame. More...
 
uint32_t statsTxFrameErr
 The transmit frame is error. More...
 
uint32_t statsTxOverFlowErr
 Transmit overflow. More...
 
uint32_t statsTxLateCollisionErr
 Transmit late collision. More...
 
uint32_t statsTxExcessCollisionErr
 Transmit excess collision. More...
 
uint32_t statsTxUnderFlowErr
 Transmit under flow error. More...
 
uint32_t statsTxTsErr
 Transmit time stamp error. More...
 

Field Documentation

uint32_t enet_data_error_stats_t::statsRxLenGreaterErr
uint32_t enet_data_error_stats_t::statsRxFcsErr
uint32_t enet_data_error_stats_t::statsRxOverRunErr
uint32_t enet_data_error_stats_t::statsRxTruncateErr
uint32_t enet_data_error_stats_t::statsRxProtocolChecksumErr
uint32_t enet_data_error_stats_t::statsRxIpHeadChecksumErr
uint32_t enet_data_error_stats_t::statsRxMacErr
uint32_t enet_data_error_stats_t::statsRxPhyErr
uint32_t enet_data_error_stats_t::statsRxCollisionErr
uint32_t enet_data_error_stats_t::statsTxErr
uint32_t enet_data_error_stats_t::statsTxFrameErr
uint32_t enet_data_error_stats_t::statsTxOverFlowErr
uint32_t enet_data_error_stats_t::statsTxLateCollisionErr
uint32_t enet_data_error_stats_t::statsTxExcessCollisionErr
uint32_t enet_data_error_stats_t::statsTxUnderFlowErr
uint32_t enet_data_error_stats_t::statsTxTsErr
struct enet_buffer_config_t

Note that for the internal DMA requirements, the buffers have a corresponding alignment requirements.

  1. The aligned receive and transmit buffer size must be evenly divisible by ENET_BUFF_ALIGNMENT. when the data buffers are in cacheable region when cache is enabled, all those size should be aligned to the maximum value of "ENET_BUFF_ALIGNMENT" and the cache line size.
  2. The aligned transmit and receive buffer descriptor start address must be at least 64 bit aligned. However, it's recommended to be evenly divisible by ENET_BUFF_ALIGNMENT. buffer descriptors should be put in non-cacheable region when cache is enabled.
  3. The aligned transmit and receive data buffer start address must be evenly divisible by ENET_BUFF_ALIGNMENT. Receive buffers should be continuous with the total size equal to "rxBdNumber * rxBuffSizeAlign". Transmit buffers should be continuous with the total size equal to "txBdNumber * txBuffSizeAlign". when the data buffers are in cacheable region when cache is enabled, all those size should be aligned to the maximum value of "ENET_BUFF_ALIGNMENT" and the cache line size.

Data Fields

uint16_t rxBdNumber
 Receive buffer descriptor number. More...
 
uint16_t txBdNumber
 Transmit buffer descriptor number. More...
 
uint32_t rxBuffSizeAlign
 Aligned receive data buffer size. More...
 
uint32_t txBuffSizeAlign
 Aligned transmit data buffer size. More...
 
volatile enet_rx_bd_struct_t * rxBdStartAddrAlign
 Aligned receive buffer descriptor start address: should be non-cacheable. More...
 
volatile enet_tx_bd_struct_t * txBdStartAddrAlign
 Aligned transmit buffer descriptor start address: should be non-cacheable. More...
 
uint8_t * rxBufferAlign
 Receive data buffer start address. More...
 
uint8_t * txBufferAlign
 Transmit data buffer start address. More...
 

Field Documentation

uint16_t enet_buffer_config_t::rxBdNumber
uint16_t enet_buffer_config_t::txBdNumber
uint32_t enet_buffer_config_t::rxBuffSizeAlign
uint32_t enet_buffer_config_t::txBuffSizeAlign
volatile enet_rx_bd_struct_t* enet_buffer_config_t::rxBdStartAddrAlign
volatile enet_tx_bd_struct_t* enet_buffer_config_t::txBdStartAddrAlign
uint8_t* enet_buffer_config_t::rxBufferAlign
uint8_t* enet_buffer_config_t::txBufferAlign
struct enet_ptp_time_t

Data Fields

uint64_t second
 Second. More...
 
uint32_t nanosecond
 Nanosecond. More...
 

Field Documentation

uint64_t enet_ptp_time_t::second
uint32_t enet_ptp_time_t::nanosecond
struct enet_ptp_time_data_t

Data Fields

uint8_t version
 PTP version. More...
 
uint8_t sourcePortId [kENET_PtpSrcPortIdLen]
 PTP source port ID. More...
 
uint16_t sequenceId
 PTP sequence ID. More...
 
uint8_t messageType
 PTP message type. More...
 
enet_ptp_time_t timeStamp
 PTP timestamp. More...
 

Field Documentation

uint8_t enet_ptp_time_data_t::version
uint8_t enet_ptp_time_data_t::sourcePortId[kENET_PtpSrcPortIdLen]
uint16_t enet_ptp_time_data_t::sequenceId
uint8_t enet_ptp_time_data_t::messageType
enet_ptp_time_t enet_ptp_time_data_t::timeStamp
struct enet_ptp_time_data_ring_t

Data Fields

uint32_t front
 The first index of the ring. More...
 
uint32_t end
 The end index of the ring. More...
 
uint32_t size
 The size of the ring. More...
 
enet_ptp_time_data_t * ptpTsData
 PTP message data structure. More...
 

Field Documentation

uint32_t enet_ptp_time_data_ring_t::front
uint32_t enet_ptp_time_data_ring_t::end
uint32_t enet_ptp_time_data_ring_t::size
enet_ptp_time_data_t* enet_ptp_time_data_ring_t::ptpTsData
struct enet_ptp_config_t

Data Fields

uint8_t ptpTsRxBuffNum
 Receive 1588 timestamp buffer number.
 
uint8_t ptpTsTxBuffNum
 Transmit 1588 timestamp buffer number.
 
enet_ptp_time_data_t * rxPtpTsData
 The start address of 1588 receive timestamp buffers.
 
enet_ptp_time_data_t * txPtpTsData
 The start address of 1588 transmit timestamp buffers.
 
enet_ptp_timer_channel_t channel
 Used for ERRATA_2579: the PTP 1588 timer channel for time interrupt. More...
 
uint32_t ptp1588ClockSrc_Hz
 The clock source of the PTP 1588 timer. More...
 

Field Documentation

enet_ptp_timer_channel_t enet_ptp_config_t::channel
uint32_t enet_ptp_config_t::ptp1588ClockSrc_Hz
struct enet_config_t

Note:

  1. macSpecialConfig is used for a special control configuration, A logical OR of "enet_special_control_flag_t". For a special configuration for MAC, set this parameter to 0.
  2. txWatermark is used for a cut-through operation. It is in steps of 64 bytes: 0/1 - 64 bytes written to TX FIFO before transmission of a frame begins. 2 - 128 bytes written to TX FIFO .... 3 - 192 bytes written to TX FIFO .... The maximum of txWatermark is 0x2F - 4032 bytes written to TX FIFO .... txWatermark allows minimizing the transmit latency to set the txWatermark to 0 or 1 or for larger bus access latency 3 or larger due to contention for the system bus.
  3. rxFifoFullThreshold is similar to the txWatermark for cut-through operation in RX. It is in 64-bit words. The minimum is ENET_FIFO_MIN_RX_FULL and the maximum is 0xFF. If the end of the frame is stored in FIFO and the frame size if smaller than the txWatermark, the frame is still transmitted. The rule is the same for rxFifoFullThreshold in the receive direction.
  4. When "kENET_ControlFlowControlEnable" is set in the macSpecialConfig, ensure that the pauseDuration, rxFifoEmptyThreshold, and rxFifoStatEmptyThreshold are set for flow control enabled case.
  5. When "kENET_ControlStoreAndFwdDisabled" is set in the macSpecialConfig, ensure that the rxFifoFullThreshold and txFifoWatermark are set for store and forward disable.
  6. The rxAccelerConfig and txAccelerConfig default setting with 0 - accelerator are disabled. The "enet_tx_accelerator_t" and "enet_rx_accelerator_t" are recommended to be used to enable the transmit and receive accelerator. After the accelerators are enabled, the store and forward feature should be enabled. As a result, kENET_ControlStoreAndFwdDisabled should not be set.
  7. The intCoalesceCfg can be used in the rx or tx enabled cases to decrese the CPU loading.

Data Fields

uint32_t macSpecialConfig
 Mac special configuration. More...
 
uint32_t interrupt
 Mac interrupt source. More...
 
uint16_t rxMaxFrameLen
 Receive maximum frame length. More...
 
enet_mii_mode_t miiMode
 MII mode. More...
 
enet_mii_speed_t miiSpeed
 MII Speed. More...
 
enet_mii_duplex_t miiDuplex
 MII duplex. More...
 
uint8_t rxAccelerConfig
 Receive accelerator, A logical OR of "enet_rx_accelerator_t". More...
 
uint8_t txAccelerConfig
 Transmit accelerator, A logical OR of "enet_rx_accelerator_t". More...
 
uint16_t pauseDuration
 For flow control enabled case: Pause duration. More...
 
uint8_t rxFifoEmptyThreshold
 For flow control enabled case: when RX FIFO level reaches this value, it makes MAC generate XOFF pause frame. More...
 
uint8_t rxFifoStatEmptyThreshold
 
   For flow control enabled case: number of frames in the receive FIFO,

independent of size, that can be accept. More...

 
uint8_t rxFifoFullThreshold
 
 For store and forward disable case, the data required in RX FIFO to notify

the MAC receive ready status. More...

 
uint8_t txFifoWatermark
 
 For store and forward disable case, the data required in TX FIFO

before a frame transmit start. More...

 
uint8_t ringNum
 Number of used rings. More...
 

Field Documentation

uint32_t enet_config_t::macSpecialConfig

A logical OR of "enet_special_control_flag_t".

uint32_t enet_config_t::interrupt

A logical OR of "enet_interrupt_enable_t".

uint16_t enet_config_t::rxMaxFrameLen
enet_mii_mode_t enet_config_t::miiMode
enet_mii_speed_t enet_config_t::miiSpeed
enet_mii_duplex_t enet_config_t::miiDuplex
uint8_t enet_config_t::rxAccelerConfig
uint8_t enet_config_t::txAccelerConfig
uint16_t enet_config_t::pauseDuration
uint8_t enet_config_t::rxFifoEmptyThreshold
uint8_t enet_config_t::rxFifoStatEmptyThreshold

If the limit is reached, reception continues and a pause frame is triggered.

uint8_t enet_config_t::rxFifoFullThreshold
uint8_t enet_config_t::txFifoWatermark
uint8_t enet_config_t::ringNum

default with 1 – single ring.

struct _enet_handle

Data Fields

volatile enet_rx_bd_struct_t * rxBdBase [FSL_FEATURE_ENET_QUEUE]
 Receive buffer descriptor base address pointer. More...
 
volatile enet_rx_bd_struct_t * rxBdCurrent [FSL_FEATURE_ENET_QUEUE]
 The current available receive buffer descriptor pointer. More...
 
volatile enet_tx_bd_struct_t * txBdBase [FSL_FEATURE_ENET_QUEUE]
 Transmit buffer descriptor base address pointer. More...
 
volatile enet_tx_bd_struct_t * txBdCurrent [FSL_FEATURE_ENET_QUEUE]
 The current available transmit buffer descriptor pointer. More...
 
uint32_t rxBuffSizeAlign [FSL_FEATURE_ENET_QUEUE]
 Receive buffer size alignment. More...
 
uint32_t txBuffSizeAlign [FSL_FEATURE_ENET_QUEUE]
 Transmit buffer size alignment. More...
 
uint8_t ringNum
 Number of used rings. More...
 
enet_callback_t callback
 Callback function. More...
 
void * userData
 Callback function parameter. More...
 
volatile enet_tx_bd_struct_t * txBdDirtyStatic [FSL_FEATURE_ENET_QUEUE]
 The dirty transmit buffer descriptor for error static update. More...
 
volatile enet_tx_bd_struct_t * txBdDirtyTime [FSL_FEATURE_ENET_QUEUE]
 The dirty transmit buffer descriptor for time stamp update. More...
 
uint64_t msTimerSecond
 The second for Master PTP timer . More...
 
enet_ptp_time_data_ring_t rxPtpTsDataRing
 Receive PTP 1588 time stamp data ring buffer. More...
 
enet_ptp_time_data_ring_t txPtpTsDataRing
 Transmit PTP 1588 time stamp data ring buffer. More...
 

Field Documentation

volatile enet_rx_bd_struct_t* enet_handle_t::rxBdBase[FSL_FEATURE_ENET_QUEUE]
volatile enet_rx_bd_struct_t* enet_handle_t::rxBdCurrent[FSL_FEATURE_ENET_QUEUE]
volatile enet_tx_bd_struct_t* enet_handle_t::txBdBase[FSL_FEATURE_ENET_QUEUE]
volatile enet_tx_bd_struct_t* enet_handle_t::txBdCurrent[FSL_FEATURE_ENET_QUEUE]
uint32_t enet_handle_t::rxBuffSizeAlign[FSL_FEATURE_ENET_QUEUE]
uint32_t enet_handle_t::txBuffSizeAlign[FSL_FEATURE_ENET_QUEUE]
uint8_t enet_handle_t::ringNum
enet_callback_t enet_handle_t::callback
void* enet_handle_t::userData
volatile enet_tx_bd_struct_t* enet_handle_t::txBdDirtyStatic[FSL_FEATURE_ENET_QUEUE]
volatile enet_tx_bd_struct_t* enet_handle_t::txBdDirtyTime[FSL_FEATURE_ENET_QUEUE]
uint64_t enet_handle_t::msTimerSecond
enet_ptp_time_data_ring_t enet_handle_t::rxPtpTsDataRing
enet_ptp_time_data_ring_t enet_handle_t::txPtpTsDataRing

Macro Definition Documentation

#define FSL_ENET_DRIVER_VERSION   (MAKE_VERSION(2, 2, 3))

Version 2.2.3.

#define FSL_FEATURE_ENET_QUEUE   1 /* Singal queue for previous IP. */
#define ENET_BUFFDESCRIPTOR_RX_EMPTY_MASK   0x8000U
#define ENET_BUFFDESCRIPTOR_RX_SOFTOWNER1_MASK   0x4000U
#define ENET_BUFFDESCRIPTOR_RX_WRAP_MASK   0x2000U
#define ENET_BUFFDESCRIPTOR_RX_SOFTOWNER2_Mask   0x1000U
#define ENET_BUFFDESCRIPTOR_RX_LAST_MASK   0x0800U
#define ENET_BUFFDESCRIPTOR_RX_MISS_MASK   0x0100U
#define ENET_BUFFDESCRIPTOR_RX_BROADCAST_MASK   0x0080U
#define ENET_BUFFDESCRIPTOR_RX_MULTICAST_MASK   0x0040U
#define ENET_BUFFDESCRIPTOR_RX_LENVLIOLATE_MASK   0x0020U
#define ENET_BUFFDESCRIPTOR_RX_NOOCTET_MASK   0x0010U
#define ENET_BUFFDESCRIPTOR_RX_CRC_MASK   0x0004U
#define ENET_BUFFDESCRIPTOR_RX_OVERRUN_MASK   0x0002U
#define ENET_BUFFDESCRIPTOR_RX_TRUNC_MASK   0x0001U
#define ENET_BUFFDESCRIPTOR_TX_READY_MASK   0x8000U
#define ENET_BUFFDESCRIPTOR_TX_SOFTOWENER1_MASK   0x4000U
#define ENET_BUFFDESCRIPTOR_TX_WRAP_MASK   0x2000U
#define ENET_BUFFDESCRIPTOR_TX_SOFTOWENER2_MASK   0x1000U
#define ENET_BUFFDESCRIPTOR_TX_LAST_MASK   0x0800U
#define ENET_BUFFDESCRIPTOR_TX_TRANMITCRC_MASK   0x0400U
#define ENET_BUFFDESCRIPTOR_RX_IPV4_MASK   0x0001U
#define ENET_BUFFDESCRIPTOR_RX_IPV6_MASK   0x0002U
#define ENET_BUFFDESCRIPTOR_RX_VLAN_MASK   0x0004U
#define ENET_BUFFDESCRIPTOR_RX_PROTOCOLCHECKSUM_MASK   0x0010U
#define ENET_BUFFDESCRIPTOR_RX_IPHEADCHECKSUM_MASK   0x0020U
#define ENET_BUFFDESCRIPTOR_RX_INTERRUPT_MASK   0x0080U
#define ENET_BUFFDESCRIPTOR_RX_UNICAST_MASK   0x0100U
#define ENET_BUFFDESCRIPTOR_RX_COLLISION_MASK   0x0200U
#define ENET_BUFFDESCRIPTOR_RX_PHYERR_MASK   0x0400U
#define ENET_BUFFDESCRIPTOR_RX_MACERR_MASK   0x8000U
#define ENET_BUFFDESCRIPTOR_TX_ERR_MASK   0x8000U
#define ENET_BUFFDESCRIPTOR_TX_UNDERFLOWERR_MASK   0x2000U
#define ENET_BUFFDESCRIPTOR_TX_EXCCOLLISIONERR_MASK   0x1000U
#define ENET_BUFFDESCRIPTOR_TX_FRAMEERR_MASK   0x0800U
#define ENET_BUFFDESCRIPTOR_TX_LATECOLLISIONERR_MASK   0x0400U
#define ENET_BUFFDESCRIPTOR_TX_OVERFLOWERR_MASK   0x0200U
#define ENET_BUFFDESCRIPTOR_TX_TIMESTAMPERR_MASK   0x0100U
#define ENET_BUFFDESCRIPTOR_TX_INTERRUPT_MASK   0x4000U
#define ENET_BUFFDESCRIPTOR_TX_TIMESTAMP_MASK   0x2000U
#define ENET_BUFFDESCRIPTOR_RX_ERR_MASK
Value:
#define ENET_BUFFDESCRIPTOR_RX_LENVLIOLATE_MASK
Length violation mask.
Definition: fsl_enet.h:48
#define ENET_BUFFDESCRIPTOR_RX_TRUNC_MASK
Frame is truncated mask.
Definition: fsl_enet.h:52
#define ENET_BUFFDESCRIPTOR_RX_OVERRUN_MASK
FIFO overrun mask.
Definition: fsl_enet.h:51
#define ENET_BUFFDESCRIPTOR_RX_NOOCTET_MASK
Non-octet aligned frame mask.
Definition: fsl_enet.h:49
#define ENET_BUFFDESCRIPTOR_RX_CRC_MASK
CRC error mask.
Definition: fsl_enet.h:50
#define ENET_FRAME_MAX_FRAMELEN   1518U
#define ENET_FIFO_MIN_RX_FULL   5U
#define ENET_RX_MIN_BUFFERSIZE   256U

Typedef Documentation

typedef void(* enet_callback_t)(ENET_Type *base, enet_handle_t *handle, enet_event_t event, void *userData)

Enumeration Type Documentation

Enumerator
kStatus_ENET_RxFrameError 

A frame received but data error happen.

kStatus_ENET_RxFrameFail 

Failed to receive a frame.

kStatus_ENET_RxFrameEmpty 

No frame arrive.

kStatus_ENET_TxFrameOverLen 

Tx frame over length.

kStatus_ENET_TxFrameBusy 

Tx buffer descriptors are under process.

kStatus_ENET_TxFrameFail 

Transmit frame fail.

kStatus_ENET_PtpTsRingFull 

Timestamp ring full.

kStatus_ENET_PtpTsRingEmpty 

Timestamp ring empty.

Enumerator
kENET_MiiMode 

MII mode for data interface.

kENET_RmiiMode 

RMII mode for data interface.

Notice: "kENET_MiiSpeed1000M" only supported when mii mode is "kENET_RgmiiMode".

Enumerator
kENET_MiiSpeed10M 

Speed 10 Mbps.

kENET_MiiSpeed100M 

Speed 100 Mbps.

Enumerator
kENET_MiiHalfDuplex 

Half duplex mode.

kENET_MiiFullDuplex 

Full duplex mode.

Enumerator
kENET_MiiWriteNoCompliant 

Write frame operation, but not MII-compliant.

kENET_MiiWriteValidFrame 

Write frame operation for a valid MII management frame.

Enumerator
kENET_MiiReadValidFrame 

Read frame operation for a valid MII management frame.

kENET_MiiReadNoCompliant 

Read frame operation, but not MII-compliant.

These control flags are provided for special user requirements. Normally, these control flags are unused for ENET initialization. For special requirements, set the flags to macSpecialConfig in the enet_config_t. The kENET_ControlStoreAndFwdDisable is used to disable the FIFO store and forward. FIFO store and forward means that the FIFO read/send is started when a complete frame is stored in TX/RX FIFO. If this flag is set, configure rxFifoFullThreshold and txFifoWatermark in the enet_config_t.

Enumerator
kENET_ControlFlowControlEnable 

Enable ENET flow control: pause frame.

kENET_ControlRxPayloadCheckEnable 

Enable ENET receive payload length check.

kENET_ControlRxPadRemoveEnable 

Padding is removed from received frames.

kENET_ControlRxBroadCastRejectEnable 

Enable broadcast frame reject.

kENET_ControlMacAddrInsert 

Enable MAC address insert.

kENET_ControlStoreAndFwdDisable 

Enable FIFO store and forward.

kENET_ControlSMIPreambleDisable 

Enable SMI preamble.

kENET_ControlPromiscuousEnable 

Enable promiscuous mode.

kENET_ControlMIILoopEnable 

Enable ENET MII loop back.

kENET_ControlVLANTagEnable 

Enable normal VLAN (single vlan tag).

This enumeration uses one-bot encoding to allow a logical OR of multiple members. Members usually map to interrupt enable bits in one or more peripheral registers.

Enumerator
kENET_BabrInterrupt 

Babbling receive error interrupt source.

kENET_BabtInterrupt 

Babbling transmit error interrupt source.

kENET_GraceStopInterrupt 

Graceful stop complete interrupt source.

kENET_TxFrameInterrupt 

TX FRAME interrupt source.

kENET_TxBufferInterrupt 

TX BUFFER interrupt source.

kENET_RxFrameInterrupt 

RX FRAME interrupt source.

kENET_RxBufferInterrupt 

RX BUFFER interrupt source.

kENET_MiiInterrupt 

MII interrupt source.

kENET_EBusERInterrupt 

Ethernet bus error interrupt source.

kENET_LateCollisionInterrupt 

Late collision interrupt source.

kENET_RetryLimitInterrupt 

Collision Retry Limit interrupt source.

kENET_UnderrunInterrupt 

Transmit FIFO underrun interrupt source.

kENET_PayloadRxInterrupt 

Payload Receive error interrupt source.

kENET_WakeupInterrupt 

WAKEUP interrupt source.

kENET_TsAvailInterrupt 

TS AVAIL interrupt source for PTP.

kENET_TsTimerInterrupt 

TS WRAP interrupt source for PTP.

Enumerator
kENET_RxEvent 

Receive event.

kENET_TxEvent 

Transmit event.

kENET_ErrEvent 

Error event: BABR/BABT/EBERR/LC/RL/UN/PLR .

kENET_WakeUpEvent 

Wake up from sleep mode event.

kENET_TimeStampEvent 

Time stamp event.

kENET_TimeStampAvailEvent 

Time stamp available event.

Enumerator
kENET_TxAccelIsShift16Enabled 

Transmit FIFO shift-16.

kENET_TxAccelIpCheckEnabled 

Insert IP header checksum.

kENET_TxAccelProtoCheckEnabled 

Insert protocol checksum.

Enumerator
kENET_RxAccelPadRemoveEnabled 

Padding removal for short IP frames.

kENET_RxAccelIpCheckEnabled 

Discard with wrong IP header checksum.

kENET_RxAccelProtoCheckEnabled 

Discard with wrong protocol checksum.

kENET_RxAccelMacCheckEnabled 

Discard with Mac layer errors.

kENET_RxAccelisShift16Enabled 

Receive FIFO shift-16.

Enumerator
kENET_PtpEventMsgType 

PTP event message type.

kENET_PtpSrcPortIdLen 

PTP message sequence id length.

kENET_PtpEventPort 

PTP event port number.

kENET_PtpGnrlPort 

PTP general port number.

Enumerator
kENET_PtpTimerChannel1 

IEEE 1588 PTP timer Channel 1.

kENET_PtpTimerChannel2 

IEEE 1588 PTP timer Channel 2.

kENET_PtpTimerChannel3 

IEEE 1588 PTP timer Channel 3.

kENET_PtpTimerChannel4 

IEEE 1588 PTP timer Channel 4.

Enumerator
kENET_PtpChannelDisable 

Disable timer channel.

kENET_PtpChannelRisingCapture 

Input capture on rising edge.

kENET_PtpChannelFallingCapture 

Input capture on falling edge.

kENET_PtpChannelBothCapture 

Input capture on both edges.

kENET_PtpChannelSoftCompare 

Output compare software only.

kENET_PtpChannelToggleCompare 

Toggle output on compare.

kENET_PtpChannelClearCompare 

Clear output on compare.

kENET_PtpChannelSetCompare 

Set output on compare.

kENET_PtpChannelClearCompareSetOverflow 

Clear output on compare, set output on overflow.

kENET_PtpChannelSetCompareClearOverflow 

Set output on compare, clear output on overflow.

kENET_PtpChannelPulseLowonCompare 

Pulse output low on compare for one IEEE 1588 clock cycle.

kENET_PtpChannelPulseHighonCompare 

Pulse output high on compare for one IEEE 1588 clock cycle.

Function Documentation

void ENET_GetDefaultConfig ( enet_config_t *  config)

The purpose of this API is to get the default ENET MAC controller configure structure for ENET_Init(). User may use the initialized structure unchanged in ENET_Init(), or modify some fields of the structure before calling ENET_Init(). Example:

Parameters
configThe ENET mac controller configuration structure pointer.
void ENET_Init ( ENET_Type *  base,
enet_handle_t *  handle,
const enet_config_t *  config,
const enet_buffer_config_t *  bufferConfig,
uint8_t *  macAddr,
uint32_t  srcClock_Hz 
)

This function ungates the module clock and initializes it with the ENET configuration.

Parameters
baseENET peripheral base address.
handleENET handler pointer.
configENET mac configuration structure pointer. The "enet_config_t" type mac configuration return from ENET_GetDefaultConfig can be used directly. It is also possible to verify the Mac configuration using other methods.
bufferConfigENET buffer configuration structure pointer. The buffer configuration should be prepared for ENET Initialization. It is the start address of "ringNum" enet_buffer_config structures. To support added multi-ring features in some soc and compatible with the previous enet driver version. For single ring supported, this bufferConfig is a buffer configure structure pointer, for multi-ring supported and used case, this bufferConfig pointer should be a buffer configure structure array pointer.
macAddrENET mac address of Ethernet device. This MAC address should be provided.
srcClock_HzThe internal module clock source for MII clock.
Note
ENET has two buffer descriptors legacy buffer descriptors and enhanced IEEE 1588 buffer descriptors. The legacy descriptor is used by default. To use the IEEE 1588 feature, use the enhanced IEEE 1588 buffer descriptor by defining "ENET_ENHANCEDBUFFERDESCRIPTOR_MODE" and calling ENET_Ptp1588Configure() to configure the 1588 feature and related buffers after calling ENET_Init().
void ENET_Deinit ( ENET_Type *  base)

This function gates the module clock, clears ENET interrupts, and disables the ENET module.

Parameters
baseENET peripheral base address.
static void ENET_Reset ( ENET_Type *  base)
inlinestatic

This function restores the ENET module to reset state. Note that this function sets all registers to reset state. As a result, the ENET module can't work after calling this function.

Parameters
baseENET peripheral base address.
void ENET_SetMII ( ENET_Type *  base,
enet_mii_speed_t  speed,
enet_mii_duplex_t  duplex 
)

This API is provided to dynamically change the speed and dulpex for MAC.

Parameters
baseENET peripheral base address.
speedThe speed of the RMII mode.
duplexThe duplex of the RMII mode.
void ENET_SetSMI ( ENET_Type *  base,
uint32_t  srcClock_Hz,
bool  isPreambleDisabled 
)
Parameters
baseENET peripheral base address.
srcClock_HzThis is the ENET module clock frequency. Normally it's the system clock. See clock distribution.
isPreambleDisabledThe preamble disable flag.
  • true Enables the preamble.
  • false Disables the preamble.
static bool ENET_GetSMI ( ENET_Type *  base)
inlinestatic

This API is used to get the SMI configuration to check whether the MII management interface has been set.

Parameters
baseENET peripheral base address.
Returns
The SMI setup status true or false.
static uint32_t ENET_ReadSMIData ( ENET_Type *  base)
inlinestatic
Parameters
baseENET peripheral base address.
Returns
The data read from PHY
void ENET_StartSMIRead ( ENET_Type *  base,
uint32_t  phyAddr,
uint32_t  phyReg,
enet_mii_read_t  operation 
)

Used for standard IEEE802.3 MDIO Clause 22 format.

Parameters
baseENET peripheral base address.
phyAddrThe PHY address.
phyRegThe PHY register. Range from 0 ~ 31.
operationThe read operation.
void ENET_StartSMIWrite ( ENET_Type *  base,
uint32_t  phyAddr,
uint32_t  phyReg,
enet_mii_write_t  operation,
uint32_t  data 
)

Used for standard IEEE802.3 MDIO Clause 22 format.

Parameters
baseENET peripheral base address.
phyAddrThe PHY address.
phyRegThe PHY register. Range from 0 ~ 31.
operationThe write operation.
dataThe data written to PHY.
void ENET_SetMacAddr ( ENET_Type *  base,
uint8_t *  macAddr 
)
Parameters
baseENET peripheral base address.
macAddrThe six-byte Mac address pointer. The pointer is allocated by application and input into the API.
void ENET_GetMacAddr ( ENET_Type *  base,
uint8_t *  macAddr 
)
Parameters
baseENET peripheral base address.
macAddrThe six-byte Mac address pointer. The pointer is allocated by application and input into the API.
void ENET_AddMulticastGroup ( ENET_Type *  base,
uint8_t *  address 
)
Parameters
baseENET peripheral base address.
addressThe six-byte multicast group address which is provided by application.
void ENET_LeaveMulticastGroup ( ENET_Type *  base,
uint8_t *  address 
)
Parameters
baseENET peripheral base address.
addressThe six-byte multicast group address which is provided by application.
static void ENET_ActiveRead ( ENET_Type *  base)
inlinestatic

This function is to active the enet read process. It is used for single descriptor ring/queue.

Parameters
baseENET peripheral base address.
Note
This must be called after the MAC configuration and state are ready. It must be called after the ENET_Init() and ENET_Ptp1588Configure(). This should be called when the ENET receive required.
static void ENET_EnableSleepMode ( ENET_Type *  base,
bool  enable 
)
inlinestatic

This function is used to set the MAC enter sleep mode. When entering sleep mode, the magic frame wakeup interrupt should be enabled to wake up MAC from the sleep mode and reset it to normal mode.

Parameters
baseENET peripheral base address.
enableTrue enable sleep mode, false disable sleep mode.
static void ENET_GetAccelFunction ( ENET_Type *  base,
uint32_t *  txAccelOption,
uint32_t *  rxAccelOption 
)
inlinestatic
Parameters
baseENET peripheral base address.
txAccelOptionThe transmit accelerator option. The "enet_tx_accelerator_t" is recommended to be used to as the mask to get the exact the accelerator option.
rxAccelOptionThe receive accelerator option. The "enet_rx_accelerator_t" is recommended to be used to as the mask to get the exact the accelerator option.
static void ENET_EnableInterrupts ( ENET_Type *  base,
uint32_t  mask 
)
inlinestatic

This function enables the ENET interrupt according to the provided mask. The mask is a logical OR of enumeration members. See enet_interrupt_enable_t. For example, to enable the TX frame interrupt and RX frame interrupt, do the following.

Parameters
baseENET peripheral base address.
maskENET interrupts to enable. This is a logical OR of the enumeration :: enet_interrupt_enable_t.
static void ENET_DisableInterrupts ( ENET_Type *  base,
uint32_t  mask 
)
inlinestatic

This function disables the ENET interrupts according to the provided mask. The mask is a logical OR of enumeration members. See enet_interrupt_enable_t. For example, to disable the TX frame interrupt and RX frame interrupt, do the following.

Parameters
baseENET peripheral base address.
maskENET interrupts to disable. This is a logical OR of the enumeration :: enet_interrupt_enable_t.
static uint32_t ENET_GetInterruptStatus ( ENET_Type *  base)
inlinestatic
Parameters
baseENET peripheral base address.
Returns
The event status of the interrupt source. This is the logical OR of members of the enumeration :: enet_interrupt_enable_t.
static void ENET_ClearInterruptStatus ( ENET_Type *  base,
uint32_t  mask 
)
inlinestatic

This function clears enabled ENET interrupts according to the provided mask. The mask is a logical OR of enumeration members. See the enet_interrupt_enable_t. For example, to clear the TX frame interrupt and RX frame interrupt, do the following.

Parameters
baseENET peripheral base address.
maskENET interrupt source to be cleared. This is the logical OR of members of the enumeration :: enet_interrupt_enable_t.
void ENET_SetCallback ( enet_handle_t *  handle,
enet_callback_t  callback,
void *  userData 
)

This API is provided for the application callback required case when ENET interrupt is enabled. This API should be called after calling ENET_Init.

Parameters
handleENET handler pointer. Should be provided by application.
callbackThe ENET callback function.
userDataThe callback function parameter.
void ENET_GetRxErrBeforeReadFrame ( enet_handle_t *  handle,
enet_data_error_stats_t *  eErrorStatic 
)

This API must be called after the ENET_GetRxFrameSize and before the ENET_ReadFrame(). If the ENET_GetRxFrameSize returns kStatus_ENET_RxFrameError, the ENET_GetRxErrBeforeReadFrame can be used to get the exact error statistics. This is an example.

* status = ENET_GetRxFrameSize(&g_handle, &length);
* if (status == kStatus_ENET_RxFrameError)
* {
* // Get the error information of the received frame.
* ENET_GetRxErrBeforeReadFrame(&g_handle, &eErrStatic);
* // update the receive buffer.
* ENET_ReadFrame(EXAMPLE_ENET, &g_handle, NULL, 0);
* }
*
Parameters
handleThe ENET handler structure pointer. This is the same handler pointer used in the ENET_Init.
eErrorStaticThe error statistics structure pointer.
status_t ENET_GetTxErrAfterSendFrame ( enet_handle_t *  handle,
enet_data_error_stats_t *  eErrorStatic 
)

This interface gets the error statistics of the transmit frame. Because the error information is reported by the uDMA after the data delivery, this interface should be called after the data transmit API. It is recommended to call this function on transmit interrupt handler. After calling the ENET_SendFrame, the transmit interrupt notifies the transmit completion.

Parameters
handleThe PTP handler pointer. This is the same handler pointer used in the ENET_Init.
eErrorStaticThe error statistics structure pointer.
Returns
The execute status.
status_t ENET_GetRxFrameSize ( enet_handle_t *  handle,
uint32_t *  length 
)

This function gets a received frame size from the ENET buffer descriptors.

Note
The FCS of the frame is automatically removed by MAC and the size is the length without the FCS. After calling ENET_GetRxFrameSize, ENET_ReadFrame() should be called to update the receive buffers If the result is not "kStatus_ENET_RxFrameEmpty".
Parameters
handleThe ENET handler structure. This is the same handler pointer used in the ENET_Init.
lengthThe length of the valid frame received.
Return values
kStatus_ENET_RxFrameEmptyNo frame received. Should not call ENET_ReadFrame to read frame.
kStatus_ENET_RxFrameErrorData error happens. ENET_ReadFrame should be called with NULL data and NULL length to update the receive buffers.
kStatus_SuccessReceive a frame Successfully then the ENET_ReadFrame should be called with the right data buffer and the captured data length input.
status_t ENET_ReadFrame ( ENET_Type *  base,
enet_handle_t *  handle,
uint8_t *  data,
uint32_t  length 
)

This function reads a frame (both the data and the length) from the ENET buffer descriptors. The ENET_GetRxFrameSize should be used to get the size of the prepared data buffer. This is an example:

* uint32_t length;
* enet_handle_t g_handle;
* //Get the received frame size firstly.
* status = ENET_GetRxFrameSize(&g_handle, &length);
* if (length != 0)
* {
* //Allocate memory here with the size of "length"
* uint8_t *data = memory allocate interface;
* if (!data)
* {
* ENET_ReadFrame(ENET, &g_handle, NULL, 0);
* //Add the console warning log.
* }
* else
* {
* status = ENET_ReadFrame(ENET, &g_handle, data, length);
* //Call stack input API to deliver the data to stack
* }
* }
* else if (status == kStatus_ENET_RxFrameError)
* {
* //Update the received buffer when a error frame is received.
* ENET_ReadFrame(ENET, &g_handle, NULL, 0);
* }
*
Parameters
baseENET peripheral base address.
handleThe ENET handler structure. This is the same handler pointer used in the ENET_Init.
dataThe data buffer provided by user to store the frame which memory size should be at least "length".
lengthThe size of the data buffer which is still the length of the received frame.
Returns
The execute status, successful or failure.
status_t ENET_SendFrame ( ENET_Type *  base,
enet_handle_t *  handle,
const uint8_t *  data,
uint32_t  length 
)
Note
The CRC is automatically appended to the data. Input the data to send without the CRC.
Parameters
baseENET peripheral base address.
handleThe ENET handler pointer. This is the same handler pointer used in the ENET_Init.
dataThe data buffer provided by user to be send.
lengthThe length of the data to be send.
Return values
kStatus_SuccessSend frame succeed.
kStatus_ENET_TxFrameBusyTransmit buffer descriptor is busy under transmission. The transmit busy happens when the data send rate is over the MAC capacity. The waiting mechanism is recommended to be added after each call return with kStatus_ENET_TxFrameBusy.
void ENET_TransmitIRQHandler ( ENET_Type *  base,
enet_handle_t *  handle 
)
Parameters
baseENET peripheral base address.
handleThe ENET handler pointer.
void ENET_ReceiveIRQHandler ( ENET_Type *  base,
enet_handle_t *  handle 
)
Parameters
baseENET peripheral base address.
handleThe ENET handler pointer.
void ENET_ErrorIRQHandler ( ENET_Type *  base,
enet_handle_t *  handle 
)
Parameters
baseENET peripheral base address.
handleThe ENET handler pointer.
void ENET_CommonFrame0IRQHandler ( ENET_Type *  base)

This is used for the combined tx/rx/error interrupt for single/mutli-ring (frame 0).

Parameters
baseENET peripheral base address.
void ENET_Ptp1588Configure ( ENET_Type *  base,
enet_handle_t *  handle,
enet_ptp_config_t *  ptpConfig 
)

The function sets the clock for PTP 1588 timer and enables time stamp interrupts and transmit interrupts for PTP 1588 features. This API should be called when the 1588 feature is enabled or the ENET_ENHANCEDBUFFERDESCRIPTOR_MODE is defined. ENET_Init should be called before calling this API.

Note
The PTP 1588 time-stamp second increase though time-stamp interrupt handler and the transmit time-stamp store is done through transmit interrupt handler. As a result, the TS interrupt and TX interrupt are enabled when you call this API.
Parameters
baseENET peripheral base address.
handleENET handler pointer.
ptpConfigThe ENET PTP1588 configuration.
void ENET_Ptp1588StartTimer ( ENET_Type *  base,
uint32_t  ptpClkSrc 
)

This function is used to initialize the PTP timer. After the PTP starts, the PTP timer starts running.

Parameters
baseENET peripheral base address.
ptpClkSrcThe clock source of the PTP timer.
static void ENET_Ptp1588StopTimer ( ENET_Type *  base)
inlinestatic

This function is used to stops the ENET PTP timer.

Parameters
baseENET peripheral base address.
void ENET_Ptp1588AdjustTimer ( ENET_Type *  base,
uint32_t  corrIncrease,
uint32_t  corrPeriod 
)
Parameters
baseENET peripheral base address.
corrIncreaseThe correction increment value. This value is added every time the correction timer expires. A value less than the PTP timer frequency(1/ptpClkSrc) slows down the timer, a value greater than the 1/ptpClkSrc speeds up the timer.
corrPeriodThe PTP timer correction counter wrap-around value. This defines after how many timer clock the correction counter should be reset and trigger a correction increment on the timer. A value of 0 disables the correction counter and no correction occurs.
static void ENET_Ptp1588SetChannelMode ( ENET_Type *  base,
enet_ptp_timer_channel_t  channel,
enet_ptp_timer_channel_mode_t  mode,
bool  intEnable 
)
inlinestatic
Parameters
baseENET peripheral base address.
channelThe ENET PTP timer channel number.
modeThe PTP timer channel mode, see "enet_ptp_timer_channel_mode_t".
intEnableEnables or disables the interrupt.
static void ENET_Ptp1588SetChannelCmpValue ( ENET_Type *  base,
enet_ptp_timer_channel_t  channel,
uint32_t  cmpValue 
)
inlinestatic
Parameters
baseENET peripheral base address.
channelThe PTP timer channel, see "enet_ptp_timer_channel_t".
cmpValueThe compare value for the compare setting.
static bool ENET_Ptp1588GetChannelStatus ( ENET_Type *  base,
enet_ptp_timer_channel_t  channel 
)
inlinestatic
Parameters
baseENET peripheral base address.
channelThe IEEE 1588 timer channel number.
Returns
True or false, Compare or capture operation status
static void ENET_Ptp1588ClearChannelStatus ( ENET_Type *  base,
enet_ptp_timer_channel_t  channel 
)
inlinestatic
Parameters
baseENET peripheral base address.
channelThe IEEE 1588 timer channel number.
void ENET_Ptp1588GetTimer ( ENET_Type *  base,
enet_handle_t *  handle,
enet_ptp_time_t *  ptpTime 
)
Parameters
baseENET peripheral base address.
handleThe ENET state pointer. This is the same state pointer used in the ENET_Init.
ptpTimeThe PTP timer structure.
void ENET_Ptp1588SetTimer ( ENET_Type *  base,
enet_handle_t *  handle,
enet_ptp_time_t *  ptpTime 
)
Parameters
baseENET peripheral base address.
handleThe ENET state pointer. This is the same state pointer used in the ENET_Init.
ptpTimeThe timer to be set to the PTP timer.
void ENET_Ptp1588TimerIRQHandler ( ENET_Type *  base,
enet_handle_t *  handle 
)
Parameters
baseENET peripheral base address.
handleThe ENET state pointer. This is the same state pointer used in the ENET_Init.
status_t ENET_GetRxFrameTime ( enet_handle_t *  handle,
enet_ptp_time_data_t *  ptpTimeData 
)

This function is used for PTP stack to get the timestamp captured by the ENET driver.

Parameters
handleThe ENET handler pointer.This is the same state pointer used in ENET_Init.
ptpTimeDataThe special PTP timestamp data for search the receive timestamp.
Return values
kStatus_SuccessGet 1588 timestamp success.
kStatus_ENET_PtpTsRingEmpty1588 timestamp ring empty.
kStatus_ENET_PtpTsRingFull1588 timestamp ring full.
status_t ENET_GetTxFrameTime ( enet_handle_t *  handle,
enet_ptp_time_data_t *  ptpTimeData 
)

This function is used for PTP stack to get the timestamp captured by the ENET driver.

Parameters
handleThe ENET handler pointer.This is the same state pointer used in ENET_Init.
ptpTimeDataThe special PTP timestamp data for search the receive timestamp.
Return values
kStatus_SuccessGet 1588 timestamp success.
kStatus_ENET_PtpTsRingEmpty1588 timestamp ring empty.
kStatus_ENET_PtpTsRingFull1588 timestamp ring full.