MCUXpresso SDK API Reference Manual  Rev. 0
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Ltc_driver_aes_with_dpa

Overview

Functions

status_t LTC_AES_EncryptEcbDPA (LTC_Type *base, ltc_dpa_handle_t *handle, const uint8_t *plaintext, uint8_t *ciphertext, size_t size)
 Encrypts AES using the ECB block mode. More...
 
status_t LTC_AES_DecryptEcbDPA (LTC_Type *base, ltc_dpa_handle_t *handle, const uint8_t *ciphertext, uint8_t *plaintext, size_t size)
 Decrypts AES using ECB block mode. More...
 
status_t LTC_AES_EncryptCbcDPA (LTC_Type *base, ltc_dpa_handle_t *handle, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t iv[LTC_DPA_AES_IV_SIZE])
 Encrypts AES using CBC block mode. More...
 
status_t LTC_AES_DecryptCbcDPA (LTC_Type *base, ltc_dpa_handle_t *handle, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t iv[LTC_DPA_AES_IV_SIZE])
 Decrypts AES using CBC block mode. More...
 
status_t LTC_AES_CryptCtrDPA (LTC_Type *base, ltc_dpa_handle_t *handle, const uint8_t *input, uint8_t *output, size_t size, uint8_t counter[LTC_DPA_AES_BLOCK_SIZE], uint8_t counterlast[LTC_DPA_AES_BLOCK_SIZE], size_t *szLeft)
 Encrypts or decrypts AES using CTR block mode. More...
 
status_t LTC_AES_EncryptTagGcmDPA (LTC_Type *base, ltc_dpa_handle_t *handle, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, uint8_t *tag, size_t tagSize)
 Encrypts AES and tags using GCM block mode. More...
 
status_t LTC_AES_DecryptTagGcmDPA (LTC_Type *base, ltc_dpa_handle_t *handle, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, const uint8_t *tag, size_t tagSize)
 Decrypts AES and authenticates using GCM block mode. More...
 
status_t LTC_AES_EncryptTagCcmDPA (LTC_Type *base, ltc_dpa_handle_t *handle, const uint8_t *plaintext, uint8_t *ciphertext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, uint8_t *tag, size_t tagSize)
 Encrypts AES and tags using CCM block mode. More...
 
status_t LTC_AES_DecryptTagCcmDPA (LTC_Type *base, ltc_dpa_handle_t *handle, const uint8_t *ciphertext, uint8_t *plaintext, size_t size, const uint8_t *iv, size_t ivSize, const uint8_t *aad, size_t aadSize, const uint8_t *tag, size_t tagSize)
 Decrypts AES and authenticates using CCM block mode. More...
 

Function Documentation

status_t LTC_AES_EncryptEcbDPA ( LTC_Type *  base,
ltc_dpa_handle_t *  handle,
const uint8_t *  plaintext,
uint8_t *  ciphertext,
size_t  size 
)

Encrypts AES using the ECB block mode.

Parameters
baseLTC peripheral base address
handlepointer to ltc_dpa_handle_t structure which stores the transaction state.
plaintextInput plain text to encrypt
[out]ciphertextOutput cipher text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
Returns
Status from encrypt operation
status_t LTC_AES_DecryptEcbDPA ( LTC_Type *  base,
ltc_dpa_handle_t *  handle,
const uint8_t *  ciphertext,
uint8_t *  plaintext,
size_t  size 
)

Decrypts AES using ECB block mode.

Parameters
baseLTC peripheral base address
handlepointer to ltc_dpa_handle_t structure which stores the transaction state.
ciphertextInput cipher text to decrypt
[out]plaintextOutput plain text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
Returns
Status from decrypt operation
status_t LTC_AES_EncryptCbcDPA ( LTC_Type *  base,
ltc_dpa_handle_t *  handle,
const uint8_t *  plaintext,
uint8_t *  ciphertext,
size_t  size,
const uint8_t  iv[LTC_DPA_AES_IV_SIZE] 
)
Parameters
baseLTC peripheral base address
handlepointer to ltc_dpa_handle_t structure which stores the transaction state.
plaintextInput plain text to encrypt
[out]ciphertextOutput cipher text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
ivInput initial vector to combine with the first input block.
Returns
Status from encrypt operation
status_t LTC_AES_DecryptCbcDPA ( LTC_Type *  base,
ltc_dpa_handle_t *  handle,
const uint8_t *  ciphertext,
uint8_t *  plaintext,
size_t  size,
const uint8_t  iv[LTC_DPA_AES_IV_SIZE] 
)
Parameters
baseLTC peripheral base address
handlepointer to ltc_dpa_handle_t structure which stores the transaction state.
ciphertextInput cipher text to decrypt
[out]plaintextOutput plain text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
ivInput initial vector to combine with the first input block.
keyInput key to use for decryption
Returns
Status from decrypt operation
status_t LTC_AES_CryptCtrDPA ( LTC_Type *  base,
ltc_dpa_handle_t *  handle,
const uint8_t *  input,
uint8_t *  output,
size_t  size,
uint8_t  counter[LTC_DPA_AES_BLOCK_SIZE],
uint8_t  counterlast[LTC_DPA_AES_BLOCK_SIZE],
size_t *  szLeft 
)

Encrypts or decrypts AES using CTR block mode. AES CTR mode uses only forward AES cipher and same algorithm for encryption and decryption. The only difference between encryption and decryption is that, for encryption, the input argument is plain text and the output argument is cipher text. For decryption, the input argument is cipher text and the output argument is plain text.

Parameters
baseLTC peripheral base address
handlepointer to ltc_dpa_handle_t structure which stores the transaction state.
inputInput data for CTR block mode
[out]outputOutput data for CTR block mode
sizeSize of input and output data in bytes
[in,out]counterInput counter (updates on return)
[out]counterlastOutput cipher of last counter, for chained CTR calls. NULL can be passed if chained calls are not used.
[out]szLeftOutput number of bytes in left unused in counterlast block. NULL can be passed if chained calls are not used.
Returns
Status from encrypt operation
status_t LTC_AES_EncryptTagGcmDPA ( LTC_Type *  base,
ltc_dpa_handle_t *  handle,
const uint8_t *  plaintext,
uint8_t *  ciphertext,
size_t  size,
const uint8_t *  iv,
size_t  ivSize,
const uint8_t *  aad,
size_t  aadSize,
uint8_t *  tag,
size_t  tagSize 
)

Encrypts AES and optionally tags using GCM block mode. If plaintext is NULL, only the GHASH is calculated and output in the 'tag' field.

Parameters
baseLTC peripheral base address
handlepointer to ltc_dpa_handle_t structure which stores the transaction state.
plaintextInput plain text to encrypt
[out]ciphertextOutput cipher text.
sizeSize of input and output data in bytes
ivInput initial vector
ivSizeSize of the IV
aadInput additional authentication data
aadSizeInput size in bytes of AAD
[out]tagOutput hash tag. Set to NULL to skip tag processing.
tagSizeInput size of the tag to generate, in bytes. Must be 4,8,12,13,14,15 or 16.
Returns
Status from encrypt operation
status_t LTC_AES_DecryptTagGcmDPA ( LTC_Type *  base,
ltc_dpa_handle_t *  handle,
const uint8_t *  ciphertext,
uint8_t *  plaintext,
size_t  size,
const uint8_t *  iv,
size_t  ivSize,
const uint8_t *  aad,
size_t  aadSize,
const uint8_t *  tag,
size_t  tagSize 
)

Decrypts AES and optionally authenticates using GCM block mode. If ciphertext is NULL, only the GHASH is calculated and compared with the received GHASH in 'tag' field.

Parameters
baseLTC peripheral base address
handlepointer to ltc_dpa_handle_t structure which stores the transaction state.
ciphertextInput cipher text to decrypt
[out]plaintextOutput plain text.
sizeSize of input and output data in bytes
ivInput initial vector
ivSizeSize of the IV
aadInput additional authentication data
aadSizeInput size in bytes of AAD
tagInput hash tag to compare. Set to NULL to skip tag processing.
tagSizeInput size of the tag, in bytes. Must be 4, 8, 12, 13, 14, 15, or 16.
Returns
Status from decrypt operation
status_t LTC_AES_EncryptTagCcmDPA ( LTC_Type *  base,
ltc_dpa_handle_t *  handle,
const uint8_t *  plaintext,
uint8_t *  ciphertext,
size_t  size,
const uint8_t *  iv,
size_t  ivSize,
const uint8_t *  aad,
size_t  aadSize,
uint8_t *  tag,
size_t  tagSize 
)

Encrypts AES and optionally tags using CCM block mode.

Parameters
baseLTC peripheral base address
handlepointer to ltc_dpa_handle_t structure which stores the transaction state.
plaintextInput plain text to encrypt
[out]ciphertextOutput cipher text.
sizeSize of input and output data in bytes. Zero means authentication only.
ivNonce
ivSizeLength of the Nonce in bytes. Must be 7, 8, 9, 10, 11, 12, or 13.
aadInput additional authentication data. Can be NULL if aadSize is zero.
aadSizeInput size in bytes of AAD. Zero means data mode only (authentication skipped).
[out]tagGenerated output tag. Set to NULL to skip tag processing.
tagSizeInput size of the tag to generate, in bytes. Must be 4, 6, 8, 10, 12, 14, or 16.
Returns
Status from encrypt operation
status_t LTC_AES_DecryptTagCcmDPA ( LTC_Type *  base,
ltc_dpa_handle_t *  handle,
const uint8_t *  ciphertext,
uint8_t *  plaintext,
size_t  size,
const uint8_t *  iv,
size_t  ivSize,
const uint8_t *  aad,
size_t  aadSize,
const uint8_t *  tag,
size_t  tagSize 
)

Decrypts AES and optionally authenticates using CCM block mode.

Parameters
baseLTC peripheral base address
handlepointer to ltc_dpa_handle_t structure which stores the transaction state.
ciphertextInput cipher text to decrypt
[out]plaintextOutput plain text.
sizeSize of input and output data in bytes. Zero means authentication only.
ivNonce
ivSizeLength of the Nonce in bytes. Must be 7, 8, 9, 10, 11, 12, or 13.
aadInput additional authentication data. Can be NULL if aadSize is zero.
aadSizeInput size in bytes of AAD. Zero means data mode only (authentication skipped).
tagReceived tag. Set to NULL to skip tag processing.
tagSizeInput size of the received tag to compare with the computed tag, in bytes. Must be 4, 6, 8, 10, 12, 14, or 16.
Returns
Status from decrypt operation