MCX Lab Heart Rate Demo

Objectives

In this lab, you will learn:

  • How to use Application Code Hub to import an example into the VS Code workspace

  • How to build, clean, debug, and run the example

  • How to connect the Serial Monitor for UART console

  • How FreeMASTER can be used as a real-time debug monitor and data visualization tool

Heart Rate Monitor Lab

The NXP Application Code Hub provides a complete example of how to use the MCXA-153 microcontroller in a Heart Rate and SPO2 monitor application. This lab will walk through the steps to import, build, program and debug the example. The final section of the lab shows how to use FreeMASTER as a data-visualization tool for the acquired sensor data from the FRDM-MCXA153 evaluation board.

1. Verify Installation

The prework instructions should be completed before starting this lab. The instructions walk through the installation for the required software.
After finishing, the system should have the following:

  • Visual Studio Code - Base software tool distributed by Microsoft

  • MCUXpresso for Visual Studio Code Extension - NXP developed extension to configure VS Code for embedded MCU development

  • MCXUXpresso Installer - required to install 3rd party tools for MCUXpresso projects to correctly import/build/debug.

  • FRDM-MCXA153 SDK 2.14.0 - required to provide software libraries for middleware and drivers referenced in the example

  • Link to Installation and Preparation

2. Import Project with Application Code Hub

The Application Code Hub (ACH) repository enables engineers to easily find microcontroller software examples, code snippets, application software packs and demos developed by NXP in-house experts. This space provides a quick, easy and consistent way to find microcontroller applications. Find more information at www.nxp.com/ach

The MCUXpresso for VS Code extension has integrated the Application Code Hub into the development environment. The extension provides an Import Wizard to simplify adding examples from the Application Code Hub. The wizard handles the steps required to clone the selected project repository.

Note: The Application Code Hub examples are delivered from GitHub at www.github.com/nxp-appcodehub The integrated viewer makes it easier for customers to explore. Alternatively, customers can manually add the projects using traditional methods to clone GitHub repositories and importing the local project folder.

Here are the steps to import a new Example from the Application Code Hub:

  1. Go to the Quick Start Panel

  2. Select Application Code Hub

    ACH Quickstart Panel

  3. Filter Visible Examples (MCX + Sensors)
    Go to the filter section next to the Search bar and select two filters.
    MCX in the Device Families Section and Sensor in the Categories section of the filters.

  4. Search for Keywords in Examples
    Search for the keyword ‘heart rate’.
    Select the demo “frdm mcxa153 freemaster heart rate”.

    ACH Filter Values

  5. Read Overview of Heart Rate Demo
    The Application Code Hub provides a consistent Readme Overview for every project. The FreeMASTER Heart Rate demo overview is previewed after clicking on the application card.
    Scroll through the readme to become familiar with the available contents like required hardware, software and setup instructions.

    ACH Readme File

  6. Select Destination for Project
    The wizard automatically provides a prompt to browse to a desired destination folder. Choose the Folder C:\VS-Code-Projects\Heart-Rate.

  7. Import Project into Workspace
    Select Import Project(s) after entering the desired location.
    If a valid project is not available, the wizard only displays Import Repository, to allow a code repo, without a project, to be added to workspace.

    ACH Import HRM Example

  8. Select Detected Project(s)
    The import wizard will scan the example repo and list valid projects that were discovered. This allows the user to select only the projects they want created. Select the mcuxpresso project listed at the top of the VS Code window below the Workspace Search bar.
    ACH Select Project(s)

  9. Choose a Toolchain
    The last selection is to identify the Compiler toolchain to be used for the project. GCC will be used for this project.
    Select Arm GNU Toolchain 12.3.Rel1 (Or latest version available from MCUXpresso Installer prework) The scan may locate Compilers associated with MCUXpresso IDE. Verify the path and version between listed compilers. ACH Choose a Toolchain

At this time the wizard completes importing the project into the workspace.
A Successful Conversion notification is displayed at the bottom of the screen. It is important to recognize that the selected Heart Rate example is a working project within the MCUXpresso IDE (Eclipse based). The VS Code extension has a ability to convert an existing project with a few requirements.
ACH Succesful Convert

4. Build the application

The MCXA153 FreeMASTER Heart Rate project needs to build the application image. After the code builds without any errors, the application can be run on the FRDM board.

The following steps require that you return to the MCUXpresso perspective by clicking the MCUXpresso for VS Code X icon in the left navigation pane.

  1. Build the project by clicking the Build Selected icon.

    Build project

    After a successful build, the Terminal console displays the memory usage (or compiler errors if any).

    Build output

5. Connect Serial Monitor to the board

To use the Serial Monitor integrated into VS Code:

  1. Connect the USB-C cable to J15 to power the FRDM board. The onboard debugger provides a USB-UART bridge to interface with the Serial monitor.

  2. Click on the Serial Monitor found as a tab in the Terminal window at the Bottom of VS Code Window.

    Note: The default COM settings are valid for NXP eval boards: “115200, None…”

  3. Click Start Monitoring to connect the monitor to the FRDM board’s auto-detected COM port.

    It can be disconnected by clicking Stop Monitoring after debug.

    Serial Monitor

6. Flash/Debug the Application

This section uses the on-board debugger to connect to the MCU, and program the flash. LinkServer from NXP manages the GDB server for communicating with the NXP MCULink on-board debug probe. It includes support for flash programming.

  1. Click the play icon to Debug the application:

    Debug project
    The application is flashed to the FRDM board and VS Code switches to the Debug perspective.
    Return to the Serial Monitor tab under the Terminals. It switches to the OUTPUT terminal when a Debug session is started.

  2. The execution will be paused.
    Click Continue/Play icon to continue execution.
    The application will advance to the start of main().
    Click Continue/Play icon a 2nd time for the Heart Rate application to launch inside main().
    Continue debugging

  3. View Heart Rate Values in Serial Terminal The Heart Rate application using the serial port to display information.

  • The following should be displayed in the Serial Monitor tab after main() starts:

    sensor_init
    init complete
    
  • Place a finger on the sensor near the Heart silkscreened on Heart Rate 4 click board. The following should be displayed in the Serial Monitor tab after a finger is placed on the sensor:

    g_sample_count:0, hr:0 ecg:104, blood:0:
    g_sample_count:0, hr:0 ecg:106, blood:0:
    g_sample_count:0, hr:0 ecg:127, blood:0:
    
  • A heart rate value will be calculated and displayed after g_sample_count reaches 250 valid samples:

    g_sample_count:249, hr:0 ecg:104, blood:81:
    g_sample_count:250, hr:72 ecg:86, blood:81:
    g_sample_count:251, hr:72 ecg:68, blood:81:
    

7. FreeMASTER Data Visualization

FreeMASTER is a standalone application provided by NXP to help developers visualize, monitor and manipulate data available from their projects.
The Heart Rate example includes a /freemaster folder that helps users get started using the tool.
The settings in the Application Code Hub were established for an MCUXpresso IDE based project. There are a few changes that need to be made after the project is converted to a VS Code project.
The following steps will properly configure FreeMASTER to work with the Heart Rate example project:

  1. Launch FreeMASTER Application
    There are two options for launching FreeMASTER.

    • Click on the heart_rate.pmpx using File Explorer. The FreeMASTER application should be associated with .pmpx file extensions. This will also automatically load the included project settings. (Folder location may vary based on choices made in Section 2)
      ACH FreeMASTER File Explorer

    • Launch FreeMASTER by searching Windows Applications.
      ACH FreeMASTER File Explorer
      This will not load project settings. You will be required to Open Project using the FreeMaster menu as shown. Open the .pmpx project file located in the location chosen in Section 2)
      ACH FreeMASTER Open Project

  2. Verify Project Options
    FreeMASTER has a few key settings to verify once a project is opened. A user should verify they are correctly set for the type of Debug Probe and location of the project output files.

    1. Click Project -> Options from the menu bar.
      ACH FreeMASTER Project Open

    2. Verify that the correct method is set for communicating with the board. The on-board Debug Probe for the FRDM-MCXA153 is by default shipped with NXP CMSIS-DAP firmware.
      Select FreeMASTER CMSIS-DAP Communication Plug-in found under the Comm tab, for Plug-in module:
      ACH FreeMASTER COMM Options

      Note: SEGGER and PEMicro options are available for alternate debug probes or on-board firmware)

    3. Verify that the correct Default symbol file is targeted for the VS Code project. The symbol file in VS Code projects is output under an /armgcc folder.
      Select the /armgcc folder within VS Code project MAP Files tab
      The window will autodetect the Binary ELF File, and display this under File format:.
      ACH FreeMASTER Project Open

  3. Visualize Data From Heart Rate Project
    The NXP software team has included a default visualization for the Heart Rate project. The demonstration showcases the different styles for project data to be shown.
    The following visualization settings are preset for the Heart Rate project:

  • Welcome HTML Page: The HTML Pages (Under Options) points to welcome.html file. This provides structured web view for displaying elements. Beyond scope of this lab, but .html file can be reviewed to see how target values/charts are referenced in html.

  • Oscilloscope Visual: View plots the values of a project variable. The plot axis are configured for scale and color. Heart Rate, SPO2 and ECG are configured.

  • Variable Watch Table: After variables are configured to be tracked, they can be added to this table view.
    Click GO icon on the menu bar to initiate the project data visualization! The following points are highlighted for the FreeMASTER output.

    1. Clicking on the elements listed under the Project Tree changes the view to the specific Oscilloscope Visual.

    2. View the captured values for the variables in a Table view

    3. Visualization of data organized based on the layout defined in the Welcome.html

    ACH FreeMASTER Project Open

  1. Customize FreeMASTER for Application Variable
    The FreeMASTER tool makes it easy for users to add new values to the visualization. The following steps will add the ability to see the value of the IR detected by the shield sensor. The on-board IR sensor detects the amount of IR light reflected back into the small opening of the black casing. The reflection works best when object is within 1” of the sensor. This is NOT a long range IR detector.

    1. Select new variable from List of all valid symbol files, found under Project->Options
      FreeMASTER List of Valid Symbol Files
      Click on View to open a list of available variables:
      FreeMASTER ELF Variables

    2. Add selected Variable to the FreeMASTER project
      Use values located in the symbol file to configure the parameters for a New “IR Value” variable in the project.
      Click Project->Variables from the menu bar to add a New variable
      FreeMASTER Add Variable

      Note: You can also us VS Code Explorer to search and review the variable details in the project source files.

    3. Add Oscilloscope Visual for new Variable The New “IR Value” variable can be displayed by adding an Oscilloscope to the Project Tree
      Under the Variables tab, add IR Value to the Graph Block
      FreeMASTER Oscilloscope

    4. Restart the capture of application data with new Visualization
      Click Go again to have the new variable data populated in the new Visualization.
      FreeMASTER Visualize IR


You have now succesfully completed the MCXA FreeMASTER Heart Rate Lab.
Return to Getting Started with MCX using Application Code Hub