Zephyr Lab MCXN947 Debug

Objectives

In this lab, you will learn:

  • How to build and debug a Zephyr application in VS Code

  • How to use various debugging tools and controls

  • How to enable Zephyr thread awareness using Kconfig symbols

  • How to view thread details in the debugger

  • How to enable and use the Peripherals view

Debug Lab

In this lab, we will go through detailed steps to run the Zephyr Synchronization sample application. The Debug lab includes steps to build/debug the application and details on debug tools/controls in VS Code. It also includes steps to enable thread awareness by setting up Kconfig symbols for the application example. We will take a closer look at key features like Thread status, Stack usage, Call Stack, Thread structure, and more.

1. Import Synchronization application example

Follow the steps to import the example, similar to the steps in the Zephyr Lab MCXN947 Hello World.

  1. To import the synchronization application from the Zephyr Repository, click Import Example from Repository in the Quickstart Panel.

    Import Example

  2. Select the following board settings to import the example:

    • For the board, you can type n947 to filter the board target frdm_mcxn947/mcxn947/cpu0. Be sure this board target ends with cpu0.

    • For the example template, type sync to filter the app zephyr/samples/synchronization

    • For Application type, select Repository Application

    • Click Import

      Import Synchronization

2. Enable thread awareness and build the example

To enable thread awareness for debugging, we need to add specific Kconfig symbols to the application example. These steps will modify the prj.conf file and verify the generated .config file, similar to the Zephyr Lab MCXN947 Kconfig guide.

  1. Add the following Kconfig symbols to the prj.conf file and save the file (Ctrl+S):

    CONFIG_DEBUG_THREAD_INFO=y
    CONFIG_INIT_STACKS=y
    CONFIG_THREAD_STACK_INFO=y
    

    CONFIG Values

  2. Build the project by clicking the Build Selected icon.

    Build Selected

    After the build, the Terminal window displays the memory usage (or compiler errors if any).

3. Exploring Debug Tools and Controls

After building the application and enabling thread awareness, let’s explore the debug tools and controls in the Run and Debug view.

  1. If not already connected to the board, connect the USB Type-C cable to J17, to power and debug the board. Connect the Serial monitor to the board’s COM port and click Start Monitoring.

    Serical Monitor

  2. Click the play icon to Debug the Synchronization application.

    Debug Project

  3. Download the SVD file. A pop-up appears in the lower right corner. This lab uses this file to view the hardware peripheral registers while debugging. The SVD file contains the list of peripheral registers and their bitfields for the debugger. Click the Download button to save the SVD file in your project.

    Download SVD

  4. The following debug tools/controls are enabled in the Run and Debug view:

    1. Debug controls: Resume/Pause, Step over, Step into, Restart, Stop

    2. Variables: Locals and Registers

    3. Watch: Add expressions to monitor

    4. Call Stack: List of active subroutines in the program

    5. Breakpoints: Add, toggle, and view breakpoints in the code

      Debug Perspective

  5. To continue with the debug execution click Resume. The application prints hello world (both threads) in the Serial Monitor view.

    Serial Monitor Output

4. Debugging with Thread awareness – RTOS Details

The synchronization application has two threads (threadA and threadB) taking turns printing a message to the console. The example uses semaphores to synchronize the two tasks.

  1. While the debug session is active, go to the Run and Debug view, and open the source file with the main() subroutine in the editor.

    Add a breakpoint by double-clicking on the left side of line 48. A red dot next to the line and an entry in the Breakpoints window confirms the addition of the breakpoint.

    Add Breakpoint

  2. The debug session will halt at the helloLoop(), and the debug controls can be used to resume or step through the code. The synchronization application will print to the terminal after clicking Resume a couple of times.

    When the debugger halts at the breakpoint, the application threads and details are displayed in the RTOS Details view. Click the RTOS Details tab to see the thread details. These details include the status of each thread along with its priorities, stack pointer, and stack usage.

    Pause the debug session to notice the changes in the status of each thread.

    RTOS Details

  3. Along with the RTOS Details view, the Call Stack window provides more information about the threads in the application:

    • Running thread:

      Running Thread

    • Pending thread:

      Pending Thread

    • Idle Thread:

      Idle Thread

  4. The Watch window and the Variables window can be used to add local variables and CPU registers that need to be monitored.

    Watch and Variables

  5. The Peripherals View will be added to the Run And Debug view when the SVD file is downloaded.

    Peripherals View

    Registers and bitfields can be viewed for the different peripherals (eg. LPUART4).

    Peripherals View LPUART4

5. Clean up after lab

This lab is completed. But the following steps will clean up the VS Code workspace:

  1. Click Stop to end the debug session.

    Stop Debugger

  2. Close all Editor tabs. Right-Click on a tab, and select Close All.

  3. If this is the last lab and you are done using the board, you should disconnect the Serial Monitor. Find the Serial Monitor view, and click Stop Monitoring.

    Stop Serial Monitor

Additional Resources

VS Code Debugging Peripherals View RTOS Details View


Lab completed. Return to the MCXN947 Zephyr Labs Overview Training Zephyr Getting Started MCXN947