This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

Build an example application

To build an example application, perform the following steps.

  1. Drag and drop the SDK zip file into the Installed SDKs view to install an SDK.

    In the window that appears, click OKand wait until the import has finished.

  2. On the Quickstart Panel, click Import SDK example(s).

  3. In the window that appears, select mimxrt700evk or kits and click Next.

  4. Expand the demo_apps folder and select hello_world_demo_cm33_core0. Then, click Next.

  5. Click Finish.

Parent topic:Run a demo using MCUXpresso IDE