This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

epdc

Overview

This example shows how to use the PXP to process pixels, apply waveform mode then use the EPDC to drive the E-INK panel.

In this example, first an image of RGB888 pixel format is processed by PXP to generate Y4 pixel data. Then PXP waveform engine will apply the waveform mode 2 to the pixel data for EPDC to update high quality image to the screen. The same image is updated to screen 4 times on different locations. Collision shall occur and non-collided update(s) will appear on screen together within one fresh, the collided update(s) will wait until the previous update(s) to finish then refresh. Next the panel is cleared and PXP waveform engine will constantly apply the waveform mode 1 to black dot for EPDC to draw line on panel to simulate pen input. The update shall be non-flashy and quicker than image update.

Supported Boards