This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

led_blinky_peripheral

Overview

The LED Blinky demo application provides a sanity check for the new SDK build environments and board bring up. The LED Blinky demo uses the systick interrupt to realize the function of timing delay. The example takes turns to shine the LED. The purpose of this demo is to provide a simple project for debugging and further development. The code of this demo has been prepared and updated for use with the MCUXpresso Configuration Tools (Pins/Clocks/Peripherals).

Supported Boards