erpc_server_matrix_multiply_spi
Overview
This example demonstrates usage of eRPC between two boards using SPI transport layer. One board acts like a server and the second as client. When client starts, it generates two random matrixes and sends them to server. Server then performs matrix multiplication and sends result data back to client. Client then prints the result matrix.
Optional HW setup is to use the PC as the eRPC client and the board as the eRPC server. In this case the LIBUSBSIOSPITransport (Python) is used on the PC side and the SPI slave transport on the board side. The libusbsio Python module is used for accessing the NXP libusbsio APIs and thus allowing to exercise SPI, I2C bus and GPIO pins from Python application (over USBSIO interface of NXP LPCLink2 and MCUlink Pro devices). This configuration is supported for selected boards only. Note, that when more than one board with LPCLink2/MCUlink devices is connected to the PC the Python application is not able to automatically detect which one to use to establish the communication. Thus, please ensure only one board with running eRPC server application is connected to the PC when starting the Python application on the PC side or use the -d command line argument of the Python application to specify the targetted LPCLink2/MCUlink device index.
eRPC documentation
eRPC specific files are stored in: middleware\multicore\erpc eRPC documentation is stored in: middleware\multicore\erpc\doc eRPC is open-source project stored on github: https://github.com/EmbeddedRPC/erpc eRPC documentation can be also found in: http://embeddedrpc.github.io
PC Side Setup (Optional for PC-to-board communication)
Make sure you have Python installed on your PC
Install serial module by executing following command in command line: “python -m pip install pyserial”
Install eRPC module to Python by executing setup.py located in: middleware\multicore\erpc\erpc_python - “python setup.py install”
Install libusbsio module to Python by executing following command in command line: “python -m pip install libusbsio”
usage: run_spi.py [-h] [-b BD] [-g CS_PORT] [-p CS_PIN] [-d DEVIDX]
eRPC Matrix Multiply example
optional arguments: -h, –help show this help message and exit -b BD, –bd BD Baud rate (default value is 500000) -g CS_PORT, –csport CS_PORT Chip select GPIO port number (see the board schematics) -p CS_PIN, –cspin CS_PIN Chip select GPIO pin number (see the board schematics) -d DEVIDX, –devidx DEVIDX LIBUSBSIO device index (default value is 0 - only one board connected to the host PC)
Example: To run PC side as a client with a board connected as a server: “run_spi.py –bd 500000 –csport 0 –cspin 15”