This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

digital_key_car_anchor

Overview

The Digital Key Car Anchor application implements one of the multiple Bluetooth Low Energy anchors that can reside inside a vehicle as part of the Car Connectivity Consortium (CCC) Digital Key Release 3 secure car access specification. The anchor performs a dual role. Inside the CCC Digital Key scope, it is a Bluetooth Low Energy peripheral. This peripheral can perform both Legacy (1M PHY) and Extended Long Range (500kbps Coded PHY) advertising depending on the scenario. It can also perform searching for a CCC Digital Key-enabled device such as a smartphone. Simultaneously, it can also act as a Bluetooth Low Energy Central, scanning for non-CCC key fobs. There can be multiple anchors inside a car. The anchors must act as a single device and share information between them such as addresses, bonding data, or application-specific keys. The information must be shared such that a smartphone can connect to any one of the anchors, depending on positioning and not detect any difference.

Supported Boards

  • KW45B41Z-EVK

  • KW47-EVK