hid_host
Overview
The HID Host application implements a GATT client or server for the following profile and service:
HID over GATT Profile v1.0
Battery Service v1.0
Device Information Service v1.1
The application behaves as a GAP central node. It enters the GAP Limited Discovery Procedure and searches for HID devices to connect to. After connecting with the peripheral, it configures notifications and displays the received HID reports on a terminal connected to the UART port. The application uses pairing with bonding by default. When connected with the HID Device application, it sends the 999999 passcode to the host stack by default.
Supported Boards
KW47-EVK
FRDM-MCXW71
K32W148-EVK
MCX-W72-EVK
KW45B41Z-EVK