Build an example application

To build an example application, follow these steps.

  1. Open a GCC Arm Embedded tool chain command window. To launch the window, from the Windows operating system Start menu, go to Programs >GNU Tools Arm Embedded <version> and select GCC Command Prompt.

    |

|

  1. Change the directory to the example application project directory which has a path similar to the following:

    <install_dir>/boards/<board_name>/<example_type>/<application_name>/armgcc
    

    For this example, the exact path is:

    <install_dir>/examples/evkbmimxrt1060/demo_apps/hello_world/armgcc
    

    Note: To change directories, use the cd command.

  2. Type build_debug.bat on the command line or double click on build_debug.bat file in Windows Explorer to build it. The output is as shown in Figure 2.

    |

|

Parent topic:Run a demo using Arm GCC