How to add or remove boot header for XIP targets
The MCUXpresso SDK for i.MX RT1160 provides flexspi_nor_debug
and flexspi_nor_release
targets for each example and/or demo which supports XIP (eXecute-In-Place). These two targets add XIP_BOOT_HEADER
to the image by default. Because of this, ROM can boot and run this image directly on external flash.
Macros for the boot leader:
The following three macros are added in
flexspi_nor
targets to support XIP, as described in Table 1.^
|XIP_EXTERNAL_FLASH|1: Exclude the code which changes the clock of FLEXSPI.| |0: Make no changes.| |XIP_BOOT_HEADER_ENABLE|1: Add FLEXSPI configuration block, image vector table, boot data, and device configuration data (optional) to the image by default.| |0: Add nothing to the image by default.| |XIP_BOOT_HEADER_DCD_ENABLE|1: Add device configuration data to the image.| |0: Do NOT add device configuration data to the image.|
Table 2 shows the different effect on the built image with a different combination of these macros.
^
XIP_BOOT_HEADER_DCD_ENABLE=1
XIP_BOOT_HEADER_DCD_ENABLE=0
XIP_EXTERNAL_FLASH=1
XIP_BOOT_HEADER_ENABLE=1
- Can be programmed to
qspiflash
by IDE and can run after POR reset ifqspiflash
is the boot source.SDRAM will be initialized. | - Can be programmed to
qspiflash
by IDE, and can run after POR reset ifqspiflash
is the boot source.SDRAM will NOT be initialized. | |XIP_BOOT_HEADER_ENABLE=0| - CANNOT run after POR reset if it is programmed by IDE, even if
qspiflash
is the boot source. |—| |XIP_EXTERNAL_FLASH=0| - This image CANNOT complete XIP because when this macro is set to 1, it excludes the code, which changes the clock for FLEXSPI. |
Where to change the macros for each toolchain in MCUXpresso SDK?
Take hello_world
as an example:
IAR
MDK
ARMGCC
Change the configuration in CMakeLists.txt.
MCUX