MCUXpresso IDE New Project Wizard
MCUXpresso IDE features a new project wizard. The wizard provides functionality for the user to create new projects from the installed SDKs (and from pre-installed part support). It offers user the flexibility to select and change multiple builds. The wizard also includes a library and provides source code options. The source code is organized as software components, categorized as drivers, utilities, and middleware.
To use the wizard, start the MCUXpresso IDE. This is located in the QuickStart Panel at the bottom left of the MCUXpresso IDE window. Select New project, as shown in Figure 1.
For more details and usage of new project wizard, see the MCUXpresso_IDE_User_Guide.pdf in the MCUXpresso IDE installation folder.